| Commit message (Collapse) | Author | Age | Files | Lines |
|
|
|
|
|
|
|
|
| |
Still see issues with Bluetooth service.
So disabling for now.
This reverts commit 88c190b824fdf57ebcb4a76c1ddb9f1363927617.
Signed-off-by: Praneeth Bajjuri <praneeth@ti.com>
|
|
|
|
|
|
|
|
|
|
| |
The timestamp returned by AudioHAL's get_presentation_position()
must be from the MONOTONIC clock. An additional flag has to be
passed when opening the pcm ports in tinyalsa in order to get
timestamps from the monotonic clock.
Change-Id: Ib06c686985ae9229df59a2756c5da35e858e2d0e
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
| |
New servoice added in lollipop
Change-Id: If471b358bcfdf4ed109f9594ab26d30a226bb7ae
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
| |
GateMP is required for radio rendering on the ARM side.
Change-Id: Ib2d6e26f18dcb5ce3c69d6c172a912c659b4c843
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
The pcm input stream is said to be "steady" when the ALSA buffer
has available frames to read. However, the input stream could go
into the XRUN state when the voice thread takes too long between
explicitly starting the stream and querying the number of available
frames. For the purpose of determining whether the input stream
is ready, the XRUN state means that the ALSA buffer is full and
the audio frames can be read immediately.
The number of available frames was previously queried using the
pcm_get_htimestamp() function which returns an error when the stream
is in overrun state and doesn't update the number of available frames.
The pcm_update_avail() function does return the amount of available
frames regardless of the stream state.
Change-Id: I3afbb6f3d274b5f4fbd7133e48d2cbe51c223ccc
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
| |
Reduce the size of the ALSA buffers in order to reduce the
audio latency. The new buffer sizes allow using fast tracks.
Change-Id: I40f3af55cde72b1183d6fc8ffa8e01ecbef71a42
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
|
|
| |
Starting in kernel-3.14, Bluetooth SCO audio has a separate sound
card. Previously, BT SCO was a PCM device of the primary card.
The index of the BT SCO card is found dynamically when present in
the system.
Change-Id: I5c24e07df48b836473ce56170f9b12e5aac9f975
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
|
|
| |
Initialize to zeros the different structs used in the HAL.
The HAL uses non-NULL checks to free temporary audio buffers.
There were some aborts caused by freeing unallocated memory
because the audio buffer pointers were not zero-initialized.
Change-Id: I75ae704d5469e9e028bc7b67ef84b6a4047a7409
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
|
|
| |
WiLink 8 is now able to provide the PCM clocks until the
voice call is completely terminated, so there is no risk of
blocking read() and write() calls anymore. The workaround
is no longer needed, so it is removed.
Change-Id: Idb9c4d9dc9e2940c9ce6a9f49448a2fa9ad76ae2
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
|
|
|
| |
Replace deprecated macro audio_stream_frame_size() with the new
per-stream direction macro: audio_stream_*_frame_size().
The get_supported_devices() method is also dropped as it's not
required for API version 2.0.
Change-Id: Ia7c1b6b020832401a0a6a018f704444ad465f78f
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
|
| |
An incorrect channel mask macro was used to report the
input channel mask. The correct macro is:
audio_channel_in_mask_from_count().
Change-Id: I1b5c10980ddc7b034654d899d159df80ccc50b81
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
|
| |
Update bluedroid device configuration to enable car related
Bluetooth profiles.
Reference patch taken from device/lge/hammerhead.
Change-Id: Idc3a00c98ce5a0f89153ad248d45994ad414ef0d
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
| |
Update fastboot script to keep 7" panel as default for J6 EVM boards.
Change-Id: I26099079fa92b1b01b7da7d1e9d704ad263d08ab
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
| |
Re-enable OMAP_ENHANCEMENT flag.
Change-Id: I6d2253a96efcf5eedbc60ea5b443f4c702ca8f97
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
| |
Change-Id: I8aa3990cbb5f8aded7c5ebb7d5a32ef4b8a65b96
Signed-off-by: Sunita Nadampalli <sunitan@ti.com>
|
|\
| |
| |
| | |
sync
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
There is an audio driver for the DRA7 EVM that supports a
single PCM device (McASP3). The name of the card created
by this driver is "DRA7xxEVM", so this name has to be added
to the cards supported by this Audio HAL.
The IN_CALL mode is supported in the Audio HAL but won't
work with the "DRA7xxEVM" card because the PCM device used
for BT is not implemented by the driver.
Change-Id: Iacee36175cd4c90e74fce57f41cc6ca7c07291b9
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
| |
| |
| |
| |
| |
| |
| | |
Update external storage fstab path for kernel 3.14
Change-Id: I0f0ed41cb2faf2d27351c1deeda7c2422c15c02b
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
| |
| |
| |
| |
| |
| |
| | |
Update dtb file names for kernel 3.14
Change-Id: I83193b8eda5341d235efb7a9382916b6e82ca705
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
| |
| |
| |
| |
| |
| |
| | |
Add libdrm to list of PRODUCT_PACKAGES
Change-Id: I224079898518bc21c08c199c484216712208ef72
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
| |
| |
| |
| |
| |
| |
| |
| |
| | |
Bluetooth error is now resolved.
This reverts commit e53f56180daf92477fd6148a34a93073ef79b566.
Change-Id: Ifb7ac6dee214f87d3bc254ef5dff7dabd3c3d292
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
| |
| |
| |
| |
| |
| |
| | |
BT crashes at boot time, disable for time being
Change-Id: I1b2d67585db3c8bab3dd9628f62ea90b1e9a820e
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
| |
| |
| |
| |
| |
| |
| | |
Temporary for initial bring up.
Change-Id: I42f4363492d77258e449b8c45fef841c05204879
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|/
|
|
|
|
|
| |
Add new parameters needed in lollipop for open stream functions
Change-Id: I69073c1fa908ef37d9097ed50fedc72cdd409a6d
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
|
|
| |
The AudioHAL must leave the voice call only when it's no longer
in the IN_CALL state. Previously, the voice call leave sequence
was incorrectly executed when entering other modes (e.g. RINGTONE).
Change-Id: Id0134706fcf1f5999a765c5152ff77ba15d86015
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
| |
Commit 76b0af7cce79eed8bbe948546db1dab7e0681a14 broke the script for
GP devices. This change fixes it.
Change-Id: Icc786cb33a77519c50ec4d7d6fc37603518b65f1
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
| |
Use the correct file name for flashing QSPI on HS device EVM
Change-Id: Iaefa5cbc524d390b594ef8fffbd4ee6608e000bb
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
| |
add permission to support adding device admins
Change-Id: Id9a146418e58c2bb05326bb290fc90a03b02a2d1
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
|
| |
Add special argument --revg for flashing environemnt partition
with special dtb file if available.
Change-Id: I4f416c5292bc26f423307276383e3a9e61b521b3
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
|
|
|
| |
With this change we are able to boot with enforcing mode.
The rule added for healthd in this patch is taken from AOSP master.
When we switch to next Android version, this policy could be removed.
Change-Id: I8a87e1e4084c0186ae76b8b6f0cb87baf6e2ecf3
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
| |
Remove unused/legacy configurations from jacinto6evm device
Change-Id: I046e4d1925a92e50096d5a32bc20b605fcc69fe9
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
| |
Remove MTP host related defenitions from jacinto6evm
Change-Id: Ib58f46a505042626734039b238c986caca546360
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
|
|
|
| |
Update prebuilt kernel to more recent one
config/kernel:
commit d1683e8cecbf4132722a067d942af72c02fd7322 (origin/p-ti-android-3.8.y)
Change-Id: I4801b0ba4cff5754c63ba2d1c67703d64686f3f1
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
The Bluetooth SCO voice call has the following data flow:
Uplink:
+----------- SRC -----------+
| |
McASP7 McASP3
| |
Bluetooth Mic
Downlink:
+----------- SRC -----------+
| |
McASP7 McASP3
| |
Bluetooth Speaker
The voice call uses the ALSA PCM devices that are normally used
by the primary output and input. The primary output is switched
to a null/dummy sink when the voice call starts, and switched
back to the ALSA devices when the call ends.
The null/dummy sink consumes the data at the same rate than an
actual PCM device does, but does not render anything to an output
device (e.g. speaker).
Change-Id: I63a41de96c4ed34b60aab9240d10ad83c06c69ac
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
|
| |
Simplify the kcontrol settings through the audio_route
library. The control settings are now moved to a XML
audio paths file.
Change-Id: I72670523968a6646aea28e1625798b04f7a7799f
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
|
| |
If uninitialized, then a crash may result if they were not
successfully allocated during the constructor and then
the destructor runs.
Change-Id: Iad15e558fe6ba9b42aab482511cd30c1476f0f18
Signed-off-by: Angela Stegmaier <a0866189@ti.com>
|
|
|
|
|
|
|
| |
Increase system image size from 512M to 768M
Change-Id: If7c1f2919ebfb02e08b912a7e5974722c4947c98
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
|
|
| |
Radio now requires cmem module to run, cmem kernel module is not
present in the system by default. Adding the line for supporting
radio out of the box.
Change-Id: I9bd65cd9c78b60bb20ee4de770effe9e64f359e7
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
| |
Add system permissions for cmem and i2c-5 device accessed by radio app
Change-Id: I0372243649d368a0196eeb79f16dcbdc1472983b
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
| |
Add idc file for supporting new touch screen controller
Change-Id: Ibc6821495d00e49532f0253106b7e25f39397423
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
|
| |
Update correct sysfs path in fstab file based on latest kernel.
Also adding a missing service for sdcard storage.
Change-Id: I1b28389e7000fd2aa3db1b4c404b4d4531e676dd
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
| |
Add steps in fastboot.sh script to flash device tree file based on cpu
Change-Id: I7a3cb890035c258e46ae42bef248411c5fdcb3a1
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
|
|
| |
Since ITTIAM.WMA codecs are no longer are supported on
jacinto6, the corresponding entries have been removed from
the media codec list of supported codecs.
Change-Id: I24934fda247b8c7e0a7d33a11a0791a98c54afc0
Signed-off-by: Sunita Nadampalli <sunitan@ti.com>
|
|
|
|
|
|
|
|
| |
This patch copies the vpetest to the target folder
vpetest helps validate the vpe features on 6AJ releases
Change-Id: I05564629d2cda0eebee8a0af0d1032333cc9562f
Signed-off-by: Sundar Raman <sunds@ti.com>
|
|
|
|
|
|
|
| |
Enable the audio_hw module for the remote submix (WFD).
Change-Id: Ib7c615a919bb5de744f1857f68847989777224a0
Signed-off-by: Misael Lopez Cruz <misael.lopez@ti.com>
|
|
|
|
|
|
|
|
| |
Based on the change http://review.omapzoom.org/35065
com.ti.omap_enhancement property is no longer used
Change-Id: If6bce6ce83ad2a7543c43074666fd48e8000b9ec
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
| |
Update ueventd.jacinto6evmboard.rc file for GNSS permissions
Change-Id: If5aa0dcabc5d640388184e9677925b0b1bf01c76
Signed-off-by: Raghunandan Kamath <r-kamath@ti.com>
|
|
|
|
|
|
|
|
|
| |
- Define GNSS related services
- Create folder structures needed for GNSS
- Add step to load GNSS kernel module
Change-Id: Iff5e9bf9d680e3a276c786e94b8ba7159de82dc2
Signed-off-by: Raghunandan Kamath <r-kamath@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Remove wifi_p2p network.
--
Similar to patch:
commit a2e79fae23c5d5178ec7c534bd488eacc5d098ec on device/asus/tilapia
Author: Robert Greenwalt <rgreenwalt@google.com>
--
Change-Id: I1967b014c65a0a53fc81f570f4ec8d566b67344b
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
|
| |
WLAN/BT were disabled initially during KitKat bringup.
Enable them back.
Change-Id: I6e9ccd3235fef64f6c8b669e3caf9ee87e889b15
Signed-off-by: Eyal Reizer <eyalr@ti.com>
|