diff options
Diffstat (limited to 'omap5/sgx_src/eurasia_km/eurasiacon/build/linux2/this_makefile.mk')
-rw-r--r-- | omap5/sgx_src/eurasia_km/eurasiacon/build/linux2/this_makefile.mk | 68 |
1 files changed, 0 insertions, 68 deletions
diff --git a/omap5/sgx_src/eurasia_km/eurasiacon/build/linux2/this_makefile.mk b/omap5/sgx_src/eurasia_km/eurasiacon/build/linux2/this_makefile.mk deleted file mode 100644 index c312001..0000000 --- a/omap5/sgx_src/eurasia_km/eurasiacon/build/linux2/this_makefile.mk +++ /dev/null | |||
@@ -1,68 +0,0 @@ | |||
1 | ########################################################################### ### | ||
2 | #@Copyright Copyright (c) Imagination Technologies Ltd. All Rights Reserved | ||
3 | #@License Dual MIT/GPLv2 | ||
4 | # | ||
5 | # The contents of this file are subject to the MIT license as set out below. | ||
6 | # | ||
7 | # Permission is hereby granted, free of charge, to any person obtaining a copy | ||
8 | # of this software and associated documentation files (the "Software"), to deal | ||
9 | # in the Software without restriction, including without limitation the rights | ||
10 | # to use, copy, modify, merge, publish, distribute, sublicense, and/or sell | ||
11 | # copies of the Software, and to permit persons to whom the Software is | ||
12 | # furnished to do so, subject to the following conditions: | ||
13 | # | ||
14 | # The above copyright notice and this permission notice shall be included in | ||
15 | # all copies or substantial portions of the Software. | ||
16 | # | ||
17 | # Alternatively, the contents of this file may be used under the terms of | ||
18 | # the GNU General Public License Version 2 ("GPL") in which case the provisions | ||
19 | # of GPL are applicable instead of those above. | ||
20 | # | ||
21 | # If you wish to allow use of your version of this file only under the terms of | ||
22 | # GPL, and not to allow others to use your version of this file under the terms | ||
23 | # of the MIT license, indicate your decision by deleting the provisions above | ||
24 | # and replace them with the notice and other provisions required by GPL as set | ||
25 | # out in the file called "GPL-COPYING" included in this distribution. If you do | ||
26 | # not delete the provisions above, a recipient may use your version of this file | ||
27 | # under the terms of either the MIT license or GPL. | ||
28 | # | ||
29 | # This License is also included in this distribution in the file called | ||
30 | # "MIT-COPYING". | ||
31 | # | ||
32 | # EXCEPT AS OTHERWISE STATED IN A NEGOTIATED AGREEMENT: (A) THE SOFTWARE IS | ||
33 | # PROVIDED "AS IS", WITHOUT WARRANTY OF ANY KIND, EXPRESS OR IMPLIED, INCLUDING | ||
34 | # BUT NOT LIMITED TO THE WARRANTIES OF MERCHANTABILITY, FITNESS FOR A PARTICULAR | ||
35 | # PURPOSE AND NONINFRINGEMENT; AND (B) IN NO EVENT SHALL THE AUTHORS OR | ||
36 | # COPYRIGHT HOLDERS BE LIABLE FOR ANY CLAIM, DAMAGES OR OTHER LIABILITY, WHETHER | ||
37 | # IN AN ACTION OF CONTRACT, TORT OR OTHERWISE, ARISING FROM, OUT OF OR IN | ||
38 | # CONNECTION WITH THE SOFTWARE OR THE USE OR OTHER DEALINGS IN THE SOFTWARE. | ||
39 | ### ########################################################################### | ||
40 | |||
41 | # Find out the path of the Linux.mk makefile currently being processed, and | ||
42 | # set paths used by the build rules | ||
43 | |||
44 | # This magic is used so we can use this_makefile.mk twice: first when reading | ||
45 | # in each Linux.mk, and then again when generating rules. There we set | ||
46 | # $(THIS_MAKEFILE), and $(REMAINING_MAKEFILES) should be empty | ||
47 | ifneq ($(strip $(REMAINING_MAKEFILES)),) | ||
48 | |||
49 | # Absolute path to the Linux.mk being processed | ||
50 | THIS_MAKEFILE := $(firstword $(REMAINING_MAKEFILES)) | ||
51 | |||
52 | # The list of makefiles left to process | ||
53 | REMAINING_MAKEFILES := $(wordlist 2,$(words $(REMAINING_MAKEFILES)),$(REMAINING_MAKEFILES)) | ||
54 | |||
55 | else | ||
56 | |||
57 | # When generating rules, we should have read in every Linux.mk | ||
58 | $(if $(INTERNAL_INCLUDED_ALL_MAKEFILES),,$(error No makefiles left in $$(REMAINING_MAKEFILES), but $$(INTERNAL_INCLUDED_ALL_MAKEFILES) is not set)) | ||
59 | |||
60 | endif | ||
61 | |||
62 | # Path to the directory containing Linux.mk | ||
63 | THIS_DIR := $(patsubst %/,%,$(dir $(THIS_MAKEFILE))) | ||
64 | ifeq ($(strip $(THIS_DIR)),) | ||
65 | $(error Empty $$(THIS_DIR) for makefile "$(THIS_MAKEFILE)") | ||
66 | endif | ||
67 | |||
68 | modules := | ||