| Commit message (Collapse) | Author | Age | Files | Lines |
|
|
|
|
|
|
|
|
|
|
|
| |
sysbios-rpmsg tag: 1.20.09.23
This commit adds a sample dsp firmware image
built from the sysbios-rpmsg tree with tag
specified above.
Signed-off-by: Dilip Gopalakrishna <dilip.g@ti.com>
Change-Id: I24ba8df63d9608bcd5fb92a725115a71d8585835
Signed-off-by: Dilip Gopalakrishna <dilip.g@ti.com>
|
|
|
|
|
|
|
|
|
|
| |
Upgrade wl18xx firmware file for r8.a4.02.
wl18xx-fw.bin file is replaced by wl18xx-fw-mc.bin file
wl18xx-fw-mc.bin - FRev 8.4.0.0.8
Change-Id: I83c4fe28fa5b737c1540744ea1d187d40ee46718
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|\ |
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
Use this rule to install all wpan related firmware files.
The wpan archive needs to maintain the folder structure of
wl12xx/wpan/<technology>/.bts
Patch modified from original - Mark Lifshits <lifshitsm@ti.com>
Signed-off-by: Pavan Savoy <pavan_savoy@ti.com>
Modified to install only in the intermediates directory, and not to
remove artifacts from the intermediates directory.
Change-Id: I26a0669eea1a7b7b26ad6a2a780ad0d098f477d0
Signed-off-by: James W. Mills <jameswmills@ti.com>
|
|/
|
|
|
|
|
|
| |
wl18xx firmware files were removed due to licensing restrictions.
Now the licenses are approved, so placing them back.
Change-Id: I03195e1e7d88b11da2e3263156da9929a938af6a
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
|
| |
This will untar SGX prebuilt binaries to an intermediate directory and
install them in the Android filesystem without polluting the git tree
with untracked files.
Change-Id: I806a9aa4a939b6109399df999603706e3c34f17e
|
|
|
|
|
|
|
|
| |
Move WLAN firmware from indvidual files to tar ball approach.
Based on the way ducati binaries are handled.
Change-Id: I66bfec1b0fb01f36a4508922d0e4919d6bb1eeb0
Signed-off-by: Vishal Mahaveer <vishalm@ti.com>
|
|
|
|
|
|
|
|
|
|
| |
Having the Android.mk inclusion at the bottom of the Android.mk is
causing it to be ignored, which meand SGX/wlan/etc are no longer
installed. Moving it to the top makes it work, and the subsequent
ducati definition works as well.
Change-Id: Idcbce941b9e3b60906421b0cf944160d41ac027b
Signed-off-by: James W. Mills <jameswmills@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
This patch moves the ducati installation logic into the top-level
Android.mk for proprietary-open, and generalizes the procedure so that
new devices can be added easily. Benefis include:
* Unpacking into an intermediate location
* Only unpacked if enabled for a specific device
* All devices can use the same PRODUCT_PACKAGE definition
* User-defined ducati TGZ location
Change-Id: I48314920b138230e73b3a56e1ff899ad82289b59
Signed-off-by: James W. Mills <jameswmills@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
Add the wpan.tgz firmware tarball which constitutes of the firmware and the
right LICENSE for them.
Also add in the line in Android.mk to untar them to the relevant folder from
where they will be picked up to be installed into the relevant folder on
/system/etc/firmware/.
Change-Id: Ie2a7af0febb072862bbeb45039625ba810923766
Signed-off-by: Pavan Savoy <pavan_savoy@ti.com>
Conflicts:
Android.mk
Signed-off-by: Pavan Savoy <pavan_savoy@ti.com>
|
|
|
|
|
|
|
|
|
|
|
|
| |
This patch includes the files needed to install Ducati fw and DCC
files for the Blaze Tablet.
Versions of Ducati can be dropped in with an accompanying mk file, and
each device capable of using that version of ducati can include the
makefile at the device level
Change-Id: I1df3fb99eac48106032a404184f09668d0148cda
Signed-off-by: James W. Mills <jameswmills@ti.com>
|
|
|
|
|
|
|
|
| |
Release a binary version of Ducati, complete with DCC files, all under
license.
Change-Id: I62f1784dfb1b815e8f58b69716b19bb53ca32b2e
Signed-off-by: James W. Mills <jameswmills@ti.com>
|
|
|
|
|
|
|
|
|
| |
This change allows all licensed material to be license-bound, and
prevents any single component from being downloaded without the proper
license agreement.
Change-Id: I353122644b1696438a7c7a33a26d43087e19440a
Signed-off-by: James W. Mills <jameswmills@ti.com>
|
|
IMG DDK 1.8@550175 binaries
Change-Id: I215a17b72d2b3a2e57e06546403a9f643cebee04
Signed-off-by: Hemant Hariyani <hemanthariyani@ti.com>
|