summaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorNishanth Menon2014-11-11 17:28:38 -0600
committerNishanth Menon2014-11-11 17:28:38 -0600
commit88fc70c0850794fb0bce52f63dfcc0d8f3d5062e (patch)
treebd2acd9a43827c481dfcca8049f0206c2f7979ef /overlay
downloaddevice-ti-x15-88fc70c0850794fb0bce52f63dfcc0d8f3d5062e.tar.gz
device-ti-x15-88fc70c0850794fb0bce52f63dfcc0d8f3d5062e.tar.xz
device-ti-x15-88fc70c0850794fb0bce52f63dfcc0d8f3d5062e.zip
initial baseline from TI's code
Signed-off-by: Nishanth Menon <nm@ti.com>
Diffstat (limited to 'overlay')
-rw-r--r--overlay/frameworks/base/core/res/res/values/config.xml104
-rw-r--r--overlay/frameworks/base/core/res/res/xml/storage_list.xml56
-rw-r--r--overlay/frameworks/base/packages/SettingsProvider/res/values/config.xml24
-rw-r--r--overlay/packages/apps/Launcher2/res/xml/default_workspace.xml91
-rw-r--r--overlay/packages/apps/SoundRecorder/res/values/styles.xml23
5 files changed, 298 insertions, 0 deletions
diff --git a/overlay/frameworks/base/core/res/res/values/config.xml b/overlay/frameworks/base/core/res/res/values/config.xml
new file mode 100644
index 0000000..009fd1f
--- /dev/null
+++ b/overlay/frameworks/base/core/res/res/values/config.xml
@@ -0,0 +1,104 @@
1<?xml version="1.0" encoding="utf-8"?>
2<!--
3/*
4** Copyright 2011, The Android Open Source Project
5**
6** Licensed under the Apache License, Version 2.0 (the "License");
7** you may not use this file except in compliance with the License.
8** You may obtain a copy of the License at
9**
10** http://www.apache.org/licenses/LICENSE-2.0
11**
12** Unless required by applicable law or agreed to in writing, software
13** distributed under the License is distributed on an "AS IS" BASIS,
14** WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
15** See the License for the specific language governing permissions and
16** limitations under the License.
17*/
18-->
19
20<!-- These resources are around just to allow their values to be customized
21 for different hardware and product builds. -->
22<resources>
23
24 <!-- This device is not "voice capable"; it's data-only. -->
25 <bool name="config_voice_capable">false</bool>
26
27 <!-- This device does not allow sms service. -->
28 <bool name="config_sms_capable">false</bool>
29
30 <!-- List of regexpressions describing the interface (if any) that represent tetherable
31 Wifi interfaces. If the device doesn't want to support tethering over Wifi this
32 should be empty. An example would be "softap.*" -->
33 <string-array translatable="false" name="config_tether_wifi_regexs">
34 <item>"wlan\\d"</item>
35 </string-array>
36
37 <!-- Array of ConnectivityManager.TYPE_xxxx values allowable for tethering -->
38 <!-- [1,7,9] for TYPE_WIFI, TYPE_BLUETOOTH and TYPE_ETHERNET-->
39 <integer-array translatable="false" name="config_tether_upstream_types">
40 <item>1</item>
41 <item>7</item>
42 <item>9</item>
43 </integer-array>
44
45 <!-- This string array should be overridden by the device to present a list of network
46 attributes. This is used by the connectivity manager to decide which networks can coexist
47 based on the hardware -->
48 <!-- An Array of "[Connection name],[ConnectivityManager connection type],
49 [associated radio-type],[priority],[restoral-timer(ms)],[dependencyMet] -->
50 <!-- the 5th element "resore-time" indicates the number of milliseconds to delay
51 before automatically restore the default connection. Set -1 if the connection
52 does not require auto-restore. -->
53 <!-- the 6th element indicates boot-time dependency-met value. -->
54 <string-array translatable="false" name="networkAttributes">
55 <item>"wifi,1,1,1,-1,true"</item>
56 <item>"bluetooth,7,7,1,-1,true"</item>
57 <item>"ethernet,9,9,0,-1,true"</item>
58 </string-array>
59
60 <!-- This string array should be overridden by the device to present a list of radio
61 attributes. This is used by the connectivity manager to decide which networks can coexist
62 based on the hardware -->
63 <!-- An Array of "[ConnectivityManager connectionType],
64 [# simultaneous connection types]" -->
65 <string-array translatable="false" name="radioAttributes">
66 <item>"1,1"</item>
67 <item>"7,1"</item>
68 <item>"9,1"</item>
69 </string-array>
70
71 <!-- Integer indicating the framework scan interval in milliseconds. This is used in the scenario
72 where the chipset does not support background scanning (config_wifi_background_scan_suport
73 is false) to set up a periodic wake up scan so that the device can connect to a new access
74 point on the move. A value of 0 means no periodic scans will be used in the framework. -->
75 <integer translatable="false" name="config_wifi_framework_scan_interval">0</integer>
76
77 <!-- Boolean indicating whether the wifi chipset has dual frequency band support -->
78 <bool translatable="false" name="config_wifi_dual_band_support">true</bool>
79
80 <!-- List of regexpressions describing the interface (if any) that represent tetherable
81 bluetooth interfaces. If the device doesn't want to support tethering over bluetooth this
82 should be empty. -->
83 <string-array translatable="false" name="config_tether_bluetooth_regexs">
84 <item>"bt-pan"</item>
85 </string-array>
86
87 <!-- Separate software navigation bar required on this device. -->
88 <bool name="config_showNavigationBar">true</bool>
89
90 <!-- Whether WiFi display is supported by this device.
91 There are many prerequisites for this feature to work correctly.
92 Here are a few of them:
93 * The WiFi radio must support WiFi P2P.
94 * The WiFi radio must support concurrent connections to the WiFi display and
95 to an access point.
96 * The Audio Flinger audio_policy.conf file must specify a rule for the "r_submix"
97 remote submix module. This module is used to record and stream system
98 audio output to the WiFi display encoder in the media server.
99 * The remote submix module "audio.r_submix.default" must be installed on the device.
100 * The device must be provisioned with HDCP keys (for protected content).
101 -->
102 <bool name="config_enableWifiDisplay">true</bool>
103
104</resources>
diff --git a/overlay/frameworks/base/core/res/res/xml/storage_list.xml b/overlay/frameworks/base/core/res/res/xml/storage_list.xml
new file mode 100644
index 0000000..4d73c29
--- /dev/null
+++ b/overlay/frameworks/base/core/res/res/xml/storage_list.xml
@@ -0,0 +1,56 @@
1<?xml version="1.0" encoding="utf-8"?>
2<!--
3**
4** Copyright 2011, The Android Open Source Project
5**
6** Licensed under the Apache License, Version 2.0 (the "License")
7** you may not use this file except in compliance with the License.
8** You may obtain a copy of the License at
9**
10** http://www.apache.org/licenses/LICENSE-2.0
11**
12** Unless required by applicable law or agreed to in writing, software
13** distributed under the License is distributed on an "AS IS" BASIS,
14** WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
15** See the License for the specific language governing permissions and
16** limitations under the License.
17*/
18-->
19
20<!-- The <device> element should contain one or more <storage> elements.
21 Exactly one of these should have the attribute primary="true".
22 This storage will be the primary external storage and should have path="/storage/sdcard0".
23 Each storage should have both a path and description attribute set.
24 The following boolean attributes are optional:
25
26 primary: this storage is the primary external storage
27 removable: this is removable storage (for example, a real SD card)
28 emulated: the storage is emulated via the FUSE sdcard daemon
29 mtp-reserve: number of megabytes of storage MTP should reserve for free storage
30 (used for emulated storage that is shared with system's data partition)
31
32 A storage should not have both emulated and removable set to true
33-->
34
35<StorageList xmlns:android="http://schemas.android.com/apk/res/android">
36 <!-- internal emulated storage -->
37 <storage
38 android:storageDescription="@string/storage_internal"
39 android:primary="true"
40 android:emulated="true"
41 android:mtpReserve="100" />
42 <!-- external SD card -->
43 <storage android:mountPoint="/storage/sdcard1"
44 android:storageDescription="@string/storage_sd_card"
45 android:removable="true" />
46 <!-- external USB slots -->
47 <storage android:mountPoint="/storage/usb0"
48 android:storageDescription="@string/storage_usb"
49 android:allowMassStorage="true"
50 android:removable="true" />
51 <!-- external USB slots -->
52 <storage android:mountPoint="/storage/usb1"
53 android:storageDescription="@string/storage_usb"
54 android:allowMassStorage="true"
55 android:removable="true" />
56</StorageList>
diff --git a/overlay/frameworks/base/packages/SettingsProvider/res/values/config.xml b/overlay/frameworks/base/packages/SettingsProvider/res/values/config.xml
new file mode 100644
index 0000000..5b8c48b
--- /dev/null
+++ b/overlay/frameworks/base/packages/SettingsProvider/res/values/config.xml
@@ -0,0 +1,24 @@
1<?xml version="1.0" encoding="utf-8"?>
2<!-- Copyright (C) 2007 The Android Open Source Project
3
4 Licensed under the Apache License, Version 2.0 (the "License");
5 you may not use this file except in compliance with the License.
6 You may obtain a copy of the License at
7
8 http://www.apache.org/licenses/LICENSE-2.0
9
10 Unless required by applicable law or agreed to in writing, software
11 distributed under the License is distributed on an "AS IS" BASIS,
12 WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 See the License for the specific language governing permissions and
14 limitations under the License.
15-->
16
17<resources>
18 <!-- Turn off GPS as a default. -->
19 <string name="def_location_providers_allowed" translatable="false"></string>
20 <!-- DIsable lock screen -->
21 <bool name="def_lockscreen_disabled">true</bool>
22 <!-- Keep screen on allways -->
23 <bool name="def_stay_on_while_plugged_in">true</bool>
24</resources>
diff --git a/overlay/packages/apps/Launcher2/res/xml/default_workspace.xml b/overlay/packages/apps/Launcher2/res/xml/default_workspace.xml
new file mode 100644
index 0000000..284b752
--- /dev/null
+++ b/overlay/packages/apps/Launcher2/res/xml/default_workspace.xml
@@ -0,0 +1,91 @@
1<?xml version="1.0" encoding="utf-8"?>
2<!-- Copyright (C) 2009 The Android Open Source Project
3
4 Licensed under the Apache License, Version 2.0 (the "License");
5 you may not use this file except in compliance with the License.
6 You may obtain a copy of the License at
7
8 http://www.apache.org/licenses/LICENSE-2.0
9
10 Unless required by applicable law or agreed to in writing, software
11 distributed under the License is distributed on an "AS IS" BASIS,
12 WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 See the License for the specific language governing permissions and
14 limitations under the License.
15-->
16
17<favorites xmlns:launcher="http://schemas.android.com/apk/res/com.android.launcher">
18 <!-- Far-left screen [0] -->
19
20 <!-- Left screen [1] -->
21 <appwidget
22 launcher:packageName="com.android.settings"
23 launcher:className="com.android.settings.widget.SettingsAppWidgetProvider"
24 launcher:screen="1"
25 launcher:x="0"
26 launcher:y="3"
27 launcher:spanX="4"
28 launcher:spanY="1" />
29
30 <!-- Middle screen [2] -->
31 <appwidget
32 launcher:packageName="com.android.deskclock"
33 launcher:className="com.android.alarmclock.DigitalAppWidgetProvider"
34 launcher:screen="2"
35 launcher:x="0"
36 launcher:y="0"
37 launcher:spanX="4"
38 launcher:spanY="2" />
39 <favorite
40 launcher:packageName="com.android.music"
41 launcher:className="com.android.music.MusicBrowserActivity"
42 launcher:screen="2"
43 launcher:x="0"
44 launcher:y="3" />
45
46 <!-- Right screen [3] -->
47 <favorite
48 launcher:packageName="com.android.gallery3d"
49 launcher:className="com.android.gallery3d.app.Gallery"
50 launcher:screen="3"
51 launcher:x="1"
52 launcher:y="3" />
53 <favorite
54 launcher:packageName="com.android.settings"
55 launcher:className="com.android.settings.Settings"
56 launcher:screen="3"
57 launcher:x="2"
58 launcher:y="3" />
59
60 <!-- Far-right screen [4] -->
61
62 <!-- Hotseat (We use the screen as the position of the item in the hotseat) -->
63 <favorite
64 launcher:packageName="com.android.dialer"
65 launcher:className="com.android.dialer.DialtactsActivity"
66 launcher:container="-101"
67 launcher:screen="0"
68 launcher:x="0"
69 launcher:y="0" />
70 <favorite
71 launcher:packageName="com.android.contacts"
72 launcher:className="com.android.contacts.activities.PeopleActivity"
73 launcher:container="-101"
74 launcher:screen="1"
75 launcher:x="1"
76 launcher:y="0" />
77 <favorite
78 launcher:packageName="com.android.mms"
79 launcher:className="com.android.mms.ui.ConversationList"
80 launcher:container="-101"
81 launcher:screen="3"
82 launcher:x="3"
83 launcher:y="0" />
84 <favorite
85 launcher:packageName="com.android.browser"
86 launcher:className="com.android.browser.BrowserActivity"
87 launcher:container="-101"
88 launcher:screen="4"
89 launcher:x="4"
90 launcher:y="0" />
91</favorites>
diff --git a/overlay/packages/apps/SoundRecorder/res/values/styles.xml b/overlay/packages/apps/SoundRecorder/res/values/styles.xml
new file mode 100644
index 0000000..9dc0515
--- /dev/null
+++ b/overlay/packages/apps/SoundRecorder/res/values/styles.xml
@@ -0,0 +1,23 @@
1<?xml version="1.0" encoding="utf-8"?>
2<!-- Copyright (C) 2011 The Android Open Source Project
3
4 Licensed under the Apache License, Version 2.0 (the "License");
5 you may not use this file except in compliance with the License.
6 You may obtain a copy of the License at
7
8 http://www.apache.org/licenses/LICENSE-2.0
9
10 Unless required by applicable law or agreed to in writing, software
11 distributed under the License is distributed on an "AS IS" BASIS,
12 WITHOUT WARRANTIES OR CONDITIONS OF ANY KIND, either express or implied.
13 See the License for the specific language governing permissions and
14 limitations under the License.
15-->
16<resources>
17 <style name="Theme.SoundRecorder" parent="@android:style/Theme.Holo">
18 <item name="android:windowCloseOnTouchOutside">true</item>
19 </style>
20 <style name="MediaButton" parent="@android:style/MediaButton">
21 <item name="android:background">@android:drawable/btn_default</item>
22 </style>
23</resources>