aboutsummaryrefslogblamecommitdiffstats
blob: 9eb7fed0bbaa9895973a14e551c76de31fffe533 (plain) (tree)
1
2
3
4
5
6
7
8
9
10
11


                                                       
                                                                    






                                                                     
                         

                         
                         
                        

                          
                         
                               
 


                                            


                          
                                                            

                                    
                 
 
                                                                   

                                   
 
                              

  
                

                            
                   
                                 
                                 

  






                               

                                                               
 


                                                        
                                                                      


                                                                      
                              
 
                                                                          


                                   
   















                                                                          
























                                                                             











                                                                    

                                                  
                                         



                                                                       
                                                 









                                                   

                                 
                                                
                                                     



                                                       
 
                       
                         
                                      
                                      
                                           
 
                                                                  
                                                  
                                 
                                

                   
                     
 



                                                          

                                                                    

 









                                                                                
                                                              
 

                


                                               

                                                                               
                      
                                              

                                        

 
   
                                             

                                                                
                             



                                                                      
                               
  

                                                                     
                                                                
                                                                      
                                                                  





                                                                    
                                                                       
                                                                

                                                                

                                          


                                   
                           
                                      


                                                          

                                          
                                       

                                          
                                     
                                                                                
                             
 



                                                                           




                                                                                
                                                                  
         

                             
                                      
 
                                                                               
 




                                                                           




                                                     
   









                                                                      
                                                     



                            







































                                                                             















                                                                            











                                                                   

                                             


































                                                                         



                                                                  





                                                                       



                                                                    

                                       
                                                           

                
                                    

                                                              
                                             



                                                      
 
                           

                                          

                   
                            
 
                          
 
                                          
 
                                                                
                                       
                            
                                                
                                                
 
                                      
























                                                                              
 










                                                             







































                                                                               
                                    




                                                  







                                      







                                                              
                              



                                              
















                                                                      
                                                                      






                                                     











                                                                    







                                                                    










                                                                     
 




                                               
 





                                                                                 
 
                                       
 

                                                 


                                      

















                                                                     
/* Kernel thread helper functions.
 *   Copyright (C) 2004 IBM Corporation, Rusty Russell.
 *
 * Creation is done via kthreadd, so that we get a clean environment
 * even if we're invoked from userspace (think modprobe, hotplug cpu,
 * etc.).
 */
#include <linux/sched.h>
#include <linux/kthread.h>
#include <linux/completion.h>
#include <linux/err.h>
#include <linux/cpuset.h>
#include <linux/unistd.h>
#include <linux/file.h>
#include <linux/export.h>
#include <linux/mutex.h>
#include <linux/slab.h>
#include <linux/freezer.h>
#include <linux/ptrace.h>
#include <trace/events/sched.h>

static DEFINE_SPINLOCK(kthread_create_lock);
static LIST_HEAD(kthread_create_list);
struct task_struct *kthreadd_task;

struct kthread_create_info
{
	/* Information passed to kthread() from kthreadd. */
	int (*threadfn)(void *data);
	void *data;
	int node;

	/* Result passed back to kthread_create() from kthreadd. */
	struct task_struct *result;
	struct completion done;

	struct list_head list;
};

struct kthread {
	unsigned long flags;
	unsigned int cpu;
	void *data;
	struct completion parked;
	struct completion exited;
};

enum KTHREAD_BITS {
	KTHREAD_IS_PER_CPU = 0,
	KTHREAD_SHOULD_STOP,
	KTHREAD_SHOULD_PARK,
	KTHREAD_IS_PARKED,
};

#define to_kthread(tsk)	\
	container_of((tsk)->vfork_done, struct kthread, exited)

/**
 * kthread_should_stop - should this kthread return now?
 *
 * When someone calls kthread_stop() on your kthread, it will be woken
 * and this will return true.  You should then return, and your return
 * value will be passed through to kthread_stop().
 */
bool kthread_should_stop(void)
{
	return test_bit(KTHREAD_SHOULD_STOP, &to_kthread(current)->flags);
}
EXPORT_SYMBOL(kthread_should_stop);

/**
 * kthread_should_park - should this kthread park now?
 *
 * When someone calls kthread_park() on your kthread, it will be woken
 * and this will return true.  You should then do the necessary
 * cleanup and call kthread_parkme()
 *
 * Similar to kthread_should_stop(), but this keeps the thread alive
 * and in a park position. kthread_unpark() "restarts" the thread and
 * calls the thread function again.
 */
bool kthread_should_park(void)
{
	return test_bit(KTHREAD_SHOULD_PARK, &to_kthread(current)->flags);
}

/**
 * kthread_freezable_should_stop - should this freezable kthread return now?
 * @was_frozen: optional out parameter, indicates whether %current was frozen
 *
 * kthread_should_stop() for freezable kthreads, which will enter
 * refrigerator if necessary.  This function is safe from kthread_stop() /
 * freezer deadlock and freezable kthreads should use this function instead
 * of calling try_to_freeze() directly.
 */
bool kthread_freezable_should_stop(bool *was_frozen)
{
	bool frozen = false;

	might_sleep();

	if (unlikely(freezing(current)))
		frozen = __refrigerator(true);

	if (was_frozen)
		*was_frozen = frozen;

	return kthread_should_stop();
}
EXPORT_SYMBOL_GPL(kthread_freezable_should_stop);

/**
 * kthread_data - return data value specified on kthread creation
 * @task: kthread task in question
 *
 * Return the data value specified when kthread @task was created.
 * The caller is responsible for ensuring the validity of @task when
 * calling this function.
 */
void *kthread_data(struct task_struct *task)
{
	return to_kthread(task)->data;
}

static void __kthread_parkme(struct kthread *self)
{
	__set_current_state(TASK_PARKED);
	while (test_bit(KTHREAD_SHOULD_PARK, &self->flags)) {
		if (!test_and_set_bit(KTHREAD_IS_PARKED, &self->flags))
			complete(&self->parked);
		schedule();
		__set_current_state(TASK_PARKED);
	}
	clear_bit(KTHREAD_IS_PARKED, &self->flags);
	__set_current_state(TASK_RUNNING);
}

void kthread_parkme(void)
{
	__kthread_parkme(to_kthread(current));
}

static int kthread(void *_create)
{
	/* Copy data: it's on kthread's stack */
	struct kthread_create_info *create = _create;
	int (*threadfn)(void *data) = create->threadfn;
	void *data = create->data;
	struct kthread self;
	int ret;

	self.flags = 0;
	self.data = data;
	init_completion(&self.exited);
	init_completion(&self.parked);
	current->vfork_done = &self.exited;

	/* OK, tell user we're spawned, wait for stop or wakeup */
	__set_current_state(TASK_UNINTERRUPTIBLE);
	create->result = current;
	complete(&create->done);
	schedule();

	ret = -EINTR;

	if (!test_bit(KTHREAD_SHOULD_STOP, &self.flags)) {
		__kthread_parkme(&self);
		ret = threadfn(data);
	}
	/* we can't just return, we must preserve "self" on stack */
	do_exit(ret);
}

/* called from do_fork() to get node information for about to be created task */
int tsk_fork_get_node(struct task_struct *tsk)
{
#ifdef CONFIG_NUMA
	if (tsk == kthreadd_task)
		return tsk->pref_node_fork;
#endif
	return numa_node_id();
}

static void create_kthread(struct kthread_create_info *create)
{
	int pid;

#ifdef CONFIG_NUMA
	current->pref_node_fork = create->node;
#endif
	/* We want our own signal handler (we take no signals by default). */
	pid = kernel_thread(kthread, create, CLONE_FS | CLONE_FILES | SIGCHLD);
	if (pid < 0) {
		create->result = ERR_PTR(pid);
		complete(&create->done);
	}
}

/**
 * kthread_create_on_node - create a kthread.
 * @threadfn: the function to run until signal_pending(current).
 * @data: data ptr for @threadfn.
 * @node: memory node number.
 * @namefmt: printf-style name for the thread.
 *
 * Description: This helper function creates and names a kernel
 * thread.  The thread will be stopped: use wake_up_process() to start
 * it.  See also kthread_run().
 *
 * If thread is going to be bound on a particular cpu, give its node
 * in @node, to get NUMA affinity for kthread stack, or else give -1.
 * When woken, the thread will run @threadfn() with @data as its
 * argument. @threadfn() can either call do_exit() directly if it is a
 * standalone thread for which no one will call kthread_stop(), or
 * return when 'kthread_should_stop()' is true (which means
 * kthread_stop() has been called).  The return value should be zero
 * or a negative error number; it will be passed to kthread_stop().
 *
 * Returns a task_struct or ERR_PTR(-ENOMEM).
 */
struct task_struct *kthread_create_on_node(int (*threadfn)(void *data),
					   void *data, int node,
					   const char namefmt[],
					   ...)
{
	struct kthread_create_info create;

	create.threadfn = threadfn;
	create.data = data;
	create.node = node;
	init_completion(&create.done);

	spin_lock(&kthread_create_lock);
	list_add_tail(&create.list, &kthread_create_list);
	spin_unlock(&kthread_create_lock);

	wake_up_process(kthreadd_task);
	wait_for_completion(&create.done);

	if (!IS_ERR(create.result)) {
		static const struct sched_param param = { .sched_priority = 0 };
		va_list args;

		va_start(args, namefmt);
		vsnprintf(create.result->comm, sizeof(create.result->comm),
			  namefmt, args);
		va_end(args);
		/*
		 * root may have changed our (kthreadd's) priority or CPU mask.
		 * The kernel thread should not inherit these properties.
		 */
		sched_setscheduler_nocheck(create.result, SCHED_NORMAL, &param);
		set_cpus_allowed_ptr(create.result, cpu_all_mask);
	}
	return create.result;
}
EXPORT_SYMBOL(kthread_create_on_node);

static void __kthread_bind(struct task_struct *p, unsigned int cpu, long state)
{
	/* Must have done schedule() in kthread() before we set_task_cpu */
	if (!wait_task_inactive(p, state)) {
		WARN_ON(1);
		return;
	}
	/* It's safe because the task is inactive. */
	do_set_cpus_allowed(p, cpumask_of(cpu));
	p->flags |= PF_THREAD_BOUND;
}

/**
 * kthread_bind - bind a just-created kthread to a cpu.
 * @p: thread created by kthread_create().
 * @cpu: cpu (might not be online, must be possible) for @k to run on.
 *
 * Description: This function is equivalent to set_cpus_allowed(),
 * except that @cpu doesn't need to be online, and the thread must be
 * stopped (i.e., just returned from kthread_create()).
 */
void kthread_bind(struct task_struct *p, unsigned int cpu)
{
	__kthread_bind(p, cpu, TASK_UNINTERRUPTIBLE);
}
EXPORT_SYMBOL(kthread_bind);

/**
 * kthread_create_on_cpu - Create a cpu bound kthread
 * @threadfn: the function to run until signal_pending(current).
 * @data: data ptr for @threadfn.
 * @cpu: The cpu on which the thread should be bound,
 * @namefmt: printf-style name for the thread. Format is restricted
 *	     to "name.*%u". Code fills in cpu number.
 *
 * Description: This helper function creates and names a kernel thread
 * The thread will be woken and put into park mode.
 */
struct task_struct *kthread_create_on_cpu(int (*threadfn)(void *data),
					  void *data, unsigned int cpu,
					  const char *namefmt)
{
	struct task_struct *p;

	p = kthread_create_on_node(threadfn, data, cpu_to_node(cpu), namefmt,
				   cpu);
	if (IS_ERR(p))
		return p;
	set_bit(KTHREAD_IS_PER_CPU, &to_kthread(p)->flags);
	to_kthread(p)->cpu = cpu;
	/* Park the thread to get it out of TASK_UNINTERRUPTIBLE state */
	kthread_park(p);
	return p;
}

static struct kthread *task_get_live_kthread(struct task_struct *k)
{
	struct kthread *kthread;

	get_task_struct(k);
	kthread = to_kthread(k);
	/* It might have exited */
	barrier();
	if (k->vfork_done != NULL)
		return kthread;
	return NULL;
}

static void __kthread_unpark(struct task_struct *k, struct kthread *kthread)
{
	clear_bit(KTHREAD_SHOULD_PARK, &kthread->flags);
	/*
	 * We clear the IS_PARKED bit here as we don't wait
	 * until the task has left the park code. So if we'd
	 * park before that happens we'd see the IS_PARKED bit
	 * which might be about to be cleared.
	 */
	if (test_and_clear_bit(KTHREAD_IS_PARKED, &kthread->flags)) {
		if (test_bit(KTHREAD_IS_PER_CPU, &kthread->flags))
			__kthread_bind(k, kthread->cpu, TASK_PARKED);
		wake_up_state(k, TASK_PARKED);
	}
}

/**
 * kthread_unpark - unpark a thread created by kthread_create().
 * @k:		thread created by kthread_create().
 *
 * Sets kthread_should_park() for @k to return false, wakes it, and
 * waits for it to return. If the thread is marked percpu then its
 * bound to the cpu again.
 */
void kthread_unpark(struct task_struct *k)
{
	struct kthread *kthread = task_get_live_kthread(k);

	if (kthread)
		__kthread_unpark(k, kthread);
	put_task_struct(k);
}

/**
 * kthread_park - park a thread created by kthread_create().
 * @k: thread created by kthread_create().
 *
 * Sets kthread_should_park() for @k to return true, wakes it, and
 * waits for it to return. This can also be called after kthread_create()
 * instead of calling wake_up_process(): the thread will park without
 * calling threadfn().
 *
 * Returns 0 if the thread is parked, -ENOSYS if the thread exited.
 * If called by the kthread itself just the park bit is set.
 */
int kthread_park(struct task_struct *k)
{
	struct kthread *kthread = task_get_live_kthread(k);
	int ret = -ENOSYS;

	if (kthread) {
		if (!test_bit(KTHREAD_IS_PARKED, &kthread->flags)) {
			set_bit(KTHREAD_SHOULD_PARK, &kthread->flags);
			if (k != current) {
				wake_up_process(k);
				wait_for_completion(&kthread->parked);
			}
		}
		ret = 0;
	}
	put_task_struct(k);
	return ret;
}

/**
 * kthread_stop - stop a thread created by kthread_create().
 * @k: thread created by kthread_create().
 *
 * Sets kthread_should_stop() for @k to return true, wakes it, and
 * waits for it to exit. This can also be called after kthread_create()
 * instead of calling wake_up_process(): the thread will exit without
 * calling threadfn().
 *
 * If threadfn() may call do_exit() itself, the caller must ensure
 * task_struct can't go away.
 *
 * Returns the result of threadfn(), or %-EINTR if wake_up_process()
 * was never called.
 */
int kthread_stop(struct task_struct *k)
{
	struct kthread *kthread = task_get_live_kthread(k);
	int ret;

	trace_sched_kthread_stop(k);
	if (kthread) {
		set_bit(KTHREAD_SHOULD_STOP, &kthread->flags);
		__kthread_unpark(k, kthread);
		wake_up_process(k);
		wait_for_completion(&kthread->exited);
	}
	ret = k->exit_code;

	put_task_struct(k);
	trace_sched_kthread_stop_ret(ret);

	return ret;
}
EXPORT_SYMBOL(kthread_stop);

int kthreadd(void *unused)
{
	struct task_struct *tsk = current;

	/* Setup a clean context for our children to inherit. */
	set_task_comm(tsk, "kthreadd");
	ignore_signals(tsk);
	set_cpus_allowed_ptr(tsk, cpu_all_mask);
	set_mems_allowed(node_states[N_MEMORY]);

	current->flags |= PF_NOFREEZE;

	for (;;) {
		set_current_state(TASK_INTERRUPTIBLE);
		if (list_empty(&kthread_create_list))
			schedule();
		__set_current_state(TASK_RUNNING);

		spin_lock(&kthread_create_lock);
		while (!list_empty(&kthread_create_list)) {
			struct kthread_create_info *create;

			create = list_entry(kthread_create_list.next,
					    struct kthread_create_info, list);
			list_del_init(&create->list);
			spin_unlock(&kthread_create_lock);

			create_kthread(create);

			spin_lock(&kthread_create_lock);
		}
		spin_unlock(&kthread_create_lock);
	}

	return 0;
}

void __init_kthread_worker(struct kthread_worker *worker,
				const char *name,
				struct lock_class_key *key)
{
	spin_lock_init(&worker->lock);
	lockdep_set_class_and_name(&worker->lock, key, name);
	INIT_LIST_HEAD(&worker->work_list);
	worker->task = NULL;
}
EXPORT_SYMBOL_GPL(__init_kthread_worker);

/**
 * kthread_worker_fn - kthread function to process kthread_worker
 * @worker_ptr: pointer to initialized kthread_worker
 *
 * This function can be used as @threadfn to kthread_create() or
 * kthread_run() with @worker_ptr argument pointing to an initialized
 * kthread_worker.  The started kthread will process work_list until
 * the it is stopped with kthread_stop().  A kthread can also call
 * this function directly after extra initialization.
 *
 * Different kthreads can be used for the same kthread_worker as long
 * as there's only one kthread attached to it at any given time.  A
 * kthread_worker without an attached kthread simply collects queued
 * kthread_works.
 */
int kthread_worker_fn(void *worker_ptr)
{
	struct kthread_worker *worker = worker_ptr;
	struct kthread_work *work;

	WARN_ON(worker->task);
	worker->task = current;
repeat:
	set_current_state(TASK_INTERRUPTIBLE);	/* mb paired w/ kthread_stop */

	if (kthread_should_stop()) {
		__set_current_state(TASK_RUNNING);
		spin_lock_irq(&worker->lock);
		worker->task = NULL;
		spin_unlock_irq(&worker->lock);
		return 0;
	}

	work = NULL;
	spin_lock_irq(&worker->lock);
	if (!list_empty(&worker->work_list)) {
		work = list_first_entry(&worker->work_list,
					struct kthread_work, node);
		list_del_init(&work->node);
	}
	worker->current_work = work;
	spin_unlock_irq(&worker->lock);

	if (work) {
		__set_current_state(TASK_RUNNING);
		work->func(work);
	} else if (!freezing(current))
		schedule();

	try_to_freeze();
	goto repeat;
}
EXPORT_SYMBOL_GPL(kthread_worker_fn);

/* insert @work before @pos in @worker */
static void insert_kthread_work(struct kthread_worker *worker,
			       struct kthread_work *work,
			       struct list_head *pos)
{
	lockdep_assert_held(&worker->lock);

	list_add_tail(&work->node, pos);
	work->worker = worker;
	if (likely(worker->task))
		wake_up_process(worker->task);
}

/**
 * queue_kthread_work - queue a kthread_work
 * @worker: target kthread_worker
 * @work: kthread_work to queue
 *
 * Queue @work to work processor @task for async execution.  @task
 * must have been created with kthread_worker_create().  Returns %true
 * if @work was successfully queued, %false if it was already pending.
 */
bool queue_kthread_work(struct kthread_worker *worker,
			struct kthread_work *work)
{
	bool ret = false;
	unsigned long flags;

	spin_lock_irqsave(&worker->lock, flags);
	if (list_empty(&work->node)) {
		insert_kthread_work(worker, work, &worker->work_list);
		ret = true;
	}
	spin_unlock_irqrestore(&worker->lock, flags);
	return ret;
}
EXPORT_SYMBOL_GPL(queue_kthread_work);

struct kthread_flush_work {
	struct kthread_work	work;
	struct completion	done;
};

static void kthread_flush_work_fn(struct kthread_work *work)
{
	struct kthread_flush_work *fwork =
		container_of(work, struct kthread_flush_work, work);
	complete(&fwork->done);
}

/**
 * flush_kthread_work - flush a kthread_work
 * @work: work to flush
 *
 * If @work is queued or executing, wait for it to finish execution.
 */
void flush_kthread_work(struct kthread_work *work)
{
	struct kthread_flush_work fwork = {
		KTHREAD_WORK_INIT(fwork.work, kthread_flush_work_fn),
		COMPLETION_INITIALIZER_ONSTACK(fwork.done),
	};
	struct kthread_worker *worker;
	bool noop = false;

retry:
	worker = work->worker;
	if (!worker)
		return;

	spin_lock_irq(&worker->lock);
	if (work->worker != worker) {
		spin_unlock_irq(&worker->lock);
		goto retry;
	}

	if (!list_empty(&work->node))
		insert_kthread_work(worker, &fwork.work, work->node.next);
	else if (worker->current_work == work)
		insert_kthread_work(worker, &fwork.work, worker->work_list.next);
	else
		noop = true;

	spin_unlock_irq(&worker->lock);

	if (!noop)
		wait_for_completion(&fwork.done);
}
EXPORT_SYMBOL_GPL(flush_kthread_work);

/**
 * flush_kthread_worker - flush all current works on a kthread_worker
 * @worker: worker to flush
 *
 * Wait until all currently executing or pending works on @worker are
 * finished.
 */
void flush_kthread_worker(struct kthread_worker *worker)
{
	struct kthread_flush_work fwork = {
		KTHREAD_WORK_INIT(fwork.work, kthread_flush_work_fn),
		COMPLETION_INITIALIZER_ONSTACK(fwork.done),
	};

	queue_kthread_work(worker, &fwork.work);
	wait_for_completion(&fwork.done);
}
EXPORT_SYMBOL_GPL(flush_kthread_worker);