diff options
author | George Cherian | 2013-07-31 03:59:19 -0500 |
---|---|---|
committer | Somnath Mukherjee | 2013-08-09 00:26:09 -0500 |
commit | fca727e66070b18b2fce6922efdf48cb61e01720 (patch) | |
tree | 7d5d48cc4c27583b63f483a02186dc2b20c3922e | |
parent | 5f00ae3ddba3ad66200c8e1eaf78399018bf7618 (diff) | |
download | kernel-audio-fca727e66070b18b2fce6922efdf48cb61e01720.tar.gz kernel-audio-fca727e66070b18b2fce6922efdf48cb61e01720.tar.xz kernel-audio-fca727e66070b18b2fce6922efdf48cb61e01720.zip |
usb: host: xhci: Enable XHCI_SPURIOUS_SUCCESS for all controllers with xhci 1.0
Xhci controllers with hci_version > 0.96 gives spurious success events on short packet completion.
During webcam capture the "ERROR Transfer event TRB DMA ptr not part of current TD" was observed.
The same application works fine with synopsis controllers hci_version 0.96.
The same Issue is seen with Intel Pantherpoint xhci controller. So enabling this quirk in xhci_gen_setup if
controller verion is greater than 0.96.
For xhci-pci move the quirk to much generic place xhci_gen_setup.
Note from Sarah:
The xHCI 1.0 spec changed how hardware handles short packets. The HW
will notify SW of the TRB where the short packet occurred, and it will
also give a successful status for the last TRB in a TD (the one with the
IOC flag set). On the second successful status, that warning will be
triggered in the driver.
Software is now supposed to not assume the TD is not completed until it
gets that last successful status. That means we have a slight race
condition, although it should have little practical impact. This patch
papers over that issue.
It's on my long-term to-do list to fix this race condition, but it is a
much more involved patch that will probably be too big for stable. This
patch is needed for stable to avoid serious log spam.
This patch should be backported to kernels as old as 3.0, that
contain the commit ad808333d8201d53075a11bc8dd83b81f3d68f0b "Intel xhci:
Ignore spurious successful event."
The patch will have to be modified for kernels older than 3.2, since
that kernel added the xhci_gen_setup function for xhci platform devices.
The correct conflict resolution for kernels older than 3.2 is to set
XHCI_SPURIOUS_SUCCESS in xhci_pci_quirks for all xHCI 1.0 hosts.
upstream-status: http://marc.info/?l=linux-usb&m=137265657724242&w=2
Change-Id: I4f5b93a6031118facd971985e40c77280e53ffe3
Signed-off-by: George Cherian <george.cherian@ti.com>
Signed-off-by: Sarah Sharp <sarah.a.sharp@linux.intel.com>
[backported to 3.8]
Signed-off-by: Ravi Babu <ravibabu@ti.com>
-rw-r--r-- | drivers/usb/host/xhci-pci.c | 1 | ||||
-rw-r--r-- | drivers/usb/host/xhci.c | 7 |
2 files changed, 7 insertions, 1 deletions
diff --git a/drivers/usb/host/xhci-pci.c b/drivers/usb/host/xhci-pci.c index af259e0ec172..b66037811aa5 100644 --- a/drivers/usb/host/xhci-pci.c +++ b/drivers/usb/host/xhci-pci.c | |||
@@ -93,7 +93,6 @@ static void xhci_pci_quirks(struct device *dev, struct xhci_hcd *xhci) | |||
93 | } | 93 | } |
94 | if (pdev->vendor == PCI_VENDOR_ID_INTEL && | 94 | if (pdev->vendor == PCI_VENDOR_ID_INTEL && |
95 | pdev->device == PCI_DEVICE_ID_INTEL_PANTHERPOINT_XHCI) { | 95 | pdev->device == PCI_DEVICE_ID_INTEL_PANTHERPOINT_XHCI) { |
96 | xhci->quirks |= XHCI_SPURIOUS_SUCCESS; | ||
97 | xhci->quirks |= XHCI_EP_LIMIT_QUIRK; | 96 | xhci->quirks |= XHCI_EP_LIMIT_QUIRK; |
98 | xhci->limit_active_eps = 64; | 97 | xhci->limit_active_eps = 64; |
99 | xhci->quirks |= XHCI_SW_BW_CHECKING; | 98 | xhci->quirks |= XHCI_SW_BW_CHECKING; |
diff --git a/drivers/usb/host/xhci.c b/drivers/usb/host/xhci.c index 849470b18831..603bcca19a0a 100644 --- a/drivers/usb/host/xhci.c +++ b/drivers/usb/host/xhci.c | |||
@@ -4661,6 +4661,13 @@ int xhci_gen_setup(struct usb_hcd *hcd, xhci_get_quirks_t get_quirks) | |||
4661 | 4661 | ||
4662 | get_quirks(dev, xhci); | 4662 | get_quirks(dev, xhci); |
4663 | 4663 | ||
4664 | /* In xhci controllers which follow xhci 1.0 spec gives a spurious | ||
4665 | * success event after a short transfer. This quirk will ignore such | ||
4666 | * spurious event. | ||
4667 | */ | ||
4668 | if (xhci->hci_version > 0x96) | ||
4669 | xhci->quirks |= XHCI_SPURIOUS_SUCCESS; | ||
4670 | |||
4664 | /* Make sure the HC is halted. */ | 4671 | /* Make sure the HC is halted. */ |
4665 | retval = xhci_halt(xhci); | 4672 | retval = xhci_halt(xhci); |
4666 | if (retval) | 4673 | if (retval) |