diff options
author | Haavard Skinnemoen | 2007-05-01 16:26:34 -0500 |
---|---|---|
committer | Jean Delvare | 2007-05-01 16:26:34 -0500 |
commit | 1c23af90dc44d05bbb6a3b5246ab664b1f943943 (patch) | |
tree | 184dc150ca69a9dfbc00996e35659ef41beb202c /MAINTAINERS | |
parent | 16538e6b32600f76ad212d42fc2b1f801e32ab4b (diff) | |
download | kernel-audio-1c23af90dc44d05bbb6a3b5246ab664b1f943943.tar.gz kernel-audio-1c23af90dc44d05bbb6a3b5246ab664b1f943943.tar.xz kernel-audio-1c23af90dc44d05bbb6a3b5246ab664b1f943943.zip |
i2c: Bitbanging I2C bus driver using the GPIO API
This is a very simple bitbanging I2C bus driver utilizing the new
arch-neutral GPIO API. Useful for chips that don't have a built-in
I2C controller, additional I2C busses, or testing purposes.
To use, include something similar to the following in the
board-specific setup code:
#include <linux/i2c-gpio.h>
static struct i2c_gpio_platform_data i2c_gpio_data = {
.sda_pin = GPIO_PIN_FOO,
.scl_pin = GPIO_PIN_BAR,
};
static struct platform_device i2c_gpio_device = {
.name = "i2c-gpio",
.id = 0,
.dev = {
.platform_data = &i2c_gpio_data,
},
};
Register this platform_device, set up the I2C pins as GPIO if
required and you're ready to go. This will use default values for
udelay and timeout, and will work with GPIO hardware that does not
support open drain mode, but allows sensing of the SDA and SCL lines
even when they are being driven.
Signed-off-by: Haavard Skinnemoen <hskinnemoen@atmel.com>
Signed-off-by: Jean Delvare <khali@linux-fr.org>
Diffstat (limited to 'MAINTAINERS')
-rw-r--r-- | MAINTAINERS | 5 |
1 files changed, 5 insertions, 0 deletions
diff --git a/MAINTAINERS b/MAINTAINERS index 2b378ab99fc3..4da678505788 100644 --- a/MAINTAINERS +++ b/MAINTAINERS | |||
@@ -1466,6 +1466,11 @@ L: linux-scsi@vger.kernel.org | |||
1466 | W: http://www.icp-vortex.com/ | 1466 | W: http://www.icp-vortex.com/ |
1467 | S: Supported | 1467 | S: Supported |
1468 | 1468 | ||
1469 | GENERIC GPIO I2C DRIVER | ||
1470 | P: Haavard Skinnemoen | ||
1471 | M: hskinnemoen@atmel.com | ||
1472 | S: Supported | ||
1473 | |||
1469 | GENERIC HDLC DRIVER, N2, C101, PCI200SYN and WANXL DRIVERS | 1474 | GENERIC HDLC DRIVER, N2, C101, PCI200SYN and WANXL DRIVERS |
1470 | P: Krzysztof Halasa | 1475 | P: Krzysztof Halasa |
1471 | M: khc@pm.waw.pl | 1476 | M: khc@pm.waw.pl |