diff options
author | Michael Witten | 2012-04-01 19:33:02 -0500 |
---|---|---|
committer | Jiri Kosina | 2012-04-17 03:23:32 -0500 |
commit | 6d12760c9f3d961a8bfc23ba9702d12f7eea35dd (patch) | |
tree | 79f8100f2b5df8061c646e03a9a1aa7afd38055c /README | |
parent | a6144bb9e7b4c82f7366bd74f8beac826f5f6b7f (diff) | |
download | kernel-audio-6d12760c9f3d961a8bfc23ba9702d12f7eea35dd.tar.gz kernel-audio-6d12760c9f3d961a8bfc23ba9702d12f7eea35dd.tar.xz kernel-audio-6d12760c9f3d961a8bfc23ba9702d12f7eea35dd.zip |
README: `Alternately' -> `Alternatively'
Also, one `Alternate' was changed to `Alternative' for the
sake of consistency.
Signed-off-by: Michael Witten <mfwitten@gmail.com>
Acked-by: Randy Dunlap <rdunlap@xenotime.net>
Signed-off-by: Jiri Kosina <jkosina@suse.cz>
Diffstat (limited to 'README')
-rw-r--r-- | README | 6 |
1 files changed, 3 insertions, 3 deletions
@@ -163,7 +163,7 @@ CONFIGURING the kernel: | |||
163 | new version with minimal work, use "make oldconfig", which will | 163 | new version with minimal work, use "make oldconfig", which will |
164 | only ask you for the answers to new questions. | 164 | only ask you for the answers to new questions. |
165 | 165 | ||
166 | - Alternate configuration commands are: | 166 | - Alternative configuration commands are: |
167 | "make config" Plain text interface. | 167 | "make config" Plain text interface. |
168 | "make menuconfig" Text based color menus, radiolists & dialogs. | 168 | "make menuconfig" Text based color menus, radiolists & dialogs. |
169 | "make nconfig" Enhanced text based color menus. | 169 | "make nconfig" Enhanced text based color menus. |
@@ -328,7 +328,7 @@ IF SOMETHING GOES WRONG: | |||
328 | sense of the dump (but compiling with CONFIG_KALLSYMS is usually preferred). | 328 | sense of the dump (but compiling with CONFIG_KALLSYMS is usually preferred). |
329 | This utility can be downloaded from | 329 | This utility can be downloaded from |
330 | ftp://ftp.<country>.kernel.org/pub/linux/utils/kernel/ksymoops/ . | 330 | ftp://ftp.<country>.kernel.org/pub/linux/utils/kernel/ksymoops/ . |
331 | Alternately, you can do the dump lookup by hand: | 331 | Alternatively, you can do the dump lookup by hand: |
332 | 332 | ||
333 | - In debugging dumps like the above, it helps enormously if you can | 333 | - In debugging dumps like the above, it helps enormously if you can |
334 | look up what the EIP value means. The hex value as such doesn't help | 334 | look up what the EIP value means. The hex value as such doesn't help |
@@ -361,7 +361,7 @@ IF SOMETHING GOES WRONG: | |||
361 | kernel image or similar), telling me as much about your setup as | 361 | kernel image or similar), telling me as much about your setup as |
362 | possible will help. Please read the REPORTING-BUGS document for details. | 362 | possible will help. Please read the REPORTING-BUGS document for details. |
363 | 363 | ||
364 | - Alternately, you can use gdb on a running kernel. (read-only; i.e. you | 364 | - Alternatively, you can use gdb on a running kernel. (read-only; i.e. you |
365 | cannot change values or set break points.) To do this, first compile the | 365 | cannot change values or set break points.) To do this, first compile the |
366 | kernel with -g; edit arch/i386/Makefile appropriately, then do a "make | 366 | kernel with -g; edit arch/i386/Makefile appropriately, then do a "make |
367 | clean". You'll also need to enable CONFIG_PROC_FS (via "make config"). | 367 | clean". You'll also need to enable CONFIG_PROC_FS (via "make config"). |