diff options
author | Linus Torvalds | 2012-12-12 10:18:24 -0600 |
---|---|---|
committer | Linus Torvalds | 2012-12-12 10:18:24 -0600 |
commit | d206e09036d6201f90b2719484c8a59526c46125 (patch) | |
tree | 84b9057919bcb8cfd1cff47baa5fc74457e77d6d /block | |
parent | fef3ff2eb777e76cfa5ae67591982d902c17139c (diff) | |
parent | 15ef4ffaa797034d5ff82844daf8f595d7c6d53c (diff) | |
download | kernel-audio-d206e09036d6201f90b2719484c8a59526c46125.tar.gz kernel-audio-d206e09036d6201f90b2719484c8a59526c46125.tar.xz kernel-audio-d206e09036d6201f90b2719484c8a59526c46125.zip |
Merge branch 'for-3.8' of git://git.kernel.org/pub/scm/linux/kernel/git/tj/cgroup
Pull cgroup changes from Tejun Heo:
"A lot of activities on cgroup side. The big changes are focused on
making cgroup hierarchy handling saner.
- cgroup_rmdir() had peculiar semantics - it allowed cgroup
destruction to be vetoed by individual controllers and tried to
drain refcnt synchronously. The vetoing never worked properly and
caused good deal of contortions in cgroup. memcg was the last
reamining user. Michal Hocko removed the usage and cgroup_rmdir()
path has been simplified significantly. This was done in a
separate branch so that the memcg people can base further memcg
changes on top.
- The above allowed cleaning up cgroup lifecycle management and
implementation of generic cgroup iterators which are used to
improve hierarchy support.
- cgroup_freezer updated to allow migration in and out of a frozen
cgroup and handle hierarchy. If a cgroup is frozen, all descendant
cgroups are frozen.
- netcls_cgroup and netprio_cgroup updated to handle hierarchy
properly.
- Various fixes and cleanups.
- Two merge commits. One to pull in memcg and rmdir cleanups (needed
to build iterators). The other pulled in cgroup/for-3.7-fixes for
device_cgroup fixes so that further device_cgroup patches can be
stacked on top."
Fixed up a trivial conflict in mm/memcontrol.c as per Tejun (due to
commit bea8c150a7 ("memcg: fix hotplugged memory zone oops") in master
touching code close to commit 2ef37d3fe4 ("memcg: Simplify
mem_cgroup_force_empty_list error handling") in for-3.8)
* 'for-3.8' of git://git.kernel.org/pub/scm/linux/kernel/git/tj/cgroup: (65 commits)
cgroup: update Documentation/cgroups/00-INDEX
cgroup_rm_file: don't delete the uncreated files
cgroup: remove subsystem files when remounting cgroup
cgroup: use cgroup_addrm_files() in cgroup_clear_directory()
cgroup: warn about broken hierarchies only after css_online
cgroup: list_del_init() on removed events
cgroup: fix lockdep warning for event_control
cgroup: move list add after list head initilization
netprio_cgroup: allow nesting and inherit config on cgroup creation
netprio_cgroup: implement netprio[_set]_prio() helpers
netprio_cgroup: use cgroup->id instead of cgroup_netprio_state->prioidx
netprio_cgroup: reimplement priomap expansion
netprio_cgroup: shorten variable names in extend_netdev_table()
netprio_cgroup: simplify write_priomap()
netcls_cgroup: move config inheritance to ->css_online() and remove .broken_hierarchy marking
cgroup: remove obsolete guarantee from cgroup_task_migrate.
cgroup: add cgroup->id
cgroup, cpuset: remove cgroup_subsys->post_clone()
cgroup: s/CGRP_CLONE_CHILDREN/CGRP_CPUSET_CLONE_CHILDREN/
cgroup: rename ->create/post_create/pre_destroy/destroy() to ->css_alloc/online/offline/free()
...
Diffstat (limited to 'block')
-rw-r--r-- | block/blk-cgroup.c | 15 |
1 files changed, 7 insertions, 8 deletions
diff --git a/block/blk-cgroup.c b/block/blk-cgroup.c index d0b770391ad4..3f6d39d23bb6 100644 --- a/block/blk-cgroup.c +++ b/block/blk-cgroup.c | |||
@@ -600,7 +600,7 @@ struct cftype blkcg_files[] = { | |||
600 | }; | 600 | }; |
601 | 601 | ||
602 | /** | 602 | /** |
603 | * blkcg_pre_destroy - cgroup pre_destroy callback | 603 | * blkcg_css_offline - cgroup css_offline callback |
604 | * @cgroup: cgroup of interest | 604 | * @cgroup: cgroup of interest |
605 | * | 605 | * |
606 | * This function is called when @cgroup is about to go away and responsible | 606 | * This function is called when @cgroup is about to go away and responsible |
@@ -610,7 +610,7 @@ struct cftype blkcg_files[] = { | |||
610 | * | 610 | * |
611 | * This is the blkcg counterpart of ioc_release_fn(). | 611 | * This is the blkcg counterpart of ioc_release_fn(). |
612 | */ | 612 | */ |
613 | static int blkcg_pre_destroy(struct cgroup *cgroup) | 613 | static void blkcg_css_offline(struct cgroup *cgroup) |
614 | { | 614 | { |
615 | struct blkcg *blkcg = cgroup_to_blkcg(cgroup); | 615 | struct blkcg *blkcg = cgroup_to_blkcg(cgroup); |
616 | 616 | ||
@@ -632,10 +632,9 @@ static int blkcg_pre_destroy(struct cgroup *cgroup) | |||
632 | } | 632 | } |
633 | 633 | ||
634 | spin_unlock_irq(&blkcg->lock); | 634 | spin_unlock_irq(&blkcg->lock); |
635 | return 0; | ||
636 | } | 635 | } |
637 | 636 | ||
638 | static void blkcg_destroy(struct cgroup *cgroup) | 637 | static void blkcg_css_free(struct cgroup *cgroup) |
639 | { | 638 | { |
640 | struct blkcg *blkcg = cgroup_to_blkcg(cgroup); | 639 | struct blkcg *blkcg = cgroup_to_blkcg(cgroup); |
641 | 640 | ||
@@ -643,7 +642,7 @@ static void blkcg_destroy(struct cgroup *cgroup) | |||
643 | kfree(blkcg); | 642 | kfree(blkcg); |
644 | } | 643 | } |
645 | 644 | ||
646 | static struct cgroup_subsys_state *blkcg_create(struct cgroup *cgroup) | 645 | static struct cgroup_subsys_state *blkcg_css_alloc(struct cgroup *cgroup) |
647 | { | 646 | { |
648 | static atomic64_t id_seq = ATOMIC64_INIT(0); | 647 | static atomic64_t id_seq = ATOMIC64_INIT(0); |
649 | struct blkcg *blkcg; | 648 | struct blkcg *blkcg; |
@@ -740,10 +739,10 @@ static int blkcg_can_attach(struct cgroup *cgrp, struct cgroup_taskset *tset) | |||
740 | 739 | ||
741 | struct cgroup_subsys blkio_subsys = { | 740 | struct cgroup_subsys blkio_subsys = { |
742 | .name = "blkio", | 741 | .name = "blkio", |
743 | .create = blkcg_create, | 742 | .css_alloc = blkcg_css_alloc, |
743 | .css_offline = blkcg_css_offline, | ||
744 | .css_free = blkcg_css_free, | ||
744 | .can_attach = blkcg_can_attach, | 745 | .can_attach = blkcg_can_attach, |
745 | .pre_destroy = blkcg_pre_destroy, | ||
746 | .destroy = blkcg_destroy, | ||
747 | .subsys_id = blkio_subsys_id, | 746 | .subsys_id = blkio_subsys_id, |
748 | .base_cftypes = blkcg_files, | 747 | .base_cftypes = blkcg_files, |
749 | .module = THIS_MODULE, | 748 | .module = THIS_MODULE, |