aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorOhad Ben-Cohen2011-10-20 14:41:24 -0500
committerOhad Ben-Cohen2012-02-08 14:54:05 -0600
commit779b96d20ca97cfa19162b340bff0c27b405b4b2 (patch)
tree4f371baad4fcde0c4ae2050535174ab632b411f5 /samples/rpmsg
parentbcabbccabffe7326f046f25737ba1084f463c65c (diff)
downloadkernel-audio-779b96d20ca97cfa19162b340bff0c27b405b4b2.tar.gz
kernel-audio-779b96d20ca97cfa19162b340bff0c27b405b4b2.tar.xz
kernel-audio-779b96d20ca97cfa19162b340bff0c27b405b4b2.zip
samples/rpmsg: add an rpmsg driver sample
Add an rpmsg driver sample, which demonstrates how to communicate with an AMP-configured remote processor over the rpmsg bus. Note how once probed, the driver can immediately start sending messages using the rpmsg_send() API, without having to worry about creating endpoints or allocating rpmsg addresses: all that work is done by the rpmsg bus, and the required information is already embedded in the rpmsg channel that the driver is probed with. In this sample, the driver simply sends a "Hello World!" message to the remote processor repeatedly. Designed with Brian Swetland <swetland@google.com>. Signed-off-by: Ohad Ben-Cohen <ohad@wizery.com> Cc: Brian Swetland <swetland@google.com> Cc: Arnd Bergmann <arnd@arndb.de> Cc: Grant Likely <grant.likely@secretlab.ca> Cc: Tony Lindgren <tony@atomide.com> Cc: Russell King <linux@arm.linux.org.uk> Cc: Rusty Russell <rusty@rustcorp.com.au> Cc: Andrew Morton <akpm@linux-foundation.org> Cc: Greg KH <greg@kroah.com> Cc: Stephen Boyd <sboyd@codeaurora.org>
Diffstat (limited to 'samples/rpmsg')
-rw-r--r--samples/rpmsg/Makefile1
-rw-r--r--samples/rpmsg/rpmsg_client_sample.c100
2 files changed, 101 insertions, 0 deletions
diff --git a/samples/rpmsg/Makefile b/samples/rpmsg/Makefile
new file mode 100644
index 000000000000..2d4973c69663
--- /dev/null
+++ b/samples/rpmsg/Makefile
@@ -0,0 +1 @@
obj-$(CONFIG_SAMPLE_RPMSG_CLIENT) += rpmsg_client_sample.o
diff --git a/samples/rpmsg/rpmsg_client_sample.c b/samples/rpmsg/rpmsg_client_sample.c
new file mode 100644
index 000000000000..23ea9f2ae11d
--- /dev/null
+++ b/samples/rpmsg/rpmsg_client_sample.c
@@ -0,0 +1,100 @@
1/*
2 * Remote processor messaging - sample client driver
3 *
4 * Copyright (C) 2011 Texas Instruments, Inc.
5 * Copyright (C) 2011 Google, Inc.
6 *
7 * Ohad Ben-Cohen <ohad@wizery.com>
8 * Brian Swetland <swetland@google.com>
9 *
10 * This software is licensed under the terms of the GNU General Public
11 * License version 2, as published by the Free Software Foundation, and
12 * may be copied, distributed, and modified under those terms.
13 *
14 * This program is distributed in the hope that it will be useful,
15 * but WITHOUT ANY WARRANTY; without even the implied warranty of
16 * MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE. See the
17 * GNU General Public License for more details.
18 */
19
20#include <linux/kernel.h>
21#include <linux/module.h>
22#include <linux/rpmsg.h>
23
24#define MSG "hello world!"
25#define MSG_LIMIT 100
26
27static void rpmsg_sample_cb(struct rpmsg_channel *rpdev, void *data, int len,
28 void *priv, u32 src)
29{
30 int ret;
31 static int rx_count;
32
33 dev_info(&rpdev->dev, "incoming msg %d (src: 0x%x)\n", ++rx_count, src);
34
35 print_hex_dump(KERN_DEBUG, __func__, DUMP_PREFIX_NONE, 16, 1,
36 data, len, true);
37
38 /* samples should not live forever */
39 if (rx_count >= MSG_LIMIT) {
40 dev_info(&rpdev->dev, "goodbye!\n");
41 return;
42 }
43
44 /* send a new message now */
45 ret = rpmsg_send(rpdev, MSG, strlen(MSG));
46 if (ret)
47 dev_err(&rpdev->dev, "rpmsg_send failed: %d\n", ret);
48}
49
50static int rpmsg_sample_probe(struct rpmsg_channel *rpdev)
51{
52 int ret;
53
54 dev_info(&rpdev->dev, "new channel: 0x%x -> 0x%x!\n",
55 rpdev->src, rpdev->dst);
56
57 /* send a message to our remote processor */
58 ret = rpmsg_send(rpdev, MSG, strlen(MSG));
59 if (ret) {
60 dev_err(&rpdev->dev, "rpmsg_send failed: %d\n", ret);
61 return ret;
62 }
63
64 return 0;
65}
66
67static void __devexit rpmsg_sample_remove(struct rpmsg_channel *rpdev)
68{
69 dev_info(&rpdev->dev, "rpmsg sample client driver is removed\n");
70}
71
72static struct rpmsg_device_id rpmsg_driver_sample_id_table[] = {
73 { .name = "rpmsg-client-sample" },
74 { },
75};
76MODULE_DEVICE_TABLE(rpmsg, rpmsg_driver_sample_id_table);
77
78static struct rpmsg_driver rpmsg_sample_client = {
79 .drv.name = KBUILD_MODNAME,
80 .drv.owner = THIS_MODULE,
81 .id_table = rpmsg_driver_sample_id_table,
82 .probe = rpmsg_sample_probe,
83 .callback = rpmsg_sample_cb,
84 .remove = __devexit_p(rpmsg_sample_remove),
85};
86
87static int __init rpmsg_client_sample_init(void)
88{
89 return register_rpmsg_driver(&rpmsg_sample_client);
90}
91module_init(rpmsg_client_sample_init);
92
93static void __exit rpmsg_client_sample_fini(void)
94{
95 unregister_rpmsg_driver(&rpmsg_sample_client);
96}
97module_exit(rpmsg_client_sample_fini);
98
99MODULE_DESCRIPTION("Remote processor messaging sample client driver");
100MODULE_LICENSE("GPL v2");