diff options
author | Alain Knaff | 2009-01-07 02:10:27 -0600 |
---|---|---|
committer | H. Peter Anvin | 2009-01-07 02:10:27 -0600 |
commit | a26ee60f90daffe1de6be0d093af86e7279b3dfd (patch) | |
tree | 01239fb6b173ff46711480b9601c69b92e1715a5 /usr | |
parent | fb9a4ca9820fd4d7c4906bd393004662451e273e (diff) | |
download | kernel-audio-a26ee60f90daffe1de6be0d093af86e7279b3dfd.tar.gz kernel-audio-a26ee60f90daffe1de6be0d093af86e7279b3dfd.tar.xz kernel-audio-a26ee60f90daffe1de6be0d093af86e7279b3dfd.zip |
bzip2/lzma: fix built-in initramfs vs CONFIG_RD_GZIP
Impact: Resolves build failures in some configurations
Makes it possible to disable CONFIG_RD_GZIP . In that case, the
built-in initramfs will be compressed by whatever compressor is
available (bzip2 or lzma) or left uncompressed if none is available.
It also removes a couple of warnings which occur when no ramdisk
compression at all is chosen.
It also restores the select ZLIB_INFLATE in drivers/block/Kconfig
which somehow came missing. This is needed to activate compilation of
the stuff in zlib_deflate.
Signed-off-by: Alain Knaff <alain@knaff.lu>
Signed-off-by: H. Peter Anvin <hpa@zytor.com>
Diffstat (limited to 'usr')
-rw-r--r-- | usr/Makefile | 42 | ||||
-rw-r--r-- | usr/initramfs_data.S | 2 | ||||
-rw-r--r-- | usr/initramfs_data.bz2.S | 29 | ||||
-rw-r--r-- | usr/initramfs_data.gz.S | 29 | ||||
-rw-r--r-- | usr/initramfs_data.lzma.S | 29 |
5 files changed, 118 insertions, 13 deletions
diff --git a/usr/Makefile b/usr/Makefile index 201f27f8cbaf..451cdff7dff9 100644 --- a/usr/Makefile +++ b/usr/Makefile | |||
@@ -5,14 +5,32 @@ | |||
5 | klibcdirs:; | 5 | klibcdirs:; |
6 | PHONY += klibcdirs | 6 | PHONY += klibcdirs |
7 | 7 | ||
8 | # Find out "preferred" ramdisk compressor. Order of preference is | ||
9 | # 1. bzip2 efficient, and likely to be present | ||
10 | # 2. gzip former default | ||
11 | # 3. lzma | ||
12 | # 4. none | ||
13 | |||
14 | # None of the above | ||
15 | suffix_y = | ||
16 | |||
17 | # Lzma, but no gzip nor bzip2 | ||
18 | suffix_$(CONFIG_RD_LZMA) = .lzma | ||
19 | |||
20 | # Gzip, but no bzip2 | ||
21 | suffix_$(CONFIG_RD_GZIP) = .gz | ||
22 | |||
23 | # Bzip2 | ||
24 | suffix_$(CONFIG_RD_BZIP2) = .bz2 | ||
25 | |||
8 | 26 | ||
9 | # Generate builtin.o based on initramfs_data.o | 27 | # Generate builtin.o based on initramfs_data.o |
10 | obj-$(CONFIG_BLK_DEV_INITRD) := initramfs_data.o | 28 | obj-$(CONFIG_BLK_DEV_INITRD) := initramfs_data$(suffix_y).o |
11 | 29 | ||
12 | # initramfs_data.o contains the initramfs_data.cpio.gz image. | 30 | # initramfs_data.o contains the compressed initramfs_data.cpio image. |
13 | # The image is included using .incbin, a dependency which is not | 31 | # The image is included using .incbin, a dependency which is not |
14 | # tracked automatically. | 32 | # tracked automatically. |
15 | $(obj)/initramfs_data.o: $(obj)/initramfs_data.cpio.gz FORCE | 33 | $(obj)/initramfs_data$(suffix_y).o: $(obj)/initramfs_data.cpio$(suffix_y) FORCE |
16 | 34 | ||
17 | ##### | 35 | ##### |
18 | # Generate the initramfs cpio archive | 36 | # Generate the initramfs cpio archive |
@@ -25,28 +43,28 @@ ramfs-args := \ | |||
25 | $(if $(CONFIG_INITRAMFS_ROOT_UID), -u $(CONFIG_INITRAMFS_ROOT_UID)) \ | 43 | $(if $(CONFIG_INITRAMFS_ROOT_UID), -u $(CONFIG_INITRAMFS_ROOT_UID)) \ |
26 | $(if $(CONFIG_INITRAMFS_ROOT_GID), -g $(CONFIG_INITRAMFS_ROOT_GID)) | 44 | $(if $(CONFIG_INITRAMFS_ROOT_GID), -g $(CONFIG_INITRAMFS_ROOT_GID)) |
27 | 45 | ||
28 | # .initramfs_data.cpio.gz.d is used to identify all files included | 46 | # .initramfs_data.cpio.d is used to identify all files included |
29 | # in initramfs and to detect if any files are added/removed. | 47 | # in initramfs and to detect if any files are added/removed. |
30 | # Removed files are identified by directory timestamp being updated | 48 | # Removed files are identified by directory timestamp being updated |
31 | # The dependency list is generated by gen_initramfs.sh -l | 49 | # The dependency list is generated by gen_initramfs.sh -l |
32 | ifneq ($(wildcard $(obj)/.initramfs_data.cpio.gz.d),) | 50 | ifneq ($(wildcard $(obj)/.initramfs_data.cpio.d),) |
33 | include $(obj)/.initramfs_data.cpio.gz.d | 51 | include $(obj)/.initramfs_data.cpio.d |
34 | endif | 52 | endif |
35 | 53 | ||
36 | quiet_cmd_initfs = GEN $@ | 54 | quiet_cmd_initfs = GEN $@ |
37 | cmd_initfs = $(initramfs) -o $@ $(ramfs-args) $(ramfs-input) | 55 | cmd_initfs = $(initramfs) -o $@ $(ramfs-args) $(ramfs-input) |
38 | 56 | ||
39 | targets := initramfs_data.cpio.gz | 57 | targets := initramfs_data.cpio.gz initramfs_data.cpio.bz2 initramfs_data.cpio.lzma initramfs_data.cpio |
40 | # do not try to update files included in initramfs | 58 | # do not try to update files included in initramfs |
41 | $(deps_initramfs): ; | 59 | $(deps_initramfs): ; |
42 | 60 | ||
43 | $(deps_initramfs): klibcdirs | 61 | $(deps_initramfs): klibcdirs |
44 | # We rebuild initramfs_data.cpio.gz if: | 62 | # We rebuild initramfs_data.cpio if: |
45 | # 1) Any included file is newer then initramfs_data.cpio.gz | 63 | # 1) Any included file is newer then initramfs_data.cpio |
46 | # 2) There are changes in which files are included (added or deleted) | 64 | # 2) There are changes in which files are included (added or deleted) |
47 | # 3) If gen_init_cpio are newer than initramfs_data.cpio.gz | 65 | # 3) If gen_init_cpio are newer than initramfs_data.cpio |
48 | # 4) arguments to gen_initramfs.sh changes | 66 | # 4) arguments to gen_initramfs.sh changes |
49 | $(obj)/initramfs_data.cpio.gz: $(obj)/gen_init_cpio $(deps_initramfs) klibcdirs | 67 | $(obj)/initramfs_data.cpio$(suffix_y): $(obj)/gen_init_cpio $(deps_initramfs) klibcdirs |
50 | $(Q)$(initramfs) -l $(ramfs-input) > $(obj)/.initramfs_data.cpio.gz.d | 68 | $(Q)$(initramfs) -l $(ramfs-input) > $(obj)/.initramfs_data.cpio.d |
51 | $(call if_changed,initfs) | 69 | $(call if_changed,initfs) |
52 | 70 | ||
diff --git a/usr/initramfs_data.S b/usr/initramfs_data.S index c2e1ad424f4a..7c6973d8d829 100644 --- a/usr/initramfs_data.S +++ b/usr/initramfs_data.S | |||
@@ -26,5 +26,5 @@ SECTIONS | |||
26 | */ | 26 | */ |
27 | 27 | ||
28 | .section .init.ramfs,"a" | 28 | .section .init.ramfs,"a" |
29 | .incbin "usr/initramfs_data.cpio.gz" | 29 | .incbin "usr/initramfs_data.cpio" |
30 | 30 | ||
diff --git a/usr/initramfs_data.bz2.S b/usr/initramfs_data.bz2.S new file mode 100644 index 000000000000..bc54d090365c --- /dev/null +++ b/usr/initramfs_data.bz2.S | |||
@@ -0,0 +1,29 @@ | |||
1 | /* | ||
2 | initramfs_data includes the compressed binary that is the | ||
3 | filesystem used for early user space. | ||
4 | Note: Older versions of "as" (prior to binutils 2.11.90.0.23 | ||
5 | released on 2001-07-14) dit not support .incbin. | ||
6 | If you are forced to use older binutils than that then the | ||
7 | following trick can be applied to create the resulting binary: | ||
8 | |||
9 | |||
10 | ld -m elf_i386 --format binary --oformat elf32-i386 -r \ | ||
11 | -T initramfs_data.scr initramfs_data.cpio.gz -o initramfs_data.o | ||
12 | ld -m elf_i386 -r -o built-in.o initramfs_data.o | ||
13 | |||
14 | initramfs_data.scr looks like this: | ||
15 | SECTIONS | ||
16 | { | ||
17 | .init.ramfs : { *(.data) } | ||
18 | } | ||
19 | |||
20 | The above example is for i386 - the parameters vary from architectures. | ||
21 | Eventually look up LDFLAGS_BLOB in an older version of the | ||
22 | arch/$(ARCH)/Makefile to see the flags used before .incbin was introduced. | ||
23 | |||
24 | Using .incbin has the advantage over ld that the correct flags are set | ||
25 | in the ELF header, as required by certain architectures. | ||
26 | */ | ||
27 | |||
28 | .section .init.ramfs,"a" | ||
29 | .incbin "usr/initramfs_data.cpio.bz2" | ||
diff --git a/usr/initramfs_data.gz.S b/usr/initramfs_data.gz.S new file mode 100644 index 000000000000..890c8dd1d6bd --- /dev/null +++ b/usr/initramfs_data.gz.S | |||
@@ -0,0 +1,29 @@ | |||
1 | /* | ||
2 | initramfs_data includes the compressed binary that is the | ||
3 | filesystem used for early user space. | ||
4 | Note: Older versions of "as" (prior to binutils 2.11.90.0.23 | ||
5 | released on 2001-07-14) dit not support .incbin. | ||
6 | If you are forced to use older binutils than that then the | ||
7 | following trick can be applied to create the resulting binary: | ||
8 | |||
9 | |||
10 | ld -m elf_i386 --format binary --oformat elf32-i386 -r \ | ||
11 | -T initramfs_data.scr initramfs_data.cpio.gz -o initramfs_data.o | ||
12 | ld -m elf_i386 -r -o built-in.o initramfs_data.o | ||
13 | |||
14 | initramfs_data.scr looks like this: | ||
15 | SECTIONS | ||
16 | { | ||
17 | .init.ramfs : { *(.data) } | ||
18 | } | ||
19 | |||
20 | The above example is for i386 - the parameters vary from architectures. | ||
21 | Eventually look up LDFLAGS_BLOB in an older version of the | ||
22 | arch/$(ARCH)/Makefile to see the flags used before .incbin was introduced. | ||
23 | |||
24 | Using .incbin has the advantage over ld that the correct flags are set | ||
25 | in the ELF header, as required by certain architectures. | ||
26 | */ | ||
27 | |||
28 | .section .init.ramfs,"a" | ||
29 | .incbin "usr/initramfs_data.cpio.gz" | ||
diff --git a/usr/initramfs_data.lzma.S b/usr/initramfs_data.lzma.S new file mode 100644 index 000000000000..e11469e48562 --- /dev/null +++ b/usr/initramfs_data.lzma.S | |||
@@ -0,0 +1,29 @@ | |||
1 | /* | ||
2 | initramfs_data includes the compressed binary that is the | ||
3 | filesystem used for early user space. | ||
4 | Note: Older versions of "as" (prior to binutils 2.11.90.0.23 | ||
5 | released on 2001-07-14) dit not support .incbin. | ||
6 | If you are forced to use older binutils than that then the | ||
7 | following trick can be applied to create the resulting binary: | ||
8 | |||
9 | |||
10 | ld -m elf_i386 --format binary --oformat elf32-i386 -r \ | ||
11 | -T initramfs_data.scr initramfs_data.cpio.gz -o initramfs_data.o | ||
12 | ld -m elf_i386 -r -o built-in.o initramfs_data.o | ||
13 | |||
14 | initramfs_data.scr looks like this: | ||
15 | SECTIONS | ||
16 | { | ||
17 | .init.ramfs : { *(.data) } | ||
18 | } | ||
19 | |||
20 | The above example is for i386 - the parameters vary from architectures. | ||
21 | Eventually look up LDFLAGS_BLOB in an older version of the | ||
22 | arch/$(ARCH)/Makefile to see the flags used before .incbin was introduced. | ||
23 | |||
24 | Using .incbin has the advantage over ld that the correct flags are set | ||
25 | in the ELF header, as required by certain architectures. | ||
26 | */ | ||
27 | |||
28 | .section .init.ramfs,"a" | ||
29 | .incbin "usr/initramfs_data.cpio.lzma" | ||