| Commit message (Collapse) | Author | Age | Files | Lines |
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
audit_trim_trees()
commit 12b2f117f3bf738c1a00a6f64393f1953a740bd4 upstream.
audit_trim_trees() calls get_tree(). If a failure occurs we must call
put_tree().
[akpm@linux-foundation.org: run put_tree() before mutex_lock() for small scalability improvement]
Signed-off-by: Chen Gang <gang.chen@asianux.com>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Cc: Eric Paris <eparis@redhat.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Jonghwan Choi <jhbird.choi@samsung.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 7fe70b579c9e3daba71635e31b6189394e7b79d3 upstream.
ftrace_dump() had a lot of issues. What ftrace_dump() does, is when
ftrace_dump_on_oops is set (via a kernel parameter or sysctl), it
will dump out the ftrace buffers to the console when either a oops,
panic, or a sysrq-z occurs.
This was written a long time ago when ftrace was fragile to recursion.
But it wasn't written well even for that.
There's a possible deadlock that can occur if a ftrace_dump() is happening
and an NMI triggers another dump. This is because it grabs a lock
before checking if the dump ran.
It also totally disables ftrace, and tracing for no good reasons.
As the ring_buffer now checks if it is read via a oops or NMI, where
there's a chance that the buffer gets corrupted, it will disable
itself. No need to have ftrace_dump() do the same.
ftrace_dump() is now cleaned up where it uses an atomic counter to
make sure only one dump happens at a time. A simple atomic_inc_return()
is enough that is needed for both other CPUs and NMIs. No need for
a spinlock, as if one CPU is running the dump, no other CPU needs
to do it too.
The tracing_on variable is turned off and not turned on. The original
code did this, but it wasn't pretty. By just disabling this variable
we get the result of not seeing traces that happen between crashes.
For sysrq-z, it doesn't get turned on, but the user can always write
a '1' to the tracing_on file. If they are using sysrq-z, then they should
know about tracing_on.
The new code is much easier to read and less error prone. No more
deadlock possibility when an NMI triggers here.
Reported-by: zhangwei(Jovi) <jovi.zhangwei@huawei.com>
Cc: Thomas Gleixner <tglx@linutronix.de>
Cc: Peter Zijlstra <a.p.zijlstra@chello.nl>
Cc: Frederic Weisbecker <fweisbec@gmail.com>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
| |
commit 7ee2b9e56495c56dcaffa2bab19b39451d9fdc8a upstream.
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 6f7a05d7018de222e40ca003721037a530979974 upstream.
Vitaliy reported that a per cpu HPET timer interrupt crashes the
system during hibernation. What happens is that the per cpu HPET timer
gets shut down when the nonboot cpus are stopped. When the nonboot
cpus are onlined again the HPET code sets up the MSI interrupt which
fires before the clock event device is registered. The event handler
is still set to hrtimer_interrupt, which then crashes the machine due
to highres mode not being active.
See http://bugs.debian.org/cgi-bin/bugreport.cgi?bug=700333
There is no real good way to avoid that in the HPET code. The HPET
code alrady has a mechanism to detect spurious interrupts when event
handler == NULL for a similar reason.
We can handle that in the clockevent/tick layer and replace the
previous functional handler with a dummy handler like we do in
tick_setup_new_device().
The original clockevents code did this in clockevents_exchange_device(),
but that got removed by commit 7c1e76897 (clockevents: prevent
clockevent event_handler ending up handler_noop) which forgot to fix
it up in tick_shutdown(). Same issue with the broadcast device.
Reported-by: Vitaliy Fillipov <vitalif@yourcmc.ru>
Cc: Ben Hutchings <ben@decadent.org.uk>
Cc: 700333@bugs.debian.org
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 712317ad97f41e738e1a19aa0a6392a78a84094e upstream.
We should store file xattrs in struct cfent instead of struct cftype,
because cftype is a type while cfent is object instance of cftype.
For example each cgroup has a tasks file, and each tasks file is
associated with a uniq cfent, but all those files share the same
struct cftype.
Alexey Kodanev reported a crash, which can be reproduced:
# mount -t cgroup -o xattr /sys/fs/cgroup
# mkdir /sys/fs/cgroup/test
# setfattr -n trusted.value -v test_value /sys/fs/cgroup/tasks
# rmdir /sys/fs/cgroup/test
# umount /sys/fs/cgroup
oops!
In this case, simple_xattrs_free() will free the same struct simple_xattrs
twice.
tj: Dropped unused local variable @cft from cgroup_diput().
Reported-by: Alexey Kodanev <alexey.kodanev@oracle.com>
Signed-off-by: Li Zefan <lizefan@huawei.com>
Signed-off-by: Tejun Heo <tj@kernel.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 3ac1707a13a3da9cfc8f242a15b2fae6df2c5f88 upstream.
The 3rd parameter of flex_array_prealloc() is the number of elements,
not the index of the last element.
The effect of the bug is, when opening cgroup.procs, a flex array will
be allocated and all elements of the array is allocated with
GFP_KERNEL flag, but the last one is GFP_ATOMIC, and if we fail to
allocate memory for it, it'll trigger a BUG_ON().
Signed-off-by: Li Zefan <lizefan@huawei.com>
Signed-off-by: Tejun Heo <tj@kernel.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 8f294b5a139ee4b75e890ad5b443c93d1e558a8b upstream.
The settimeofday01 test in the LTP testsuite effectively does
gettimeofday(current time);
settimeofday(Jan 1, 1970 + 100 seconds);
settimeofday(current time);
This test causes a stack trace to be displayed on the console during the
setting of timeofday to Jan 1, 1970 + 100 seconds:
[ 131.066751] ------------[ cut here ]------------
[ 131.096448] WARNING: at kernel/time/clockevents.c:209 clockevents_program_event+0x135/0x140()
[ 131.104935] Hardware name: Dinar
[ 131.108150] Modules linked in: sg nfsv3 nfs_acl nfsv4 auth_rpcgss nfs dns_resolver fscache lockd sunrpc nf_conntrack_netbios_ns nf_conntrack_broadcast ipt_MASQUERADE ip6table_mangle ip6t_REJECT nf_conntrack_ipv6 nf_defrag_ipv6 iptable_nat nf_nat_ipv4 nf_nat iptable_mangle ipt_REJECT nf_conntrack_ipv4 nf_defrag_ipv4 xt_conntrack nf_conntrack ebtable_filter ebtables ip6table_filter ip6_tables iptable_filter ip_tables kvm_amd kvm sp5100_tco bnx2 i2c_piix4 crc32c_intel k10temp fam15h_power ghash_clmulni_intel amd64_edac_mod pcspkr serio_raw edac_mce_amd edac_core microcode xfs libcrc32c sr_mod sd_mod cdrom ata_generic crc_t10dif pata_acpi radeon i2c_algo_bit drm_kms_helper ttm drm ahci pata_atiixp libahci libata usb_storage i2c_core dm_mirror dm_region_hash dm_log dm_mod
[ 131.176784] Pid: 0, comm: swapper/28 Not tainted 3.8.0+ #6
[ 131.182248] Call Trace:
[ 131.184684] <IRQ> [<ffffffff810612af>] warn_slowpath_common+0x7f/0xc0
[ 131.191312] [<ffffffff8106130a>] warn_slowpath_null+0x1a/0x20
[ 131.197131] [<ffffffff810b9fd5>] clockevents_program_event+0x135/0x140
[ 131.203721] [<ffffffff810bb584>] tick_program_event+0x24/0x30
[ 131.209534] [<ffffffff81089ab1>] hrtimer_interrupt+0x131/0x230
[ 131.215437] [<ffffffff814b9600>] ? cpufreq_p4_target+0x130/0x130
[ 131.221509] [<ffffffff81619119>] smp_apic_timer_interrupt+0x69/0x99
[ 131.227839] [<ffffffff8161805d>] apic_timer_interrupt+0x6d/0x80
[ 131.233816] <EOI> [<ffffffff81099745>] ? sched_clock_cpu+0xc5/0x120
[ 131.240267] [<ffffffff814b9ff0>] ? cpuidle_wrap_enter+0x50/0xa0
[ 131.246252] [<ffffffff814b9fe9>] ? cpuidle_wrap_enter+0x49/0xa0
[ 131.252238] [<ffffffff814ba050>] cpuidle_enter_tk+0x10/0x20
[ 131.257877] [<ffffffff814b9c89>] cpuidle_idle_call+0xa9/0x260
[ 131.263692] [<ffffffff8101c42f>] cpu_idle+0xaf/0x120
[ 131.268727] [<ffffffff815f8971>] start_secondary+0x255/0x257
[ 131.274449] ---[ end trace 1151a50552231615 ]---
When we change the system time to a low value like this, the value of
timekeeper->offs_real will be a negative value.
It seems that the WARN occurs because an hrtimer has been started in the time
between the releasing of the timekeeper lock and the IPI call (via a call to
on_each_cpu) in clock_was_set() in the do_settimeofday() code. The end result
is that a REALTIME_CLOCK timer has been added with softexpires = expires =
KTIME_MAX. The hrtimer_interrupt() fires/is called and the loop at
kernel/hrtimer.c:1289 is executed. In this loop the code subtracts the
clock base's offset (which was set to timekeeper->offs_real in
do_settimeofday()) from the current hrtimer_cpu_base->expiry value (which
was KTIME_MAX):
KTIME_MAX - (a negative value) = overflow
A simple check for an overflow can resolve this problem. Using KTIME_MAX
instead of the overflow value will result in the hrtimer function being run,
and the reprogramming of the timer after that.
Reviewed-by: Rik van Riel <riel@redhat.com>
Cc: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Prarit Bhargava <prarit@redhat.com>
[jstultz: Tweaked commit subject]
Signed-off-by: John Stultz <john.stultz@linaro.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 51fd36f3fad8447c487137ae26b9d0b3ce77bb25 upstream.
One can trigger an overflow when using ktime_add_ns() on a 32bit
architecture not supporting CONFIG_KTIME_SCALAR.
When passing a very high value for u64 nsec, e.g. 7881299347898368000
the do_div() function converts this value to seconds (7881299347) which
is still to high to pass to the ktime_set() function as long. The result
in is a negative value.
The problem on my system occurs in the tick-sched.c,
tick_nohz_stop_sched_tick() when time_delta is set to
timekeeping_max_deferment(). The check for time_delta < KTIME_MAX is
valid, thus ktime_add_ns() is called with a too large value resulting in
a negative expire value. This leads to an endless loop in the ticker code:
time_delta: 7881299347898368000
expires = ktime_add_ns(last_update, time_delta)
expires: negative value
This fix caps the value to KTIME_MAX.
This error doesn't occurs on 64bit or architectures supporting
CONFIG_KTIME_SCALAR (e.g. ARM, x86-32).
Signed-off-by: David Engraf <david.engraf@sysgo.com>
[jstultz: Minor tweaks to commit message & header]
Signed-off-by: John Stultz <john.stultz@linaro.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 9f50afccfdc15d95d7331acddcb0f7703df089ae upstream.
The ftrace_graph_count can be decreased with a "!" pattern, so that
the enabled flag should be updated too.
Link: http://lkml.kernel.org/r/1365663698-2413-1-git-send-email-namhyung@kernel.org
Signed-off-by: Namhyung Kim <namhyung@kernel.org>
Cc: Frederic Weisbecker <fweisbec@gmail.com>
Cc: Ingo Molnar <mingo@kernel.org>
Cc: Namhyung Kim <namhyung.kim@lge.com>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit ed6f1c996bfe4b6e520cf7a74b51cd6988d84420 upstream.
Check return value and bail out if it's NULL.
Link: http://lkml.kernel.org/r/1365553093-10180-2-git-send-email-namhyung@kernel.org
Signed-off-by: Namhyung Kim <namhyung@kernel.org>
Cc: Frederic Weisbecker <fweisbec@gmail.com>
Cc: Namhyung Kim <namhyung.kim@lge.com>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 39e30cd1537937d3c00ef87e865324e981434e5b upstream.
The first page was allocated separately, so no need to start from 0.
Link: http://lkml.kernel.org/r/1364820385-32027-2-git-send-email-namhyung@kernel.org
Signed-off-by: Namhyung Kim <namhyung@kernel.org>
Cc: Frederic Weisbecker <fweisbec@gmail.com>
Cc: Namhyung Kim <namhyung.kim@lge.com>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 4df297129f622bdc18935c856f42b9ddd18f9f28 upstream.
Currently, the depth reported in the stack tracer stack_trace file
does not match the stack_max_size file. This is because the stack_max_size
includes the overhead of stack tracer itself while the depth does not.
The first time a max is triggered, a calculation is not performed that
figures out the overhead of the stack tracer and subtracts it from
the stack_max_size variable. The overhead is stored and is subtracted
from the reported stack size for comparing for a new max.
Now the stack_max_size corresponds to the reported depth:
# cat stack_max_size
4640
# cat stack_trace
Depth Size Location (48 entries)
----- ---- --------
0) 4640 32 _raw_spin_lock+0x18/0x24
1) 4608 112 ____cache_alloc+0xb7/0x22d
2) 4496 80 kmem_cache_alloc+0x63/0x12f
3) 4416 16 mempool_alloc_slab+0x15/0x17
[...]
While testing against and older gcc on x86 that uses mcount instead
of fentry, I found that pasing in ip + MCOUNT_INSN_SIZE let the
stack trace show one more function deep which was missing before.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit d4ecbfc49b4b1d4b597fb5ba9e4fa25d62f105c5 upstream.
When gcc 4.6 on x86 is used, the function tracer will use the new
option -mfentry which does a call to "fentry" at every function
instead of "mcount". The significance of this is that fentry is
called as the first operation of the function instead of the mcount
usage of being called after the stack.
This causes the stack tracer to show some bogus results for the size
of the last function traced, as well as showing "ftrace_call" instead
of the function. This is due to the stack frame not being set up
by the function that is about to be traced.
# cat stack_trace
Depth Size Location (48 entries)
----- ---- --------
0) 4824 216 ftrace_call+0x5/0x2f
1) 4608 112 ____cache_alloc+0xb7/0x22d
2) 4496 80 kmem_cache_alloc+0x63/0x12f
The 216 size for ftrace_call includes both the ftrace_call stack
(which includes the saving of registers it does), as well as the
stack size of the parent.
To fix this, if CC_USING_FENTRY is defined, then the stack_tracer
will reserve the first item in stack_dump_trace[] array when
calling save_stack_trace(), and it will fill it in with the parent ip.
Then the code will look for the parent pointer on the stack and
give the real size of the parent's stack pointer:
# cat stack_trace
Depth Size Location (14 entries)
----- ---- --------
0) 2640 48 update_group_power+0x26/0x187
1) 2592 224 update_sd_lb_stats+0x2a5/0x4ac
2) 2368 160 find_busiest_group+0x31/0x1f1
3) 2208 256 load_balance+0xd9/0x662
I'm Cc'ing stable, although it's not urgent, as it only shows bogus
size for item #0, the rest of the trace is legit. It should still be
corrected in previous stable releases.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 87889501d0adfae10e3b0f0e6f2d7536eed9ae84 upstream.
Use the stack of stack_trace_call() instead of check_stack() as
the test pointer for max stack size. It makes it a bit cleaner
and a little more accurate.
Adding stable, as a later fix depends on this patch.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 05cbbf643b8eea1be21082c53cdb856d1dc6d765 upstream.
The test that checks function recursion does things differently
if the arch does not support all ftrace features. But that really
doesn't make a difference with how the test runs, and either way
the count variable should be 2 at the end.
Currently the test wrongly fails for archs that don't support all
the ftrace features.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 935d8aabd4331f47a89c3e1daa5779d23cf244ee upstream.
Nothing is using it yet, but this will allow us to delay the open-time
checks to use time, without breaking the normal UNIX permission
semantics where permissions are determined by the opener (and the file
descriptor can then be passed to a different process, or the process can
drop capabilities).
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Cc: Shea Levy <shea@shealevy.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 41c21e351e79004dbb4efa4bc14a53a7e0af38c5 upstream.
Changing uid/gid/projid mappings doesn't change your id within the
namespace; it reconfigures the namespace. Unprivileged programs should
*not* be able to write these files. (We're also checking the privileges
on the wrong task.)
Given the write-once nature of these files and the other security
checks, this is likely impossible to usefully exploit.
Signed-off-by: Andy Lutomirski <luto@amacapital.net>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
| |
commit e3211c120a85b792978bcb4be7b2886df18d27f0 upstream.
Signed-off-by: Andy Lutomirski <luto@amacapital.net>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
id_map
commit 6708075f104c3c9b04b23336bb0366ca30c3931b upstream.
When we require privilege for setting /proc/<pid>/uid_map or
/proc/<pid>/gid_map no longer allow an unprivileged user to
open the file and pass it to a privileged program to write
to the file.
Instead when privilege is required require both the opener and the
writer to have the necessary capabilities.
I have tested this code and verified that setting /proc/<pid>/uid_map
fails when an unprivileged user opens the file and a privielged user
attempts to set the mapping, that unprivileged users can still map
their own id, and that a privileged users can still setup an arbitrary
mapping.
Reported-by: Andy Lutomirski <luto@amacapital.net>
Signed-off-by: "Eric W. Biederman" <ebiederm@xmission.com>
Signed-off-by: Andy Lutomirski <luto@amacapital.net>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 8176cced706b5e5d15887584150764894e94e02f upstream.
Trinity discovered that we fail to check all 64 bits of
attr.config passed by user space, resulting to out-of-bounds
access of the perf_swevent_enabled array in
sw_perf_event_destroy().
Introduced in commit b0a873ebb ("perf: Register PMU
implementations").
Signed-off-by: Tommi Rantala <tt.rantala@gmail.com>
Cc: Peter Zijlstra <a.p.zijlstra@chello.nl>
Cc: davej@redhat.com
Cc: Paul Mackerras <paulus@samba.org>
Cc: Arnaldo Carvalho de Melo <acme@ghostprotocols.net>
Link: http://lkml.kernel.org/r/1365882554-30259-1-git-send-email-tt.rantala@gmail.com
Signed-off-by: Ingo Molnar <mingo@kernel.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit fd9b86d37a600488dbd80fe60cca46b822bff1cd upstream.
Commit 201c373e8e ("sched/debug: Limit sd->*_idx range on
sysctl") was an incomplete bug fix.
This patch fixes sd->*_idx limit range to [0 ~ CPU_LOAD_IDX_MAX-1]
avoiding array overflow caused by setting sd->*_idx to CPU_LOAD_IDX_MAX
on sysctl.
Signed-off-by: Libin <huawei.libin@huawei.com>
Cc: <jiang.liu@huawei.com>
Cc: <guohanjun@huawei.com>
Cc: Peter Zijlstra <peterz@infradead.org>
Link: http://lkml.kernel.org/r/51626610.2040607@huawei.com
Signed-off-by: Ingo Molnar <mingo@kernel.org>
Signed-off-by: Jonghwan Choi <jhbird.choi@samsung.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 383efcd00053ec40023010ce5034bd702e7ab373 upstream.
try_to_wake_up_local() should only be invoked to wake up another
task in the same runqueue and BUG_ON()s are used to enforce the
rule. Missing try_to_wake_up_local() can stall workqueue
execution but such stalls are likely to be finite either by
another work item being queued or the one blocked getting
unblocked. There's no reason to trigger BUG while holding rq
lock crashing the whole system.
Convert BUG_ON()s in try_to_wake_up_local() to WARN_ON_ONCE()s.
Signed-off-by: Tejun Heo <tj@kernel.org>
Acked-by: Steven Rostedt <rostedt@goodmis.org>
Cc: Peter Zijlstra <peterz@infradead.org>
Link: http://lkml.kernel.org/r/20130318192234.GD3042@htj.dyndns.org
Signed-off-by: Ingo Molnar <mingo@kernel.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit b9e146d8eb3b9ecae5086d373b50fa0c1f3e7f0f upstream.
This fixes a kernel memory contents leak via the tkill and tgkill syscalls
for compat processes.
This is visible in the siginfo_t->_sifields._rt.si_sigval.sival_ptr field
when handling signals delivered from tkill.
The place of the infoleak:
int copy_siginfo_to_user32(compat_siginfo_t __user *to, siginfo_t *from)
{
...
put_user_ex(ptr_to_compat(from->si_ptr), &to->si_ptr);
...
}
Signed-off-by: Emese Revfy <re.emese@gmail.com>
Reviewed-by: PaX Team <pageexec@freemail.hu>
Signed-off-by: Kees Cook <keescook@chromium.org>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Cc: Oleg Nesterov <oleg@redhat.com>
Cc: "Eric W. Biederman" <ebiederm@xmission.com>
Cc: Serge Hallyn <serge.hallyn@canonical.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 84cc8fd2fe65866e49d70b38b3fdf7219dd92fe0 upstream.
The current code makes the assumption that a cpu_base lock won't be
held if the CPU corresponding to that cpu_base is offline, which isn't
always true.
If a hrtimer is not queued, then it will not be migrated by
migrate_hrtimers() when a CPU is offlined. Therefore, the hrtimer's
cpu_base may still point to a CPU which has subsequently gone offline
if the timer wasn't enqueued at the time the CPU went down.
Normally this wouldn't be a problem, but a cpu_base's lock is blindly
reinitialized each time a CPU is brought up. If a CPU is brought
online during the period that another thread is performing a hrtimer
operation on a stale hrtimer, then the lock will be reinitialized
under its feet, and a SPIN_BUG() like the following will be observed:
<0>[ 28.082085] BUG: spinlock already unlocked on CPU#0, swapper/0/0
<0>[ 28.087078] lock: 0xc4780b40, value 0x0 .magic: dead4ead, .owner: <none>/-1, .owner_cpu: -1
<4>[ 42.451150] [<c0014398>] (unwind_backtrace+0x0/0x120) from [<c0269220>] (do_raw_spin_unlock+0x44/0xdc)
<4>[ 42.460430] [<c0269220>] (do_raw_spin_unlock+0x44/0xdc) from [<c071b5bc>] (_raw_spin_unlock+0x8/0x30)
<4>[ 42.469632] [<c071b5bc>] (_raw_spin_unlock+0x8/0x30) from [<c00a9ce0>] (__hrtimer_start_range_ns+0x1e4/0x4f8)
<4>[ 42.479521] [<c00a9ce0>] (__hrtimer_start_range_ns+0x1e4/0x4f8) from [<c00aa014>] (hrtimer_start+0x20/0x28)
<4>[ 42.489247] [<c00aa014>] (hrtimer_start+0x20/0x28) from [<c00e6190>] (rcu_idle_enter_common+0x1ac/0x320)
<4>[ 42.498709] [<c00e6190>] (rcu_idle_enter_common+0x1ac/0x320) from [<c00e6440>] (rcu_idle_enter+0xa0/0xb8)
<4>[ 42.508259] [<c00e6440>] (rcu_idle_enter+0xa0/0xb8) from [<c000f268>] (cpu_idle+0x24/0xf0)
<4>[ 42.516503] [<c000f268>] (cpu_idle+0x24/0xf0) from [<c06ed3c0>] (rest_init+0x88/0xa0)
<4>[ 42.524319] [<c06ed3c0>] (rest_init+0x88/0xa0) from [<c0c00978>] (start_kernel+0x3d0/0x434)
As an example, this particular crash occurred when hrtimer_start() was
executed on CPU #0. The code locked the hrtimer's current cpu_base
corresponding to CPU #1. CPU #0 then tried to switch the hrtimer's
cpu_base to an optimal CPU which was online. In this case, it selected
the cpu_base corresponding to CPU #3.
Before it could proceed, CPU #1 came online and reinitialized the
spinlock corresponding to its cpu_base. Thus now CPU #0 held a lock
which was reinitialized. When CPU #0 finally ended up unlocking the
old cpu_base corresponding to CPU #1 so that it could switch to CPU
#3, we hit this SPIN_BUG() above while in switch_hrtimer_base().
CPU #0 CPU #1
---- ----
... <offline>
hrtimer_start()
lock_hrtimer_base(base #1)
... init_hrtimers_cpu()
switch_hrtimer_base() ...
... raw_spin_lock_init(&cpu_base->lock)
raw_spin_unlock(&cpu_base->lock) ...
<spin_bug>
Solve this by statically initializing the lock.
Signed-off-by: Michael Bohan <mbohan@codeaurora.org>
Link: http://lkml.kernel.org/r/1363745965-23475-1-git-send-email-mbohan@codeaurora.org
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit f2530dc71cf0822f90bb63ea4600caaef33a66bb upstream.
The smpboot threads rely on the park/unpark mechanism which binds per
cpu threads on a particular core. Though the functionality is racy:
CPU0 CPU1 CPU2
unpark(T) wake_up_process(T)
clear(SHOULD_PARK) T runs
leave parkme() due to !SHOULD_PARK
bind_to(CPU2) BUG_ON(wrong CPU)
We cannot let the tasks move themself to the target CPU as one of
those tasks is actually the migration thread itself, which requires
that it starts running on the target cpu right away.
The solution to this problem is to prevent wakeups in park mode which
are not from unpark(). That way we can guarantee that the association
of the task to the target cpu is working correctly.
Add a new task state (TASK_PARKED) which prevents other wakeups and
use this state explicitly for the unpark wakeup.
Peter noticed: Also, since the task state is visible to userspace and
all the parked tasks are still in the PID space, its a good hint in ps
and friends that these tasks aren't really there for the moment.
The migration thread has another related issue.
CPU0 CPU1
Bring up CPU2
create_thread(T)
park(T)
wait_for_completion()
parkme()
complete()
sched_set_stop_task()
schedule(TASK_PARKED)
The sched_set_stop_task() call is issued while the task is on the
runqueue of CPU1 and that confuses the hell out of the stop_task class
on that cpu. So we need the same synchronizaion before
sched_set_stop_task().
Reported-by: Dave Jones <davej@redhat.com>
Reported-and-tested-by: Dave Hansen <dave@sr71.net>
Reported-and-tested-by: Borislav Petkov <bp@alien8.de>
Acked-by: Peter Ziljstra <peterz@infradead.org>
Cc: Srivatsa S. Bhat <srivatsa.bhat@linux.vnet.ibm.com>
Cc: dhillf@gmail.com
Cc: Ingo Molnar <mingo@kernel.org>
Link: http://lkml.kernel.org/r/alpine.LFD.2.02.1304091635430.21884@ionos
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit a1cbcaa9ea87b87a96b9fc465951dcf36e459ca2 upstream.
The sched_clock_remote() implementation has the following inatomicity
problem on 32bit systems when accessing the remote scd->clock, which
is a 64bit value.
CPU0 CPU1
sched_clock_local() sched_clock_remote(CPU0)
...
remote_clock = scd[CPU0]->clock
read_low32bit(scd[CPU0]->clock)
cmpxchg64(scd->clock,...)
read_high32bit(scd[CPU0]->clock)
While the update of scd->clock is using an atomic64 mechanism, the
readout on the remote cpu is not, which can cause completely bogus
readouts.
It is a quite rare problem, because it requires the update to hit the
narrow race window between the low/high readout and the update must go
across the 32bit boundary.
The resulting misbehaviour is, that CPU1 will see the sched_clock on
CPU1 ~4 seconds ahead of it's own and update CPU1s sched_clock value
to this bogus timestamp. This stays that way due to the clamping
implementation for about 4 seconds until the synchronization with
CLOCK_MONOTONIC undoes the problem.
The issue is hard to observe, because it might only result in a less
accurate SCHED_OTHER timeslicing behaviour. To create observable
damage on realtime scheduling classes, it is necessary that the bogus
update of CPU1 sched_clock happens in the context of an realtime
thread, which then gets charged 4 seconds of RT runtime, which results
in the RT throttler mechanism to trigger and prevent scheduling of RT
tasks for a little less than 4 seconds. So this is quite unlikely as
well.
The issue was quite hard to decode as the reproduction time is between
2 days and 3 weeks and intrusive tracing makes it less likely, but the
following trace recorded with trace_clock=global, which uses
sched_clock_local(), gave the final hint:
<idle>-0 0d..30 400269.477150: hrtimer_cancel: hrtimer=0xf7061e80
<idle>-0 0d..30 400269.477151: hrtimer_start: hrtimer=0xf7061e80 ...
irq/20-S-587 1d..32 400273.772118: sched_wakeup: comm= ... target_cpu=0
<idle>-0 0dN.30 400273.772118: hrtimer_cancel: hrtimer=0xf7061e80
What happens is that CPU0 goes idle and invokes
sched_clock_idle_sleep_event() which invokes sched_clock_local() and
CPU1 runs a remote wakeup for CPU0 at the same time, which invokes
sched_remote_clock(). The time jump gets propagated to CPU0 via
sched_remote_clock() and stays stale on both cores for ~4 seconds.
There are only two other possibilities, which could cause a stale
sched clock:
1) ktime_get() which reads out CLOCK_MONOTONIC returns a sporadic
wrong value.
2) sched_clock() which reads the TSC returns a sporadic wrong value.
#1 can be excluded because sched_clock would continue to increase for
one jiffy and then go stale.
#2 can be excluded because it would not make the clock jump
forward. It would just result in a stale sched_clock for one jiffy.
After quite some brain twisting and finding the same pattern on other
traces, sched_clock_remote() remained the only place which could cause
such a problem and as explained above it's indeed racy on 32bit
systems.
So while on 64bit systems the readout is atomic, we need to verify the
remote readout on 32bit machines. We need to protect the local->clock
readout in sched_clock_remote() on 32bit as well because an NMI could
hit between the low and the high readout, call sched_clock_local() and
modify local->clock.
Thanks to Siegfried Wulsch for bearing with my debug requests and
going through the tedious tasks of running a bunch of reproducer
systems to generate the debug information which let me decode the
issue.
Reported-by: Siegfried Wulsch <Siegfried.Wulsch@rovema.de>
Acked-by: Peter Zijlstra <peterz@infradead.org>
Cc: Steven Rostedt <rostedt@goodmis.org>
Link: http://lkml.kernel.org/r/alpine.LFD.2.02.1304051544160.21884@ionos
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 7f49ef69db6bbf756c0abca7e9b65b32e999eec8 upstream.
As ftrace_filter_lseek is now used with ftrace_pid_fops, it needs to
be moved out of the #ifdef CONFIG_DYNAMIC_FTRACE section as the
ftrace_pid_fops is defined when DYNAMIC_FTRACE is not.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Cc: Namhyung Kim <namhyung@kernel.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 6a76f8c0ab19f215af2a3442870eeb5f0e81998d upstream.
Currently set_ftrace_pid and set_graph_function files use seq_lseek
for their fops. However seq_open() is called only for FMODE_READ in
the fops->open() so that if an user tries to seek one of those file
when she open it for writing, it sees NULL seq_file and then panic.
It can be easily reproduced with following command:
$ cd /sys/kernel/debug/tracing
$ echo 1234 | sudo tee -a set_ftrace_pid
In this example, GNU coreutils' tee opens the file with fopen(, "a")
and then the fopen() internally calls lseek().
Link: http://lkml.kernel.org/r/1365663302-2170-1-git-send-email-namhyung@kernel.org
Signed-off-by: Namhyung Kim <namhyung@kernel.org>
Cc: Frederic Weisbecker <fweisbec@gmail.com>
Cc: Ingo Molnar <mingo@kernel.org>
Cc: Namhyung Kim <namhyung.kim@lge.com>
Cc: stable@vger.kernel.org
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 6f389a8f1dd22a24f3d9afc2812b30d639e94625 upstream.
As commit 40dc166c (PM / Core: Introduce struct syscore_ops for core
subsystems PM) say, syscore_ops operations should be carried with one
CPU on-line and interrupts disabled. However, after commit f96972f2d
(kernel/sys.c: call disable_nonboot_cpus() in kernel_restart()),
syscore_shutdown() is called before disable_nonboot_cpus(), so break
the rules. We have a MIPS machine with a 8259A PIC, and there is an
external timer (HPET) linked at 8259A. Since 8259A has been shutdown
too early (by syscore_shutdown()), disable_nonboot_cpus() runs without
timer interrupt, so it hangs and reboot fails. This patch call
syscore_shutdown() a little later (after disable_nonboot_cpus()) to
avoid reboot failure, this is the same way as poweroff does.
For consistency, add disable_nonboot_cpus() to kernel_halt().
Signed-off-by: Huacai Chen <chenhc@lemote.com>
Signed-off-by: Rafael J. Wysocki <rafael.j.wysocki@intel.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 83e03b3fe4daffdebbb42151d5410d730ae50bd1 upstream.
On the failure path, stat->start and stat->pages will refer same page.
So it'll attempt to free the same page again and get kernel panic.
Link: http://lkml.kernel.org/r/1364820385-32027-1-git-send-email-namhyung@kernel.org
Signed-off-by: Namhyung Kim <namhyung@kernel.org>
Cc: Frederic Weisbecker <fweisbec@gmail.com>
Cc: Namhyung Kim <namhyung.kim@lge.com>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 5000c418840b309251c5887f0b56503aae30f84c upstream.
If we reenable ftrace via syctl, we currently set ftrace_trace_function
based on the previous simplistic algorithm. This is inconsistent with
what update_ftrace_function does. So better call that helper instead.
Link: http://lkml.kernel.org/r/5151D26F.1070702@siemens.com
Signed-off-by: Jan Kiszka <jan.kiszka@siemens.com>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 613f04a0f51e6e68ac6fe571ab79da3c0a5eb4da upstream.
The latency tracers require the buffers to be in overwrite mode,
otherwise they get screwed up. Force the buffers to stay in overwrite
mode when latency tracers are enabled.
Added a flag_changed() method to the tracer structure to allow
the tracers to see what flags are being changed, and also be able
to prevent the change from happing.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Lingzhu Xiang <lxiang@redhat.com>
Reviewed-by: CAI Qian <caiqian@redhat.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 522cff142d7d2f9230839c9e1f21a4d8bcc22a4a upstream.
__ARCH_HAS_SA_RESTORER is the preferred conditional for use in 3.9 and
later kernels, per Kees.
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Cc: Emese Revfy <re.emese@gmail.com>
Cc: Emese Revfy <re.emese@gmail.com>
Cc: PaX Team <pageexec@freemail.hu>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Cc: Oleg Nesterov <oleg@redhat.com>
Cc: "Eric W. Biederman" <ebiederm@xmission.com>
Cc: Serge Hallyn <serge.hallyn@canonical.com>
Cc: Julien Tinnes <jln@google.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Cc: Ben Hutchings <ben@decadent.org.uk>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 87a8ebd637dafc255070f503909a053cf0d98d3f upstream.
Only allow unprivileged mounts of proc and sysfs if they are already
mounted when the user namespace is created.
proc and sysfs are interesting because they have content that is
per namespace, and so fresh mounts are needed when new namespaces
are created while at the same time proc and sysfs have content that
is shared between every instance.
Respect the policy of who may see the shared content of proc and sysfs
by only allowing new mounts if there was an existing mount at the time
the user namespace was created.
In practice there are only two interesting cases: proc and sysfs are
mounted at their usual places, proc and sysfs are not mounted at all
(some form of mount namespace jail).
Acked-by: Serge Hallyn <serge.hallyn@canonical.com>
Signed-off-by: "Eric W. Biederman" <ebiederm@xmission.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 3151527ee007b73a0ebd296010f1c0454a919c7d upstream.
Guarantee that the policy of which files may be access that is
established by setting the root directory will not be violated
by user namespaces by verifying that the root directory points
to the root of the mount namespace at the time of user namespace
creation.
Changing the root is a privileged operation, and as a matter of policy
it serves to limit unprivileged processes to files below the current
root directory.
For reasons of simplicity and comprehensibility the privilege to
change the root directory is gated solely on the CAP_SYS_CHROOT
capability in the user namespace. Therefore when creating a user
namespace we must ensure that the policy of which files may be access
can not be violated by changing the root directory.
Anyone who runs a processes in a chroot and would like to use user
namespace can setup the same view of filesystems with a mount
namespace instead. With this result that this is not a practical
limitation for using user namespaces.
Acked-by: Serge Hallyn <serge.hallyn@canonical.com>
Reported-by: Andy Lutomirski <luto@amacapital.net>
Signed-off-by: "Eric W. Biederman" <ebiederm@xmission.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 751c644b95bb48aaa8825f0c66abbcc184d92051 upstream.
When a multi-threaded init exits and the initial thread is not the
last thread to exit the initial thread hangs around as a zombie
until the last thread exits. In that case zap_pid_ns_processes
needs to wait until there are only 2 hashed pids in the pid
namespace not one.
v2. Replace thread_pid_vnr(me) == 1 with the test thread_group_leader(me)
as suggested by Oleg.
Reported-by: Caj Larsson <caj@omnicloud.com>
Cc: Oleg Nesterov <oleg@redhat.com>
Signed-off-by: "Eric W. Biederman" <ebiederm@xmission.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit a7dc19b8652c862d5b7c4d2339bd3c428bd29c4a upstream.
Currently tick_check_broadcast_device doesn't reject clock_event_devices
with CLOCK_EVT_FEAT_DUMMY, and may select them in preference to real
hardware if they have a higher rating value. In this situation, the
dummy timer is responsible for broadcasting to itself, and the core
clockevents code may attempt to call non-existent callbacks for
programming the dummy, eventually leading to a panic.
This patch makes tick_check_broadcast_device always reject dummy timers,
preventing this problem.
Signed-off-by: Mark Rutland <mark.rutland@arm.com>
Cc: linux-arm-kernel@lists.infradead.org
Cc: Jon Medhurst (Tixy) <tixy@linaro.org>
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 80902822658aab18330569587cdb69ac1dfdcea8 upstream.
Changing the overwrite mode for the ring buffer via the trace
option only sets the normal buffer. But the snapshot buffer could
swap with it, and then the snapshot would be in non overwrite mode
and the normal buffer would be in overwrite mode, even though the
option flag states otherwise.
Keep the two buffers overwrite modes in sync.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 69d34da2984c95b33ea21518227e1f9470f11d95 upstream.
Seems that the tracer flags have never been protected from
synchronous writes. Luckily, admins don't usually modify the
tracing flags via two different tasks. But if scripts were to
be used to modify them, then they could get corrupted.
Move the trace_types_lock that protects against tracers changing
to also protect the flags being set.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 740466bc89ad8bd5afcc8de220f715f62b21e365 upstream.
Because function tracing is very invasive, and can even trace
calls to rcu_read_lock(), RCU access in function tracing is done
with preempt_disable_notrace(). This requires a synchronize_sched()
for updates and not a synchronize_rcu().
Function probes (traceon, traceoff, etc) must be freed after
a synchronize_sched() after its entry has been removed from the
hash. But call_rcu() is used. Fix this by using call_rcu_sched().
Also fix the usage to use hlist_del_rcu() instead of hlist_del().
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Cc: Paul McKenney <paulmck@linux.vnet.ibm.com>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 2721e72dd10f71a3ba90f59781becf02638aa0d9 upstream.
Although the swap is wrapped with a spin_lock, the assignment
of the temp buffer used to swap is not within that lock.
It needs to be moved into that lock, otherwise two swaps
happening on two different CPUs, can end up using the wrong
temp buffer to assign in the swap.
Luckily, all current callers of the swap function appear to have
their own locks. But in case something is added that allows two
different callers to call the swap, then there's a chance that
this race can trigger and corrupt the buffers.
New code is coming soon that will allow for this race to trigger.
I've Cc'd stable, so this bug will not show up if someone backports
one of the changes that can trigger this bug.
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 2ca39528c01a933f6689cd6505ce65bd6d68a530 upstream.
When the new signal handlers are set up, the location of sa_restorer is
not cleared, leaking a parent process's address space location to
children. This allows for a potential bypass of the parent's ASLR by
examining the sa_restorer value returned when calling sigaction().
Based on what should be considered "secret" about addresses, it only
matters across the exec not the fork (since the VMAs haven't changed
until the exec). But since exec sets SIG_DFL and keeps sa_restorer,
this is where it should be fixed.
Given the few uses of sa_restorer, a "set" function was not written
since this would be the only use. Instead, we use
__ARCH_HAS_SA_RESTORER, as already done in other places.
Example of the leak before applying this patch:
$ cat /proc/$$/maps
...
7fb9f3083000-7fb9f3238000 r-xp 00000000 fd:01 404469 .../libc-2.15.so
...
$ ./leak
...
7f278bc74000-7f278be29000 r-xp 00000000 fd:01 404469 .../libc-2.15.so
...
1 0 (nil) 0x7fb9f30b94a0
2 4000000 (nil) 0x7f278bcaa4a0
3 4000000 (nil) 0x7f278bcaa4a0
4 0 (nil) 0x7fb9f30b94a0
...
[akpm@linux-foundation.org: use SA_RESTORER for backportability]
Signed-off-by: Kees Cook <keescook@chromium.org>
Reported-by: Emese Revfy <re.emese@gmail.com>
Cc: Emese Revfy <re.emese@gmail.com>
Cc: PaX Team <pageexec@freemail.hu>
Cc: Al Viro <viro@zeniv.linux.org.uk>
Cc: Oleg Nesterov <oleg@redhat.com>
Cc: "Eric W. Biederman" <ebiederm@xmission.com>
Cc: Serge Hallyn <serge.hallyn@canonical.com>
Cc: Julien Tinnes <jln@google.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit e66eded8309ebf679d3d3c1f5820d1f2ca332c71 upstream.
Don't allowing sharing the root directory with processes in a
different user namespace. There doesn't seem to be any point, and to
allow it would require the overhead of putting a user namespace
reference in fs_struct (for permission checks) and incrementing that
reference count on practically every call to fork.
So just perform the inexpensive test of forbidding sharing fs_struct
acrosss processes in different user namespaces. We already disallow
other forms of threading when unsharing a user namespace so this
should be no real burden in practice.
This updates setns, clone, and unshare to disallow multiple user
namespaces sharing an fs_struct.
Signed-off-by: "Eric W. Biederman" <ebiederm@xmission.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit db05021d49a994ee40a9735d9c3cb0060c9babb8 upstream.
The prompt to enable DYNAMIC_FTRACE (the ability to nop and
enable function tracing at run time) had a confusing statement:
"enable/disable ftrace tracepoints dynamically"
This was written before tracepoints were added to the kernel,
but now that tracepoints have been added, this is very confusing
and has confused people enough to give wrong information during
presentations.
Not only that, I looked at the help text, and it still references
that dreaded daemon that use to wake up once a second to update
the nop locations and brick NICs, that hasn't been around for over
five years.
Time to bring the text up to the current decade.
Reported-by: Ezequiel Garcia <elezegarcia@gmail.com>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit e5ab012c3271990e8457055c25cafddc1ae8aa6b upstream.
As it stands, irq_exit() may or may not be called with
irqs disabled, depending on __ARCH_IRQ_EXIT_IRQS_DISABLED
that the arch can define.
It makes tick_nohz_irq_exit() unsafe. For example two
interrupts can race in tick_nohz_stop_sched_tick(): the inner
most one computes the expiring time on top of the timer list,
then it's interrupted right before reprogramming the
clock. The new interrupt enqueues a new timer list timer,
it reprogram the clock to take it into account and it exits.
The CPUs resumes the inner most interrupt and performs the clock
reprogramming without considering the new timer list timer.
This regression has been introduced by:
280f06774afedf849f0b34248ed6aff57d0f6908
("nohz: Separate out irq exit and idle loop dyntick logic")
Let's fix it right now with the appropriate protections.
A saner long term solution will be to remove
__ARCH_IRQ_EXIT_IRQS_DISABLED and mandate that irq_exit() is called
with interrupts disabled.
Signed-off-by: Frederic Weisbecker <fweisbec@gmail.com>
Cc: Peter Zijlstra <peterz@infradead.org>
Cc: Ingo Molnar <mingo@kernel.org>
Cc: Linus Torvalds <torvalds@linuxfoundation.org>
Link: http://lkml.kernel.org/r/1361373336-11337-1-git-send-email-fweisbec@gmail.com
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 71b5707e119653039e6e95213f00479668c79b75 upstream.
In cgroup_exit() put_css_set_taskexit() is called without any lock,
which might lead to accessing a freed cgroup:
thread1 thread2
---------------------------------------------
exit()
cgroup_exit()
put_css_set_taskexit()
atomic_dec(cgrp->count);
rmdir();
/* not safe !! */
check_for_release(cgrp);
rcu_read_lock() can be used to make sure the cgroup is alive.
Signed-off-by: Li Zefan <lizefan@huawei.com>
Signed-off-by: Tejun Heo <tj@kernel.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 63f43f55c9bbc14f76b582644019b8a07dc8219a upstream.
rename() will change dentry->d_name. The result of this race can
be worse than seeing partially rewritten name, but we might access
a stale pointer because rename() will re-allocate memory to hold
a longer name.
It's safe in the protection of dentry->d_lock.
v2: check NULL dentry before acquiring dentry lock.
Signed-off-by: Li Zefan <lizefan@huawei.com>
Signed-off-by: Tejun Heo <tj@kernel.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit a2c1c57be8d9fd5b716113c8991d3d702eeacf77 upstream.
To avoid executing the same work item concurrenlty, workqueue hashes
currently busy workers according to their current work items and looks
up the the table when it wants to execute a new work item. If there
already is a worker which is executing the new work item, the new item
is queued to the found worker so that it gets executed only after the
current execution finishes.
Unfortunately, a work item may be freed while being executed and thus
recycled for different purposes. If it gets recycled for a different
work item and queued while the previous execution is still in
progress, workqueue may make the new work item wait for the old one
although the two aren't really related in any way.
In extreme cases, this false dependency may lead to deadlock although
it's extremely unlikely given that there aren't too many self-freeing
work item users and they usually don't wait for other work items.
To alleviate the problem, record the current work function in each
busy worker and match it together with the work item address in
find_worker_executing_work(). While this isn't complete, it ensures
that unrelated work items don't interact with each other and in the
very unlikely case where a twisted wq user triggers it, it's always
onto itself making the culprit easy to spot.
Signed-off-by: Tejun Heo <tj@kernel.org>
Reported-by: Andrey Isakov <andy51@gmx.ru>
Bugzilla: https://bugzilla.kernel.org/show_bug.cgi?id=51701
Cc: stable@vger.kernel.org
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit df1778be1a33edffa51d094eeda87c858ded6560 upstream.
The null check of `strchr() + 1' is broken, which is always non-null,
leading to OOB read. Instead, check the result of strchr().
Signed-off-by: Xi Wang <xi.wang@gmail.com>
Cc: "Eric W. Biederman" <ebiederm@xmission.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
| |
commit 8c189ea64eea01ca20d102ddb74d6936dd16c579 upstream.
Commit: c1bf08ac "ftrace: Be first to run code modification on modules"
changed ftrace module notifier's priority to INT_MAX in order to
process the ftrace nops before anything else could touch them
(namely kprobes). This was the correct thing to do.
Unfortunately, the ftrace module notifier also contains the ftrace
clean up code. As opposed to the set up code, this code should be
run *after* all the module notifiers have run in case a module is doing
correct clean-up and unregisters its ftrace hooks. Basically, ftrace
needs to do clean up on module removal, as it needs to know about code
being removed so that it doesn't try to modify that code. But after it
removes the module from its records, if a ftrace user tries to remove
a probe, that removal will fail due as the record of that code segment
no longer exists.
Nothing really bad happens if the probe removal is called after ftrace
did the clean up, but the ftrace removal function will return an error.
Correct code (such as kprobes) will produce a WARN_ON() if it fails
to remove the probe. As people get annoyed by frivolous warnings, it's
best to do the ftrace clean up after everything else.
By splitting the ftrace_module_notifier into two notifiers, one that
does the module load setup that is run at high priority, and the other
that is called for module clean up that is run at low priority, the
problem is solved.
Reported-by: Frank Ch. Eigler <fche@redhat.com>
Acked-by: Masami Hiramatsu <masami.hiramatsu.pt@hitachi.com>
Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|