aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* misc: remove __dev* attributes.Greg Kroah-Hartman2013-01-031-2/+2
| | | | | | | | | | | | | | CONFIG_HOTPLUG is going away as an option. As a result, the __dev* markings need to be removed. This change removes the last of the __dev* markings from the kernel from a variety of different, tiny, places. Based on patches originally written by Bill Pemberton, but redone by me in order to handle some of the coding style issues better, by hand. Cc: Bill Pemberton <wfp5p@virginia.edu> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* samples/rpmsg: add an rpmsg driver sampleOhad Ben-Cohen2012-02-082-0/+101
Add an rpmsg driver sample, which demonstrates how to communicate with an AMP-configured remote processor over the rpmsg bus. Note how once probed, the driver can immediately start sending messages using the rpmsg_send() API, without having to worry about creating endpoints or allocating rpmsg addresses: all that work is done by the rpmsg bus, and the required information is already embedded in the rpmsg channel that the driver is probed with. In this sample, the driver simply sends a "Hello World!" message to the remote processor repeatedly. Designed with Brian Swetland <swetland@google.com>. Signed-off-by: Ohad Ben-Cohen <ohad@wizery.com> Cc: Brian Swetland <swetland@google.com> Cc: Arnd Bergmann <arnd@arndb.de> Cc: Grant Likely <grant.likely@secretlab.ca> Cc: Tony Lindgren <tony@atomide.com> Cc: Russell King <linux@arm.linux.org.uk> Cc: Rusty Russell <rusty@rustcorp.com.au> Cc: Andrew Morton <akpm@linux-foundation.org> Cc: Greg KH <greg@kroah.com> Cc: Stephen Boyd <sboyd@codeaurora.org>