aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* samples/seccomp: be less stupid about cross compilingArnd Bergmann2013-02-051-0/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | The seccomp filters are currently built for the build host, not for the machine that they are going to run on, but they are also built for with the -m32 flag if the kernel is built for a 32 bit machine, both of which seems rather odd. It broke allyesconfig on my machine, which is x86-64, but building for 32 bit ARM, with this error message: In file included from /usr/include/stdio.h:28:0, from samples/seccomp/bpf-fancy.c:15: /usr/include/features.h:324:26: fatal error: bits/predefs.h: No such file or directory because there are no 32 bit libc headers installed on this machine. We should really be building all the samples for the target machine rather than the build host, but since the infrastructure for that appears to be missing right now, let's be a little bit smarter and not pass the '-m32' flag to the HOSTCC when cross- compiling. Signed-off-by: Arnd Bergmann <arnd@arndb.de> Acked-by: Kees Cook <keescook@chromium.org> Cc: Heiko Carstens <heiko.carstens@de.ibm.com> Cc: James Morris <james.l.morris@oracle.com> Acked-by: Will Drewry <wad@chromium.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* misc: remove __dev* attributes.Greg Kroah-Hartman2013-01-031-2/+2
| | | | | | | | | | | | | | CONFIG_HOTPLUG is going away as an option. As a result, the __dev* markings need to be removed. This change removes the last of the __dev* markings from the kernel from a variety of different, tiny, places. Based on patches originally written by Bill Pemberton, but redone by me in order to handle some of the coding style issues better, by hand. Cc: Bill Pemberton <wfp5p@virginia.edu> Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
* samples/seccomp: fix 31 bit build on s390Heiko Carstens2012-09-111-8/+16
| | | | | | | | | | | | | | | On s390 the flag to force 31 builds is -m31 instead of -m32 unlike on all (?) other architectures. Fixes this compile error: HOSTCC samples/seccomp/bpf-direct.o cc1: error: unrecognized command line option "-m32" make[2]: *** [samples/seccomp/bpf-direct.o] Error 1 Signed-off-by: Heiko Carstens <heiko.carstens@de.ibm.com> Acked-by: Kees Cook <keescook@chromium.org> Signed-off-by: James Morris <james.l.morris@oracle.com>
* Merge tag 'v3.6-rc2' into nextJames Morris2012-08-172-0/+391
|\ | | | | | | | | | | Linux 3.6-rc2 Resync with Linus.
| * Merge branch 'for-linus' of ↵Linus Torvalds2012-07-242-0/+391
| |\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/jikos/hid Pull HID updates from Jiri Kosina: "The list of changes worth pointing out explicitly: - We are getting 'UHID', which is a new framework for implementing HID transport drivers in userspace (this is different from HIDRAW, which is transport-independent and provides report parsing facilities; uhid is for the other (transport) part of the pipeline). It's needed for (and currently being used by) Bluetooth-LowEnergy, as its specification mandates things we don't want in the kernel. Written by David Herrmann. - there have been quite a few bugs in runtime suspend/resume paths (probably never reported to actually happen in the wild, but still). Alan Stern fixed those. - a few other driver updates and fixes and random new device support." * 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/jikos/hid: (45 commits) HID: add ASUS AIO keyboard model AK1D HID: add support for Cypress barcode scanner 04B4:ED81 HID: Allow drivers to be their own listener HID: usbhid: fix error paths in suspend HID: usbhid: check for suspend or reset before restarting HID: usbhid: replace HID_REPORTED_IDLE with HID_SUSPENDED HID: usbhid: inline some simple routines HID: usbhid: fix autosuspend calls HID: usbhid: fix use-after-free bug HID: hid-core: optimize in case of hidraw HID: hidraw: fix list->buffer memleak HID: uhid: Fix sending events with invalid data HID: roccat: added sensor sysfs attribute for Savu HID: Add driver for Holtek based keyboards with broken HID HID: Add suport for the brightness control keys on HP keyboards HID: magicmouse: Implement Multi-touch Protocol B (MT-B) HID: magicmouse: Removing report_touches switch HID: roccat: rename roccat_common functions to roccat_common2 HID: roccat: fix wrong hid_err usage on struct usb_device HID: roccat: move functionality to roccat-common ...
| | * HID: uhid: add example programDavid Herrmann2012-06-182-0/+391
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This adds an example user-space program that emulates a 3 button mouse with wheel. It detects keyboard presses and moves the mouse accordingly. It register a fake HID device to feed the raw HID reports into the kernel. In this example, you could use uinput to get the same result, but this shows how to get the same behavior with uhid so you don't need HID parsers in user-space. Signed-off-by: David Herrmann <dh.herrmann@googlemail.com> Signed-off-by: Jiri Kosina <jkosina@suse.cz>
* | | samples/seccomp: fix endianness bug in LO_ARG defineHeiko Carstens2012-08-021-5/+10
|/ / | | | | | | | | | | | | | | | | | | | | | | The LO_ARG define needs to consider endianness also for 32 bit builds. The "bpf_fancy" test case didn't work on s390 in 32 bit and compat mode because the LO_ARG define resulted in a BPF program which read the upper halve of the 64 bit system call arguments instead of the lower halves. Signed-off-by: Heiko Carstens <heiko.carstens@de.ibm.com> Acked-by: Kees Cook <keescook@chromium.org> Signed-off-by: James Morris <james.l.morris@oracle.com>
* / samples: seccomp: add .gitignore for untracked executablesChad Williamson2012-06-281-0/+3
|/ | | | | | | | | | | git status should be clean following make allmodconfig && make. Add a .gitignore file to the samples/seccomp directory to ignore binaries produced there. Signed-off-by: Chad Williamson <chad@dahc.us> Reviewed-By: Will Drewry <wad@chromium.org> Acked-by: Kees Cook <keescook@chromium.org> Signed-off-by: James Morris <james.l.morris@oracle.com>
* samples/seccomp: fix dependencies on arch macrosWill Drewry2012-04-182-11/+19
| | | | | | | | | | | | | | | | | | | | | | | This change fixes the compilation error triggered here for i386 allmodconfig in linux-next: http://kisskb.ellerman.id.au/kisskb/buildresult/6123842/ Logic attempting to predict the host architecture has been removed from the Makefile. Instead, the bpf-direct sample should now compile on any architecture, but if the architecture is not supported, it will compile a minimal main() function. This change also ensures the samples are not compiled when there is no seccomp filter support. (Note, I wasn't able to reproduce the error locally, but the existing approach was clearly flawed. This tweak should resolve your issue and avoid other future weirdness.) Reported-by: Paul Gortmaker <paul.gortmaker@windriver.com> Suggested-by: Kees Cook <keescook@chromium.org> Signed-off-by: Will Drewry <wad@chromium.org> Signed-off-by: James Morris <james.l.morris@oracle.com>
* Documentation: prctl/seccomp_filterWill Drewry2012-04-137-1/+712
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Documents how system call filtering using Berkeley Packet Filter programs works and how it may be used. Includes an example for x86 and a semi-generic example using a macro-based code generator. Acked-by: Eric Paris <eparis@redhat.com> Signed-off-by: Will Drewry <wad@chromium.org> Acked-by: Kees Cook <keescook@chromium.org> v18: - added acked by - update no new privs numbers v17: - remove @compat note and add Pitfalls section for arch checking (keescook@chromium.org) v16: - v15: - v14: - rebase/nochanges v13: - rebase on to 88ebdda6159ffc15699f204c33feb3e431bf9bdc v12: - comment on the ptrace_event use - update arch support comment - note the behavior of SECCOMP_RET_DATA when there are multiple filters (keescook@chromium.org) - lots of samples/ clean up incl 64-bit bpf-direct support (markus@chromium.org) - rebase to linux-next v11: - overhaul return value language, updates (keescook@chromium.org) - comment on do_exit(SIGSYS) v10: - update for SIGSYS - update for new seccomp_data layout - update for ptrace option use v9: - updated bpf-direct.c for SIGILL v8: - add PR_SET_NO_NEW_PRIVS to the samples. v7: - updated for all the new stuff in v7: TRAP, TRACE - only talk about PR_SET_SECCOMP now - fixed bad JLE32 check (coreyb@linux.vnet.ibm.com) - adds dropper.c: a simple system call disabler v6: - tweak the language to note the requirement of PR_SET_NO_NEW_PRIVS being called prior to use. (luto@mit.edu) v5: - update sample to use system call arguments - adds a "fancy" example using a macro-based generator - cleaned up bpf in the sample - update docs to mention arguments - fix prctl value (eparis@redhat.com) - language cleanup (rdunlap@xenotime.net) v4: - update for no_new_privs use - minor tweaks v3: - call out BPF <-> Berkeley Packet Filter (rdunlap@xenotime.net) - document use of tentative always-unprivileged - guard sample compilation for i386 and x86_64 v2: - move code to samples (corbet@lwn.net) Signed-off-by: James Morris <james.l.morris@oracle.com>
* samples/rpmsg: add an rpmsg driver sampleOhad Ben-Cohen2012-02-084-1/+110
| | | | | | | | | | | | | | | | | | | | | | | | | | | Add an rpmsg driver sample, which demonstrates how to communicate with an AMP-configured remote processor over the rpmsg bus. Note how once probed, the driver can immediately start sending messages using the rpmsg_send() API, without having to worry about creating endpoints or allocating rpmsg addresses: all that work is done by the rpmsg bus, and the required information is already embedded in the rpmsg channel that the driver is probed with. In this sample, the driver simply sends a "Hello World!" message to the remote processor repeatedly. Designed with Brian Swetland <swetland@google.com>. Signed-off-by: Ohad Ben-Cohen <ohad@wizery.com> Cc: Brian Swetland <swetland@google.com> Cc: Arnd Bergmann <arnd@arndb.de> Cc: Grant Likely <grant.likely@secretlab.ca> Cc: Tony Lindgren <tony@atomide.com> Cc: Russell King <linux@arm.linux.org.uk> Cc: Rusty Russell <rusty@rustcorp.com.au> Cc: Andrew Morton <akpm@linux-foundation.org> Cc: Greg KH <greg@kroah.com> Cc: Stephen Boyd <sboyd@codeaurora.org>
* samples: drop unused Kconfig symbolPaul Bolle2011-10-311-6/+0
| | | | | Signed-off-by: Paul Bolle <pebolle@tiscali.nl> Signed-off-by: Michal Marek <mmarek@suse.cz>
* perf: Add context field to perf_eventAvi Kivity2011-07-011-1/+1
| | | | | | | | | | | | | | | | | The perf_event overflow handler does not receive any caller-derived argument, so many callers need to resort to looking up the perf_event in their local data structure. This is ugly and doesn't scale if a single callback services many perf_events. Fix by adding a context parameter to perf_event_create_kernel_counter() (and derived hardware breakpoints APIs) and storing it in the perf_event. The field can be accessed from the callback as event->overflow_handler_context. All callers are updated. Signed-off-by: Avi Kivity <avi@redhat.com> Signed-off-by: Peter Zijlstra <a.p.zijlstra@chello.nl> Link: http://lkml.kernel.org/r/1309362157-6596-2-git-send-email-avi@redhat.com Signed-off-by: Ingo Molnar <mingo@elte.hu>
* perf: Remove the nmi parameter from the swevent and overflow interfacePeter Zijlstra2011-07-011-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The nmi parameter indicated if we could do wakeups from the current context, if not, we would set some state and self-IPI and let the resulting interrupt do the wakeup. For the various event classes: - hardware: nmi=0; PMI is in fact an NMI or we run irq_work_run from the PMI-tail (ARM etc.) - tracepoint: nmi=0; since tracepoint could be from NMI context. - software: nmi=[0,1]; some, like the schedule thing cannot perform wakeups, and hence need 0. As one can see, there is very little nmi=1 usage, and the down-side of not using it is that on some platforms some software events can have a jiffy delay in wakeup (when arch_irq_work_raise isn't implemented). The up-side however is that we can remove the nmi parameter and save a bunch of conditionals in fast paths. Signed-off-by: Peter Zijlstra <a.p.zijlstra@chello.nl> Cc: Michael Cree <mcree@orcon.net.nz> Cc: Will Deacon <will.deacon@arm.com> Cc: Deng-Cheng Zhu <dengcheng.zhu@gmail.com> Cc: Anton Blanchard <anton@samba.org> Cc: Eric B Munson <emunson@mgebm.net> Cc: Heiko Carstens <heiko.carstens@de.ibm.com> Cc: Paul Mundt <lethal@linux-sh.org> Cc: David S. Miller <davem@davemloft.net> Cc: Frederic Weisbecker <fweisbec@gmail.com> Cc: Jason Wessel <jason.wessel@windriver.com> Cc: Don Zickus <dzickus@redhat.com> Link: http://lkml.kernel.org/n/tip-agjev8eu666tvknpb3iaj0fg@git.kernel.org Signed-off-by: Ingo Molnar <mingo@elte.hu>
*-. Merge branches 'doc', 'multitouch', 'upstream' and 'upstream-fixes' into ↵Jiri Kosina2011-05-232-2/+2
|\ \ | | | | | | | | | for-linus
| | * Fix common misspellingsLucas De Marchi2011-03-312-2/+2
| |/ | | | | | | | | | | Fixes generated by 'codespell' and manually reviewed. Signed-off-by: Lucas De Marchi <lucas.demarchi@profusion.mobi>
* | HID: hid-example: fix some build issuesRandy Dunlap2011-04-212-2/+4
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | samples/hid-example.o needs some Kconfig and Makefile additions in order to build. It should use <linux/*.h> headers from the build tree, so use HEADERS_CHECK to require that those header files be present. Change the kconfig symbol from tristate to bool since userspace cannot be built as loadable modules. However, I don't understand why the userspace header files are not present as reported in Andrew's build log, since it builds OK on x86_64 without any of these changes. Signed-off-by: Randy Dunlap <randy.dunlap@oracle.com> Cc: Alan Ott <alan@signal11.us> Cc: Jiri Kosina <jkosina@suse.cz> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Jiri Kosina <jkosina@suse.cz>
* | HID: hidraw: fix samples miscompilationJiri Kosina2011-04-081-0/+11
| | | | | | | | | | | | | | | | | | | | | | | | On systems where userspace doesn't have new hidraw.h populated to /usr/include, the hidraw sample won't compile as it's missing the new ioctl defitions. Introduce temporary ugly workaround to define the ioctls "manually" in such cases, just to avoid miscompilation in allmodconfig cases. Reported-by: Stephen Rothwell <sfr@canb.auug.org.au> Signed-off-by: Jiri Kosina <jkosina@suse.cz>
* | HID: Documentation for hidrawAlan Ott2011-03-224-1/+182
|/ | | | | | | Documenation for the hidraw driver, with sample program. Signed-off-by: Alan Ott <alan@signal11.us> Signed-off-by: Jiri Kosina <jkosina@suse.cz>
* kdb: Add kdb kernel module sampleJason Wessel2010-10-294-1/+69
| | | | | | | Add an example of how to add a dynamic kdb shell command via a kernel module. Signed-off-by: Jason Wessel <jason.wessel@windriver.com>
* Merge branch 'llseek' of git://git.kernel.org/pub/scm/linux/kernel/git/arnd/bklLinus Torvalds2010-10-224-0/+4
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | * 'llseek' of git://git.kernel.org/pub/scm/linux/kernel/git/arnd/bkl: vfs: make no_llseek the default vfs: don't use BKL in default_llseek llseek: automatically add .llseek fop libfs: use generic_file_llseek for simple_attr mac80211: disallow seeks in minstrel debug code lirc: make chardev nonseekable viotape: use noop_llseek raw: use explicit llseek file operations ibmasmfs: use generic_file_llseek spufs: use llseek in all file operations arm/omap: use generic_file_llseek in iommu_debug lkdtm: use generic_file_llseek in debugfs net/wireless: use generic_file_llseek in debugfs drm: use noop_llseek
| * llseek: automatically add .llseek fopArnd Bergmann2010-10-154-0/+4
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | All file_operations should get a .llseek operation so we can make nonseekable_open the default for future file operations without a .llseek pointer. The three cases that we can automatically detect are no_llseek, seq_lseek and default_llseek. For cases where we can we can automatically prove that the file offset is always ignored, we use noop_llseek, which maintains the current behavior of not returning an error from a seek. New drivers should normally not use noop_llseek but instead use no_llseek and call nonseekable_open at open time. Existing drivers can be converted to do the same when the maintainer knows for certain that no user code relies on calling seek on the device file. The generated code is often incorrectly indented and right now contains comments that clarify for each added line why a specific variant was chosen. In the version that gets submitted upstream, the comments will be gone and I will manually fix the indentation, because there does not seem to be a way to do that using coccinelle. Some amount of new code is currently sitting in linux-next that should get the same modifications, which I will do at the end of the merge window. Many thanks to Julia Lawall for helping me learn to write a semantic patch that does all this. ===== begin semantic patch ===== // This adds an llseek= method to all file operations, // as a preparation for making no_llseek the default. // // The rules are // - use no_llseek explicitly if we do nonseekable_open // - use seq_lseek for sequential files // - use default_llseek if we know we access f_pos // - use noop_llseek if we know we don't access f_pos, // but we still want to allow users to call lseek // @ open1 exists @ identifier nested_open; @@ nested_open(...) { <+... nonseekable_open(...) ...+> } @ open exists@ identifier open_f; identifier i, f; identifier open1.nested_open; @@ int open_f(struct inode *i, struct file *f) { <+... ( nonseekable_open(...) | nested_open(...) ) ...+> } @ read disable optional_qualifier exists @ identifier read_f; identifier f, p, s, off; type ssize_t, size_t, loff_t; expression E; identifier func; @@ ssize_t read_f(struct file *f, char *p, size_t s, loff_t *off) { <+... ( *off = E | *off += E | func(..., off, ...) | E = *off ) ...+> } @ read_no_fpos disable optional_qualifier exists @ identifier read_f; identifier f, p, s, off; type ssize_t, size_t, loff_t; @@ ssize_t read_f(struct file *f, char *p, size_t s, loff_t *off) { ... when != off } @ write @ identifier write_f; identifier f, p, s, off; type ssize_t, size_t, loff_t; expression E; identifier func; @@ ssize_t write_f(struct file *f, const char *p, size_t s, loff_t *off) { <+... ( *off = E | *off += E | func(..., off, ...) | E = *off ) ...+> } @ write_no_fpos @ identifier write_f; identifier f, p, s, off; type ssize_t, size_t, loff_t; @@ ssize_t write_f(struct file *f, const char *p, size_t s, loff_t *off) { ... when != off } @ fops0 @ identifier fops; @@ struct file_operations fops = { ... }; @ has_llseek depends on fops0 @ identifier fops0.fops; identifier llseek_f; @@ struct file_operations fops = { ... .llseek = llseek_f, ... }; @ has_read depends on fops0 @ identifier fops0.fops; identifier read_f; @@ struct file_operations fops = { ... .read = read_f, ... }; @ has_write depends on fops0 @ identifier fops0.fops; identifier write_f; @@ struct file_operations fops = { ... .write = write_f, ... }; @ has_open depends on fops0 @ identifier fops0.fops; identifier open_f; @@ struct file_operations fops = { ... .open = open_f, ... }; // use no_llseek if we call nonseekable_open //////////////////////////////////////////// @ nonseekable1 depends on !has_llseek && has_open @ identifier fops0.fops; identifier nso ~= "nonseekable_open"; @@ struct file_operations fops = { ... .open = nso, ... +.llseek = no_llseek, /* nonseekable */ }; @ nonseekable2 depends on !has_llseek @ identifier fops0.fops; identifier open.open_f; @@ struct file_operations fops = { ... .open = open_f, ... +.llseek = no_llseek, /* open uses nonseekable */ }; // use seq_lseek for sequential files ///////////////////////////////////// @ seq depends on !has_llseek @ identifier fops0.fops; identifier sr ~= "seq_read"; @@ struct file_operations fops = { ... .read = sr, ... +.llseek = seq_lseek, /* we have seq_read */ }; // use default_llseek if there is a readdir /////////////////////////////////////////// @ fops1 depends on !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier readdir_e; @@ // any other fop is used that changes pos struct file_operations fops = { ... .readdir = readdir_e, ... +.llseek = default_llseek, /* readdir is present */ }; // use default_llseek if at least one of read/write touches f_pos ///////////////////////////////////////////////////////////////// @ fops2 depends on !fops1 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier read.read_f; @@ // read fops use offset struct file_operations fops = { ... .read = read_f, ... +.llseek = default_llseek, /* read accesses f_pos */ }; @ fops3 depends on !fops1 && !fops2 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier write.write_f; @@ // write fops use offset struct file_operations fops = { ... .write = write_f, ... + .llseek = default_llseek, /* write accesses f_pos */ }; // Use noop_llseek if neither read nor write accesses f_pos /////////////////////////////////////////////////////////// @ fops4 depends on !fops1 && !fops2 && !fops3 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier read_no_fpos.read_f; identifier write_no_fpos.write_f; @@ // write fops use offset struct file_operations fops = { ... .write = write_f, .read = read_f, ... +.llseek = noop_llseek, /* read and write both use no f_pos */ }; @ depends on has_write && !has_read && !fops1 && !fops2 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier write_no_fpos.write_f; @@ struct file_operations fops = { ... .write = write_f, ... +.llseek = noop_llseek, /* write uses no f_pos */ }; @ depends on has_read && !has_write && !fops1 && !fops2 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; identifier read_no_fpos.read_f; @@ struct file_operations fops = { ... .read = read_f, ... +.llseek = noop_llseek, /* read uses no f_pos */ }; @ depends on !has_read && !has_write && !fops1 && !fops2 && !has_llseek && !nonseekable1 && !nonseekable2 && !seq @ identifier fops0.fops; @@ struct file_operations fops = { ... +.llseek = noop_llseek, /* no read or write fn */ }; ===== End semantic patch ===== Signed-off-by: Arnd Bergmann <arnd@arndb.de> Cc: Julia Lawall <julia@diku.dk> Cc: Christoph Hellwig <hch@infradead.org>
* | kfifo: fix scatterlist usageIra W. Snyder2010-10-011-8/+9
|/ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The kfifo_dma family of functions use sg_mark_end() on the last element in their scatterlist. This forces use of a fresh scatterlist for each DMA operation, which makes recycling a single scatterlist impossible. Change the behavior of the kfifo_dma functions to match the usage of the dma_map_sg function. This means that users must respect the returned nents value. The sample code is updated to reflect the change. This bug is trivial to cause: call kfifo_dma_in_prepare() such that it prepares a scatterlist with a single entry comprising the whole fifo. This is the case when you map the entirety of a newly created empty fifo. This causes the setup_sgl() function to mark the first scatterlist entry as the end of the chain, no matter what comes after it. Afterwards, add and remove some data from the fifo such that another call to kfifo_dma_in_prepare() will create two scatterlist entries. It returns nents=2. However, due to the previous sg_mark_end() call, sg_is_last() will now return true for the first scatterlist element. This causes the sample code to print a single scatterlist element when it should print two. By removing the call to sg_mark_end(), we make the API as similar as possible to the DMA mapping API. All users are required to respect the returned nents. Signed-off-by: Ira W. Snyder <iws@ovro.caltech.edu> Cc: Stefani Seibold <stefani@seibold.net> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* kfifo: add explicit error checking in all the examplesAndrea Righi2010-08-204-51/+144
| | | | | | | | | | Provide a check in all the kfifo examples to validate the correct execution of each testcase. Signed-off-by: Andrea Righi <arighi@develer.com> Acked-by: Stefani Seibold <stefani@seibold.net> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* kfifo: fix a memory leak in dma exampleAndrea Righi2010-08-201-3/+1
| | | | | | | | | | We use a dynamically allocated kfifo in the dma example, so we need to free it when unloading the module. Signed-off-by: Andrea Righi <arighi@develer.com> Acked-by: Stefani Seibold <stefani@seibold.net> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* kfifo: fix kernel BUG in dma exampleAndrea Righi2010-08-201-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The scatterlist is used uninitialized in kfifo_dma_in_prepare(). This triggers the following bug if CONFIG_DEBUG_SG=y: ------------[ cut here ]------------ kernel BUG at include/linux/scatterlist.h:65! invalid opcode: 0000 [#1] PREEMPT SMP ... Call Trace: [<ffffffff810a1eab>] setup_sgl+0x6b/0xe0 [<ffffffffa03d7000>] ? example_init+0x0/0x265 [dma_example] [<ffffffff810a2021>] __kfifo_dma_in_prepare+0x21/0x30 [<ffffffffa03d7124>] example_init+0x124/0x265 [dma_example] [<ffffffff810f9c55>] ? trace_module_notify+0x25/0x370 [<ffffffff81110c6e>] ? free_pages_prepare+0x11e/0x1e0 [<ffffffff8106f2b1>] ? get_parent_ip+0x11/0x50 [<ffffffff810f9c55>] ? trace_module_notify+0x25/0x370 [<ffffffff810b65fd>] ? trace_hardirqs_on+0xd/0x10 [<ffffffff814beade>] ? mutex_unlock+0xe/0x10 [<ffffffff810f9c71>] ? trace_module_notify+0x41/0x370 [<ffffffff810a77d5>] ? __blocking_notifier_call_chain+0x45/0x80 [<ffffffff81137b7a>] ? vfree+0x2a/0x30 [<ffffffff810a6ac3>] ? up_read+0x23/0x40 [<ffffffff810a77f5>] ? __blocking_notifier_call_chain+0x65/0x80 [<ffffffff810001e3>] do_one_initcall+0x43/0x180 [<ffffffff810c577a>] sys_init_module+0xba/0x200 [<ffffffff8103819b>] system_call_fastpath+0x16/0x1b RIP [<ffffffff810a1e31>] setup_sgl_buf+0x1a1/0x1b0 RSP <ffff88006720dc98> ---[ end trace a72b979fd3c1d3a5 ]--- Add the proper initialization to avoid the bug. Signed-off-by: Andrea Righi <arighi@develer.com> Acked-by: Stefani Seibold <stefani@seibold.net> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* kfifo: add explicit error checking in byte stream exampleAndrea Righi2010-08-201-6/+27
| | | | | | | | | | | Provide a static array of expected items that kfifo should contain at the end of the test to validate it. Signed-off-by: Andrea Righi <arighi@develer.com> Cc: Stefani Seibold <stefani@seibold.net> Cc: Greg KH <greg@kroah.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* kfifo: add kfifo_skip() testcaseAndrea Righi2010-08-201-0/+4
| | | | | | | | | | Add a testcase for kfifo_skip() to the byte stream fifo example. Signed-off-by: Andrea Righi <arighi@develer.com> Cc: Greg KH <greg@kroah.com> Acked-by: Stefani Seibold <stefani@seibold.net> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* kfifo: add example files to the kernel sample directoryStefani Seibold2010-08-117-1/+614
| | | | | | | | | | | | | | | | Add four examples to the kernel sample directory. It shows how to handle: - a byte stream fifo - a integer type fifo - a dynamic record sized fifo - the fifo DMA functions [akpm@linux-foundation.org: coding-style fixes] Signed-off-by: Stefani Seibold <stefani@seibold.net> Cc: Greg KH <greg@kroah.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* SAMPLES: kprobe_example: Make it print something on MIPS.David Daney2010-08-051-0/+9
| | | | | | | | | | | | | | | | This KProbes example is a little useless if it doesn't print anything. For MIPS print similar messages to those produced on x86 and PPC. Signed-off-by: David Daney <ddaney@caviumnetworks.com> To: linux-mips@linux-mips.org To: ananth@in.ibm.com To: anil.s.keshavamurthy@intel.com To: davem@davemloft.net To: masami.hiramatsu.pt@hitachi.com Cc: linux-kernel@vger.kernel.org Cc: hschauhan@nulltrace.org Patchwork: https://patchwork.linux-mips.org/patch/1528/ Signed-off-by: Ralf Baechle <ralf@linux-mips.org>
* tracing: Let tracepoints have data passed to tracepoint callbacksSteven Rostedt2010-05-143-12/+12
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This patch adds data to be passed to tracepoint callbacks. The created functions from DECLARE_TRACE() now need a mandatory data parameter. For example: DECLARE_TRACE(mytracepoint, int value, value) Will create the register function: int register_trace_mytracepoint((void(*)(void *data, int value))probe, void *data); As the first argument, all callbacks (probes) must take a (void *data) parameter. So a callback for the above tracepoint will look like: void myprobe(void *data, int value) { } The callback may choose to ignore the data parameter. This change allows callbacks to register a private data pointer along with the function probe. void mycallback(void *data, int value); register_trace_mytracepoint(mycallback, mydata); Then the mycallback() will receive the "mydata" as the first parameter before the args. A more detailed example: DECLARE_TRACE(mytracepoint, TP_PROTO(int status), TP_ARGS(status)); /* In the C file */ DEFINE_TRACE(mytracepoint, TP_PROTO(int status), TP_ARGS(status)); [...] trace_mytracepoint(status); /* In a file registering this tracepoint */ int my_callback(void *data, int status) { struct my_struct my_data = data; [...] } [...] my_data = kmalloc(sizeof(*my_data), GFP_KERNEL); init_my_data(my_data); register_trace_mytracepoint(my_callback, my_data); The same callback can also be registered to the same tracepoint as long as the data registered is different. Note, the data must also be used to unregister the callback: unregister_trace_mytracepoint(my_callback, my_data); Because of the data parameter, tracepoints declared this way can not have no args. That is: DECLARE_TRACE(mytracepoint, TP_PROTO(void), TP_ARGS()); will cause an error. If no arguments are needed, a new macro can be used instead: DECLARE_TRACE_NOARGS(mytracepoint); Since there are no arguments, the proto and args fields are left out. This is part of a series to make the tracepoint footprint smaller: text data bss dec hex filename 4913961 1088356 861512 6863829 68bbd5 vmlinux.orig 4914025 1088868 861512 6864405 68be15 vmlinux.class 4918492 1084612 861512 6864616 68bee8 vmlinux.tracepoint Again, this patch also increases the size of the kernel, but lays the ground work for decreasing it. v5: Fixed net/core/drop_monitor.c to handle these updates. v4: Moved the DECLARE_TRACE() DECLARE_TRACE_NOARGS out of the #ifdef CONFIG_TRACE_POINTS, since the two are the same in both cases. The __DECLARE_TRACE() is what changes. Thanks to Frederic Weisbecker for pointing this out. v3: Made all register_* functions require data to be passed and all callbacks to take a void * parameter as its first argument. This makes the calling functions comply with C standards. Also added more comments to the modifications of DECLARE_TRACE(). v2: Made the DECLARE_TRACE() have the ability to pass arguments and added a new DECLARE_TRACE_NOARGS() for tracepoints that do not need any arguments. Acked-by: Mathieu Desnoyers <mathieu.desnoyers@efficios.com> Acked-by: Masami Hiramatsu <mhiramat@redhat.com> Acked-by: Frederic Weisbecker <fweisbec@gmail.com> Cc: Neil Horman <nhorman@tuxdriver.com> Cc: David S. Miller <davem@davemloft.net> Signed-off-by: Steven Rostedt <rostedt@goodmis.org>
* include cleanup: Update gfp.h and slab.h includes to prepare for breaking ↵Tejun Heo2010-03-301-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | implicit slab.h inclusion from percpu.h percpu.h is included by sched.h and module.h and thus ends up being included when building most .c files. percpu.h includes slab.h which in turn includes gfp.h making everything defined by the two files universally available and complicating inclusion dependencies. percpu.h -> slab.h dependency is about to be removed. Prepare for this change by updating users of gfp and slab facilities include those headers directly instead of assuming availability. As this conversion needs to touch large number of source files, the following script is used as the basis of conversion. http://userweb.kernel.org/~tj/misc/slabh-sweep.py The script does the followings. * Scan files for gfp and slab usages and update includes such that only the necessary includes are there. ie. if only gfp is used, gfp.h, if slab is used, slab.h. * When the script inserts a new include, it looks at the include blocks and try to put the new include such that its order conforms to its surrounding. It's put in the include block which contains core kernel includes, in the same order that the rest are ordered - alphabetical, Christmas tree, rev-Xmas-tree or at the end if there doesn't seem to be any matching order. * If the script can't find a place to put a new include (mostly because the file doesn't have fitting include block), it prints out an error message indicating which .h file needs to be added to the file. The conversion was done in the following steps. 1. The initial automatic conversion of all .c files updated slightly over 4000 files, deleting around 700 includes and adding ~480 gfp.h and ~3000 slab.h inclusions. The script emitted errors for ~400 files. 2. Each error was manually checked. Some didn't need the inclusion, some needed manual addition while adding it to implementation .h or embedding .c file was more appropriate for others. This step added inclusions to around 150 files. 3. The script was run again and the output was compared to the edits from #2 to make sure no file was left behind. 4. Several build tests were done and a couple of problems were fixed. e.g. lib/decompress_*.c used malloc/free() wrappers around slab APIs requiring slab.h to be added manually. 5. The script was run on all .h files but without automatically editing them as sprinkling gfp.h and slab.h inclusions around .h files could easily lead to inclusion dependency hell. Most gfp.h inclusion directives were ignored as stuff from gfp.h was usually wildly available and often used in preprocessor macros. Each slab.h inclusion directive was examined and added manually as necessary. 6. percpu.h was updated not to include slab.h. 7. Build test were done on the following configurations and failures were fixed. CONFIG_GCOV_KERNEL was turned off for all tests (as my distributed build env didn't work with gcov compiles) and a few more options had to be turned off depending on archs to make things build (like ipr on powerpc/64 which failed due to missing writeq). * x86 and x86_64 UP and SMP allmodconfig and a custom test config. * powerpc and powerpc64 SMP allmodconfig * sparc and sparc64 SMP allmodconfig * ia64 SMP allmodconfig * s390 SMP allmodconfig * alpha SMP allmodconfig * um on x86_64 SMP allmodconfig 8. percpu.h modifications were reverted so that it could be applied as a separate patch and serve as bisection point. Given the fact that I had only a couple of failures from tests on step 6, I'm fairly confident about the coverage of this conversion patch. If there is a breakage, it's likely to be something in one of the arch headers which should be easily discoverable easily on most builds of the specific arch. Signed-off-by: Tejun Heo <tj@kernel.org> Guess-its-ok-by: Christoph Lameter <cl@linux-foundation.org> Cc: Ingo Molnar <mingo@redhat.com> Cc: Lee Schermerhorn <Lee.Schermerhorn@hp.com>
* Merge commit 'v2.6.34-rc1' into perf/urgentIngo Molnar2010-03-092-5/+5
|\ | | | | | | | | | | | | | | | | Conflicts: tools/perf/util/probe-event.c Merge reason: Pick up -rc1 and resolve the conflict as well. Signed-off-by: Ingo Molnar <mingo@elte.hu>
| * Driver core: Constify struct sysfs_ops in struct kobj_typeEmese Revfy2010-03-071-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Constify struct sysfs_ops. This is part of the ops structure constification effort started by Arjan van de Ven et al. Benefits of this constification: * prevents modification of data that is shared (referenced) by many other structure instances at runtime * detects/prevents accidental (but not intentional) modification attempts on archs that enforce read-only kernel data at runtime * potentially better optimized code as the compiler can assume that the const data cannot be changed * the compiler/linker move const data into .rodata and therefore exclude them from false sharing Signed-off-by: Emese Revfy <re.emese@gmail.com> Acked-by: David Teigland <teigland@redhat.com> Acked-by: Matt Domsch <Matt_Domsch@dell.com> Acked-by: Maciej Sosnowski <maciej.sosnowski@intel.com> Acked-by: Hans J. Koch <hjk@linutronix.de> Acked-by: Pekka Enberg <penberg@cs.helsinki.fi> Acked-by: Jens Axboe <jens.axboe@oracle.com> Acked-by: Stephen Hemminger <shemminger@vyatta.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
| * kset-example: Spelling fixes.Radu Voicilas2010-03-071-2/+2
| | | | | | | | | | | | | | | | No change in functionality. Signed-off-by: Radu Voicilas <rvoicilas@gmail.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
| * kobject-example: Spelling fixes.Radu Voicilas2010-03-071-2/+2
| | | | | | | | | | | | | | | | No change in functionality. Signed-off-by: Radu Voicilas <rvoicilas@gmail.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* | percpu: Add __percpu sparse annotations to hw_breakpointTejun Heo2010-02-271-3/+3
|/ | | | | | | | | | | | | | | | | | | | Add __percpu sparse annotations to hw_breakpoint. These annotations are to make sparse consider percpu variables to be in a different address space and warn if accessed without going through percpu accessors. This patch doesn't affect normal builds. In kernel/hw_breakpoint.c, per_cpu(nr_task_bp_pinned, cpu)'s will trigger spurious noderef related warnings from sparse. Changing it to &per_cpu(nr_task_bp_pinned[0], cpu) will work around the problem but deemed to ugly by the maintainer. Leave it alone until better solution can be found. Signed-off-by: Tejun Heo <tj@kernel.org> Cc: Stephen Rothwell <sfr@canb.auug.org.au> Cc: K.Prasad <prasad@linux.vnet.ibm.com> LKML-Reference: <4B7B4B7A.9050902@kernel.org> Signed-off-by: Frederic Weisbecker <fweisbec@gmail.com>
* Merge branch 'perf-fixes-for-linus' of ↵Linus Torvalds2009-12-111-2/+5
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-2.6-tip * 'perf-fixes-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-2.6-tip: (57 commits) x86, perf events: Check if we have APIC enabled perf_event: Fix variable initialization in other codepaths perf kmem: Fix unused argument build warning perf symbols: perf_header__read_build_ids() offset'n'size should be u64 perf symbols: dsos__read_build_ids() should read both user and kernel buildids perf tools: Align long options which have no short forms perf kmem: Show usage if no option is specified sched: Mark sched_clock() as notrace perf sched: Add max delay time snapshot perf tools: Correct size given to memset perf_event: Fix perf_swevent_hrtimer() variable initialization perf sched: Fix for getting task's execution time tracing/kprobes: Fix field creation's bad error handling perf_event: Cleanup for cpu_clock_perf_event_update() perf_event: Allocate children's perf_event_ctxp at the right time perf_event: Clean up __perf_event_init_context() hw-breakpoints: Modify breakpoints without unregistering them perf probe: Update perf-probe document perf probe: Support --del option trace-kprobe: Support delete probe syntax ...
| * hw-breakpoints: Use overflow handler instead of the event callbackFrederic Weisbecker2009-12-061-2/+5
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | struct perf_event::event callback was called when a breakpoint triggers. But this is a rather opaque callback, pretty tied-only to the breakpoint API and not really integrated into perf as it triggers even when we don't overflow. We prefer to use overflow_handler() as it fits into the perf events rules, being called only when we overflow. Reported-by: Peter Zijlstra <peterz@infradead.org> Signed-off-by: Frederic Weisbecker <fweisbec@gmail.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Arnaldo Carvalho de Melo <acme@redhat.com> Cc: "K. Prasad" <prasad@linux.vnet.ibm.com>
* | Merge branch 'for-next' into for-linusJiri Kosina2009-12-071-3/+0
|\ \ | |/ |/| | | | | | | Conflicts: kernel/irq/chip.c
| * Kconfig: Remove useless and sometimes wrong commentsMichael Roth2009-11-091-3/+0
| | | | | | | | | | | | | | Additionally, some excessive newlines removed. Signed-off-by: Michael Roth <mroth@nessie.de> Signed-off-by: Jiri Kosina <jkosina@suse.cz>
* | hw-breakpoints: Use struct perf_event_attr to define kernel breakpointsFrederic Weisbecker2009-11-261-5/+5
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Kernel breakpoints are created using functions in which we pass breakpoint parameters as individual variables: address, length and type. Although it fits well for x86, this just does not scale across architectures that may support this api later as these may have more or different needs. Pass in a perf_event_attr structure instead because it is meant to evolve as much as possible into a generic hardware breakpoint parameter structure. Reported-by: K.Prasad <prasad@linux.vnet.ibm.com> Signed-off-by: Frederic Weisbecker <fweisbec@gmail.com> LKML-Reference: <1259294154-5197-2-git-send-regression-fweisbec@gmail.com> Signed-off-by: Ingo Molnar <mingo@elte.hu>
* | hw-breakpoints: Simplify error handling in breakpoint creation requestsFrederic Weisbecker2009-11-261-3/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This simplifies the error handling when we create a breakpoint. We don't need to check the NULL return value corner case anymore since we have improved perf_event_create_kernel_counter() to always return an error code in the failure case. Signed-off-by: Frederic Weisbecker <fweisbec@gmail.com> Cc: Peter Zijlstra <peterz@infradead.org> Cc: Arnaldo Carvalho de Melo <acme@redhat.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Steven Rostedt <rostedt@goodmis.org> Cc: Prasad <prasad@linux.vnet.ibm.com> LKML-Reference: <1259210142-5714-3-git-send-regression-fweisbec@gmail.com> Signed-off-by: Ingo Molnar <mingo@elte.hu>
* | hw-breakpoint: Attribute authorship of hw-breakpoint related filesK.Prasad2009-11-231-0/+2
| | | | | | | | | | | | | | | | | | | | | | | | Attribute authorship to developers of hw-breakpoint related files. Signed-off-by: K.Prasad <prasad@linux.vnet.ibm.com> Cc: Alan Stern <stern@rowland.harvard.edu> Cc: Frederic Weisbecker <fweisbec@gmail.com> LKML-Reference: <20091123154713.GA5593@in.ibm.com> [ v2: moved it to latest -tip ] Signed-off-by: Ingo Molnar <mingo@elte.hu>
* | hw-breakpoints: Fix broken hw-breakpoint sample moduleFrederic Weisbecker2009-11-101-19/+24
| | | | | | | | | | | | | | | | | | The hw-breakpoint sample module has been broken during the hw-breakpoint internals refactoring. Propagate the changes to it. Reported-by: "K. Prasad" <prasad@linux.vnet.ibm.com> Signed-off-by: Frederic Weisbecker <fweisbec@gmail.com>
* | Merge commit 'perf/core' into perf/hw-breakpointFrederic Weisbecker2009-10-177-159/+4
|\| | | | | | | | | | | | | | | | | | | | | | | Conflicts: kernel/Makefile kernel/trace/Makefile kernel/trace/trace.h samples/Makefile Merge reason: We need to be uptodate with the perf events development branch because we plan to rewrite the breakpoints API on top of perf events.
| * const: constify remaining file_operationsAlexey Dobriyan2009-10-011-1/+1
| | | | | | | | | | | | | | | | [akpm@linux-foundation.org: fix KVM] Signed-off-by: Alexey Dobriyan <adobriyan@gmail.com> Acked-by: Mike Frysinger <vapier@gentoo.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
| * tracing: Remove markersChristoph Hellwig2009-09-185-156/+1
| | | | | | | | | | | | | | | | | | | | | | | | Now that the last users of markers have migrated to the event tracer we can kill off the (now orphan) support code. Signed-off-by: Christoph Hellwig <hch@lst.de> Acked-by: Mathieu Desnoyers <mathieu.desnoyers@polymtl.ca> Cc: Steven Rostedt <rostedt@goodmis.org> Cc: Frederic Weisbecker <fweisbec@gmail.com> LKML-Reference: <20090917173527.GA1699@lst.de> Signed-off-by: Ingo Molnar <mingo@elte.hu>
| * debugfs: Change debuhgfs directory of trace-events-sample.hGeunSik Lim2009-09-151-1/+1
| | | | | | | | | | | | | | | | Default directory of debug filesystem for ftrace is /sys/kernel/debug/. Signed-off-by: GeunSik Lim <geunsik.lim@samsung.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* | Merge branch 'linus' into tracing/hw-breakpointsIngo Molnar2009-09-151-0/+1
|\| | | | | | | | | | | | | | | | | | | Conflicts: arch/x86/kernel/process_64.c Semantic conflict fixed in: arch/x86/kvm/x86.c Signed-off-by: Ingo Molnar <mingo@elte.hu>