aboutsummaryrefslogtreecommitdiffstats
blob: eb6791188cf51a19b22861ea23909f93be08935d (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
/*
 * linux/lib/cmdline.c
 * Helper functions generally used for parsing kernel command line
 * and module options.
 *
 * Code and copyrights come from init/main.c and arch/i386/kernel/setup.c.
 *
 * This source code is licensed under the GNU General Public License,
 * Version 2.  See the file COPYING for more details.
 *
 * GNU Indent formatting options for this file: -kr -i8 -npsl -pcs
 *
 */

#include <linux/export.h>
#include <linux/kernel.h>
#include <linux/string.h>

/*
 *	If a hyphen was found in get_option, this will handle the
 *	range of numbers, M-N.  This will expand the range and insert
 *	the values[M, M+1, ..., N] into the ints array in get_options.
 */

static int get_range(char **str, int *pint)
{
	int x, inc_counter, upper_range;

	(*str)++;
	upper_range = simple_strtol((*str), NULL, 0);
	inc_counter = upper_range - *pint;
	for (x = *pint; x < upper_range; x++)
		*pint++ = x;
	return inc_counter;
}

/**
 *	get_option - Parse integer from an option string
 *	@str: option string
 *	@pint: (output) integer value parsed from @str
 *
 *	Read an int from an option string; if available accept a subsequent
 *	comma as well.
 *
 *	Return values:
 *	0 - no int in string
 *	1 - int found, no subsequent comma
 *	2 - int found including a subsequent comma
 *	3 - hyphen found to denote a range
 */

int get_option (char **str, int *pint)
{
	char *cur = *str;

	if (!cur || !(*cur))
		return 0;
	*pint = simple_strtol (cur, str, 0);
	if (cur == *str)
		return 0;
	if (**str == ',') {
		(*str)++;
		return 2;
	}
	if (**str == '-')
		return 3;

	return 1;
}

/**
 *	get_options - Parse a string into a list of integers
 *	@str: String to be parsed
 *	@nints: size of integer array
 *	@ints: integer array
 *
 *	This function parses a string containing a comma-separated
 *	list of integers, a hyphen-separated range of _positive_ integers,
 *	or a combination of both.  The parse halts when the array is
 *	full, or when no more numbers can be retrieved from the
 *	string.
 *
 *	Return value is the character in the string which caused
 *	the parse to end (typically a null terminator, if @str is
 *	completely parseable).
 */
 
char *get_options(const char *str, int nints, int *ints)
{
	int res, i = 1;

	while (i < nints) {
		res = get_option ((char **)&str, ints + i);
		if (res == 0)
			break;
		if (res == 3) {
			int range_nums;
			range_nums = get_range((char **)&str, ints + i);
			if (range_nums < 0)
				break;
			/*
			 * Decrement the result by one to leave out the
			 * last number in the range.  The next iteration
			 * will handle the upper number in the range
			 */
			i += (range_nums - 1);
		}
		i++;
		if (res == 1)
			break;
	}
	ints[0] = i - 1;
	return (char *)str;
}

/**
 *	memparse - parse a string with mem suffixes into a number
 *	@ptr: Where parse begins
 *	@retptr: (output) Optional pointer to next char after parse completes
 *
 *	Parses a string into a number.  The number stored at @ptr is
 *	potentially suffixed with %K (for kilobytes, or 1024 bytes),
 *	%M (for megabytes, or 1048576 bytes), or %G (for gigabytes, or
 *	1073741824).  If the number is suffixed with K, M, or G, then
 *	the return value is the number multiplied by one kilobyte, one
 *	megabyte, or one gigabyte, respectively.
 */

unsigned long long memparse(const char *ptr, char **retptr)
{
	char *endptr;	/* local pointer to end of parsed string */

	unsigned long long ret = simple_strtoull(ptr, &endptr, 0);

	switch (*endptr) {
	case 'G':
	case 'g':
		ret <<= 10;
	case 'M':
	case 'm':
		ret <<= 10;
	case 'K':
	case 'k':
		ret <<= 10;
		endptr++;
	default:
		break;
	}

	if (retptr)
		*retptr = endptr;

	return ret;
}


EXPORT_SYMBOL(memparse);
EXPORT_SYMBOL(get_option);
EXPORT_SYMBOL(get_options);