aboutsummaryrefslogtreecommitdiffstats
blob: 978416dd31ca0efeacfd938e961b241aca7633af (plain) (blame)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
22
23
24
25
26
27
28
29
30
31
32
33
34
35
36
37
38
39
40
41
42
43
44
45
46
47
48
49
50
51
52
53
54
55
56
57
58
59
60
61
62
63
64
65
66
67
68
69
70
71
72
73
74
75
76
77
78
79
80
81
82
83
84
85
86
87
88
89
90
91
92
93
94
95
96
97
98
99
100
101
102
103
104
105
106
107
108
109
110
111
112
113
114
115
116
117
118
119
120
121
122
123
124
125
126
127
128
129
130
131
132
133
134
135
136
137
138
139
140
141
142
143
144
145
146
147
148
149
150
151
152
153
154
155
156
157
158
159
160
161
162
163
164
165
166
167
168
169
170
171
172
173
174
175
176
177
178
179
180
181
182
183
184
185
186
187
188
189
190
191
192
193
194
195
196
197
198
199
200
201
202
203
204
205
206
207
208
209
210
211
212
213
214
215
216
217
218
219
220
221
222
223
224
225
226
227
228
229
230
231
232
233
234
235
236
237
238
239
240
241
242
243
244
245
246
247
248
249
250
251
252
253
254
255
256
257
258
259
260
261
262
263
264
265
266
267
268
269
270
271
272
273
274
275
276
277
278
####
# kbuild: Generic definitions

# Convenient variables
comma   := ,
squote  := '
empty   :=
space   := $(empty) $(empty)

###
# Name of target with a '.' as filename prefix. foo/bar.o => foo/.bar.o
dot-target = $(dir $@).$(notdir $@)

###
# The temporary file to save gcc -MD generated dependencies must not
# contain a comma
depfile = $(subst $(comma),_,$(dot-target).d)

###
# filename of target with directory and extension stripped
basetarget = $(basename $(notdir $@))

###
# filename of first prerequisite with directory and extension stripped
baseprereq = $(basename $(notdir $<))

###
# Escape single quote for use in echo statements
escsq = $(subst $(squote),'\$(squote)',$1)

###
# Easy method for doing a status message
       kecho := :
 quiet_kecho := echo
silent_kecho := :
kecho := $($(quiet)kecho)

###
# filechk is used to check if the content of a generated file is updated.
# Sample usage:
# define filechk_sample
#	echo $KERNELRELEASE
# endef
# version.h : Makefile
#	$(call filechk,sample)
# The rule defined shall write to stdout the content of the new file.
# The existing file will be compared with the new one.
# - If no file exist it is created
# - If the content differ the new file is used
# - If they are equal no change, and no timestamp update
# - stdin is piped in from the first prerequisite ($<) so one has
#   to specify a valid file as first prerequisite (often the kbuild file)
define filechk
	$(Q)set -e;				\
	$(kecho) '  CHK     $@';		\
	mkdir -p $(dir $@);			\
	$(filechk_$(1)) < $< > $@.tmp;		\
	if [ -r $@ ] && cmp -s $@ $@.tmp; then	\
		rm -f $@.tmp;			\
	else					\
		$(kecho) '  UPD     $@';	\
		mv -f $@.tmp $@;		\
	fi
endef

######
# gcc support functions
# See documentation in Documentation/kbuild/makefiles.txt

# cc-cross-prefix
# Usage: CROSS_COMPILE := $(call cc-cross-prefix, m68k-linux-gnu- m68k-linux-)
# Return first prefix where a prefix$(CC) is found in PATH.
# If no $(CC) found in PATH with listed prefixes return nothing
cc-cross-prefix =  \
	$(word 1, $(foreach c,$(1),                                   \
		$(shell set -e;                                       \
		if (which $(strip $(c))$(CC)) > /dev/null 2>&1 ; then \
			echo $(c);                                    \
		fi)))

# output directory for tests below
TMPOUT := $(if $(KBUILD_EXTMOD),$(firstword $(KBUILD_EXTMOD))/)

# try-run
# Usage: option = $(call try-run, $(CC)...-o "$$TMP",option-ok,otherwise)
# Exit code chooses option. "$$TMP" is can be used as temporary file and
# is automatically cleaned up.
try-run = $(shell set -e;		\
	TMP="$(TMPOUT).$$$$.tmp";	\
	TMPO="$(TMPOUT).$$$$.o";	\
	if ($(1)) >/dev/null 2>&1;	\
	then echo "$(2)";		\
	else echo "$(3)";		\
	fi;				\
	rm -f "$$TMP" "$$TMPO")

# as-option
# Usage: cflags-y += $(call as-option,-Wa$(comma)-isa=foo,)

as-option = $(call try-run,\
	$(CC) $(KBUILD_CFLAGS) $(1) -c -x assembler /dev/null -o "$$TMP",$(1),$(2))

# as-instr
# Usage: cflags-y += $(call as-instr,instr,option1,option2)

as-instr = $(call try-run,\
	printf "%b\n" "$(1)" | $(CC) $(KBUILD_AFLAGS) -c -x assembler -o "$$TMP" -,$(2),$(3))

# cc-option
# Usage: cflags-y += $(call cc-option,-march=winchip-c6,-march=i586)

cc-option = $(call try-run,\
	$(CC) $(KBUILD_CPPFLAGS) $(KBUILD_CFLAGS) $(1) -c -x c /dev/null -o "$$TMP",$(1),$(2))

# cc-option-yn
# Usage: flag := $(call cc-option-yn,-march=winchip-c6)
cc-option-yn = $(call try-run,\
	$(CC) $(KBUILD_CPPFLAGS) $(KBUILD_CFLAGS) $(1) -c -x c /dev/null -o "$$TMP",y,n)

# cc-option-align
# Prefix align with either -falign or -malign
cc-option-align = $(subst -functions=0,,\
	$(call cc-option,-falign-functions=0,-malign-functions=0))

# cc-disable-warning
# Usage: cflags-y += $(call cc-disable-warning,unused-but-set-variable)
cc-disable-warning = $(call try-run,\
	$(CC) $(KBUILD_CPPFLAGS) $(KBUILD_CFLAGS) -W$(strip $(1)) -c -x c /dev/null -o "$$TMP",-Wno-$(strip $(1)))

# cc-version
# Usage gcc-ver := $(call cc-version)
cc-version = $(shell $(CONFIG_SHELL) $(srctree)/scripts/gcc-version.sh $(CC))

# cc-fullversion
# Usage gcc-ver := $(call cc-fullversion)
cc-fullversion = $(shell $(CONFIG_SHELL) \
	$(srctree)/scripts/gcc-version.sh -p $(CC))

# cc-ifversion
# Usage:  EXTRA_CFLAGS += $(call cc-ifversion, -lt, 0402, -O1)
cc-ifversion = $(shell [ $(call cc-version, $(CC)) $(1) $(2) ] && echo $(3))

# cc-ldoption
# Usage: ldflags += $(call cc-ldoption, -Wl$(comma)--hash-style=both)
cc-ldoption = $(call try-run,\
	$(CC) $(1) -nostdlib -x c /dev/null -o "$$TMP",$(1),$(2))

# ld-option
# Usage: LDFLAGS += $(call ld-option, -X)
ld-option = $(call try-run,\
	$(CC) /dev/null -c -o "$$TMPO" ; $(LD) $(1) "$$TMPO" -o "$$TMP",$(1),$(2))

# ar-option
# Usage: KBUILD_ARFLAGS := $(call ar-option,D)
# Important: no spaces around options
ar-option = $(call try-run, $(AR) rc$(1) "$$TMP",$(1),$(2))

######

###
# Shorthand for $(Q)$(MAKE) -f scripts/Makefile.build obj=
# Usage:
# $(Q)$(MAKE) $(build)=dir
build := -f $(if $(KBUILD_SRC),$(srctree)/)scripts/Makefile.build obj

###
# Shorthand for $(Q)$(MAKE) -f scripts/Makefile.modbuiltin obj=
# Usage:
# $(Q)$(MAKE) $(modbuiltin)=dir
modbuiltin := -f $(if $(KBUILD_SRC),$(srctree)/)scripts/Makefile.modbuiltin obj

# Prefix -I with $(srctree) if it is not an absolute path.
# skip if -I has no parameter
addtree = $(if $(patsubst -I%,%,$(1)), \
$(if $(filter-out -I/%,$(1)),$(patsubst -I%,-I$(srctree)/%,$(1))) $(1))

# Find all -I options and call addtree
flags = $(foreach o,$($(1)),$(if $(filter -I%,$(o)),$(call addtree,$(o)),$(o)))

# echo command.
# Short version is used, if $(quiet) equals `quiet_', otherwise full one.
echo-cmd = $(if $($(quiet)cmd_$(1)),\
	echo '  $(call escsq,$($(quiet)cmd_$(1)))$(echo-why)';)

# printing commands
cmd = @$(echo-cmd) $(cmd_$(1))

# Add $(obj)/ for paths that are not absolute
objectify = $(foreach o,$(1),$(if $(filter /%,$(o)),$(o),$(obj)/$(o)))

###
# if_changed      - execute command if any prerequisite is newer than
#                   target, or command line has changed
# if_changed_dep  - as if_changed, but uses fixdep to reveal dependencies
#                   including used config symbols
# if_changed_rule - as if_changed but execute rule instead
# See Documentation/kbuild/makefiles.txt for more info

ifneq ($(KBUILD_NOCMDDEP),1)
# Check if both arguments has same arguments. Result is empty string if equal.
# User may override this check using make KBUILD_NOCMDDEP=1
arg-check = $(strip $(filter-out $(cmd_$(1)), $(cmd_$@)) \
                    $(filter-out $(cmd_$@),   $(cmd_$(1))) )
else
arg-check = $(if $(strip $(cmd_$@)),,1)
endif

# >'< substitution is for echo to work,
# >$< substitution to preserve $ when reloading .cmd file
# note: when using inline perl scripts [perl -e '...$$t=1;...']
# in $(cmd_xxx) double $$ your perl vars
make-cmd = $(subst \\,\\\\,$(subst \#,\\\#,$(subst $$,$$$$,$(call escsq,$(cmd_$(1))))))

# Find any prerequisites that is newer than target or that does not exist.
# PHONY targets skipped in both cases.
any-prereq = $(filter-out $(PHONY),$?) $(filter-out $(PHONY) $(wildcard $^),$^)

# Execute command if command has changed or prerequisite(s) are updated.
#
if_changed = $(if $(strip $(any-prereq) $(arg-check)),                       \
	@set -e;                                                             \
	$(echo-cmd) $(cmd_$(1));                                             \
	echo 'cmd_$@ := $(make-cmd)' > $(dot-target).cmd)

# Execute the command and also postprocess generated .d dependencies file.
if_changed_dep = $(if $(strip $(any-prereq) $(arg-check) ),                  \
	@set -e;                                                             \
	$(echo-cmd) $(cmd_$(1));                                             \
	scripts/basic/fixdep $(depfile) $@ '$(make-cmd)' > $(dot-target).tmp;\
	rm -f $(depfile);                                                    \
	mv -f $(dot-target).tmp $(dot-target).cmd)

# Usage: $(call if_changed_rule,foo)
# Will check if $(cmd_foo) or any of the prerequisites changed,
# and if so will execute $(rule_foo).
if_changed_rule = $(if $(strip $(any-prereq) $(arg-check) ),                 \
	@set -e;                                                             \
	$(rule_$(1)))

###
# why - tell why a a target got build
#       enabled by make V=2
#       Output (listed in the order they are checked):
#          (1) - due to target is PHONY
#          (2) - due to target missing
#          (3) - due to: file1.h file2.h
#          (4) - due to command line change
#          (5) - due to missing .cmd file
#          (6) - due to target not in $(targets)
# (1) PHONY targets are always build
# (2) No target, so we better build it
# (3) Prerequisite is newer than target
# (4) The command line stored in the file named dir/.target.cmd
#     differed from actual command line. This happens when compiler
#     options changes
# (5) No dir/.target.cmd file (used to store command line)
# (6) No dir/.target.cmd file and target not listed in $(targets)
#     This is a good hint that there is a bug in the kbuild file
ifeq ($(KBUILD_VERBOSE),2)
why =                                                                        \
    $(if $(filter $@, $(PHONY)),- due to target is PHONY,                    \
        $(if $(wildcard $@),                                                 \
            $(if $(strip $(any-prereq)),- due to: $(any-prereq),             \
                $(if $(arg-check),                                           \
                    $(if $(cmd_$@),- due to command line change,             \
                        $(if $(filter $@, $(targets)),                       \
                            - due to missing .cmd file,                      \
                            - due to $(notdir $@) not in $$(targets)         \
                         )                                                   \
                     )                                                       \
                 )                                                           \
             ),                                                              \
             - due to target missing                                         \
         )                                                                   \
     )

echo-why = $(call escsq, $(strip $(why)))
endif