aboutsummaryrefslogblamecommitdiffstats
blob: 610001d385dd466c48394873c972e3430b7789ba (plain) (tree)
1
2
3

                       
 






















                                                                             
 
                     
                          
                    
                       
                           
 





































                                                                         

                                                      





                                         

                                         






                         


                                    
                                  
 



                                                 


                                                              


                                     



                              







                                                           
 

                                       
 

                                                                    

                                  
                                             
 















                                                                               
                                       
                         



                                  






                                                     


















                                                                      











                                             

                       
                                    
                             
 

                                           
                            
#ifndef _ASM_X86_ACPI_H
#define _ASM_X86_ACPI_H

/*
 *  Copyright (C) 2001 Paul Diefenbaugh <paul.s.diefenbaugh@intel.com>
 *  Copyright (C) 2001 Patrick Mochel <mochel@osdl.org>
 *
 * ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
 *
 *  This program is free software; you can redistribute it and/or modify
 *  it under the terms of the GNU General Public License as published by
 *  the Free Software Foundation; either version 2 of the License, or
 *  (at your option) any later version.
 *
 *  This program is distributed in the hope that it will be useful,
 *  but WITHOUT ANY WARRANTY; without even the implied warranty of
 *  MERCHANTABILITY or FITNESS FOR A PARTICULAR PURPOSE.  See the
 *  GNU General Public License for more details.
 *
 *  You should have received a copy of the GNU General Public License
 *  along with this program; if not, write to the Free Software
 *  Foundation, Inc., 59 Temple Place, Suite 330, Boston, MA  02111-1307  USA
 *
 * ~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~~
 */
#include <acpi/pdc_intel.h>

#include <asm/numa.h>
#include <asm/processor.h>
#include <asm/mmu.h>
#include <asm/mpspec.h>
#include <asm/trampoline.h>

#define COMPILER_DEPENDENT_INT64   long long
#define COMPILER_DEPENDENT_UINT64  unsigned long long

/*
 * Calling conventions:
 *
 * ACPI_SYSTEM_XFACE        - Interfaces to host OS (handlers, threads)
 * ACPI_EXTERNAL_XFACE      - External ACPI interfaces
 * ACPI_INTERNAL_XFACE      - Internal ACPI interfaces
 * ACPI_INTERNAL_VAR_XFACE  - Internal variable-parameter list interfaces
 */
#define ACPI_SYSTEM_XFACE
#define ACPI_EXTERNAL_XFACE
#define ACPI_INTERNAL_XFACE
#define ACPI_INTERNAL_VAR_XFACE

/* Asm macros */

#define ACPI_ASM_MACROS
#define BREAKPOINT3
#define ACPI_DISABLE_IRQS() local_irq_disable()
#define ACPI_ENABLE_IRQS()  local_irq_enable()
#define ACPI_FLUSH_CPU_CACHE()	wbinvd()

int __acpi_acquire_global_lock(unsigned int *lock);
int __acpi_release_global_lock(unsigned int *lock);

#define ACPI_ACQUIRE_GLOBAL_LOCK(facs, Acq) \
	((Acq) = __acpi_acquire_global_lock(&facs->global_lock))

#define ACPI_RELEASE_GLOBAL_LOCK(facs, Acq) \
	((Acq) = __acpi_release_global_lock(&facs->global_lock))

/*
 * Math helper asm macros
 */
#define ACPI_DIV_64_BY_32(n_hi, n_lo, d32, q32, r32) \
	asm("divl %2;"				     \
	    : "=a"(q32), "=d"(r32)		     \
	    : "r"(d32),				     \
	     "0"(n_lo), "1"(n_hi))


#define ACPI_SHIFT_RIGHT_64(n_hi, n_lo) \
	asm("shrl   $1,%2	;"	\
	    "rcrl   $1,%3;"		\
	    : "=r"(n_hi), "=r"(n_lo)	\
	    : "0"(n_hi), "1"(n_lo))

#ifdef CONFIG_ACPI
extern int acpi_lapic;
extern int acpi_ioapic;
extern int acpi_noirq;
extern int acpi_strict;
extern int acpi_disabled;
extern int acpi_pci_disabled;
extern int acpi_skip_timer_override;
extern int acpi_use_timer_override;
extern int acpi_fix_pin2_polarity;

extern u8 acpi_sci_flags;
extern int acpi_sci_override_gsi;
void acpi_pic_sci_set_trigger(unsigned int, u16);

extern int (*__acpi_register_gsi)(struct device *dev, u32 gsi,
				  int trigger, int polarity);

static inline void disable_acpi(void)
{
	acpi_disabled = 1;
	acpi_pci_disabled = 1;
	acpi_noirq = 1;
}

extern int acpi_gsi_to_irq(u32 gsi, unsigned int *irq);

static inline void acpi_noirq_set(void) { acpi_noirq = 1; }
static inline void acpi_disable_pci(void)
{
	acpi_pci_disabled = 1;
	acpi_noirq_set();
}

/* Low-level suspend routine. */
extern int acpi_suspend_lowlevel(void);

extern const unsigned char acpi_wakeup_code[];
#define acpi_wakeup_address (__pa(TRAMPOLINE_SYM(acpi_wakeup_code)))

/* early initialization routine */
extern void acpi_reserve_wakeup_memory(void);

/*
 * Check if the CPU can handle C2 and deeper
 */
static inline unsigned int acpi_processor_cstate_check(unsigned int max_cstate)
{
	/*
	 * Early models (<=5) of AMD Opterons are not supposed to go into
	 * C2 state.
	 *
	 * Steppings 0x0A and later are good
	 */
	if (boot_cpu_data.x86 == 0x0F &&
	    boot_cpu_data.x86_vendor == X86_VENDOR_AMD &&
	    boot_cpu_data.x86_model <= 0x05 &&
	    boot_cpu_data.x86_mask < 0x0A)
		return 1;
	else if (amd_e400_c1e_detected)
		return 1;
	else
		return max_cstate;
}

static inline bool arch_has_acpi_pdc(void)
{
	struct cpuinfo_x86 *c = &cpu_data(0);
	return (c->x86_vendor == X86_VENDOR_INTEL ||
		c->x86_vendor == X86_VENDOR_CENTAUR);
}

static inline void arch_acpi_set_pdc_bits(u32 *buf)
{
	struct cpuinfo_x86 *c = &cpu_data(0);

	buf[2] |= ACPI_PDC_C_CAPABILITY_SMP;

	if (cpu_has(c, X86_FEATURE_EST))
		buf[2] |= ACPI_PDC_EST_CAPABILITY_SWSMP;

	if (cpu_has(c, X86_FEATURE_ACPI))
		buf[2] |= ACPI_PDC_T_FFH;

	/*
	 * If mwait/monitor is unsupported, C2/C3_FFH will be disabled
	 */
	if (!cpu_has(c, X86_FEATURE_MWAIT))
		buf[2] &= ~(ACPI_PDC_C_C2C3_FFH);
}

#else /* !CONFIG_ACPI */

#define acpi_lapic 0
#define acpi_ioapic 0
static inline void acpi_noirq_set(void) { }
static inline void acpi_disable_pci(void) { }
static inline void disable_acpi(void) { }

#endif /* !CONFIG_ACPI */

#define ARCH_HAS_POWER_INIT	1

#ifdef CONFIG_ACPI_NUMA
extern int acpi_numa;
extern int x86_acpi_numa_init(void);
#endif /* CONFIG_ACPI_NUMA */

#define acpi_unlazy_tlb(x)	leave_mm(x)

#endif /* _ASM_X86_ACPI_H */