aboutsummaryrefslogblamecommitdiffstats
blob: 3f2ad2640d8522410eb846341b9a8bd6f0d00f26 (plain) (tree)
1
2
3
4
5
6
7
8
9
  
                        
   

                                  
                       
                      
                      
                     
 
                         
                         
                     
 
                    




                                                                       
                                 
                         
                          
 


                                                          


                          









                                                                       
                                            
 

                                                     
                       
 

                                              

                                                        

                                                      



                                                                       
                                                     








                                                            
                                             
                                                             
                                   



                                                                        

                                                             
                 

                                                      
                
                                       

















                                                                          
                                      
 
                                                                         
















                                                                     
                  




                                                                 
                                        
                                                                 

                                                          





                                     

         
                      
                                           

                                                                            
              
                                        



                                                      





                                               

                                
                               
 






                                                          

                                



                               
                                                
 
                            
                   
 
                                            
                                                        





                                                 
                                               
 
                                    

                                            
                                              

                                                 

                            

 
                                        
 
                                   
 

                               























                                                    














                                                                    

                                   
 
                                              

                                                                           
 


                              
/*
 * RTC related functions
 */
#include <linux/platform_device.h>
#include <linux/mc146818rtc.h>
#include <linux/acpi.h>
#include <linux/bcd.h>
#include <linux/pnp.h>
#include <linux/of.h>

#include <asm/vsyscall.h>
#include <asm/x86_init.h>
#include <asm/time.h>

#ifdef CONFIG_X86_32
/*
 * This is a special lock that is owned by the CPU and holds the index
 * register we are working with.  It is required for NMI access to the
 * CMOS/RTC registers.  See include/asm-i386/mc146818rtc.h for details.
 */
volatile unsigned long cmos_lock;
EXPORT_SYMBOL(cmos_lock);
#endif /* CONFIG_X86_32 */

/* For two digit years assume time is always after that */
#define CMOS_YEARS_OFFS 2000

DEFINE_SPINLOCK(rtc_lock);
EXPORT_SYMBOL(rtc_lock);

/*
 * In order to set the CMOS clock precisely, set_rtc_mmss has to be
 * called 500 ms after the second nowtime has started, because when
 * nowtime is written into the registers of the CMOS clock, it will
 * jump to the next second precisely 500 ms later. Check the Motorola
 * MC146818A or Dallas DS12887 data sheet for details.
 *
 * BUG: This routine does not handle hour overflow properly; it just
 *      sets the minutes. Usually you'll only notice that after reboot!
 */
int mach_set_rtc_mmss(unsigned long nowtime)
{
	int real_seconds, real_minutes, cmos_minutes;
	unsigned char save_control, save_freq_select;
	int retval = 0;

	 /* tell the clock it's being set */
	save_control = CMOS_READ(RTC_CONTROL);
	CMOS_WRITE((save_control|RTC_SET), RTC_CONTROL);

	/* stop and reset prescaler */
	save_freq_select = CMOS_READ(RTC_FREQ_SELECT);
	CMOS_WRITE((save_freq_select|RTC_DIV_RESET2), RTC_FREQ_SELECT);

	cmos_minutes = CMOS_READ(RTC_MINUTES);
	if (!(save_control & RTC_DM_BINARY) || RTC_ALWAYS_BCD)
		cmos_minutes = bcd2bin(cmos_minutes);

	/*
	 * since we're only adjusting minutes and seconds,
	 * don't interfere with hour overflow. This avoids
	 * messing with unknown time zones but requires your
	 * RTC not to be off by more than 15 minutes
	 */
	real_seconds = nowtime % 60;
	real_minutes = nowtime / 60;
	/* correct for half hour time zone */
	if (((abs(real_minutes - cmos_minutes) + 15)/30) & 1)
		real_minutes += 30;
	real_minutes %= 60;

	if (abs(real_minutes - cmos_minutes) < 30) {
		if (!(save_control & RTC_DM_BINARY) || RTC_ALWAYS_BCD) {
			real_seconds = bin2bcd(real_seconds);
			real_minutes = bin2bcd(real_minutes);
		}
		CMOS_WRITE(real_seconds, RTC_SECONDS);
		CMOS_WRITE(real_minutes, RTC_MINUTES);
	} else {
		printk_once(KERN_NOTICE
		       "set_rtc_mmss: can't update from %d to %d\n",
		       cmos_minutes, real_minutes);
		retval = -1;
	}

	/* The following flags have to be released exactly in this order,
	 * otherwise the DS12887 (popular MC146818A clone with integrated
	 * battery and quartz) will not reset the oscillator and will not
	 * update precisely 500 ms later. You won't find this mentioned in
	 * the Dallas Semiconductor data sheets, but who believes data
	 * sheets anyway ...                           -- Markus Kuhn
	 */
	CMOS_WRITE(save_control, RTC_CONTROL);
	CMOS_WRITE(save_freq_select, RTC_FREQ_SELECT);

	return retval;
}

unsigned long mach_get_cmos_time(void)
{
	unsigned int status, year, mon, day, hour, min, sec, century = 0;

	/*
	 * If UIP is clear, then we have >= 244 microseconds before
	 * RTC registers will be updated.  Spec sheet says that this
	 * is the reliable way to read RTC - registers. If UIP is set
	 * then the register access might be invalid.
	 */
	while ((CMOS_READ(RTC_FREQ_SELECT) & RTC_UIP))
		cpu_relax();

	sec = CMOS_READ(RTC_SECONDS);
	min = CMOS_READ(RTC_MINUTES);
	hour = CMOS_READ(RTC_HOURS);
	day = CMOS_READ(RTC_DAY_OF_MONTH);
	mon = CMOS_READ(RTC_MONTH);
	year = CMOS_READ(RTC_YEAR);

#ifdef CONFIG_ACPI
	if (acpi_gbl_FADT.header.revision >= FADT2_REVISION_ID &&
	    acpi_gbl_FADT.century)
		century = CMOS_READ(acpi_gbl_FADT.century);
#endif

	status = CMOS_READ(RTC_CONTROL);
	WARN_ON_ONCE(RTC_ALWAYS_BCD && (status & RTC_DM_BINARY));

	if (RTC_ALWAYS_BCD || !(status & RTC_DM_BINARY)) {
		sec = bcd2bin(sec);
		min = bcd2bin(min);
		hour = bcd2bin(hour);
		day = bcd2bin(day);
		mon = bcd2bin(mon);
		year = bcd2bin(year);
	}

	if (century) {
		century = bcd2bin(century);
		year += century * 100;
		printk(KERN_INFO "Extended CMOS year: %d\n", century * 100);
	} else
		year += CMOS_YEARS_OFFS;

	return mktime(year, mon, day, hour, min, sec);
}

/* Routines for accessing the CMOS RAM/RTC. */
unsigned char rtc_cmos_read(unsigned char addr)
{
	unsigned char val;

	lock_cmos_prefix(addr);
	outb(addr, RTC_PORT(0));
	val = inb(RTC_PORT(1));
	lock_cmos_suffix(addr);

	return val;
}
EXPORT_SYMBOL(rtc_cmos_read);

void rtc_cmos_write(unsigned char val, unsigned char addr)
{
	lock_cmos_prefix(addr);
	outb(addr, RTC_PORT(0));
	outb(val, RTC_PORT(1));
	lock_cmos_suffix(addr);
}
EXPORT_SYMBOL(rtc_cmos_write);

int update_persistent_clock(struct timespec now)
{
	unsigned long flags;
	int retval;

	spin_lock_irqsave(&rtc_lock, flags);
	retval = x86_platform.set_wallclock(now.tv_sec);
	spin_unlock_irqrestore(&rtc_lock, flags);

	return retval;
}

/* not static: needed by APM */
void read_persistent_clock(struct timespec *ts)
{
	unsigned long retval, flags;

	spin_lock_irqsave(&rtc_lock, flags);
	retval = x86_platform.get_wallclock();
	spin_unlock_irqrestore(&rtc_lock, flags);

	ts->tv_sec = retval;
	ts->tv_nsec = 0;
}

unsigned long long native_read_tsc(void)
{
	return __native_read_tsc();
}
EXPORT_SYMBOL(native_read_tsc);


static struct resource rtc_resources[] = {
	[0] = {
		.start	= RTC_PORT(0),
		.end	= RTC_PORT(1),
		.flags	= IORESOURCE_IO,
	},
	[1] = {
		.start	= RTC_IRQ,
		.end	= RTC_IRQ,
		.flags	= IORESOURCE_IRQ,
	}
};

static struct platform_device rtc_device = {
	.name		= "rtc_cmos",
	.id		= -1,
	.resource	= rtc_resources,
	.num_resources	= ARRAY_SIZE(rtc_resources),
};

static __init int add_rtc_cmos(void)
{
#ifdef CONFIG_PNP
	static const char *ids[] __initconst =
	    { "PNP0b00", "PNP0b01", "PNP0b02", };
	struct pnp_dev *dev;
	struct pnp_id *id;
	int i;

	pnp_for_each_dev(dev) {
		for (id = dev->id; id; id = id->next) {
			for (i = 0; i < ARRAY_SIZE(ids); i++) {
				if (compare_pnp_id(id, ids[i]) != 0)
					return 0;
			}
		}
	}
#endif
	if (of_have_populated_dt())
		return 0;

	platform_device_register(&rtc_device);
	dev_info(&rtc_device.dev,
		 "registered platform RTC device (no PNP device found)\n");

	return 0;
}
device_initcall(add_rtc_cmos);