aboutsummaryrefslogblamecommitdiffstats
blob: 0d5b17bf5e5131dfd03dc176a8c7fa4f9cbec9b1 (plain) (tree)
1
2
3
4
5
6
7
8
9
10
11










                                                                          






                                                                           










                                                                             
   
 


                          

                             
 

                   

                    


                                                         

                                                         




                                                                         






                                                                               

                       


                                                                                


                                                                       



                                                                   






                                                                                 



                                                                              
                                                                    



                                                                              



                                               


                                          




                                                    

                                             


                                             

                                            
                                         


                                  
                                          


                                    
                        




                                                                          
                                                                     


                                                                     
                                                                          


                                                                     
                                                                          

                                                                    
                                                              
                                                                          

                                                                   
                                                                          

                                                          

                                                                  
 

                                                            
                                                                 




                                                                            


                                                       








                                                                                   





                                                                       









                                                                             


                                                              
                                                         











                                                                                
                          

                                                                               
                         

                                                                                  
                           



                                                             
 
                               
/*
 * irq_domain - IRQ translation domains
 *
 * Translation infrastructure between hw and linux irq numbers.  This is
 * helpful for interrupt controllers to implement mapping between hardware
 * irq numbers and the Linux irq number space.
 *
 * irq_domains also have a hook for translating device tree interrupt
 * representation into a hardware irq number that can be mapped back to a
 * Linux irq number without any extra platform support code.
 *
 * Interrupt controller "domain" data structure. This could be defined as a
 * irq domain controller. That is, it handles the mapping between hardware
 * and virtual interrupt numbers for a given interrupt domain. The domain
 * structure is generally created by the PIC code for a given PIC instance
 * (though a domain can cover more than one PIC if they have a flat number
 * model). It's the domain callbacks that are responsible for setting the
 * irq_chip on a given irq_desc after it's been mapped.
 *
 * The host code and data structures are agnostic to whether or not
 * we use an open firmware device-tree. We do have references to struct
 * device_node in two places: in irq_find_host() to find the host matching
 * a given interrupt controller node, and of course as an argument to its
 * counterpart domain->ops->match() callback. However, those are treated as
 * generic pointers by the core and the fact that it's actually a device-node
 * pointer is purely a convention between callers and implementation. This
 * code could thus be used on other architectures by replacing those two
 * by some sort of arch-specific void * "token" used to identify interrupt
 * controllers.
 */

#ifndef _LINUX_IRQDOMAIN_H
#define _LINUX_IRQDOMAIN_H

#include <linux/types.h>
#include <linux/radix-tree.h>

struct device_node;
struct irq_domain;
struct of_device_id;

/* Number of irqs reserved for a legacy isa controller */
#define NUM_ISA_INTERRUPTS	16

/**
 * struct irq_domain_ops - Methods for irq_domain objects
 * @match: Match an interrupt controller device node to a host, returns
 *         1 on a match
 * @map: Create or update a mapping between a virtual irq number and a hw
 *       irq number. This is called only once for a given mapping.
 * @unmap: Dispose of such a mapping
 * @xlate: Given a device tree node and interrupt specifier, decode
 *         the hardware irq number and linux irq type value.
 *
 * Functions below are provided by the driver and called whenever a new mapping
 * is created or an old mapping is disposed. The driver can then proceed to
 * whatever internal data structures management is required. It also needs
 * to setup the irq_desc when returning from map().
 */
struct irq_domain_ops {
	int (*match)(struct irq_domain *d, struct device_node *node);
	int (*map)(struct irq_domain *d, unsigned int virq, irq_hw_number_t hw);
	void (*unmap)(struct irq_domain *d, unsigned int virq);
	int (*xlate)(struct irq_domain *d, struct device_node *node,
		     const u32 *intspec, unsigned int intsize,
		     unsigned long *out_hwirq, unsigned int *out_type);
};

/**
 * struct irq_domain - Hardware interrupt number translation object
 * @link: Element in global irq_domain list.
 * @revmap_type: Method used for reverse mapping hwirq numbers to linux irq. This
 *               will be one of the IRQ_DOMAIN_MAP_* values.
 * @revmap_data: Revmap method specific data.
 * @ops: pointer to irq_domain methods
 * @host_data: private data pointer for use by owner.  Not touched by irq_domain
 *             core code.
 * @irq_base: Start of irq_desc range assigned to the irq_domain.  The creator
 *            of the irq_domain is responsible for allocating the array of
 *            irq_desc structures.
 * @nr_irq: Number of irqs managed by the irq domain
 * @hwirq_base: Starting number for hwirqs managed by the irq domain
 * @of_node: (optional) Pointer to device tree nodes associated with the
 *           irq_domain.  Used when decoding device tree interrupt specifiers.
 */
struct irq_domain {
	struct list_head link;

	/* type of reverse mapping_technique */
	unsigned int revmap_type;
	union {
		struct {
			unsigned int size;
			unsigned int first_irq;
			irq_hw_number_t first_hwirq;
		} legacy;
		struct {
			unsigned int size;
			unsigned int *revmap;
		} linear;
		struct {
			unsigned int max_irq;
		} nomap;
		struct radix_tree_root tree;
	} revmap_data;
	const struct irq_domain_ops *ops;
	void *host_data;
	irq_hw_number_t inval_irq;

	/* Optional device node pointer */
	struct device_node *of_node;
};

#ifdef CONFIG_IRQ_DOMAIN
struct irq_domain *irq_domain_add_simple(struct device_node *of_node,
					 unsigned int size,
					 unsigned int first_irq,
					 const struct irq_domain_ops *ops,
					 void *host_data);
struct irq_domain *irq_domain_add_legacy(struct device_node *of_node,
					 unsigned int size,
					 unsigned int first_irq,
					 irq_hw_number_t first_hwirq,
					 const struct irq_domain_ops *ops,
					 void *host_data);
struct irq_domain *irq_domain_add_linear(struct device_node *of_node,
					 unsigned int size,
					 const struct irq_domain_ops *ops,
					 void *host_data);
struct irq_domain *irq_domain_add_nomap(struct device_node *of_node,
					 unsigned int max_irq,
					 const struct irq_domain_ops *ops,
					 void *host_data);
struct irq_domain *irq_domain_add_tree(struct device_node *of_node,
					 const struct irq_domain_ops *ops,
					 void *host_data);

extern struct irq_domain *irq_find_host(struct device_node *node);
extern void irq_set_default_host(struct irq_domain *host);

static inline struct irq_domain *irq_domain_add_legacy_isa(
				struct device_node *of_node,
				const struct irq_domain_ops *ops,
				void *host_data)
{
	return irq_domain_add_legacy(of_node, NUM_ISA_INTERRUPTS, 0, 0, ops,
				     host_data);
}

extern void irq_domain_remove(struct irq_domain *host);

extern int irq_domain_associate_many(struct irq_domain *domain,
				     unsigned int irq_base,
				     irq_hw_number_t hwirq_base, int count);
static inline int irq_domain_associate(struct irq_domain *domain, unsigned int irq,
					irq_hw_number_t hwirq)
{
	return irq_domain_associate_many(domain, irq, hwirq, 1);
}

extern unsigned int irq_create_mapping(struct irq_domain *host,
				       irq_hw_number_t hwirq);
extern void irq_dispose_mapping(unsigned int virq);
extern unsigned int irq_find_mapping(struct irq_domain *host,
				     irq_hw_number_t hwirq);
extern unsigned int irq_create_direct_mapping(struct irq_domain *host);
extern int irq_create_strict_mappings(struct irq_domain *domain,
				      unsigned int irq_base,
				      irq_hw_number_t hwirq_base, int count);

static inline int irq_create_identity_mapping(struct irq_domain *host,
					      irq_hw_number_t hwirq)
{
	return irq_create_strict_mappings(host, hwirq, hwirq, 1);
}

extern unsigned int irq_linear_revmap(struct irq_domain *host,
				      irq_hw_number_t hwirq);

extern const struct irq_domain_ops irq_domain_simple_ops;

/* stock xlate functions */
int irq_domain_xlate_onecell(struct irq_domain *d, struct device_node *ctrlr,
			const u32 *intspec, unsigned int intsize,
			irq_hw_number_t *out_hwirq, unsigned int *out_type);
int irq_domain_xlate_twocell(struct irq_domain *d, struct device_node *ctrlr,
			const u32 *intspec, unsigned int intsize,
			irq_hw_number_t *out_hwirq, unsigned int *out_type);
int irq_domain_xlate_onetwocell(struct irq_domain *d, struct device_node *ctrlr,
			const u32 *intspec, unsigned int intsize,
			irq_hw_number_t *out_hwirq, unsigned int *out_type);

#if defined(CONFIG_OF_IRQ)
extern void irq_domain_generate_simple(const struct of_device_id *match,
					u64 phys_base, unsigned int irq_start);
#else /* CONFIG_OF_IRQ */
static inline void irq_domain_generate_simple(const struct of_device_id *match,
					u64 phys_base, unsigned int irq_start) { }
#endif /* !CONFIG_OF_IRQ */

#else /* CONFIG_IRQ_DOMAIN */
static inline void irq_dispose_mapping(unsigned int virq) { }
#endif /* !CONFIG_IRQ_DOMAIN */

#endif /* _LINUX_IRQDOMAIN_H */