aboutsummaryrefslogblamecommitdiffstats
blob: 5ca0951e1855b103ff65337cef6f94449f34d6c5 (plain) (tree)
1
2
3
4
5
6


                           
                          

                        

































                                                                     















                                                                         










                                                                           




                                                                           



                                                         
                                                         
                                                         
                                                         
                                                         
                                                                                                                                 
                                                         
                                                         


                                                         








                                                                          

                                                                         









                                                                           

                                                                                  
 
                                         
#ifndef __LINUX_UACCESS_H__
#define __LINUX_UACCESS_H__

#include <linux/preempt.h>
#include <asm/uaccess.h>

/*
 * These routines enable/disable the pagefault handler in that
 * it will not take any locks and go straight to the fixup table.
 *
 * They have great resemblance to the preempt_disable/enable calls
 * and in fact they are identical; this is because currently there is
 * no other way to make the pagefault handlers do this. So we do
 * disable preemption but we don't necessarily care about that.
 */
static inline void pagefault_disable(void)
{
	inc_preempt_count();
	/*
	 * make sure to have issued the store before a pagefault
	 * can hit.
	 */
	barrier();
}

static inline void pagefault_enable(void)
{
	/*
	 * make sure to issue those last loads/stores before enabling
	 * the pagefault handler again.
	 */
	barrier();
	dec_preempt_count();
	/*
	 * make sure we do..
	 */
	barrier();
	preempt_check_resched();
}

#ifndef ARCH_HAS_NOCACHE_UACCESS

static inline unsigned long __copy_from_user_inatomic_nocache(void *to,
				const void __user *from, unsigned long n)
{
	return __copy_from_user_inatomic(to, from, n);
}

static inline unsigned long __copy_from_user_nocache(void *to,
				const void __user *from, unsigned long n)
{
	return __copy_from_user(to, from, n);
}

#endif		/* ARCH_HAS_NOCACHE_UACCESS */

/**
 * probe_kernel_address(): safely attempt to read from a location
 * @addr: address to read from - its type is type typeof(retval)*
 * @retval: read into this variable
 *
 * Safely read from address @addr into variable @revtal.  If a kernel fault
 * happens, handle that and return -EFAULT.
 * We ensure that the __get_user() is executed in atomic context so that
 * do_page_fault() doesn't attempt to take mmap_sem.  This makes
 * probe_kernel_address() suitable for use within regions where the caller
 * already holds mmap_sem, or other locks which nest inside mmap_sem.
 * This must be a macro because __get_user() needs to know the types of the
 * args.
 *
 * We don't include enough header files to be able to do the set_fs().  We
 * require that the probe_kernel_address() caller will do that.
 */
#define probe_kernel_address(addr, retval)		\
	({						\
		long ret;				\
		mm_segment_t old_fs = get_fs();		\
							\
		set_fs(KERNEL_DS);			\
		pagefault_disable();			\
		ret = __copy_from_user_inatomic(&(retval), (__force typeof(retval) __user *)(addr), sizeof(retval));		\
		pagefault_enable();			\
		set_fs(old_fs);				\
		ret;					\
	})

/*
 * probe_kernel_read(): safely attempt to read from a location
 * @dst: pointer to the buffer that shall take the data
 * @src: address to read from
 * @size: size of the data chunk
 *
 * Safely read from address @src to the buffer at @dst.  If a kernel fault
 * happens, handle that and return -EFAULT.
 */
extern long probe_kernel_read(void *dst, const void *src, size_t size);
extern long __probe_kernel_read(void *dst, const void *src, size_t size);

/*
 * probe_kernel_write(): safely attempt to write to a location
 * @dst: address to write to
 * @src: pointer to the data that shall be written
 * @size: size of the data chunk
 *
 * Safely write to address @dst from the buffer at @src.  If a kernel fault
 * happens, handle that and return -EFAULT.
 */
extern long notrace probe_kernel_write(void *dst, const void *src, size_t size);
extern long notrace __probe_kernel_write(void *dst, const void *src, size_t size);

#endif		/* __LINUX_UACCESS_H__ */