aboutsummaryrefslogblamecommitdiffstats
blob: 63633a320fb7c1d32c864459fb49c156e44574ff (plain) (tree)
1
2
3
4
5
6
7
8
9







                                                            
                          



                            
                              
                        
 

                      
                                  
 


                                                                       

                                
 
  



















                                                                      
                                                            

                                           
                                                       
                                                  
                                                                   




                     
 
  

                                             
                                                                  
 
                                   
                                 
 
                                   

                                                                   
                                                                                 





                                                              
                                                         



                                                                      
                 


                                                        
                                           

                         
                                                  
                                                   



                                                                  
                                             
                         
         
 
                                      
                                             
            

                                                          
                                                                  
                                      
                                                          
                                              

                                     
                                  



                                 
                              
                      
 
                                                     



                                          


                                    



                                                   
                                                
                               
         

                                     



                                                           
                                                   
 
                              
              
 



                                                     
                                    
                                   
 


                                  
                                                
                                     
                          
                                                      

                                 
                                    
                                           
                                   
         

                                     

                                                        

 






                                                                  






                                                                      
   
           

                                                         

                                 
                            
 
                                         


                                                                        

                                                                         


                                       
 






                                                                      

                              




                                                                                

                                      
                                                       

 
           
                                                                               








                                                        


                                                          































                                                                          
                                                            
                                           
 
                                                

                       









                                                        


                                                                             
                                                                               

                                  
                                                                      



                                                 

         



                                                                 

         
                          
                                             


                            
                                                     







                                                              
                                                       
                              
                                  
 

                                                                



                                 
                             
 
                               


                                                            
 



                                        

                                                                       
 




                                                                      
 



                                    
                                  











                                                                      
/*
 * linux/kernel/irq/spurious.c
 *
 * Copyright (C) 1992, 1998-2004 Linus Torvalds, Ingo Molnar
 *
 * This file contains spurious interrupt handling.
 */

#include <linux/jiffies.h>
#include <linux/irq.h>
#include <linux/module.h>
#include <linux/kallsyms.h>
#include <linux/interrupt.h>
#include <linux/moduleparam.h>
#include <linux/timer.h>

#include "internals.h"

static int irqfixup __read_mostly;

#define POLL_SPURIOUS_IRQ_INTERVAL (HZ/10)
static void poll_spurious_irqs(unsigned long dummy);
static DEFINE_TIMER(poll_spurious_irq_timer, poll_spurious_irqs, 0, 0);
static int irq_poll_cpu;
static atomic_t irq_poll_active;

/*
 * We wait here for a poller to finish.
 *
 * If the poll runs on this CPU, then we yell loudly and return
 * false. That will leave the interrupt line disabled in the worst
 * case, but it should never happen.
 *
 * We wait until the poller is done and then recheck disabled and
 * action (about to be disabled). Only if it's still active, we return
 * true and let the handler run.
 */
bool irq_wait_for_poll(struct irq_desc *desc)
{
	if (WARN_ONCE(irq_poll_cpu == smp_processor_id(),
		      "irq poll in progress on cpu %d for irq %d\n",
		      smp_processor_id(), desc->irq_data.irq))
		return false;

#ifdef CONFIG_SMP
	do {
		raw_spin_unlock(&desc->lock);
		while (irqd_irq_inprogress(&desc->irq_data))
			cpu_relax();
		raw_spin_lock(&desc->lock);
	} while (irqd_irq_inprogress(&desc->irq_data));
	/* Might have been disabled in meantime */
	return !irqd_irq_disabled(&desc->irq_data) && desc->action;
#else
	return false;
#endif
}


/*
 * Recovery handler for misrouted interrupts.
 */
static int try_one_irq(int irq, struct irq_desc *desc, bool force)
{
	irqreturn_t ret = IRQ_NONE;
	struct irqaction *action;

	raw_spin_lock(&desc->lock);

	/* PER_CPU and nested thread interrupts are never polled */
	if (irq_settings_is_per_cpu(desc) || irq_settings_is_nested_thread(desc))
		goto out;

	/*
	 * Do not poll disabled interrupts unless the spurious
	 * disabled poller asks explicitely.
	 */
	if (irqd_irq_disabled(&desc->irq_data) && !force)
		goto out;

	/*
	 * All handlers must agree on IRQF_SHARED, so we test just the
	 * first.
	 */
	action = desc->action;
	if (!action || !(action->flags & IRQF_SHARED) ||
	    (action->flags & __IRQF_TIMER))
		goto out;

	/* Already running on another processor */
	if (irqd_irq_inprogress(&desc->irq_data)) {
		/*
		 * Already running: If it is shared get the other
		 * CPU to go looking for our mystery interrupt too
		 */
		desc->istate |= IRQS_PENDING;
		goto out;
	}

	/* Mark it poll in progress */
	desc->istate |= IRQS_POLL_INPROGRESS;
	do {
		if (handle_irq_event(desc) == IRQ_HANDLED)
			ret = IRQ_HANDLED;
		/* Make sure that there is still a valid action */
		action = desc->action;
	} while ((desc->istate & IRQS_PENDING) && action);
	desc->istate &= ~IRQS_POLL_INPROGRESS;
out:
	raw_spin_unlock(&desc->lock);
	return ret == IRQ_HANDLED;
}

static int misrouted_irq(int irq)
{
	struct irq_desc *desc;
	int i, ok = 0;

	if (atomic_inc_return(&irq_poll_active) != 1)
		goto out;

	irq_poll_cpu = smp_processor_id();

	for_each_irq_desc(i, desc) {
		if (!i)
			 continue;

		if (i == irq)	/* Already tried */
			continue;

		if (try_one_irq(i, desc, false))
			ok = 1;
	}
out:
	atomic_dec(&irq_poll_active);
	/* So the caller can adjust the irq error counts */
	return ok;
}

static void poll_spurious_irqs(unsigned long dummy)
{
	struct irq_desc *desc;
	int i;

	if (atomic_inc_return(&irq_poll_active) != 1)
		goto out;
	irq_poll_cpu = smp_processor_id();

	for_each_irq_desc(i, desc) {
		unsigned int state;

		if (!i)
			 continue;

		/* Racy but it doesn't matter */
		state = desc->istate;
		barrier();
		if (!(state & IRQS_SPURIOUS_DISABLED))
			continue;

		local_irq_disable();
		try_one_irq(i, desc, true);
		local_irq_enable();
	}
out:
	atomic_dec(&irq_poll_active);
	mod_timer(&poll_spurious_irq_timer,
		  jiffies + POLL_SPURIOUS_IRQ_INTERVAL);
}

static inline int bad_action_ret(irqreturn_t action_ret)
{
	if (likely(action_ret <= (IRQ_HANDLED | IRQ_WAKE_THREAD)))
		return 0;
	return 1;
}

/*
 * If 99,900 of the previous 100,000 interrupts have not been handled
 * then assume that the IRQ is stuck in some manner. Drop a diagnostic
 * and try to turn the IRQ off.
 *
 * (The other 100-of-100,000 interrupts may have been a correctly
 *  functioning device sharing an IRQ with the failing one)
 */
static void
__report_bad_irq(unsigned int irq, struct irq_desc *desc,
		 irqreturn_t action_ret)
{
	struct irqaction *action;
	unsigned long flags;

	if (bad_action_ret(action_ret)) {
		printk(KERN_ERR "irq event %d: bogus return value %x\n",
				irq, action_ret);
	} else {
		printk(KERN_ERR "irq %d: nobody cared (try booting with "
				"the \"irqpoll\" option)\n", irq);
	}
	dump_stack();
	printk(KERN_ERR "handlers:\n");

	/*
	 * We need to take desc->lock here. note_interrupt() is called
	 * w/o desc->lock held, but IRQ_PROGRESS set. We might race
	 * with something else removing an action. It's ok to take
	 * desc->lock here. See synchronize_irq().
	 */
	raw_spin_lock_irqsave(&desc->lock, flags);
	action = desc->action;
	while (action) {
		printk(KERN_ERR "[<%p>] %pf", action->handler, action->handler);
		if (action->thread_fn)
			printk(KERN_CONT " threaded [<%p>] %pf",
					action->thread_fn, action->thread_fn);
		printk(KERN_CONT "\n");
		action = action->next;
	}
	raw_spin_unlock_irqrestore(&desc->lock, flags);
}

static void
report_bad_irq(unsigned int irq, struct irq_desc *desc, irqreturn_t action_ret)
{
	static int count = 100;

	if (count > 0) {
		count--;
		__report_bad_irq(irq, desc, action_ret);
	}
}

static inline int
try_misrouted_irq(unsigned int irq, struct irq_desc *desc,
		  irqreturn_t action_ret)
{
	struct irqaction *action;

	if (!irqfixup)
		return 0;

	/* We didn't actually handle the IRQ - see if it was misrouted? */
	if (action_ret == IRQ_NONE)
		return 1;

	/*
	 * But for 'irqfixup == 2' we also do it for handled interrupts if
	 * they are marked as IRQF_IRQPOLL (or for irq zero, which is the
	 * traditional PC timer interrupt.. Legacy)
	 */
	if (irqfixup < 2)
		return 0;

	if (!irq)
		return 1;

	/*
	 * Since we don't get the descriptor lock, "action" can
	 * change under us.  We don't really care, but we don't
	 * want to follow a NULL pointer. So tell the compiler to
	 * just load it once by using a barrier.
	 */
	action = desc->action;
	barrier();
	return action && (action->flags & IRQF_IRQPOLL);
}

void note_interrupt(unsigned int irq, struct irq_desc *desc,
		    irqreturn_t action_ret)
{
	if (desc->istate & IRQS_POLL_INPROGRESS)
		return;

	/* we get here again via the threaded handler */
	if (action_ret == IRQ_WAKE_THREAD)
		return;

	if (bad_action_ret(action_ret)) {
		report_bad_irq(irq, desc, action_ret);
		return;
	}

	if (unlikely(action_ret == IRQ_NONE)) {
		/*
		 * If we are seeing only the odd spurious IRQ caused by
		 * bus asynchronicity then don't eventually trigger an error,
		 * otherwise the counter becomes a doomsday timer for otherwise
		 * working systems
		 */
		if (time_after(jiffies, desc->last_unhandled + HZ/10))
			desc->irqs_unhandled = 1;
		else
			desc->irqs_unhandled++;
		desc->last_unhandled = jiffies;
	}

	if (unlikely(try_misrouted_irq(irq, desc, action_ret))) {
		int ok = misrouted_irq(irq);
		if (action_ret == IRQ_NONE)
			desc->irqs_unhandled -= ok;
	}

	desc->irq_count++;
	if (likely(desc->irq_count < 100000))
		return;

	desc->irq_count = 0;
	if (unlikely(desc->irqs_unhandled > 99900)) {
		/*
		 * The interrupt is stuck
		 */
		__report_bad_irq(irq, desc, action_ret);
		/*
		 * Now kill the IRQ
		 */
		printk(KERN_EMERG "Disabling IRQ #%d\n", irq);
		desc->istate |= IRQS_SPURIOUS_DISABLED;
		desc->depth++;
		irq_disable(desc);

		mod_timer(&poll_spurious_irq_timer,
			  jiffies + POLL_SPURIOUS_IRQ_INTERVAL);
	}
	desc->irqs_unhandled = 0;
}

int noirqdebug __read_mostly;

int noirqdebug_setup(char *str)
{
	noirqdebug = 1;
	printk(KERN_INFO "IRQ lockup detection disabled\n");

	return 1;
}

__setup("noirqdebug", noirqdebug_setup);
module_param(noirqdebug, bool, 0644);
MODULE_PARM_DESC(noirqdebug, "Disable irq lockup detection when true");

static int __init irqfixup_setup(char *str)
{
	irqfixup = 1;
	printk(KERN_WARNING "Misrouted IRQ fixup support enabled.\n");
	printk(KERN_WARNING "This may impact system performance.\n");

	return 1;
}

__setup("irqfixup", irqfixup_setup);
module_param(irqfixup, int, 0644);

static int __init irqpoll_setup(char *str)
{
	irqfixup = 2;
	printk(KERN_WARNING "Misrouted IRQ fixup and polling support "
				"enabled\n");
	printk(KERN_WARNING "This may significantly impact system "
				"performance\n");
	return 1;
}

__setup("irqpoll", irqpoll_setup);