aboutsummaryrefslogblamecommitdiffstats
blob: 33acb5e53a5ff0415ad14cae01ea318a92aab6d1 (plain) (tree)
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15














                                                            
                            
                         
                                 
                          
 



                                                      
                                      




                                         
                                             






                                         
                                             

                  







                                             
                 
                                                 
          

                                 
                                        


                                




                                                               

                                                   

                                                                              
                                                                                
 
                                     
                                            




                                                                      



                                                                            
   

                                     
                                                
                                
                                         


                                         
                            
                                          

  


                                                                
                                                                               



                                                   
                                                   



                                          
                                                                                




                                                              
                                             







                                                   



                                                                       
                                                                  
                                 


                                                     




                                        





                                                                               
                                         

                                
                            
 
                                                
                                                    
                                                     




                                     

                            


                       
                              


                                                             
                                         

 
                                         
 
                                                       
                                     
 
                                     
                                         
                                       

                  
                                                                

                                        
 

                                             




                                                             
                                             








                                                         
                                               
         
 
                  
 
           
                    

 




                                                                               
                                                                

                                       
                                                   

                                                                          
                                     
                                                                   
                                       




                            
/*
 * The "user cache".
 *
 * (C) Copyright 1991-2000 Linus Torvalds
 *
 * We have a per-user structure to keep track of how many
 * processes, files etc the user has claimed, in order to be
 * able to have per-user limits for system resources. 
 */

#include <linux/init.h>
#include <linux/sched.h>
#include <linux/slab.h>
#include <linux/bitops.h>
#include <linux/key.h>
#include <linux/interrupt.h>
#include <linux/export.h>
#include <linux/user_namespace.h>
#include <linux/proc_fs.h>

/*
 * userns count is 1 for root user, 1 for init_uts_ns,
 * and 1 for... ?
 */
struct user_namespace init_user_ns = {
	.uid_map = {
		.nr_extents = 1,
		.extent[0] = {
			.first = 0,
			.lower_first = 0,
			.count = 4294967295U,
		},
	},
	.gid_map = {
		.nr_extents = 1,
		.extent[0] = {
			.first = 0,
			.lower_first = 0,
			.count = 4294967295U,
		},
	},
	.projid_map = {
		.nr_extents = 1,
		.extent[0] = {
			.first = 0,
			.lower_first = 0,
			.count = 4294967295U,
		},
	},
	.kref = {
		.refcount	= ATOMIC_INIT(3),
	},
	.owner = GLOBAL_ROOT_UID,
	.group = GLOBAL_ROOT_GID,
	.proc_inum = PROC_USER_INIT_INO,
};
EXPORT_SYMBOL_GPL(init_user_ns);

/*
 * UID task count cache, to get fast user lookup in "alloc_uid"
 * when changing user ID's (ie setuid() and friends).
 */

#define UIDHASH_BITS	(CONFIG_BASE_SMALL ? 3 : 7)
#define UIDHASH_SZ	(1 << UIDHASH_BITS)
#define UIDHASH_MASK		(UIDHASH_SZ - 1)
#define __uidhashfn(uid)	(((uid >> UIDHASH_BITS) + uid) & UIDHASH_MASK)
#define uidhashentry(uid)	(uidhash_table + __uidhashfn((__kuid_val(uid))))

static struct kmem_cache *uid_cachep;
struct hlist_head uidhash_table[UIDHASH_SZ];

/*
 * The uidhash_lock is mostly taken from process context, but it is
 * occasionally also taken from softirq/tasklet context, when
 * task-structs get RCU-freed. Hence all locking must be softirq-safe.
 * But free_uid() is also called with local interrupts disabled, and running
 * local_bh_enable() with local interrupts disabled is an error - we'll run
 * softirq callbacks, and they can unconditionally enable interrupts, and
 * the caller of free_uid() didn't expect that..
 */
static DEFINE_SPINLOCK(uidhash_lock);

/* root_user.__count is 1, for init task cred */
struct user_struct root_user = {
	.__count	= ATOMIC_INIT(1),
	.processes	= ATOMIC_INIT(1),
	.files		= ATOMIC_INIT(0),
	.sigpending	= ATOMIC_INIT(0),
	.locked_shm     = 0,
	.uid		= GLOBAL_ROOT_UID,
};

/*
 * These routines must be called with the uidhash spinlock held!
 */
static void uid_hash_insert(struct user_struct *up, struct hlist_head *hashent)
{
	hlist_add_head(&up->uidhash_node, hashent);
}

static void uid_hash_remove(struct user_struct *up)
{
	hlist_del_init(&up->uidhash_node);
}

static struct user_struct *uid_hash_find(kuid_t uid, struct hlist_head *hashent)
{
	struct user_struct *user;
	struct hlist_node *h;

	hlist_for_each_entry(user, h, hashent, uidhash_node) {
		if (uid_eq(user->uid, uid)) {
			atomic_inc(&user->__count);
			return user;
		}
	}

	return NULL;
}

/* IRQs are disabled and uidhash_lock is held upon function entry.
 * IRQ state (as stored in flags) is restored and uidhash_lock released
 * upon function exit.
 */
static void free_user(struct user_struct *up, unsigned long flags)
	__releases(&uidhash_lock)
{
	uid_hash_remove(up);
	spin_unlock_irqrestore(&uidhash_lock, flags);
	key_put(up->uid_keyring);
	key_put(up->session_keyring);
	kmem_cache_free(uid_cachep, up);
}

/*
 * Locate the user_struct for the passed UID.  If found, take a ref on it.  The
 * caller must undo that ref with free_uid().
 *
 * If the user_struct could not be found, return NULL.
 */
struct user_struct *find_user(kuid_t uid)
{
	struct user_struct *ret;
	unsigned long flags;

	spin_lock_irqsave(&uidhash_lock, flags);
	ret = uid_hash_find(uid, uidhashentry(uid));
	spin_unlock_irqrestore(&uidhash_lock, flags);
	return ret;
}

void free_uid(struct user_struct *up)
{
	unsigned long flags;

	if (!up)
		return;

	local_irq_save(flags);
	if (atomic_dec_and_lock(&up->__count, &uidhash_lock))
		free_user(up, flags);
	else
		local_irq_restore(flags);
}

struct user_struct *alloc_uid(kuid_t uid)
{
	struct hlist_head *hashent = uidhashentry(uid);
	struct user_struct *up, *new;

	spin_lock_irq(&uidhash_lock);
	up = uid_hash_find(uid, hashent);
	spin_unlock_irq(&uidhash_lock);

	if (!up) {
		new = kmem_cache_zalloc(uid_cachep, GFP_KERNEL);
		if (!new)
			goto out_unlock;

		new->uid = uid;
		atomic_set(&new->__count, 1);

		/*
		 * Before adding this, check whether we raced
		 * on adding the same user already..
		 */
		spin_lock_irq(&uidhash_lock);
		up = uid_hash_find(uid, hashent);
		if (up) {
			key_put(new->uid_keyring);
			key_put(new->session_keyring);
			kmem_cache_free(uid_cachep, new);
		} else {
			uid_hash_insert(new, hashent);
			up = new;
		}
		spin_unlock_irq(&uidhash_lock);
	}

	return up;

out_unlock:
	return NULL;
}

static int __init uid_cache_init(void)
{
	int n;

	uid_cachep = kmem_cache_create("uid_cache", sizeof(struct user_struct),
			0, SLAB_HWCACHE_ALIGN|SLAB_PANIC, NULL);

	for(n = 0; n < UIDHASH_SZ; ++n)
		INIT_HLIST_HEAD(uidhash_table + n);

	/* Insert the root user immediately (init already runs as root) */
	spin_lock_irq(&uidhash_lock);
	uid_hash_insert(&root_user, uidhashentry(GLOBAL_ROOT_UID));
	spin_unlock_irq(&uidhash_lock);

	return 0;
}

module_init(uid_cache_init);