/*
* Kernel iptables module to track stats for packets based on user tags.
*
* (C) 2011 Google, Inc
*
* This program is free software; you can redistribute it and/or modify
* it under the terms of the GNU General Public License version 2 as
* published by the Free Software Foundation.
*/
/*
* There are run-time debug flags enabled via the debug_mask module param, or
* via the DEFAULT_DEBUG_MASK. See xt_qtaguid_internal.h.
*/
#define DEBUG
#include <linux/file.h>
#include <linux/inetdevice.h>
#include <linux/module.h>
#include <linux/netfilter/x_tables.h>
#include <linux/netfilter/xt_qtaguid.h>
#include <linux/skbuff.h>
#include <linux/workqueue.h>
#include <net/addrconf.h>
#include <net/sock.h>
#include <net/tcp.h>
#include <net/udp.h>
#if defined(CONFIG_IP6_NF_IPTABLES) || defined(CONFIG_IP6_NF_IPTABLES_MODULE)
#include <linux/netfilter_ipv6/ip6_tables.h>
#endif
#include <linux/netfilter/xt_socket.h>
#include "xt_qtaguid_internal.h"
#include "xt_qtaguid_print.h"
/*
* We only use the xt_socket funcs within a similar context to avoid unexpected
* return values.
*/
#define XT_SOCKET_SUPPORTED_HOOKS \
((1 << NF_INET_PRE_ROUTING) | (1 << NF_INET_LOCAL_IN))
static const char *module_procdirname = "xt_qtaguid";
static struct proc_dir_entry *xt_qtaguid_procdir;
static unsigned int proc_iface_perms = S_IRUGO;
module_param_named(iface_perms, proc_iface_perms, uint, S_IRUGO | S_IWUSR);
static struct proc_dir_entry *xt_qtaguid_stats_file;
static unsigned int proc_stats_perms = S_IRUGO;
module_param_named(stats_perms, proc_stats_perms, uint, S_IRUGO | S_IWUSR);
static struct proc_dir_entry *xt_qtaguid_ctrl_file;
/* Everybody can write. But proc_ctrl_write_limited is true by default which
* limits what can be controlled. See the can_*() functions.
*/
static unsigned int proc_ctrl_perms = S_IRUGO | S_IWUGO;
module_param_named(ctrl_perms, proc_ctrl_perms, uint, S_IRUGO | S_IWUSR);
/* Limited by default, so the gid of the ctrl and stats proc entries
* will limit what can be done. See the can_*() functions.
*/
static bool proc_stats_readall_limited = true;
static bool proc_ctrl_write_limited = true;
module_param_named(stats_readall_limited, proc_stats_readall_limited, bool,
S_IRUGO | S_IWUSR);
module_param_named(ctrl_write_limited, proc_ctrl_write_limited, bool,
S_IRUGO | S_IWUSR);
/*
* Limit the number of active tags (via socket tags) for a given UID.
* Multiple processes could share the UID.
*/
static int max_sock_tags = DEFAULT_MAX_SOCK_TAGS;
module_param(max_sock_tags, int, S_IRUGO | S_IWUSR);
/*
* After the kernel has initiallized this module, it is still possible
* to make it passive.
* Setting passive to Y:
* - the iface stats handling will not act on notifications.
* - iptables matches will never match.
* - ctrl commands silently succeed.
* - stats are always empty.
* This is mostly usefull when a bug is suspected.
*/
static bool module_passive;
module_param_named(passive, module_passive, bool, S_IRUGO | S_IWUSR);
/*
* Control how qtaguid data is tracked per proc/uid.
* Setting tag_tracking_passive to Y:
* - don't create proc specific structs to track tags
* - don't check that active tag stats exceed some limits.
* - don't clean up socket tags on process exits.
* This is mostly usefull when a bug is suspected.
*/
static bool qtu_proc_handling_passive;
module_param_named(tag_tracking_passive, qtu_proc_handling_passive, bool,
S_IRUGO | S_IWUSR);
#define QTU_DEV_NAME "xt_qtaguid"
uint qtaguid_debug_mask = DEFAULT_DEBUG_MASK;
module_param_named(debug_mask, qtaguid_debug_mask, uint, S_IRUGO | S_IWUSR);
/*---------------------------------------------------------------------------*/
static const char *iface_stat_procdirname = "iface_stat";
static struct proc_dir_entry *iface_stat_procdir;
/*
* The iface_stat_all* will go away once userspace gets use to the new fields
* that have a format line.
*/
static const char *iface_stat_all_procfilename = "iface_stat_all";
static struct proc_dir_entry *iface_stat_all_procfile;
static const char *iface_stat_fmt_procfilename = "iface_stat_fmt";
static struct proc_dir_entry *iface_stat_fmt_procfile;
/*
* Ordering of locks:
* outer locks:
* iface_stat_list_lock
* sock_tag_list_lock
* inner locks:
* uid_tag_data_tree_lock
* tag_counter_set_list_lock
* Notice how sock_tag_list_lock is held sometimes when uid_tag_data_tree_lock
* is acquired.
*
* Call tree with all lock holders as of 2012-04-27:
*
* iface_stat_fmt_proc_read()
* iface_stat_list_lock
* (struct iface_stat)
*
* qtaguid_ctrl_proc_read()
* sock_tag_list_lock
* (sock_tag_tree)
* (struct proc_qtu_data->sock_tag_list)
* prdebug_full_state()
* sock_tag_list_lock
* (sock_tag_tree)
* uid_tag_data_tree_lock
* (uid_tag_data_tree)
* (proc_qtu_data_tree)
* iface_stat_list_lock
*
* qtaguid_stats_proc_read()
* iface_stat_list_lock
* struct iface_stat->tag_stat_list_lock
*
* qtudev_open()
* uid_tag_data_tree_lock
*
* qtudev_release()
* sock_tag_data_list_lock
* uid_tag_data_tree_lock
* prdebug_full_state()
* sock_tag_list_lock
* uid_tag_data_tree_lock
* iface_stat_list_lock
*
* iface_netdev_event_handler()
* iface_stat_create()
* iface_stat_list_lock
* iface_stat_update()
* iface_stat_list_lock
*
* iface_inetaddr_event_handler()
* iface_stat_create()
* iface_stat_list_lock
* iface_stat_update()
* iface_stat_list_lock
*
* iface_inet6addr_event_handler()
* iface_stat_create_ipv6()
* iface_stat_list_lock
* iface_stat_update()
* iface_stat_list_lock
*
* qtaguid_mt()
* account_for_uid()
* if_tag_stat_update()
* get_sock_stat()
* sock_tag_list_lock
* struct iface_stat->tag_stat_list_lock
* tag_stat_update()
* get_active_counter_set()
* tag_counter_set_list_lock
* tag_stat_update()
* get_active_counter_set()
* tag_counter_set_list_lock
*
*
* qtaguid_ctrl_parse()
* ctrl_cmd_delete()
* sock_tag_list_lock
* tag_counter_set_list_lock
* iface_stat_list_lock
* struct iface_stat->tag_stat_list_lock
* uid_tag_data_tree_lock
* ctrl_cmd_counter_set()
* tag_counter_set_list_lock
* ctrl_cmd_tag()
* sock_tag_list_lock
* (sock_tag_tree)
* get_tag_ref()
* uid_tag_data_tree_lock
* (uid_tag_data_tree)
* uid_tag_data_tree_lock
* (proc_qtu_data_tree)
* ctrl_cmd_untag()
* sock_tag_list_lock
* uid_tag_data_tree_lock
*
*/
static LIST_HEAD(iface_stat_list);
static DEFINE_SPINLOCK(iface_stat_list_lock);
static struct rb_root sock_tag_tree = RB_ROOT;
static DEFINE_SPINLOCK(sock_tag_list_lock);
static struct rb_root tag_counter_set_tree = RB_ROOT;
static DEFINE_SPINLOCK(tag_counter_set_list_lock);
static struct rb_root uid_tag_data_tree = RB_ROOT;
static DEFINE_SPINLOCK(uid_tag_data_tree_lock);
static struct rb_root proc_qtu_data_tree = RB_ROOT;
/* No proc_qtu_data_tree_lock; use uid_tag_data_tree_lock */
static struct qtaguid_event_counts qtu_events;
/*----------------------------------------------*/
static bool can_manipulate_uids(void)
{
/* root pwnd */
return in_egroup_p(xt_qtaguid_ctrl_file->gid)
|| unlikely(!current_fsuid()) || unlikely(!proc_ctrl_write_limited)
|| unlikely(current_fsuid() == xt_qtaguid_ctrl_file->uid);
}
static bool can_impersonate_uid(uid_t uid)
{
return uid == current_fsuid() || can_manipulate_uids();
}
static bool can_read_other_uid_stats(uid_t uid)
{
/* root pwnd */
return in_egroup_p(xt_qtaguid_stats_file->gid)
|| unlikely(!current_fsuid()) || uid == current_fsuid()
|| unlikely(!proc_stats_readall_limited)
|| unlikely(current_fsuid() == xt_qtaguid_ctrl_file->uid);
}
static inline void dc_add_byte_packets(struct data_counters *counters, int set,
enum ifs_tx_rx direction,
enum ifs_proto ifs_proto,
int bytes,
int packets)
{
counters->bpc[set][direction][ifs_proto].bytes += bytes;
counters->bpc[set][direction][ifs_proto].packets += packets;
}
static struct tag_node *tag_node_tree_search(struct rb_root *root, tag_t tag)
{
struct rb_node *node = root->rb_node;
while (node) {
struct tag_node *data = rb_entry(node, struct tag_node, node);
int result;
RB_DEBUG("qtaguid: tag_node_tree_search(0x%llx): "
" node=%p data=%p\n", tag, node, data);
result = tag_compare(tag, data->tag);
RB_DEBUG("qtaguid: tag_node_tree_search(0x%llx): "
" data.tag=0x%llx (uid=%u) res=%d\n",
tag, data->tag, get_uid_from_tag(data->tag), result);
if (result < 0)
node = node->rb_left;
else if (result > 0)
node = node->rb_right;
else
return data;
}
return NULL;
}
static void tag_node_tree_insert(struct tag_node *data, struct rb_root *root)
{
struct rb_node **new = &(root->rb_node), *parent = NULL;
/* Figure out where to put new node */
while (*new) {
struct tag_node *this = rb_entry(*new, struct tag_node,
node);
int result = tag_compare(data->tag, this->tag);
RB_DEBUG("qtaguid: %s(): tag=0x%llx"
" (uid=%u)\n", __func__,
this->tag,
get_uid_from_tag(this->tag));
parent = *new;
if (result < 0)
new = &((*new)->rb_left);
else if (result > 0)
new = &((*new)->rb_right);
else
BUG();
}
/* Add new node and rebalance tree. */
rb_link_node(&data->node, parent, new);
rb_insert_color(&data->node, root);
}
static void tag_stat_tree_insert(struct tag_stat *data, struct rb_root *root)
{
tag_node_tree_insert(&data->tn, root);
}
static struct tag_stat *tag_stat_tree_search(struct rb_root *root, tag_t tag)
{
struct tag_node *node = tag_node_tree_search(root, tag);
if (!node)
return NULL;
return rb_entry(&node->node, struct tag_stat, tn.node);
}
static void tag_counter_set_tree_insert(struct tag_counter_set *data,
struct rb_root *root)
{
tag_node_tree_insert(&data->tn, root);
}
static struct tag_counter_set *tag_counter_set_tree_search(struct rb_root *root,
tag_t tag)
{
struct tag_node *node = tag_node_tree_search(root, tag);
if (!node)
return NULL;
return rb_entry(&node->node, struct tag_counter_set, tn.node);
}
static void tag_ref_tree_insert(struct tag_ref *data, struct rb_root *root)
{
tag_node_tree_insert(&data->tn, root);
}
static struct tag_ref *tag_ref_tree_search(struct rb_root *root, tag_t tag)
{
struct tag_node *node = tag_node_tree_search(root, tag);
if (!node)
return NULL;
return rb_entry(&node->node, struct tag_ref, tn.node);
}
static struct sock_tag *sock_tag_tree_search(struct rb_root *root,
const struct sock *sk)
{
struct rb_node *node = root->rb_node;
while (node) {
struct sock_tag *data = rb_entry(node, struct sock_tag,
sock_node);
if (sk < data->sk)
node = node->rb_left;
else if (sk > data->sk)
node = node->rb_right;
else
return data;
}
return NULL;
}
static void sock_tag_tree_insert(struct sock_tag *data, struct rb_root *root)
{
struct rb_node **new = &(root->rb_node), *parent = NULL;
/* Figure out where to put new node */
while (*new) {
struct sock_tag *this = rb_entry(*new, struct sock_tag,
sock_node);
parent = *new;
if (data->sk < this->sk)
new = &((*new)->rb_left);
else if (data->sk > this->sk)
new = &((*new)->rb_right);
else
BUG();
}
/* Add new node and rebalance tree. */
rb_link_node(&data->sock_node, parent, new);
rb_insert_color(&data->sock_node, root);
}
static void sock_tag_tree_erase(struct rb_root *st_to_free_tree)
{
struct rb_node *node;
struct sock_tag *st_entry;
node = rb_first(st_to_free_tree);
while (node) {
st_entry = rb_entry(node, struct sock_tag, sock_node);
node = rb_next(node);
CT_DEBUG("qtaguid: %s(): "
"erase st: sk=%p tag=0x%llx (uid=%u)\n", __func__,
st_entry->sk,
st_entry->tag,
get_uid_from_tag(st_entry->tag));
rb_erase(&st_entry->sock_node, st_to_free_tree);
sockfd_put(st_entry->socket);
kfree(st_entry);
}
}
static struct proc_qtu_data *proc_qtu_data_tree_search(struct rb_root *root,
const pid_t pid)
{
struct rb_node *node = root->rb_node;
while (node) {
struct proc_qtu_data *data = rb_entry(node,
struct proc_qtu_data,
node);
if (pid < data->pid)
node = node->rb_left;
else if (pid > data->pid)
node = node->rb_right;
else
return data;
}
return NULL;
}
static void proc_qtu_data_tree_insert(struct proc_qtu_data *data,
struct rb_root *root)
{
struct rb_node **new = &(root->rb_node), *parent = NULL;
/* Figure out where to put new node */
while (*new) {
struct proc_qtu_data *this = rb_entry(*new,
struct proc_qtu_data,
node);
parent = *new;
if (data->pid < this->pid)
new = &((*new)->rb_left);
else if (data->pid > this->pid)
new = &((*new)->rb_right);
else
BUG();
}
/* Add new node and rebalance tree. */
rb_link_node(&data->node, parent, new);
rb_insert_color(&data->node, root);
}
static void uid_tag_data_tree_insert(struct uid_tag_data *data,
struct rb_root *root)
{
struct rb_node **new = &(root->rb_node), *parent = NULL;
/* Figure out where to put new node */
while (*new) {
struct uid_tag_data *this = rb_entry(*new,
struct uid_tag_data,
node);
parent = *new;
if (data->uid < this->uid)
new = &((*new)->rb_left);
else if (data->uid > this->uid)
new = &((*new)->rb_right);
else
BUG();
}
/* Add new node and rebalance tree. */
rb_link_node(&data->node, parent, new);
rb_insert_color(&data->node, root);
}
static struct uid_tag_data *uid_tag_data_tree_search(struct rb_root *root,
uid_t uid)
{
struct rb_node *node = root->rb_node;
while (node) {
struct uid_tag_data *data = rb_entry(node,
struct uid_tag_data,
node);
if (uid < data->uid)
node = node->rb_left;
else if (uid > data->uid)
node = node->rb_right;
else
return data;
}
return NULL;
}
/*
* Allocates a new uid_tag_data struct if needed.
* Returns a pointer to the found or allocated uid_tag_data.
* Returns a PTR_ERR on failures, and lock is not held.
* If found is not NULL:
* sets *found to true if not allocated.
* sets *found to false if allocated.
*/
struct uid_tag_data *get_uid_data(uid_t uid, bool *found_res)
{
struct uid_tag_data *utd_entry;
/* Look for top level uid_tag_data for the UID */
utd_entry = uid_tag_data_tree_search(&uid_tag_data_tree, uid);
DR_DEBUG("qtaguid: get_uid_data(%u) utd=%p\n", uid, utd_entry);
if (found_res)
*found_res = utd_entry;
if (utd_entry)
return utd_entry;
utd_entry = kzalloc(sizeof(*utd_entry), GFP_ATOMIC);
if (!utd_entry) {
pr_err("qtaguid: get_uid_data(%u): "
"tag data alloc failed\n", uid);
return ERR_PTR(-ENOMEM);
}
utd_entry->uid = uid;
utd_entry->tag_ref_tree = RB_ROOT;
uid_tag_data_tree_insert(utd_entry, &uid_tag_data_tree);
DR_DEBUG("qtaguid: get_uid_data(%u) new utd=%p\n", uid, utd_entry);
return utd_entry;
}
/* Never returns NULL. Either PTR_ERR or a valid ptr. */
static struct tag_ref *new_tag_ref(tag_t new_tag,
struct uid_tag_data *utd_entry)
{
struct tag_ref *tr_entry;
int res;
if (utd_entry->num_active_tags + 1 > max_sock_tags) {
pr_info("qtaguid: new_tag_ref(0x%llx): "
"tag ref alloc quota exceeded. max=%d\n",
new_tag, max_sock_tags);
res = -EMFILE;
goto err_res;
}
tr_entry = kzalloc(sizeof(*tr_entry), GFP_ATOMIC);
if (!tr_entry) {
pr_err("qtaguid: new_tag_ref(0x%llx): "
"tag ref alloc failed\n",
new_tag);
res = -ENOMEM;
goto err_res;
}
tr_entry->tn.tag = new_tag;
/* tr_entry->num_sock_tags handled by caller */
utd_entry->num_active_tags++;
tag_ref_tree_insert(tr_entry, &utd_entry->tag_ref_tree);
DR_DEBUG("qtaguid: new_tag_ref(0x%llx): "
" inserted new tag ref %p\n",
new_tag, tr_entry);
return tr_entry;
err_res:
return ERR_PTR(res);
}
static struct tag_ref *lookup_tag_ref(tag_t full_tag,
struct uid_tag_data **utd_res)
{
struct uid_tag_data *utd_entry;
struct tag_ref *tr_entry;
bool found_utd;
uid_t uid = get_uid_from_tag(full_tag);
DR_DEBUG("qtaguid: lookup_tag_ref(tag=0x%llx (uid=%u))\n",
full_tag, uid);
utd_entry = get_uid_data(uid, &found_utd);
if (IS_ERR_OR_NULL(utd_entry)) {
if (utd_res)
*utd_res = utd_entry;
return NULL;
}
tr_entry = tag_ref_tree_search(&utd_entry->tag_ref_tree, full_tag);
if (utd_res)
*utd_res = utd_entry;
DR_DEBUG("qtaguid: lookup_tag_ref(0x%llx) utd_entry=%p tr_entry=%p\n",
full_tag, utd_entry, tr_entry);
return tr_entry;
}
/* Never returns NULL. Either PTR_ERR or a valid ptr. */
static struct tag_ref *get_tag_ref(tag_t full_tag,
struct uid_tag_data **utd_res)
{
struct uid_tag_data *utd_entry;
struct tag_ref *tr_entry;
DR_DEBUG("qtaguid: get_tag_ref(0x%llx)\n",
full_tag);
spin_lock_bh(&uid_tag_data_tree_lock);
tr_entry = lookup_tag_ref(full_tag, &utd_entry);
BUG_ON(IS_ERR_OR_NULL(utd_entry));
if (!tr_entry)
tr_entry = new_tag_ref(full_tag, utd_entry);
spin_unlock_bh(&uid_tag_data_tree_lock);
if (utd_res)
*utd_res = utd_entry;
DR_DEBUG("qtaguid: get_tag_ref(0x%llx) utd=%p tr=%p\n",
full_tag, utd_entry, tr_entry);
return tr_entry;
}
/* Checks and maybe frees the UID Tag Data entry */
static void put_utd_entry(struct uid_tag_data *utd_entry)
{
/* Are we done with the UID tag data entry? */
if (RB_EMPTY_ROOT(&utd_entry->tag_ref_tree) &&
!utd_entry->num_pqd) {
DR_DEBUG("qtaguid: %s(): "
"erase utd_entry=%p uid=%u "
"by pid=%u tgid=%u uid=%u\n", __func__,
utd_entry, utd_entry->uid,
current->pid, current->tgid, current_fsuid());
BUG_ON(utd_entry->num_active_tags);
rb_erase(&utd_entry->node, &uid_tag_data_tree);
kfree(utd_entry);
} else {
DR_DEBUG("qtaguid: %s(): "
"utd_entry=%p still has %d tags %d proc_qtu_data\n",
__func__, utd_entry, utd_entry->num_active_tags,
utd_entry->num_pqd);
BUG_ON(!(utd_entry->num_active_tags ||
utd_entry->num_pqd));
}
}
/*
* If no sock_tags are using this tag_ref,
* decrements refcount of utd_entry, removes tr_entry
* from utd_entry->tag_ref_tree and frees.
*/
static void free_tag_ref_from_utd_entry(struct tag_ref *tr_entry,
struct uid_tag_data *utd_entry)
{
DR_DEBUG("qtaguid: %s(): %p tag=0x%llx (uid=%u)\n", __func__,
tr_entry, tr_entry->tn.tag,
get_uid_from_tag(tr_entry->tn.tag));
if (!tr_entry->num_sock_tags) {
BUG_ON(!utd_entry->num_active_tags);
utd_entry->num_active_tags--;
rb_erase(&tr_entry->tn.node, &utd_entry->tag_ref_tree);
DR_DEBUG("qtaguid: %s(): erased %p\n", __func__, tr_entry);
kfree(tr_entry);
}
}
static void put_tag_ref_tree(tag_t full_tag, struct uid_tag_data *utd_entry)
{
struct rb_node *node;
struct tag_ref *tr_entry;
tag_t acct_tag;
DR_DEBUG("qtaguid: %s(tag=0x%llx (uid=%u))\n", __func__,
full_tag, get_uid_from_tag(full_tag));
acct_tag = get_atag_from_tag(full_tag);
node = rb_first(&utd_entry->tag_ref_tree);
while (node) {
tr_entry = rb_entry(node, struct tag_ref, tn.node);
node = rb_next(node);
if (!acct_tag || tr_entry->tn.tag == full_tag)
free_tag_ref_from_utd_entry(tr_entry, utd_entry);
}
}
static int read_proc_u64(char *page, char **start, off_t off,
int count, int *eof, void *data)
{
int len;
uint64_t value;
char *p = page;
uint64_t *iface_entry = data;
if (!data)
return 0;
value = *iface_entry;
p += sprintf(p, "%llu\n", value);
len = (p - page) - off;
*eof = (len <= count) ? 1 : 0;
*start = page + off;
return len;
}
static int read_proc_bool(char *page, char **start, off_t off,
int count, int *eof, void *data)
{
int len;
bool value;
char *p = page;
bool *bool_entry = data;
if (!data)
return 0;
value = *bool_entry;
p += sprintf(p, "%u\n", value);
len = (p - page) - off;
*eof = (len <= count) ? 1 : 0;
*start = page + off;
return len;
}
static int get_active_counter_set(tag_t tag)
{
int active_set = 0;
struct tag_counter_set *tcs;
MT_DEBUG("qtaguid: get_active_counter_set(tag=0x%llx)"
" (uid=%u)\n",
tag, get_uid_from_tag(tag));
/* For now we only handle UID tags for active sets */
tag = get_utag_from_tag(tag);
spin_lock_bh(&tag_counter_set_list_lock);
tcs = tag_counter_set_tree_search(&tag_counter_set_tree, tag);
if (tcs)
active_set = tcs->active_set;
spin_unlock_bh(&tag_counter_set_list_lock);
return active_set;
}
/*
* Find the entry for tracking the specified interface.
* Caller must hold iface_stat_list_lock
*/
static struct iface_stat *get_iface_entry(const char *ifname)
{
struct iface_stat *iface_entry;
/* Find the entry for tracking the specified tag within the interface */
if (ifname == NULL) {
pr_info("qtaguid: iface_stat: get() NULL device name\n");
return NULL;
}
/* Iterate over interfaces */
list_for_each_entry(iface_entry, &iface_stat_list, list) {
if (!strcmp(ifname, iface_entry->ifname))
goto done;
}
iface_entry = NULL;
done:
return iface_entry;
}
/* This is for fmt2 only */
static int pp_iface_stat_line(bool header, char *outp,
int char_count, struct iface_stat *iface_entry)
{
int len;
if (header) {
len = snprintf(outp, char_count,
"ifname "
"total_skb_rx_bytes total_skb_rx_packets "
"total_skb_tx_bytes total_skb_tx_packets "
"rx_tcp_bytes rx_tcp_packets "
"rx_udp_bytes rx_udp_packets "
"rx_other_bytes rx_other_packets "
"tx_tcp_bytes tx_tcp_packets "
"tx_udp_bytes tx_udp_packets "
"tx_other_bytes tx_other_packets\n"
);
} else {
struct data_counters *cnts;
int cnt_set = 0; /* We only use one set for the device */
cnts = &iface_entry->totals_via_skb;
len = snprintf(
outp, char_count,
"%s "
"%llu %llu %llu %llu %llu %llu %llu %llu "
"%llu %llu %llu %llu %llu %llu %llu %llu\n",
iface_entry->ifname,
dc_sum_bytes(cnts, cnt_set, IFS_RX),
dc_sum_packets(cnts, cnt_set, IFS_RX),
dc_sum_bytes(cnts, cnt_set, IFS_TX),
dc_sum_packets(cnts, cnt_set, IFS_TX),
cnts->bpc[cnt_set][IFS_RX][IFS_TCP].bytes,
cnts->bpc[cnt_set][IFS_RX][IFS_TCP].packets,
cnts->bpc[cnt_set][IFS_RX][IFS_UDP].bytes,
cnts->bpc[cnt_set][IFS_RX][IFS_UDP].packets,
cnts->bpc[cnt_set][IFS_RX][IFS_PROTO_OTHER].bytes,
cnts->bpc[cnt_set][IFS_RX][IFS_PROTO_OTHER].packets,
cnts->bpc[cnt_set][IFS_TX][IFS_TCP].bytes,
cnts->bpc[cnt_set][IFS_TX][IFS_TCP].packets,
cnts->bpc[cnt_set][IFS_TX][IFS_UDP].bytes,
cnts->bpc[cnt_set][IFS_TX][IFS_UDP].packets,
cnts->bpc[cnt_set][IFS_TX][IFS_PROTO_OTHER].bytes,
cnts->bpc[cnt_set][IFS_TX][IFS_PROTO_OTHER].packets);
}
return len;
}
static int iface_stat_fmt_proc_read(char *page, char **num_items_returned,
off_t items_to_skip, int char_count,
int *eof, void *data)
{
char *outp = page;
int item_index = 0;
int len;
int fmt = (int)data; /* The data is just 1 (old) or 2 (uses fmt) */
struct iface_stat *iface_entry;
struct rtnl_link_stats64 dev_stats, *stats;
struct rtnl_link_stats64 no_dev_stats = {0};
if (unlikely(module_passive)) {
*eof = 1;
return 0;
}
CT_DEBUG("qtaguid:proc iface_stat_fmt "
"pid=%u tgid=%u uid=%u "
"page=%p *num_items_returned=%p off=%ld "
"char_count=%d *eof=%d\n",
current->pid, current->tgid, current_fsuid(),
page, *num_items_returned,
items_to_skip, char_count, *eof);
if (*eof)
return 0;
if (fmt == 2 && item_index++ >= items_to_skip) {
len = pp_iface_stat_line(true, outp, char_count, NULL);
if (len >= char_count) {
*outp = '\0';
return outp - page;
}
outp += len;
char_count -= len;
(*num_items_returned)++;
}
/*
* This lock will prevent iface_stat_update() from changing active,
* and in turn prevent an interface from unregistering itself.
*/
spin_lock_bh(&iface_stat_list_lock);
list_for_each_entry(iface_entry, &iface_stat_list, list) {
if (item_index++ < items_to_skip)
continue;
if (iface_entry->active) {
stats = dev_get_stats(iface_entry->net_dev,
&dev_stats);
} else {
stats = &no_dev_stats;
}
/*
* If the meaning of the data changes, then update the fmtX
* string.
*/
if (fmt == 1) {
len = snprintf(
outp, char_count,
"%s %d "
"%llu %llu %llu %llu "
"%llu %llu %llu %llu\n",
iface_entry->ifname,
iface_entry->active,
iface_entry->totals_via_dev[IFS_RX].bytes,
iface_entry->totals_via_dev[IFS_RX].packets,
iface_entry->totals_via_dev[IFS_TX].bytes,
iface_entry->totals_via_dev[IFS_TX].packets,
stats->rx_bytes, stats->rx_packets,
stats->tx_bytes, stats->tx_packets
);
} else {
len = pp_iface_stat_line(false, outp, char_count,
iface_entry);
}
if (len >= char_count) {
spin_unlock_bh(&iface_stat_list_lock);
*outp = '\0';
return outp - page;
}
outp += len;
char_count -= len;
(*num_items_returned)++;
}
spin_unlock_bh(&iface_stat_list_lock);
*eof = 1;
return outp - page;
}
static void iface_create_proc_worker(struct work_struct *work)
{
struct proc_dir_entry *proc_entry;
struct iface_stat_work *isw = container_of(work, struct iface_stat_work,
iface_work);
struct iface_stat *new_iface = isw->iface_entry;
/* iface_entries are not deleted, so safe to manipulate. */
proc_entry = proc_mkdir(new_iface->ifname, iface_stat_procdir);
if (IS_ERR_OR_NULL(proc_entry)) {
pr_err("qtaguid: iface_stat: create_proc(): alloc failed.\n");
kfree(isw);
return;
}
new_iface->proc_ptr = proc_entry;
create_proc_read_entry("tx_bytes", proc_iface_perms, proc_entry,
read_proc_u64,
&new_iface->totals_via_dev[IFS_TX].bytes);
create_proc_read_entry("rx_bytes", proc_iface_perms, proc_entry,
read_proc_u64,
&new_iface->totals_via_dev[IFS_RX].bytes);
create_proc_read_entry("tx_packets", proc_iface_perms, proc_entry,
read_proc_u64,
&new_iface->totals_via_dev[IFS_TX].packets);
create_proc_read_entry("rx_packets", proc_iface_perms, proc_entry,
read_proc_u64,
&new_iface->totals_via_dev[IFS_RX].packets);
create_proc_read_entry("active", proc_iface_perms, proc_entry,
read_proc_bool, &new_iface->active);
IF_DEBUG("qtaguid: iface_stat: create_proc(): done "
"entry=%p dev=%s\n", new_iface, new_iface->ifname);
kfree(isw);
}
/*
* Will set the entry's active state, and
* update the net_dev accordingly also.
*/
static void _iface_stat_set_active(struct iface_stat *entry,
struct net_device *net_dev,
bool activate)
{
if (activate) {
entry->net_dev = net_dev;
entry->active = true;
IF_DEBUG("qtaguid: %s(%s): "
"enable tracking. rfcnt=%d\n", __func__,
entry->ifname,
__this_cpu_read(*net_dev->pcpu_refcnt));
} else {
entry->active = false;
entry->net_dev = NULL;
IF_DEBUG("qtaguid: %s(%s): "
"disable tracking. rfcnt=%d\n", __func__,
entry->ifname,
__this_cpu_read(*net_dev->pcpu_refcnt));
}
}
/* Caller must hold iface_stat_list_lock */
static struct iface_stat *iface_alloc(struct net_device *net_dev)
{
struct iface_stat *new_iface;
struct iface_stat_work *isw;
new_iface = kzalloc(sizeof(*new_iface), GFP_ATOMIC);
if (new_iface == NULL) {
pr_err("qtaguid: iface_stat: create(%s): "
"iface_stat alloc failed\n", net_dev->name);
return NULL;
}
new_iface->ifname = kstrdup(net_dev->name, GFP_ATOMIC);
if (new_iface->ifname == NULL) {
pr_err("qtaguid: iface_stat: create(%s): "
"ifname alloc failed\n", net_dev->name);
kfree(new_iface);
return NULL;
}
spin_lock_init(&new_iface->tag_stat_list_lock);
new_iface->tag_stat_tree = RB_ROOT;
_iface_stat_set_active(new_iface, net_dev, true);
/*
* ipv6 notifier chains are atomic :(
* No create_proc_read_entry() for you!
*/
isw = kmalloc(sizeof(*isw), GFP_ATOMIC);
if (!isw) {
pr_err("qtaguid: iface_stat: create(%s): "
"work alloc failed\n", new_iface->ifname);
_iface_stat_set_active(new_iface, net_dev, false);
kfree(new_iface->ifname);
kfree(new_iface);
return NULL;
}
isw->iface_entry = new_iface;
INIT_WORK(&isw->iface_work, iface_create_proc_worker);
schedule_work(&isw->iface_work);
list_add(&new_iface->list, &iface_stat_list);
return new_iface;
}
static void iface_check_stats_reset_and_adjust(struct net_device *net_dev,
struct iface_stat *iface)
{
struct rtnl_link_stats64 dev_stats, *stats;
bool stats_rewound;
stats = dev_get_stats(net_dev, &dev_stats);
/* No empty packets */
stats_rewound =
(stats->rx_bytes < iface->last_known[IFS_RX].bytes)
|| (stats->tx_bytes < iface->last_known[IFS_TX].bytes);
IF_DEBUG("qtaguid: %s(%s): iface=%p netdev=%p "
"bytes rx/tx=%llu/%llu "
"active=%d last_known=%d "
"stats_rewound=%d\n", __func__,
net_dev ? net_dev->name : "?",
iface, net_dev,
stats->rx_bytes, stats->tx_bytes,
iface->active, iface->last_known_valid, stats_rewound);
if (iface->active && iface->last_known_valid && stats_rewound) {
pr_warn_once("qtaguid: iface_stat: %s(%s): "
"iface reset its stats unexpectedly\n", __func__,
net_dev->name);
iface->totals_via_dev[IFS_TX].bytes +=
iface->last_known[IFS_TX].bytes;
iface->totals_via_dev[IFS_TX].packets +=
iface->last_known[IFS_TX].packets;
iface->totals_via_dev[IFS_RX].bytes +=
iface->last_known[IFS_RX].bytes;
iface->totals_via_dev[IFS_RX].packets +=
iface->last_known[IFS_RX].packets;
iface->last_known_valid = false;
IF_DEBUG("qtaguid: %s(%s): iface=%p "
"used last known bytes rx/tx=%llu/%llu\n", __func__,
iface->ifname, iface, iface->last_known[IFS_RX].bytes,
iface->last_known[IFS_TX].bytes);
}
}
/*
* Create a new entry for tracking the specified interface.
* Do nothing if the entry already exists.
* Called when an interface is configured with a valid IP address.
*/
static void iface_stat_create(struct net_device *net_dev,
struct in_ifaddr *ifa)
{
struct in_device *in_dev = NULL;
const char *ifname;
struct iface_stat *entry;
__be32 ipaddr = 0;
struct iface_stat *new_iface;
IF_DEBUG("qtaguid: iface_stat: create(%s): ifa=%p netdev=%p\n",
net_dev ? net_dev->name : "?",
ifa, net_dev);
if (!net_dev) {
pr_err("qtaguid: iface_stat: create(): no net dev\n");
return;
}
ifname = net_dev->name;
if (!ifa) {
in_dev = in_dev_get(net_dev);
if (!in_dev) {
pr_err("qtaguid: iface_stat: create(%s): no inet dev\n",
ifname);
return;
}
IF_DEBUG("qtaguid: iface_stat: create(%s): in_dev=%p\n",
ifname, in_dev);
for (ifa = in_dev->ifa_list; ifa; ifa = ifa->ifa_next) {
IF_DEBUG("qtaguid: iface_stat: create(%s): "
"ifa=%p ifa_label=%s\n",
ifname, ifa,
ifa->ifa_label ? ifa->ifa_label : "(null)");
if (ifa->ifa_label && !strcmp(ifname, ifa->ifa_label))
break;
}
}
if (!ifa) {
IF_DEBUG("qtaguid: iface_stat: create(%s): no matching IP\n",
ifname);
goto done_put;
}
ipaddr = ifa->ifa_local;
spin_lock_bh(&iface_stat_list_lock);
entry = get_iface_entry(ifname);
if (entry != NULL) {
IF_DEBUG("qtaguid: iface_stat: create(%s): entry=%p\n",
ifname, entry);
iface_check_stats_reset_and_adjust(net_dev, entry);
_iface_stat_set_active(entry, net_dev, true);
IF_DEBUG("qtaguid: %s(%s): "
"tracking now %d on ip=%pI4\n", __func__,
entry->ifname, true, &ipaddr);
goto done_unlock_put;
}
new_iface = iface_alloc(net_dev);
IF_DEBUG("qtaguid: iface_stat: create(%s): done "
"entry=%p ip=%pI4\n", ifname, new_iface, &ipaddr);
done_unlock_put:
spin_unlock_bh(&iface_stat_list_lock);
done_put:
if (in_dev)
in_dev_put(in_dev);
}
static void iface_stat_create_ipv6(struct net_device *net_dev,
struct inet6_ifaddr *ifa)
{
struct in_device *in_dev;
const char *ifname;
struct iface_stat *entry;
struct iface_stat *new_iface;
int addr_type;
IF_DEBUG("qtaguid: iface_stat: create6(): ifa=%p netdev=%p->name=%s\n",
ifa, net_dev, net_dev ? net_dev->name : "");
if (!net_dev) {
pr_err("qtaguid: iface_stat: create6(): no net dev!\n");
return;
}
ifname = net_dev->name;
in_dev = in_dev_get(net_dev);
if (!in_dev) {
pr_err("qtaguid: iface_stat: create6(%s): no inet dev\n",
ifname);
return;
}
IF_DEBUG("qtaguid: iface_stat: create6(%s): in_dev=%p\n",
ifname, in_dev);
if (!ifa) {
IF_DEBUG("qtaguid: iface_stat: create6(%s): no matching IP\n",
ifname);
goto done_put;
}
addr_type = ipv6_addr_type(&ifa->addr);
spin_lock_bh(&iface_stat_list_lock);
entry = get_iface_entry(ifname);
if (entry != NULL) {
IF_DEBUG("qtaguid: %s(%s): entry=%p\n", __func__,
ifname, entry);
iface_check_stats_reset_and_adjust(net_dev, entry);
_iface_stat_set_active(entry, net_dev, true);
IF_DEBUG("qtaguid: %s(%s): "
"tracking now %d on ip=%pI6c\n", __func__,
entry->ifname, true, &ifa->addr);
goto done_unlock_put;
}
new_iface = iface_alloc(net_dev);
IF_DEBUG("qtaguid: iface_stat: create6(%s): done "
"entry=%p ip=%pI6c\n", ifname, new_iface, &ifa->addr);
done_unlock_put:
spin_unlock_bh(&iface_stat_list_lock);
done_put:
in_dev_put(in_dev);
}
static struct sock_tag *get_sock_stat_nl(const struct sock *sk)
{
MT_DEBUG("qtaguid: get_sock_stat_nl(sk=%p)\n", sk);
return sock_tag_tree_search(&sock_tag_tree, sk);
}
static struct sock_tag *get_sock_stat(const struct sock *sk)
{
struct sock_tag *sock_tag_entry;
MT_DEBUG("qtaguid: get_sock_stat(sk=%p)\n", sk);
if (!sk)
return NULL;
spin_lock_bh(&sock_tag_list_lock);
sock_tag_entry = get_sock_stat_nl(sk);
spin_unlock_bh(&sock_tag_list_lock);
return sock_tag_entry;
}
static int ipx_proto(const struct sk_buff *skb,
struct xt_action_param *par)
{
int thoff = 0, tproto;
switch (par->family) {
case NFPROTO_IPV6:
tproto = ipv6_find_hdr(skb, &thoff, -1, NULL, NULL);
if (tproto < 0)
MT_DEBUG("%s(): transport header not found in ipv6"
" skb=%p\n", __func__, skb);
break;
case NFPROTO_IPV4:
tproto = ip_hdr(skb)->protocol;
break;
default:
tproto = IPPROTO_RAW;
}
return tproto;
}
static void
data_counters_update(struct data_counters *dc, int set,
enum ifs_tx_rx direction, int proto, int bytes)
{
switch (proto) {
case IPPROTO_TCP:
dc_add_byte_packets(dc, set, direction, IFS_TCP, bytes, 1);
break;
case IPPROTO_UDP:
dc_add_byte_packets(dc, set, direction, IFS_UDP, bytes, 1);
break;
case IPPROTO_IP:
default:
dc_add_byte_packets(dc, set, direction, IFS_PROTO_OTHER, bytes,
1);
break;
}
}
/*
* Update stats for the specified interface. Do nothing if the entry
* does not exist (when a device was never configured with an IP address).
* Called when an device is being unregistered.
*/
static void iface_stat_update(struct net_device *net_dev, bool stash_only)
{
struct rtnl_link_stats64 dev_stats, *stats;
struct iface_stat *entry;
stats = dev_get_stats(net_dev, &dev_stats);
spin_lock_bh(&iface_stat_list_lock);
entry = get_iface_entry(net_dev->name);
if (entry == NULL) {
IF_DEBUG("qtaguid: iface_stat: update(%s): not tracked\n",
net_dev->name);
spin_unlock_bh(&iface_stat_list_lock);
return;
}
IF_DEBUG("qtaguid: %s(%s): entry=%p\n", __func__,
net_dev->name, entry);
if (!entry->active) {
IF_DEBUG("qtaguid: %s(%s): already disabled\n", __func__,
net_dev->name);
spin_unlock_bh(&iface_stat_list_lock);
return;
}
if (stash_only) {
entry->last_known[IFS_TX].bytes = stats->tx_bytes;
entry->last_known[IFS_TX].packets = stats->tx_packets;
entry->last_known[IFS_RX].bytes = stats->rx_bytes;
entry->last_known[IFS_RX].packets = stats->rx_packets;
entry->last_known_valid = true;
IF_DEBUG("qtaguid: %s(%s): "
"dev stats stashed rx/tx=%llu/%llu\n", __func__,
net_dev->name, stats->rx_bytes, stats->tx_bytes);
spin_unlock_bh(&iface_stat_list_lock);
return;
}
entry->totals_via_dev[IFS_TX].bytes += stats->tx_bytes;
entry->totals_via_dev[IFS_TX].packets += stats->tx_packets;
entry->totals_via_dev[IFS_RX].bytes += stats->rx_bytes;
entry->totals_via_dev[IFS_RX].packets += stats->rx_packets;
/* We don't need the last_known[] anymore */
entry->last_known_valid = false;
_iface_stat_set_active(entry, net_dev, false);
IF_DEBUG("qtaguid: %s(%s): "
"disable tracking. rx/tx=%llu/%llu\n", __func__,
net_dev->name, stats->rx_bytes, stats->tx_bytes);
spin_unlock_bh(&iface_stat_list_lock);
}
/*
* Update stats for the specified interface from the skb.
* Do nothing if the entry
* does not exist (when a device was never configured with an IP address).
* Called on each sk.
*/
static void iface_stat_update_from_skb(const struct sk_buff *skb,
struct xt_action_param *par)
{
struct iface_stat *entry;
const struct net_device *el_dev;
enum ifs_tx_rx direction = par->in ? IFS_RX : IFS_TX;
int bytes = skb->len;
int proto;
if (!skb->dev) {
MT_DEBUG("qtaguid[%d]: no skb->dev\n", par->hooknum);
el_dev = par->in ? : par->out;
} else {
const struct net_device *other_dev;
el_dev = skb->dev;
other_dev = par->in ? : par->out;
if (el_dev != other_dev) {
MT_DEBUG("qtaguid[%d]: skb->dev=%p %s vs "
"par->(in/out)=%p %s\n",
par->hooknum, el_dev, el_dev->name, other_dev,
other_dev->name);
}
}
if (unlikely(!el_dev)) {
pr_err("qtaguid[%d]: %s(): no par->in/out?!!\n",
par->hooknum, __func__);
BUG();
} else if (unlikely(!el_dev->name)) {
pr_err("qtaguid[%d]: %s(): no dev->name?!!\n",
par->hooknum, __func__);
BUG();
} else {
proto = ipx_proto(skb, par);
MT_DEBUG("qtaguid[%d]: dev name=%s type=%d fam=%d proto=%d\n",
par->hooknum, el_dev->name, el_dev->type,
par->family, proto);
}
spin_lock_bh(&iface_stat_list_lock);
entry = get_iface_entry(el_dev->name);
if (entry == NULL) {
IF_DEBUG("qtaguid: iface_stat: %s(%s): not tracked\n",
__func__, el_dev->name);
spin_unlock_bh(&iface_stat_list_lock);
return;
}
IF_DEBUG("qtaguid: %s(%s): entry=%p\n", __func__,
el_dev->name, entry);
data_counters_update(&entry->totals_via_skb, 0, direction, proto,
bytes);
spin_unlock_bh(&iface_stat_list_lock);
}
static void tag_stat_update(struct tag_stat *tag_entry,
enum ifs_tx_rx direction, int proto, int bytes)
{
int active_set;
active_set = get_active_counter_set(tag_entry->tn.tag);
MT_DEBUG("qtaguid: tag_stat_update(tag=0x%llx (uid=%u) set=%d "
"dir=%d proto=%d bytes=%d)\n",
tag_entry->tn.tag, get_uid_from_tag(tag_entry->tn.tag),
active_set, direction, proto, bytes);
data_counters_update(&tag_entry->counters, active_set, direction,
proto, bytes);
if (tag_entry->parent_counters)
data_counters_update(tag_entry->parent_counters, active_set,
direction, proto, bytes);
}
/*
* Create a new entry for tracking the specified {acct_tag,uid_tag} within
* the interface.
* iface_entry->tag_stat_list_lock should be held.
*/
static struct tag_stat *create_if_tag_stat(struct iface_stat *iface_entry,
tag_t tag)
{
struct tag_stat *new_tag_stat_entry = NULL;
IF_DEBUG("qtaguid: iface_stat: %s(): ife=%p tag=0x%llx"
" (uid=%u)\n", __func__,
iface_entry, tag, get_uid_from_tag(tag));
new_tag_stat_entry = kzalloc(sizeof(*new_tag_stat_entry), GFP_ATOMIC);
if (!new_tag_stat_entry) {
pr_err("qtaguid: iface_stat: tag stat alloc failed\n");
goto done;
}
new_tag_stat_entry->tn.tag = tag;
tag_stat_tree_insert(new_tag_stat_entry, &iface_entry->tag_stat_tree);
done:
return new_tag_stat_entry;
}
static void if_tag_stat_update(const char *ifname, uid_t uid,
const struct sock *sk, enum ifs_tx_rx direction,
int proto, int bytes)
{
struct tag_stat *tag_stat_entry;
tag_t tag, acct_tag;
tag_t uid_tag;
struct data_counters *uid_tag_counters;
struct sock_tag *sock_tag_entry;
struct iface_stat *iface_entry;
struct tag_stat *new_tag_stat = NULL;
MT_DEBUG("qtaguid: if_tag_stat_update(ifname=%s "
"uid=%u sk=%p dir=%d proto=%d bytes=%d)\n",
ifname, uid, sk, direction, proto, bytes);
iface_entry = get_iface_entry(ifname);
if (!iface_entry) {
pr_err("qtaguid: iface_stat: stat_update() %s not found\n",
ifname);
return;
}
/* It is ok to process data when an iface_entry is inactive */
MT_DEBUG("qtaguid: iface_stat: stat_update() dev=%s entry=%p\n",
ifname, iface_entry);
/*
* Look for a tagged sock.
* It will have an acct_uid.
*/
sock_tag_entry = get_sock_stat(sk);
if (sock_tag_entry) {
tag = sock_tag_entry->tag;
acct_tag = get_atag_from_tag(tag);
uid_tag = get_utag_from_tag(tag);
} else {
acct_tag = make_atag_from_value(0);
tag = combine_atag_with_uid(acct_tag, uid);
uid_tag = make_tag_from_uid(uid);
}
MT_DEBUG("qtaguid: iface_stat: stat_update(): "
" looking for tag=0x%llx (uid=%u) in ife=%p\n",
tag, get_uid_from_tag(tag), iface_entry);
/* Loop over tag list under this interface for {acct_tag,uid_tag} */
spin_lock_bh(&iface_entry->tag_stat_list_lock);
tag_stat_entry = tag_stat_tree_search(&iface_entry->tag_stat_tree,
tag);
if (tag_stat_entry) {
/*
* Updating the {acct_tag, uid_tag} entry handles both stats:
* {0, uid_tag} will also get updated.
*/
tag_stat_update(tag_stat_entry, direction, proto, bytes);
spin_unlock_bh(&iface_entry->tag_stat_list_lock);
return;
}
/* Loop over tag list under this interface for {0,uid_tag} */
tag_stat_entry = tag_stat_tree_search(&iface_entry->tag_stat_tree,
uid_tag);
if (!tag_stat_entry) {
/* Here: the base uid_tag did not exist */
/*
* No parent counters. So
* - No {0, uid_tag} stats and no {acc_tag, uid_tag} stats.
*/
new_tag_stat = create_if_tag_stat(iface_entry, uid_tag);
if (!new_tag_stat)
goto unlock;
uid_tag_counters = &new_tag_stat->counters;
} else {
uid_tag_counters = &tag_stat_entry->counters;
}
if (acct_tag) {
/* Create the child {acct_tag, uid_tag} and hook up parent. */
new_tag_stat = create_if_tag_stat(iface_entry, tag);
if (!new_tag_stat)
goto unlock;
new_tag_stat->parent_counters = uid_tag_counters;
} else {
/*
* For new_tag_stat to be still NULL here would require:
* {0, uid_tag} exists
* and {acct_tag, uid_tag} doesn't exist
* AND acct_tag == 0.
* Impossible. This reassures us that new_tag_stat
* below will always be assigned.
*/
BUG_ON(!new_tag_stat);
}
tag_stat_update(new_tag_stat, direction, proto, bytes);
unlock:
spin_unlock_bh(&iface_entry->tag_stat_list_lock);
}
static int iface_netdev_event_handler(struct notifier_block *nb,
unsigned long event, void *ptr) {
struct net_device *dev = ptr;
if (unlikely(module_passive))
return NOTIFY_DONE;
IF_DEBUG("qtaguid: iface_stat: netdev_event(): "
"ev=0x%lx/%s netdev=%p->name=%s\n",
event, netdev_evt_str(event), dev, dev ? dev->name : "");
switch (event) {
case NETDEV_UP:
iface_stat_create(dev, NULL);
atomic64_inc(&qtu_events.iface_events);
break;
case NETDEV_DOWN:
case NETDEV_UNREGISTER:
iface_stat_update(dev, event == NETDEV_DOWN);
atomic64_inc(&qtu_events.iface_events);
break;
}
return NOTIFY_DONE;
}
static int iface_inet6addr_event_handler(struct notifier_block *nb,
unsigned long event, void *ptr)
{
struct inet6_ifaddr *ifa = ptr;
struct net_device *dev;
if (unlikely(module_passive))
return NOTIFY_DONE;
IF_DEBUG("qtaguid: iface_stat: inet6addr_event(): "
"ev=0x%lx/%s ifa=%p\n",
event, netdev_evt_str(event), ifa);
switch (event) {
case NETDEV_UP:
BUG_ON(!ifa || !ifa->idev);
dev = (struct net_device *)ifa->idev->dev;
iface_stat_create_ipv6(dev, ifa);
atomic64_inc(&qtu_events.iface_events);
break;
case NETDEV_DOWN:
case NETDEV_UNREGISTER:
BUG_ON(!ifa || !ifa->idev);
dev = (struct net_device *)ifa->idev->dev;
iface_stat_update(dev, event == NETDEV_DOWN);
atomic64_inc(&qtu_events.iface_events);
break;
}
return NOTIFY_DONE;
}
static int iface_inetaddr_event_handler(struct notifier_block *nb,
unsigned long event, void *ptr)
{
struct in_ifaddr *ifa = ptr;
struct net_device *dev;
if (unlikely(module_passive))
return NOTIFY_DONE;
IF_DEBUG("qtaguid: iface_stat: inetaddr_event(): "
"ev=0x%lx/%s ifa=%p\n",
event, netdev_evt_str(event), ifa);
switch (event) {
case NETDEV_UP:
BUG_ON(!ifa || !ifa->ifa_dev);
dev = ifa->ifa_dev->dev;
iface_stat_create(dev, ifa);
atomic64_inc(&qtu_events.iface_events);
break;
case NETDEV_DOWN:
case NETDEV_UNREGISTER:
BUG_ON(!ifa || !ifa->ifa_dev);
dev = ifa->ifa_dev->dev;
iface_stat_update(dev, event == NETDEV_DOWN);
atomic64_inc(&qtu_events.iface_events);
break;
}
return NOTIFY_DONE;
}
static struct notifier_block iface_netdev_notifier_blk = {
.notifier_call = iface_netdev_event_handler,
};
static struct notifier_block iface_inetaddr_notifier_blk = {
.notifier_call = iface_inetaddr_event_handler,
};
static struct notifier_block iface_inet6addr_notifier_blk = {
.notifier_call = iface_inet6addr_event_handler,
};
static int __init iface_stat_init(struct proc_dir_entry *parent_procdir)
{
int err;
iface_stat_procdir = proc_mkdir(iface_stat_procdirname, parent_procdir);
if (!iface_stat_procdir) {
pr_err("qtaguid: iface_stat: init failed to create proc entry\n");
err = -1;
goto err;
}
iface_stat_all_procfile = create_proc_entry(iface_stat_all_procfilename,
proc_iface_perms,
parent_procdir);
if (!iface_stat_all_procfile) {
pr_err("qtaguid: iface_stat: init "
" failed to create stat_old proc entry\n");
err = -1;
goto err_zap_entry;
}
iface_stat_all_procfile->read_proc = iface_stat_fmt_proc_read;
iface_stat_all_procfile->data = (void *)1; /* fmt1 */
iface_stat_fmt_procfile = create_proc_entry(iface_stat_fmt_procfilename,
proc_iface_perms,
parent_procdir);
if (!iface_stat_fmt_procfile) {
pr_err("qtaguid: iface_stat: init "
" failed to create stat_all proc entry\n");
err = -1;
goto err_zap_all_stats_entry;
}
iface_stat_fmt_procfile->read_proc = iface_stat_fmt_proc_read;
iface_stat_fmt_procfile->data = (void *)2; /* fmt2 */
err = register_netdevice_notifier(&iface_netdev_notifier_blk);
if (err) {
pr_err("qtaguid: iface_stat: init "
"failed to register dev event handler\n");
goto err_zap_all_stats_entries;
}
err = register_inetaddr_notifier(&iface_inetaddr_notifier_blk);
if (err) {
pr_err("qtaguid: iface_stat: init "
"failed to register ipv4 dev event handler\n");
goto err_unreg_nd;
}
err = register_inet6addr_notifier(&iface_inet6addr_notifier_blk);
if (err) {
pr_err("qtaguid: iface_stat: init "
"failed to register ipv6 dev event handler\n");
goto err_unreg_ip4_addr;
}
return 0;
err_unreg_ip4_addr:
unregister_inetaddr_notifier(&iface_inetaddr_notifier_blk);
err_unreg_nd:
unregister_netdevice_notifier(&iface_netdev_notifier_blk);
err_zap_all_stats_entries:
remove_proc_entry(iface_stat_fmt_procfilename, parent_procdir);
err_zap_all_stats_entry:
remove_proc_entry(iface_stat_all_procfilename, parent_procdir);
err_zap_entry:
remove_proc_entry(iface_stat_procdirname, parent_procdir);
err:
return err;
}
static struct sock *qtaguid_find_sk(const struct sk_buff *skb,
struct xt_action_param *par)
{
struct sock *sk;
unsigned int hook_mask = (1 << par->hooknum);
MT_DEBUG("qtaguid: find_sk(skb=%p) hooknum=%d family=%d\n", skb,
par->hooknum, par->family);
/*
* Let's not abuse the the xt_socket_get*_sk(), or else it will
* return garbage SKs.
*/
if (!(hook_mask & XT_SOCKET_SUPPORTED_HOOKS))
return NULL;
switch (par->family) {
case NFPROTO_IPV6:
sk = xt_socket_get6_sk(skb, par);
break;
case NFPROTO_IPV4:
sk = xt_socket_get4_sk(skb, par);
break;
default:
return NULL;
}
/*
* Seems to be issues on the file ptr for TCP_TIME_WAIT SKs.
* http://kerneltrap.org/mailarchive/linux-netdev/2010/10/21/6287959
* Not fixed in 3.0-r3 :(
*/
if (sk) {
MT_DEBUG("qtaguid: %p->sk_proto=%u "
"->sk_state=%d\n", sk, sk->sk_protocol, sk->sk_state);
if (sk->sk_state == TCP_TIME_WAIT) {
xt_socket_put_sk(sk);
sk = NULL;
}
}
return sk;
}
static void account_for_uid(const struct sk_buff *skb,
const struct sock *alternate_sk, uid_t uid,
struct xt_action_param *par)
{
const struct net_device *el_dev;
if (!skb->dev) {
MT_DEBUG("qtaguid[%d]: no skb->dev\n", par->hooknum);
el_dev = par->in ? : par->out;
} else {
const struct net_device *other_dev;
el_dev = skb->dev;
other_dev = par->in ? : par->out;
if (el_dev != other_dev) {
MT_DEBUG("qtaguid[%d]: skb->dev=%p %s vs "
"par->(in/out)=%p %s\n",
par->hooknum, el_dev, el_dev->name, other_dev,
other_dev->name);
}
}
if (unlikely(!el_dev)) {
pr_info("qtaguid[%d]: no par->in/out?!!\n", par->hooknum);
} else if (unlikely(!el_dev->name)) {
pr_info("qtaguid[%d]: no dev->name?!!\n", par->hooknum);
} else {
int proto = ipx_proto(skb, par);
MT_DEBUG("qtaguid[%d]: dev name=%s type=%d fam=%d proto=%d\n",
par->hooknum, el_dev->name, el_dev->type,
par->family, proto);
if_tag_stat_update(el_dev->name, uid,
skb->sk ? skb->sk : alternate_sk,
par->in ? IFS_RX : IFS_TX,
proto, skb->len);
}
}
static bool qtaguid_mt(const struct sk_buff *skb, struct xt_action_param *par)
{
const struct xt_qtaguid_match_info *info = par->matchinfo;
const struct file *filp;
bool got_sock = false;
struct sock *sk;
uid_t sock_uid;
bool res;
if (unlikely(module_passive))
return (info->match ^ info->invert) == 0;
MT_DEBUG("qtaguid[%d]: entered skb=%p par->in=%p/out=%p fam=%d\n",
par->hooknum, skb, par->in, par->out, par->family);
atomic64_inc(&qtu_events.match_calls);
if (skb == NULL) {
res = (info->match ^ info->invert) == 0;
goto ret_res;
}
switch (par->hooknum) {
case NF_INET_PRE_ROUTING:
case NF_INET_POST_ROUTING:
atomic64_inc(&qtu_events.match_calls_prepost);
iface_stat_update_from_skb(skb, par);
/*
* We are done in pre/post. The skb will get processed
* further alter.
*/
res = (info->match ^ info->invert);
goto ret_res;
break;
/* default: Fall through and do UID releated work */
}
sk = skb->sk;
if (sk == NULL) {
/*
* A missing sk->sk_socket happens when packets are in-flight
* and the matching socket is already closed and gone.
*/
sk = qtaguid_find_sk(skb, par);
/*
* If we got the socket from the find_sk(), we will need to put
* it back, as nf_tproxy_get_sock_v4() got it.
*/
got_sock = sk;
if (sk)
atomic64_inc(&qtu_events.match_found_sk_in_ct);
else
atomic64_inc(&qtu_events.match_found_no_sk_in_ct);
} else {
atomic64_inc(&qtu_events.match_found_sk);
}
MT_DEBUG("qtaguid[%d]: sk=%p got_sock=%d fam=%d proto=%d\n",
par->hooknum, sk, got_sock, par->family, ipx_proto(skb, par));
if (sk != NULL) {
MT_DEBUG("qtaguid[%d]: sk=%p->sk_socket=%p->file=%p\n",
par->hooknum, sk, sk->sk_socket,
sk->sk_socket ? sk->sk_socket->file : (void *)-1LL);
filp = sk->sk_socket ? sk->sk_socket->file : NULL;
MT_DEBUG("qtaguid[%d]: filp...uid=%u\n",
par->hooknum, filp ? filp->f_cred->fsuid : -1);
}
if (sk == NULL || sk->sk_socket == NULL) {
/*
* Here, the qtaguid_find_sk() using connection tracking
* couldn't find the owner, so for now we just count them
* against the system.
*/
/*
* TODO: unhack how to force just accounting.
* For now we only do iface stats when the uid-owner is not
* requested.
*/
if (!(info->match & XT_QTAGUID_UID))
account_for_uid(skb, sk, 0, par);
MT_DEBUG("qtaguid[%d]: leaving (sk?sk->sk_socket)=%p\n",
par->hooknum,
sk ? sk->sk_socket : NULL);
res = (info->match ^ info->invert) == 0;
atomic64_inc(&qtu_events.match_no_sk);
goto put_sock_ret_res;
} else if (info->match & info->invert & XT_QTAGUID_SOCKET) {
res = false;
goto put_sock_ret_res;
}
filp = sk->sk_socket->file;
if (filp == NULL) {
MT_DEBUG("qtaguid[%d]: leaving filp=NULL\n", par->hooknum);
account_for_uid(skb, sk, 0, par);
res = ((info->match ^ info->invert) &
(XT_QTAGUID_UID | XT_QTAGUID_GID)) == 0;
atomic64_inc(&qtu_events.match_no_sk_file);
goto put_sock_ret_res;
}
sock_uid = filp->f_cred->fsuid;
/*
* TODO: unhack how to force just accounting.
* For now we only do iface stats when the uid-owner is not requested
*/
if (!(info->match & XT_QTAGUID_UID))
account_for_uid(skb, sk, sock_uid, par);
/*
* The following two tests fail the match when:
* id not in range AND no inverted condition requested
* or id in range AND inverted condition requested
* Thus (!a && b) || (a && !b) == a ^ b
*/
if (info->match & XT_QTAGUID_UID)
if ((filp->f_cred->fsuid >= info->uid_min &&
filp->f_cred->fsuid <= info->uid_max) ^
!(info->invert & XT_QTAGUID_UID)) {
MT_DEBUG("qtaguid[%d]: leaving uid not matching\n",
par->hooknum);
res = false;
goto put_sock_ret_res;
}
if (info->match & XT_QTAGUID_GID)
if ((filp->f_cred->fsgid >= info->gid_min &&
filp->f_cred->fsgid <= info->gid_max) ^
!(info->invert & XT_QTAGUID_GID)) {
MT_DEBUG("qtaguid[%d]: leaving gid not matching\n",
par->hooknum);
res = false;
goto put_sock_ret_res;
}
MT_DEBUG("qtaguid[%d]: leaving matched\n", par->hooknum);
res = true;
put_sock_ret_res:
if (got_sock)
xt_socket_put_sk(sk);
ret_res:
MT_DEBUG("qtaguid[%d]: left %d\n", par->hooknum, res);
return res;
}
#ifdef DDEBUG
/* This function is not in xt_qtaguid_print.c because of locks visibility */
static void prdebug_full_state(int indent_level, const char *fmt, ...)
{
va_list args;
char *fmt_buff;
char *buff;
if (!unlikely(qtaguid_debug_mask & DDEBUG_MASK))
return;
fmt_buff = kasprintf(GFP_ATOMIC,
"qtaguid: %s(): %s {\n", __func__, fmt);
BUG_ON(!fmt_buff);
va_start(args, fmt);
buff = kvasprintf(GFP_ATOMIC,
fmt_buff, args);
BUG_ON(!buff);
pr_debug("%s", buff);
kfree(fmt_buff);
kfree(buff);
va_end(args);
spin_lock_bh(&sock_tag_list_lock);
prdebug_sock_tag_tree(indent_level, &sock_tag_tree);
spin_unlock_bh(&sock_tag_list_lock);
spin_lock_bh(&sock_tag_list_lock);
spin_lock_bh(&uid_tag_data_tree_lock);
prdebug_uid_tag_data_tree(indent_level, &uid_tag_data_tree);
prdebug_proc_qtu_data_tree(indent_level, &proc_qtu_data_tree);
spin_unlock_bh(&uid_tag_data_tree_lock);
spin_unlock_bh(&sock_tag_list_lock);
spin_lock_bh(&iface_stat_list_lock);
prdebug_iface_stat_list(indent_level, &iface_stat_list);
spin_unlock_bh(&iface_stat_list_lock);
pr_debug("qtaguid: %s(): }\n", __func__);
}
#else
static void prdebug_full_state(int indent_level, const char *fmt, ...) {}
#endif
/*
* Procfs reader to get all active socket tags using style "1)" as described in
* fs/proc/generic.c
*/
static int qtaguid_ctrl_proc_read(char *page, char **num_items_returned,
off_t items_to_skip, int char_count, int *eof,
void *data)
{
char *outp = page;
int len;
uid_t uid;
struct rb_node *node;
struct sock_tag *sock_tag_entry;
int item_index = 0;
int indent_level = 0;
long f_count;
if (unlikely(module_passive)) {
*eof = 1;
return 0;
}
if (*eof)
return 0;
CT_DEBUG("qtaguid: proc ctrl pid=%u tgid=%u uid=%u "
"page=%p off=%ld char_count=%d *eof=%d\n",
current->pid, current->tgid, current_fsuid(),
page, items_to_skip, char_count, *eof);
spin_lock_bh(&sock_tag_list_lock);
for (node = rb_first(&sock_tag_tree);
node;
node = rb_next(node)) {
if (item_index++ < items_to_skip)
continue;
sock_tag_entry = rb_entry(node, struct sock_tag, sock_node);
uid = get_uid_from_tag(sock_tag_entry->tag);
CT_DEBUG("qtaguid: proc_read(): sk=%p tag=0x%llx (uid=%u) "
"pid=%u\n",
sock_tag_entry->sk,
sock_tag_entry->tag,
uid,
sock_tag_entry->pid
);
f_count = atomic_long_read(
&sock_tag_entry->socket->file->f_count);
len = snprintf(outp, char_count,
"sock=%p tag=0x%llx (uid=%u) pid=%u "
"f_count=%lu\n",
sock_tag_entry->sk,
sock_tag_entry->tag, uid,
sock_tag_entry->pid, f_count);
if (len >= char_count) {
spin_unlock_bh(&sock_tag_list_lock);
*outp = '\0';
return outp - page;
}
outp += len;
char_count -= len;
(*num_items_returned)++;
}
spin_unlock_bh(&sock_tag_list_lock);
if (item_index++ >= items_to_skip) {
len = snprintf(outp, char_count,
"events: sockets_tagged=%llu "
"sockets_untagged=%llu "
"counter_set_changes=%llu "
"delete_cmds=%llu "
"iface_events=%llu "
"match_calls=%llu "
"match_calls_prepost=%llu "
"match_found_sk=%llu "
"match_found_sk_in_ct=%llu "
"match_found_no_sk_in_ct=%llu "
"match_no_sk=%llu "
"match_no_sk_file=%llu\n",
atomic64_read(&qtu_events.sockets_tagged),
atomic64_read(&qtu_events.sockets_untagged),
atomic64_read(&qtu_events.counter_set_changes),
atomic64_read(&qtu_events.delete_cmds),
atomic64_read(&qtu_events.iface_events),
atomic64_read(&qtu_events.match_calls),
atomic64_read(&qtu_events.match_calls_prepost),
atomic64_read(&qtu_events.match_found_sk),
atomic64_read(&qtu_events.match_found_sk_in_ct),
atomic64_read(
&qtu_events.match_found_no_sk_in_ct),
atomic64_read(&qtu_events.match_no_sk),
atomic64_read(&qtu_events.match_no_sk_file));
if (len >= char_count) {
*outp = '\0';
return outp - page;
}
outp += len;
char_count -= len;
(*num_items_returned)++;
}
/* Count the following as part of the last item_index */
if (item_index > items_to_skip) {
prdebug_full_state(indent_level, "proc ctrl");
}
*eof = 1;
return outp - page;
}
/*
* Delete socket tags, and stat tags associated with a given
* accouting tag and uid.
*/
static int ctrl_cmd_delete(const char *input)
{
char cmd;
uid_t uid;
uid_t entry_uid;
tag_t acct_tag;
tag_t tag;
int res, argc;
struct iface_stat *iface_entry;
struct rb_node *node;
struct sock_tag *st_entry;
struct rb_root st_to_free_tree = RB_ROOT;
struct tag_stat *ts_entry;
struct tag_counter_set *tcs_entry;
struct tag_ref *tr_entry;
struct uid_tag_data *utd_entry;
argc = sscanf(input, "%c %llu %u", &cmd, &acct_tag, &uid);
CT_DEBUG("qtaguid: ctrl_delete(%s): argc=%d cmd=%c "
"user_tag=0x%llx uid=%u\n", input, argc, cmd,
acct_tag, uid);
if (argc < 2) {
res = -EINVAL;
goto err;
}
if (!valid_atag(acct_tag)) {
pr_info("qtaguid: ctrl_delete(%s): invalid tag\n", input);
res = -EINVAL;
goto err;
}
if (argc < 3) {
uid = current_fsuid();
} else if (!can_impersonate_uid(uid)) {
pr_info("qtaguid: ctrl_delete(%s): "
"insufficient priv from pid=%u tgid=%u uid=%u\n",
input, current->pid, current->tgid, current_fsuid());
res = -EPERM;
goto err;
}
tag = combine_atag_with_uid(acct_tag, uid);
CT_DEBUG("qtaguid: ctrl_delete(%s): "
"looking for tag=0x%llx (uid=%u)\n",
input, tag, uid);
/* Delete socket tags */
spin_lock_bh(&sock_tag_list_lock);
node = rb_first(&sock_tag_tree);
while (node) {
st_entry = rb_entry(node, struct sock_tag, sock_node);
entry_uid = get_uid_from_tag(st_entry->tag);
node = rb_next(node);
if (entry_uid != uid)
continue;
CT_DEBUG("qtaguid: ctrl_delete(%s): st tag=0x%llx (uid=%u)\n",
input, st_entry->tag, entry_uid);
if (!acct_tag || st_entry->tag == tag) {
rb_erase(&st_entry->sock_node, &sock_tag_tree);
/* Can't sockfd_put() within spinlock, do it later. */
sock_tag_tree_insert(st_entry, &st_to_free_tree);
tr_entry = lookup_tag_ref(st_entry->tag, NULL);
BUG_ON(tr_entry->num_sock_tags <= 0);
tr_entry->num_sock_tags--;
/*
* TODO: remove if, and start failing.
* This is a hack to work around the fact that in some
* places we have "if (IS_ERR_OR_NULL(pqd_entry))"
* and are trying to work around apps
* that didn't open the /dev/xt_qtaguid.
*/
if (st_entry->list.next && st_entry->list.prev)
list_del(&st_entry->list);
}
}
spin_unlock_bh(&sock_tag_list_lock);
sock_tag_tree_erase(&st_to_free_tree);
/* Delete tag counter-sets */
spin_lock_bh(&tag_counter_set_list_lock);
/* Counter sets are only on the uid tag, not full tag */
tcs_entry = tag_counter_set_tree_search(&tag_counter_set_tree, tag);
if (tcs_entry) {
CT_DEBUG("qtaguid: ctrl_delete(%s): "
"erase tcs: tag=0x%llx (uid=%u) set=%d\n",
input,
tcs_entry->tn.tag,
get_uid_from_tag(tcs_entry->tn.tag),
tcs_entry->active_set);
rb_erase(&tcs_entry->tn.node, &tag_counter_set_tree);
kfree(tcs_entry);
}
spin_unlock_bh(&tag_counter_set_list_lock);
/*
* If acct_tag is 0, then all entries belonging to uid are
* erased.
*/
spin_lock_bh(&iface_stat_list_lock);
list_for_each_entry(iface_entry, &iface_stat_list, list) {
spin_lock_bh(&iface_entry->tag_stat_list_lock);
node = rb_first(&iface_entry->tag_stat_tree);
while (node) {
ts_entry = rb_entry(node, struct tag_stat, tn.node);
entry_uid = get_uid_from_tag(ts_entry->tn.tag);
node = rb_next(node);
CT_DEBUG("qtaguid: ctrl_delete(%s): "
"ts tag=0x%llx (uid=%u)\n",
input, ts_entry->tn.tag, entry_uid);
if (entry_uid != uid)
continue;
if (!acct_tag || ts_entry->tn.tag == tag) {
CT_DEBUG("qtaguid: ctrl_delete(%s): "
"erase ts: %s 0x%llx %u\n",
input, iface_entry->ifname,
get_atag_from_tag(ts_entry->tn.tag),
entry_uid);
rb_erase(&ts_entry->tn.node,
&iface_entry->tag_stat_tree);
kfree(ts_entry);
}
}
spin_unlock_bh(&iface_entry->tag_stat_list_lock);
}
spin_unlock_bh(&iface_stat_list_lock);
/* Cleanup the uid_tag_data */
spin_lock_bh(&uid_tag_data_tree_lock);
node = rb_first(&uid_tag_data_tree);
while (node) {
utd_entry = rb_entry(node, struct uid_tag_data, node);
entry_uid = utd_entry->uid;
node = rb_next(node);
CT_DEBUG("qtaguid: ctrl_delete(%s): "
"utd uid=%u\n",
input, entry_uid);
if (entry_uid != uid)
continue;
/*
* Go over the tag_refs, and those that don't have
* sock_tags using them are freed.
*/
put_tag_ref_tree(tag, utd_entry);
put_utd_entry(utd_entry);
}
spin_unlock_bh(&uid_tag_data_tree_lock);
atomic64_inc(&qtu_events.delete_cmds);
res = 0;
err:
return res;
}
static int ctrl_cmd_counter_set(const char *input)
{
char cmd;
uid_t uid = 0;
tag_t tag;
int res, argc;
struct tag_counter_set *tcs;
int counter_set;
argc = sscanf(input, "%c %d %u", &cmd, &counter_set, &uid);
CT_DEBUG("qtaguid: ctrl_counterset(%s): argc=%d cmd=%c "
"set=%d uid=%u\n", input, argc, cmd,
counter_set, uid);
if (argc != 3) {
res = -EINVAL;
goto err;
}
if (counter_set < 0 || counter_set >= IFS_MAX_COUNTER_SETS) {
pr_info("qtaguid: ctrl_counterset(%s): invalid counter_set range\n",
input);
res = -EINVAL;
goto err;
}
if (!can_manipulate_uids()) {
pr_info("qtaguid: ctrl_counterset(%s): "
"insufficient priv from pid=%u tgid=%u uid=%u\n",
input, current->pid, current->tgid, current_fsuid());
res = -EPERM;
goto err;
}
tag = make_tag_from_uid(uid);
spin_lock_bh(&tag_counter_set_list_lock);
tcs = tag_counter_set_tree_search(&tag_counter_set_tree, tag);
if (!tcs) {
tcs = kzalloc(sizeof(*tcs), GFP_ATOMIC);
if (!tcs) {
spin_unlock_bh(&tag_counter_set_list_lock);
pr_err("qtaguid: ctrl_counterset(%s): "
"failed to alloc counter set\n",
input);
res = -ENOMEM;
goto err;
}
tcs->tn.tag = tag;
tag_counter_set_tree_insert(tcs, &tag_counter_set_tree);
CT_DEBUG("qtaguid: ctrl_counterset(%s): added tcs tag=0x%llx "
"(uid=%u) set=%d\n",
input, tag, get_uid_from_tag(tag), counter_set);
}
tcs->active_set = counter_set;
spin_unlock_bh(&tag_counter_set_list_lock);
atomic64_inc(&qtu_events.counter_set_changes);
res = 0;
err:
return res;
}
static int ctrl_cmd_tag(const char *input)
{
char cmd;
int sock_fd = 0;
uid_t uid = 0;
tag_t acct_tag = make_atag_from_value(0);
tag_t full_tag;
struct socket *el_socket;
int res, argc;
struct sock_tag *sock_tag_entry;
struct tag_ref *tag_ref_entry;
struct uid_tag_data *uid_tag_data_entry;
struct proc_qtu_data *pqd_entry;
/* Unassigned args will get defaulted later. */
argc = sscanf(input, "%c %d %llu %u", &cmd, &sock_fd, &acct_tag, &uid);
CT_DEBUG("qtaguid: ctrl_tag(%s): argc=%d cmd=%c sock_fd=%d "
"acct_tag=0x%llx uid=%u\n", input, argc, cmd, sock_fd,
acct_tag, uid);
if (argc < 2) {
res = -EINVAL;
goto err;
}
el_socket = sockfd_lookup(sock_fd, &res); /* This locks the file */
if (!el_socket) {
pr_info("qtaguid: ctrl_tag(%s): failed to lookup"
" sock_fd=%d err=%d pid=%u tgid=%u uid=%u\n",
input, sock_fd, res, current->pid, current->tgid,
current_fsuid());
goto err;
}
CT_DEBUG("qtaguid: ctrl_tag(%s): socket->...->f_count=%ld ->sk=%p\n",
input, atomic_long_read(&el_socket->file->f_count),
el_socket->sk);
if (argc < 3) {
acct_tag = make_atag_from_value(0);
} else if (!valid_atag(acct_tag)) {
pr_info("qtaguid: ctrl_tag(%s): invalid tag\n", input);
res = -EINVAL;
goto err_put;
}
CT_DEBUG("qtaguid: ctrl_tag(%s): "
"pid=%u tgid=%u uid=%u euid=%u fsuid=%u "
"ctrl.gid=%u in_group()=%d in_egroup()=%d\n",
input, current->pid, current->tgid, current_uid(),
current_euid(), current_fsuid(),
xt_qtaguid_ctrl_file->gid,
in_group_p(xt_qtaguid_ctrl_file->gid),
in_egroup_p(xt_qtaguid_ctrl_file->gid));
if (argc < 4) {
uid = current_fsuid();
} else if (!can_impersonate_uid(uid)) {
pr_info("qtaguid: ctrl_tag(%s): "
"insufficient priv from pid=%u tgid=%u uid=%u\n",
input, current->pid, current->tgid, current_fsuid());
res = -EPERM;
goto err_put;
}
full_tag = combine_atag_with_uid(acct_tag, uid);
spin_lock_bh(&sock_tag_list_lock);
sock_tag_entry = get_sock_stat_nl(el_socket->sk);
tag_ref_entry = get_tag_ref(full_tag, &uid_tag_data_entry);
if (IS_ERR(tag_ref_entry)) {
res = PTR_ERR(tag_ref_entry);
spin_unlock_bh(&sock_tag_list_lock);
goto err_put;
}
tag_ref_entry->num_sock_tags++;
if (sock_tag_entry) {
struct tag_ref *prev_tag_ref_entry;
CT_DEBUG("qtaguid: ctrl_tag(%s): retag for sk=%p "
"st@%p ...->f_count=%ld\n",
input, el_socket->sk, sock_tag_entry,
atomic_long_read(&el_socket->file->f_count));
/*
* This is a re-tagging, so release the sock_fd that was
* locked at the time of the 1st tagging.
* There is still the ref from this call's sockfd_lookup() so
* it can be done within the spinlock.
*/
sockfd_put(sock_tag_entry->socket);
prev_tag_ref_entry = lookup_tag_ref(sock_tag_entry->tag,
&uid_tag_data_entry);
BUG_ON(IS_ERR_OR_NULL(prev_tag_ref_entry));
BUG_ON(prev_tag_ref_entry->num_sock_tags <= 0);
prev_tag_ref_entry->num_sock_tags--;
sock_tag_entry->tag = full_tag;
} else {
CT_DEBUG("qtaguid: ctrl_tag(%s): newtag for sk=%p\n",
input, el_socket->sk);
sock_tag_entry = kzalloc(sizeof(*sock_tag_entry),
GFP_ATOMIC);
if (!sock_tag_entry) {
pr_err("qtaguid: ctrl_tag(%s): "
"socket tag alloc failed\n",
input);
spin_unlock_bh(&sock_tag_list_lock);
res = -ENOMEM;
goto err_tag_unref_put;
}
sock_tag_entry->sk = el_socket->sk;
sock_tag_entry->socket = el_socket;
sock_tag_entry->pid = current->tgid;
sock_tag_entry->tag = combine_atag_with_uid(acct_tag,
uid);
spin_lock_bh(&uid_tag_data_tree_lock);
pqd_entry = proc_qtu_data_tree_search(
&proc_qtu_data_tree, current->tgid);
/*
* TODO: remove if, and start failing.
* At first, we want to catch user-space code that is not
* opening the /dev/xt_qtaguid.
*/
if (IS_ERR_OR_NULL(pqd_entry))
pr_warn_once(
"qtaguid: %s(): "
"User space forgot to open /dev/xt_qtaguid? "
"pid=%u tgid=%u uid=%u\n", __func__,
current->pid, current->tgid,
current_fsuid());
else
list_add(&sock_tag_entry->list,
&pqd_entry->sock_tag_list);
spin_unlock_bh(&uid_tag_data_tree_lock);
sock_tag_tree_insert(sock_tag_entry, &sock_tag_tree);
atomic64_inc(&qtu_events.sockets_tagged);
}
spin_unlock_bh(&sock_tag_list_lock);
/* We keep the ref to the socket (file) until it is untagged */
CT_DEBUG("qtaguid: ctrl_tag(%s): done st@%p ...->f_count=%ld\n",
input, sock_tag_entry,
atomic_long_read(&el_socket->file->f_count));
return 0;
err_tag_unref_put:
BUG_ON(tag_ref_entry->num_sock_tags <= 0);
tag_ref_entry->num_sock_tags--;
free_tag_ref_from_utd_entry(tag_ref_entry, uid_tag_data_entry);
err_put:
CT_DEBUG("qtaguid: ctrl_tag(%s): done. ...->f_count=%ld\n",
input, atomic_long_read(&el_socket->file->f_count) - 1);
/* Release the sock_fd that was grabbed by sockfd_lookup(). */
sockfd_put(el_socket);
return res;
err:
CT_DEBUG("qtaguid: ctrl_tag(%s): done.\n", input);
return res;
}
static int ctrl_cmd_untag(const char *input)
{
char cmd;
int sock_fd = 0;
struct socket *el_socket;
int res, argc;
struct sock_tag *sock_tag_entry;
struct tag_ref *tag_ref_entry;
struct uid_tag_data *utd_entry;
struct proc_qtu_data *pqd_entry;
argc = sscanf(input, "%c %d", &cmd, &sock_fd);
CT_DEBUG("qtaguid: ctrl_untag(%s): argc=%d cmd=%c sock_fd=%d\n",
input, argc, cmd, sock_fd);
if (argc < 2) {
res = -EINVAL;
goto err;
}
el_socket = sockfd_lookup(sock_fd, &res); /* This locks the file */
if (!el_socket) {
pr_info("qtaguid: ctrl_untag(%s): failed to lookup"
" sock_fd=%d err=%d pid=%u tgid=%u uid=%u\n",
input, sock_fd, res, current->pid, current->tgid,
current_fsuid());
goto err;
}
CT_DEBUG("qtaguid: ctrl_untag(%s): socket->...->f_count=%ld ->sk=%p\n",
input, atomic_long_read(&el_socket->file->f_count),
el_socket->sk);
spin_lock_bh(&sock_tag_list_lock);
sock_tag_entry = get_sock_stat_nl(el_socket->sk);
if (!sock_tag_entry) {
spin_unlock_bh(&sock_tag_list_lock);
res = -EINVAL;
goto err_put;
}
/*
* The socket already belongs to the current process
* so it can do whatever it wants to it.
*/
rb_erase(&sock_tag_entry->sock_node, &sock_tag_tree);
tag_ref_entry = lookup_tag_ref(sock_tag_entry->tag, &utd_entry);
BUG_ON(!tag_ref_entry);
BUG_ON(tag_ref_entry->num_sock_tags <= 0);
spin_lock_bh(&uid_tag_data_tree_lock);
pqd_entry = proc_qtu_data_tree_search(
&proc_qtu_data_tree, current->tgid);
/*
* TODO: remove if, and start failing.
* At first, we want to catch user-space code that is not
* opening the /dev/xt_qtaguid.
*/
if (IS_ERR_OR_NULL(pqd_entry))
pr_warn_once("qtaguid: %s(): "
"User space forgot to open /dev/xt_qtaguid? "
"pid=%u tgid=%u uid=%u\n", __func__,
current->pid, current->tgid, current_fsuid());
else
list_del(&sock_tag_entry->list);
spin_unlock_bh(&uid_tag_data_tree_lock);
/*
* We don't free tag_ref from the utd_entry here,
* only during a cmd_delete().
*/
tag_ref_entry->num_sock_tags--;
spin_unlock_bh(&sock_tag_list_lock);
/*
* Release the sock_fd that was grabbed at tag time,
* and once more for the sockfd_lookup() here.
*/
sockfd_put(sock_tag_entry->socket);
CT_DEBUG("qtaguid: ctrl_untag(%s): done. st@%p ...->f_count=%ld\n",
input, sock_tag_entry,
atomic_long_read(&el_socket->file->f_count) - 1);
sockfd_put(el_socket);
kfree(sock_tag_entry);
atomic64_inc(&qtu_events.sockets_untagged);
return 0;
err_put:
CT_DEBUG("qtaguid: ctrl_untag(%s): done. socket->...->f_count=%ld\n",
input, atomic_long_read(&el_socket->file->f_count) - 1);
/* Release the sock_fd that was grabbed by sockfd_lookup(). */
sockfd_put(el_socket);
return res;
err:
CT_DEBUG("qtaguid: ctrl_untag(%s): done.\n", input);
return res;
}
static int qtaguid_ctrl_parse(const char *input, int count)
{
char cmd;
int res;
CT_DEBUG("qtaguid: ctrl(%s): pid=%u tgid=%u uid=%u\n",
input, current->pid, current->tgid, current_fsuid());
cmd = input[0];
/* Collect params for commands */
switch (cmd) {
case 'd':
res = ctrl_cmd_delete(input);
break;
case 's':
res = ctrl_cmd_counter_set(input);
break;
case 't':
res = ctrl_cmd_tag(input);
break;
case 'u':
res = ctrl_cmd_untag(input);
break;
default:
res = -EINVAL;
goto err;
}
if (!res)
res = count;
err:
CT_DEBUG("qtaguid: ctrl(%s): res=%d\n", input, res);
return res;
}
#define MAX_QTAGUID_CTRL_INPUT_LEN 255
static int qtaguid_ctrl_proc_write(struct file *file, const char __user *buffer,
unsigned long count, void *data)
{
char input_buf[MAX_QTAGUID_CTRL_INPUT_LEN];
if (unlikely(module_passive))
return count;
if (count >= MAX_QTAGUID_CTRL_INPUT_LEN)
return -EINVAL;
if (copy_from_user(input_buf, buffer, count))
return -EFAULT;
input_buf[count] = '\0';
return qtaguid_ctrl_parse(input_buf, count);
}
struct proc_print_info {
char *outp;
char **num_items_returned;
struct iface_stat *iface_entry;
struct tag_stat *ts_entry;
int item_index;
int items_to_skip;
int char_count;
};
static int pp_stats_line(struct proc_print_info *ppi, int cnt_set)
{
int len;
struct data_counters *cnts;
if (!ppi->item_index) {
if (ppi->item_index++ < ppi->items_to_skip)
return 0;
len = snprintf(ppi->outp, ppi->char_count,
"idx iface acct_tag_hex uid_tag_int cnt_set "
"rx_bytes rx_packets "
"tx_bytes tx_packets "
"rx_tcp_bytes rx_tcp_packets "
"rx_udp_bytes rx_udp_packets "
"rx_other_bytes rx_other_packets "
"tx_tcp_bytes tx_tcp_packets "
"tx_udp_bytes tx_udp_packets "
"tx_other_bytes tx_other_packets\n");
} else {
tag_t tag = ppi->ts_entry->tn.tag;
uid_t stat_uid = get_uid_from_tag(tag);
/* Detailed tags are not available to everybody */
if (get_atag_from_tag(tag)
&& !can_read_other_uid_stats(stat_uid)) {
CT_DEBUG("qtaguid: stats line: "
"%s 0x%llx %u: insufficient priv "
"from pid=%u tgid=%u uid=%u stats.gid=%u\n",
ppi->iface_entry->ifname,
get_atag_from_tag(tag), stat_uid,
current->pid, current->tgid, current_fsuid(),
xt_qtaguid_stats_file->gid);
return 0;
}
if (ppi->item_index++ < ppi->items_to_skip)
return 0;
cnts = &ppi->ts_entry->counters;
len = snprintf(
ppi->outp, ppi->char_count,
"%d %s 0x%llx %u %u "
"%llu %llu "
"%llu %llu "
"%llu %llu "
"%llu %llu "
"%llu %llu "
"%llu %llu "
"%llu %llu "
"%llu %llu\n",
ppi->item_index,
ppi->iface_entry->ifname,
get_atag_from_tag(tag),
stat_uid,
cnt_set,
dc_sum_bytes(cnts, cnt_set, IFS_RX),
dc_sum_packets(cnts, cnt_set, IFS_RX),
dc_sum_bytes(cnts, cnt_set, IFS_TX),
dc_sum_packets(cnts, cnt_set, IFS_TX),
cnts->bpc[cnt_set][IFS_RX][IFS_TCP].bytes,
cnts->bpc[cnt_set][IFS_RX][IFS_TCP].packets,
cnts->bpc[cnt_set][IFS_RX][IFS_UDP].bytes,
cnts->bpc[cnt_set][IFS_RX][IFS_UDP].packets,
cnts->bpc[cnt_set][IFS_RX][IFS_PROTO_OTHER].bytes,
cnts->bpc[cnt_set][IFS_RX][IFS_PROTO_OTHER].packets,
cnts->bpc[cnt_set][IFS_TX][IFS_TCP].bytes,
cnts->bpc[cnt_set][IFS_TX][IFS_TCP].packets,
cnts->bpc[cnt_set][IFS_TX][IFS_UDP].bytes,
cnts->bpc[cnt_set][IFS_TX][IFS_UDP].packets,
cnts->bpc[cnt_set][IFS_TX][IFS_PROTO_OTHER].bytes,
cnts->bpc[cnt_set][IFS_TX][IFS_PROTO_OTHER].packets);
}
return len;
}
static bool pp_sets(struct proc_print_info *ppi)
{
int len;
int counter_set;
for (counter_set = 0; counter_set < IFS_MAX_COUNTER_SETS;
counter_set++) {
len = pp_stats_line(ppi, counter_set);
if (len >= ppi->char_count) {
*ppi->outp = '\0';
return false;
}
if (len) {
ppi->outp += len;
ppi->char_count -= len;
(*ppi->num_items_returned)++;
}
}
return true;
}
/*
* Procfs reader to get all tag stats using style "1)" as described in
* fs/proc/generic.c
* Groups all protocols tx/rx bytes.
*/
static int qtaguid_stats_proc_read(char *page, char **num_items_returned,
off_t items_to_skip, int char_count, int *eof,
void *data)
{
struct proc_print_info ppi;
int len;
ppi.outp = page;
ppi.item_index = 0;
ppi.char_count = char_count;
ppi.num_items_returned = num_items_returned;
ppi.items_to_skip = items_to_skip;
if (unlikely(module_passive)) {
len = pp_stats_line(&ppi, 0);
/* The header should always be shorter than the buffer. */
BUG_ON(len >= ppi.char_count);
(*num_items_returned)++;
*eof = 1;
return len;
}
CT_DEBUG("qtaguid:proc stats pid=%u tgid=%u uid=%u "
"page=%p *num_items_returned=%p off=%ld "
"char_count=%d *eof=%d\n",
current->pid, current->tgid, current_fsuid(),
page, *num_items_returned,
items_to_skip, char_count, *eof);
if (*eof)
return 0;
/* The idx is there to help debug when things go belly up. */
len = pp_stats_line(&ppi, 0);
/* Don't advance the outp unless the whole line was printed */
if (len >= ppi.char_count) {
*ppi.outp = '\0';
return ppi.outp - page;
}
if (len) {
ppi.outp += len;
ppi.char_count -= len;
(*num_items_returned)++;
}
spin_lock_bh(&iface_stat_list_lock);
list_for_each_entry(ppi.iface_entry, &iface_stat_list, list) {
struct rb_node *node;
spin_lock_bh(&ppi.iface_entry->tag_stat_list_lock);
for (node = rb_first(&ppi.iface_entry->tag_stat_tree);
node;
node = rb_next(node)) {
ppi.ts_entry = rb_entry(node, struct tag_stat, tn.node);
if (!pp_sets(&ppi)) {
spin_unlock_bh(
&ppi.iface_entry->tag_stat_list_lock);
spin_unlock_bh(&iface_stat_list_lock);
return ppi.outp - page;
}
}
spin_unlock_bh(&ppi.iface_entry->tag_stat_list_lock);
}
spin_unlock_bh(&iface_stat_list_lock);
*eof = 1;
return ppi.outp - page;
}
/*------------------------------------------*/
static int qtudev_open(struct inode *inode, struct file *file)
{
struct uid_tag_data *utd_entry;
struct proc_qtu_data *pqd_entry;
struct proc_qtu_data *new_pqd_entry;
int res;
bool utd_entry_found;
if (unlikely(qtu_proc_handling_passive))
return 0;
DR_DEBUG("qtaguid: qtudev_open(): pid=%u tgid=%u uid=%u\n",
current->pid, current->tgid, current_fsuid());
spin_lock_bh(&uid_tag_data_tree_lock);
/* Look for existing uid data, or alloc one. */
utd_entry = get_uid_data(current_fsuid(), &utd_entry_found);
if (IS_ERR_OR_NULL(utd_entry)) {
res = PTR_ERR(utd_entry);
goto err_unlock;
}
/* Look for existing PID based proc_data */
pqd_entry = proc_qtu_data_tree_search(&proc_qtu_data_tree,
current->tgid);
if (pqd_entry) {
pr_err("qtaguid: qtudev_open(): %u/%u %u "
"%s already opened\n",
current->pid, current->tgid, current_fsuid(),
QTU_DEV_NAME);
res = -EBUSY;
goto err_unlock_free_utd;
}
new_pqd_entry = kzalloc(sizeof(*new_pqd_entry), GFP_ATOMIC);
if (!new_pqd_entry) {
pr_err("qtaguid: qtudev_open(): %u/%u %u: "
"proc data alloc failed\n",
current->pid, current->tgid, current_fsuid());
res = -ENOMEM;
goto err_unlock_free_utd;
}
new_pqd_entry->pid = current->tgid;
INIT_LIST_HEAD(&new_pqd_entry->sock_tag_list);
new_pqd_entry->parent_tag_data = utd_entry;
utd_entry->num_pqd++;
proc_qtu_data_tree_insert(new_pqd_entry,
&proc_qtu_data_tree);
spin_unlock_bh(&uid_tag_data_tree_lock);
DR_DEBUG("qtaguid: tracking data for uid=%u in pqd=%p\n",
current_fsuid(), new_pqd_entry);
file->private_data = new_pqd_entry;
return 0;
err_unlock_free_utd:
if (!utd_entry_found) {
rb_erase(&utd_entry->node, &uid_tag_data_tree);
kfree(utd_entry);
}
err_unlock:
spin_unlock_bh(&uid_tag_data_tree_lock);
return res;
}
static int qtudev_release(struct inode *inode, struct file *file)
{
struct proc_qtu_data *pqd_entry = file->private_data;
struct uid_tag_data *utd_entry = pqd_entry->parent_tag_data;
struct sock_tag *st_entry;
struct rb_root st_to_free_tree = RB_ROOT;
struct list_head *entry, *next;
struct tag_ref *tr;
if (unlikely(qtu_proc_handling_passive))
return 0;
/*
* Do not trust the current->pid, it might just be a kworker cleaning
* up after a dead proc.
*/
DR_DEBUG("qtaguid: qtudev_release(): "
"pid=%u tgid=%u uid=%u "
"pqd_entry=%p->pid=%u utd_entry=%p->active_tags=%d\n",
current->pid, current->tgid, pqd_entry->parent_tag_data->uid,
pqd_entry, pqd_entry->pid, utd_entry,
utd_entry->num_active_tags);
spin_lock_bh(&sock_tag_list_lock);
spin_lock_bh(&uid_tag_data_tree_lock);
list_for_each_safe(entry, next, &pqd_entry->sock_tag_list) {
st_entry = list_entry(entry, struct sock_tag, list);
DR_DEBUG("qtaguid: %s(): "
"erase sock_tag=%p->sk=%p pid=%u tgid=%u uid=%u\n",
__func__,
st_entry, st_entry->sk,
current->pid, current->tgid,
pqd_entry->parent_tag_data->uid);
utd_entry = uid_tag_data_tree_search(
&uid_tag_data_tree,
get_uid_from_tag(st_entry->tag));
BUG_ON(IS_ERR_OR_NULL(utd_entry));
DR_DEBUG("qtaguid: %s(): "
"looking for tag=0x%llx in utd_entry=%p\n", __func__,
st_entry->tag, utd_entry);
tr = tag_ref_tree_search(&utd_entry->tag_ref_tree,
st_entry->tag);
BUG_ON(!tr);
BUG_ON(tr->num_sock_tags <= 0);
tr->num_sock_tags--;
free_tag_ref_from_utd_entry(tr, utd_entry);
rb_erase(&st_entry->sock_node, &sock_tag_tree);
list_del(&st_entry->list);
/* Can't sockfd_put() within spinlock, do it later. */
sock_tag_tree_insert(st_entry, &st_to_free_tree);
/*
* Try to free the utd_entry if no other proc_qtu_data is
* using it (num_pqd is 0) and it doesn't have active tags
* (num_active_tags is 0).
*/
put_utd_entry(utd_entry);
}
rb_erase(&pqd_entry->node, &proc_qtu_data_tree);
BUG_ON(pqd_entry->parent_tag_data->num_pqd < 1);
pqd_entry->parent_tag_data->num_pqd--;
put_utd_entry(pqd_entry->parent_tag_data);
kfree(pqd_entry);
file->private_data = NULL;
spin_unlock_bh(&uid_tag_data_tree_lock);
spin_unlock_bh(&sock_tag_list_lock);
sock_tag_tree_erase(&st_to_free_tree);
prdebug_full_state(0, "%s(): pid=%u tgid=%u", __func__,
current->pid, current->tgid);
return 0;
}
/*------------------------------------------*/
static const struct file_operations qtudev_fops = {
.owner = THIS_MODULE,
.open = qtudev_open,
.release = qtudev_release,
};
static struct miscdevice qtu_device = {
.minor = MISC_DYNAMIC_MINOR,
.name = QTU_DEV_NAME,
.fops = &qtudev_fops,
/* How sad it doesn't allow for defaults: .mode = S_IRUGO | S_IWUSR */
};
/*------------------------------------------*/
static int __init qtaguid_proc_register(struct proc_dir_entry **res_procdir)
{
int ret;
*res_procdir = proc_mkdir(module_procdirname, init_net.proc_net);
if (!*res_procdir) {
pr_err("qtaguid: failed to create proc/.../xt_qtaguid\n");
ret = -ENOMEM;
goto no_dir;
}
xt_qtaguid_ctrl_file = create_proc_entry("ctrl", proc_ctrl_perms,
*res_procdir);
if (!xt_qtaguid_ctrl_file) {
pr_err("qtaguid: failed to create xt_qtaguid/ctrl "
" file\n");
ret = -ENOMEM;
goto no_ctrl_entry;
}
xt_qtaguid_ctrl_file->read_proc = qtaguid_ctrl_proc_read;
xt_qtaguid_ctrl_file->write_proc = qtaguid_ctrl_proc_write;
xt_qtaguid_stats_file = create_proc_entry("stats", proc_stats_perms,
*res_procdir);
if (!xt_qtaguid_stats_file) {
pr_err("qtaguid: failed to create xt_qtaguid/stats "
"file\n");
ret = -ENOMEM;
goto no_stats_entry;
}
xt_qtaguid_stats_file->read_proc = qtaguid_stats_proc_read;
/*
* TODO: add support counter hacking
* xt_qtaguid_stats_file->write_proc = qtaguid_stats_proc_write;
*/
return 0;
no_stats_entry:
remove_proc_entry("ctrl", *res_procdir);
no_ctrl_entry:
remove_proc_entry("xt_qtaguid", NULL);
no_dir:
return ret;
}
static struct xt_match qtaguid_mt_reg __read_mostly = {
/*
* This module masquerades as the "owner" module so that iptables
* tools can deal with it.
*/
.name = "owner",
.revision = 1,
.family = NFPROTO_UNSPEC,
.match = qtaguid_mt,
.matchsize = sizeof(struct xt_qtaguid_match_info),
.me = THIS_MODULE,
};
static int __init qtaguid_mt_init(void)
{
if (qtaguid_proc_register(&xt_qtaguid_procdir)
|| iface_stat_init(xt_qtaguid_procdir)
|| xt_register_match(&qtaguid_mt_reg)
|| misc_register(&qtu_device))
return -1;
return 0;
}
/*
* TODO: allow unloading of the module.
* For now stats are permanent.
* Kconfig forces'y/n' and never an 'm'.
*/
module_init(qtaguid_mt_init);
MODULE_AUTHOR("jpa <jpa@google.com>");
MODULE_DESCRIPTION("Xtables: socket owner+tag matching and associated stats");
MODULE_LICENSE("GPL");
MODULE_ALIAS("ipt_owner");
MODULE_ALIAS("ip6t_owner");
MODULE_ALIAS("ipt_qtaguid");
MODULE_ALIAS("ip6t_qtaguid");