aboutsummaryrefslogblamecommitdiffstats
blob: 0f8d92120c4effbfd1d40914135c2b56d4dfc30f (plain) (tree)
1
2
3
4
5
6
7
8
9
10
11


                                                     







                                                                  
                                        

                                                          
# builds the trace events example kernel modules;
# then to use one (as root):  insmod <module_name.ko>

# If you include a trace header outside of include/trace/events
# then the file that does the #define CREATE_TRACE_POINTS must
# have that tracer file in its main search path. This is because
# define_trace.h will include it, and must be able to find it from
# the include/trace directory.
#
# Here trace-events-sample.c does the CREATE_TRACE_POINTS.
#
CFLAGS_trace-events-sample.o := -I$(src)

obj-$(CONFIG_SAMPLE_TRACE_EVENTS) += trace-events-sample.o