aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorYinghai Lu2010-08-25 15:39:17 -0500
committerH. Peter Anvin2010-08-27 13:12:29 -0500
commit72d7c3b33c980843e756681fb4867dc1efd62a76 (patch)
tree9607345d9fa055dd501aacf0772258fb72897035 /arch/x86/kernel/head.c
parent301ff3e88ef9ff4bdb92f36a3e6170fce4c9dd34 (diff)
downloadkernel-common-72d7c3b33c980843e756681fb4867dc1efd62a76.tar.gz
kernel-common-72d7c3b33c980843e756681fb4867dc1efd62a76.tar.xz
kernel-common-72d7c3b33c980843e756681fb4867dc1efd62a76.zip
x86: Use memblock to replace early_res
1. replace find_e820_area with memblock_find_in_range 2. replace reserve_early with memblock_x86_reserve_range 3. replace free_early with memblock_x86_free_range. 4. NO_BOOTMEM will switch to use memblock too. 5. use _e820, _early wrap in the patch, in following patch, will replace them all 6. because memblock_x86_free_range support partial free, we can remove some special care 7. Need to make sure that memblock_find_in_range() is called after memblock_x86_fill() so adjust some calling later in setup.c::setup_arch() -- corruption_check and mptable_update -v2: Move reserve_brk() early Before fill_memblock_area, to avoid overlap between brk and memblock_find_in_range() that could happen We have more then 128 RAM entry in E820 tables, and memblock_x86_fill() could use memblock_find_in_range() to find a new place for memblock.memory.region array. and We don't need to use extend_brk() after fill_memblock_area() So move reserve_brk() early before fill_memblock_area(). -v3: Move find_smp_config early To make sure memblock_find_in_range not find wrong place, if BIOS doesn't put mptable in right place. -v4: Treat RESERVED_KERN as RAM in memblock.memory. and they are already in memblock.reserved already.. use __NOT_KEEP_MEMBLOCK to make sure memblock related code could be freed later. -v5: Generic version __memblock_find_in_range() is going from high to low, and for 32bit active_region for 32bit does include high pages need to replace the limit with memblock.default_alloc_limit, aka get_max_mapped() -v6: Use current_limit instead -v7: check with MEMBLOCK_ERROR instead of -1ULL or -1L -v8: Set memblock_can_resize early to handle EFI with more RAM entries -v9: update after kmemleak changes in mainline Suggested-by: David S. Miller <davem@davemloft.net> Suggested-by: Benjamin Herrenschmidt <benh@kernel.crashing.org> Suggested-by: Thomas Gleixner <tglx@linutronix.de> Signed-off-by: Yinghai Lu <yinghai@kernel.org> Signed-off-by: H. Peter Anvin <hpa@zytor.com>
Diffstat (limited to 'arch/x86/kernel/head.c')
-rw-r--r--arch/x86/kernel/head.c3
1 files changed, 2 insertions, 1 deletions
diff --git a/arch/x86/kernel/head.c b/arch/x86/kernel/head.c
index 3e66bd364a9..af0699ba48c 100644
--- a/arch/x86/kernel/head.c
+++ b/arch/x86/kernel/head.c
@@ -1,5 +1,6 @@
1#include <linux/kernel.h> 1#include <linux/kernel.h>
2#include <linux/init.h> 2#include <linux/init.h>
3#include <linux/memblock.h>
3 4
4#include <asm/setup.h> 5#include <asm/setup.h>
5#include <asm/bios_ebda.h> 6#include <asm/bios_ebda.h>
@@ -51,5 +52,5 @@ void __init reserve_ebda_region(void)
51 lowmem = 0x9f000; 52 lowmem = 0x9f000;
52 53
53 /* reserve all memory between lowmem and the 1MB mark */ 54 /* reserve all memory between lowmem and the 1MB mark */
54 reserve_early_overlap_ok(lowmem, 0x100000, "BIOS reserved"); 55 memblock_x86_reserve_range(lowmem, 0x100000, "* BIOS reserved");
55} 56}