aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorH. Peter Anvin2013-02-27 14:46:40 -0600
committerGreg Kroah-Hartman2013-03-03 16:09:03 -0600
commit93b6b299f7a97a8ce2f8ab7b14195f8d2d131905 (patch)
tree356573809b3f31e742178d20611174010cde06d9 /arch/x86/kernel/head.c
parent834f139f1613ba0ca3239a6a12be97c70698f189 (diff)
downloadkernel-common-93b6b299f7a97a8ce2f8ab7b14195f8d2d131905.tar.gz
kernel-common-93b6b299f7a97a8ce2f8ab7b14195f8d2d131905.tar.xz
kernel-common-93b6b299f7a97a8ce2f8ab7b14195f8d2d131905.zip
x86: Make sure we can boot in the case the BDA contains pure garbage
commit 7c10093692ed2e6f318387d96b829320aa0ca64c upstream. On non-BIOS platforms it is possible that the BIOS data area contains garbage instead of being zeroed or something equivalent (firmware people: we are talking of 1.5K here, so please do the sane thing.) We need on the order of 20-30K of low memory in order to boot, which may grow up to < 64K in the future. We probably want to avoid the lowest of the low memory. At the same time, it seems extremely unlikely that a legitimate EBDA would ever reach down to the 128K (which would require it to be over half a megabyte in size.) Thus, pick 128K as the cutoff for "this is insane, ignore." We may still end up reserving a bunch of extra memory on the low megabyte, but that is not really a major issue these days. In the worst case we lose 512K of RAM. This code really should be merged with trim_bios_range() in arch/x86/kernel/setup.c, but that is a bigger patch for a later merge window. Reported-by: Darren Hart <dvhart@linux.intel.com> Signed-off-by: H. Peter Anvin <hpa@linux.intel.com> Cc: Matt Fleming <matt.fleming@intel.com> Link: http://lkml.kernel.org/n/tip-oebml055yyfm8yxmria09rja@git.kernel.org Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
Diffstat (limited to 'arch/x86/kernel/head.c')
-rw-r--r--arch/x86/kernel/head.c53
1 files changed, 34 insertions, 19 deletions
diff --git a/arch/x86/kernel/head.c b/arch/x86/kernel/head.c
index af0699ba48c..f6c467484eb 100644
--- a/arch/x86/kernel/head.c
+++ b/arch/x86/kernel/head.c
@@ -5,8 +5,6 @@
5#include <asm/setup.h> 5#include <asm/setup.h>
6#include <asm/bios_ebda.h> 6#include <asm/bios_ebda.h>
7 7
8#define BIOS_LOWMEM_KILOBYTES 0x413
9
10/* 8/*
11 * The BIOS places the EBDA/XBDA at the top of conventional 9 * The BIOS places the EBDA/XBDA at the top of conventional
12 * memory, and usually decreases the reported amount of 10 * memory, and usually decreases the reported amount of
@@ -16,17 +14,30 @@
16 * chipset: reserve a page before VGA to prevent PCI prefetch 14 * chipset: reserve a page before VGA to prevent PCI prefetch
17 * into it (errata #56). Usually the page is reserved anyways, 15 * into it (errata #56). Usually the page is reserved anyways,
18 * unless you have no PS/2 mouse plugged in. 16 * unless you have no PS/2 mouse plugged in.
17 *
18 * This functions is deliberately very conservative. Losing
19 * memory in the bottom megabyte is rarely a problem, as long
20 * as we have enough memory to install the trampoline. Using
21 * memory that is in use by the BIOS or by some DMA device
22 * the BIOS didn't shut down *is* a big problem.
19 */ 23 */
24
25#define BIOS_LOWMEM_KILOBYTES 0x413
26#define LOWMEM_CAP 0x9f000U /* Absolute maximum */
27#define INSANE_CUTOFF 0x20000U /* Less than this = insane */
28
20void __init reserve_ebda_region(void) 29void __init reserve_ebda_region(void)
21{ 30{
22 unsigned int lowmem, ebda_addr; 31 unsigned int lowmem, ebda_addr;
23 32
24 /* To determine the position of the EBDA and the */ 33 /*
25 /* end of conventional memory, we need to look at */ 34 * To determine the position of the EBDA and the
26 /* the BIOS data area. In a paravirtual environment */ 35 * end of conventional memory, we need to look at
27 /* that area is absent. We'll just have to assume */ 36 * the BIOS data area. In a paravirtual environment
28 /* that the paravirt case can handle memory setup */ 37 * that area is absent. We'll just have to assume
29 /* correctly, without our help. */ 38 * that the paravirt case can handle memory setup
39 * correctly, without our help.
40 */
30 if (paravirt_enabled()) 41 if (paravirt_enabled())
31 return; 42 return;
32 43
@@ -37,19 +48,23 @@ void __init reserve_ebda_region(void)
37 /* start of EBDA area */ 48 /* start of EBDA area */
38 ebda_addr = get_bios_ebda(); 49 ebda_addr = get_bios_ebda();
39 50
40 /* Fixup: bios puts an EBDA in the top 64K segment */ 51 /*
41 /* of conventional memory, but does not adjust lowmem. */ 52 * Note: some old Dells seem to need 4k EBDA without
42 if ((lowmem - ebda_addr) <= 0x10000) 53 * reporting so, so just consider the memory above 0x9f000
43 lowmem = ebda_addr; 54 * to be off limits (bugzilla 2990).
55 */
56
57 /* If the EBDA address is below 128K, assume it is bogus */
58 if (ebda_addr < INSANE_CUTOFF)
59 ebda_addr = LOWMEM_CAP;
44 60
45 /* Fixup: bios does not report an EBDA at all. */ 61 /* If lowmem is less than 128K, assume it is bogus */
46 /* Some old Dells seem to need 4k anyhow (bugzilla 2990) */ 62 if (lowmem < INSANE_CUTOFF)
47 if ((ebda_addr == 0) && (lowmem >= 0x9f000)) 63 lowmem = LOWMEM_CAP;
48 lowmem = 0x9f000;
49 64
50 /* Paranoia: should never happen, but... */ 65 /* Use the lower of the lowmem and EBDA markers as the cutoff */
51 if ((lowmem == 0) || (lowmem >= 0x100000)) 66 lowmem = min(lowmem, ebda_addr);
52 lowmem = 0x9f000; 67 lowmem = min(lowmem, LOWMEM_CAP); /* Absolute cap */
53 68
54 /* reserve all memory between lowmem and the 1MB mark */ 69 /* reserve all memory between lowmem and the 1MB mark */
55 memblock_x86_reserve_range(lowmem, 0x100000, "* BIOS reserved"); 70 memblock_x86_reserve_range(lowmem, 0x100000, "* BIOS reserved");