diff options
author | Satoru Takeuchi | 2013-02-13 18:12:52 -0600 |
---|---|---|
committer | H. Peter Anvin | 2013-02-13 19:24:11 -0600 |
commit | 1de63d60cd5b0d33a812efa455d5933bf1564a51 (patch) | |
tree | 336e5e18d14b139bfa43f51f667214e14219053f /arch/x86 | |
parent | 323a72d83c9b2963bd1e46c8e6963e468d4658d7 (diff) | |
download | kernel-common-1de63d60cd5b0d33a812efa455d5933bf1564a51.tar.gz kernel-common-1de63d60cd5b0d33a812efa455d5933bf1564a51.tar.xz kernel-common-1de63d60cd5b0d33a812efa455d5933bf1564a51.zip |
efi: Clear EFI_RUNTIME_SERVICES rather than EFI_BOOT by "noefi" boot parameter
There was a serious problem in samsung-laptop that its platform driver is
designed to run under BIOS and running under EFI can cause the machine to
become bricked or can cause Machine Check Exceptions.
Discussion about this problem:
https://bugs.launchpad.net/ubuntu-cdimage/+bug/1040557
https://bugzilla.kernel.org/show_bug.cgi?id=47121
The patches to fix this problem:
efi: Make 'efi_enabled' a function to query EFI facilities
83e68189745ad931c2afd45d8ee3303929233e7f
samsung-laptop: Disable on EFI hardware
e0094244e41c4d0c7ad69920681972fc45d8ce34
Unfortunately this problem comes back again if users specify "noefi" option.
This parameter clears EFI_BOOT and that driver continues to run even if running
under EFI. Refer to the document, this parameter should clear
EFI_RUNTIME_SERVICES instead.
Documentation/kernel-parameters.txt:
===============================================================================
...
noefi [X86] Disable EFI runtime services support.
...
===============================================================================
Documentation/x86/x86_64/uefi.txt:
===============================================================================
...
- If some or all EFI runtime services don't work, you can try following
kernel command line parameters to turn off some or all EFI runtime
services.
noefi turn off all EFI runtime services
...
===============================================================================
Signed-off-by: Satoru Takeuchi <takeuchi_satoru@jp.fujitsu.com>
Link: http://lkml.kernel.org/r/511C2C04.2070108@jp.fujitsu.com
Cc: Matt Fleming <matt.fleming@intel.com>
Cc: <stable@vger.kernel.org>
Signed-off-by: H. Peter Anvin <hpa@linux.intel.com>
Diffstat (limited to 'arch/x86')
-rw-r--r-- | arch/x86/platform/efi/efi.c | 2 |
1 files changed, 1 insertions, 1 deletions
diff --git a/arch/x86/platform/efi/efi.c b/arch/x86/platform/efi/efi.c index 77cf0090c0a..928bf837040 100644 --- a/arch/x86/platform/efi/efi.c +++ b/arch/x86/platform/efi/efi.c | |||
@@ -87,7 +87,7 @@ EXPORT_SYMBOL(efi_enabled); | |||
87 | 87 | ||
88 | static int __init setup_noefi(char *arg) | 88 | static int __init setup_noefi(char *arg) |
89 | { | 89 | { |
90 | clear_bit(EFI_BOOT, &x86_efi_facility); | 90 | clear_bit(EFI_RUNTIME_SERVICES, &x86_efi_facility); |
91 | return 0; | 91 | return 0; |
92 | } | 92 | } |
93 | early_param("noefi", setup_noefi); | 93 | early_param("noefi", setup_noefi); |