diff options
author | Tejun Heo | 2011-03-02 07:48:06 -0600 |
---|---|---|
committer | Jens Axboe | 2011-03-02 07:48:06 -0600 |
commit | 255bb490c8c27eed484d538efe6ef6a7473bd3f6 (patch) | |
tree | 630289b9de253a1f0575f29d2de019494016ff79 /block/blk-flush.c | |
parent | 1654e7411a1ad4999fe7890ef51d2a2bbb1fcf76 (diff) | |
download | kernel-common-255bb490c8c27eed484d538efe6ef6a7473bd3f6.tar.gz kernel-common-255bb490c8c27eed484d538efe6ef6a7473bd3f6.tar.xz kernel-common-255bb490c8c27eed484d538efe6ef6a7473bd3f6.zip |
block: blk-flush shouldn't call directly into q->request_fn() __blk_run_queue()
blk-flush decomposes a flush into sequence of multiple requests. On
completion of a request, the next one is queued; however, block layer
must not implicitly call into q->request_fn() directly from completion
path. This makes the queue behave unexpectedly when seen from the
drivers and violates the assumption that q->request_fn() is called
with process context + queue_lock.
This patch makes blk-flush the following two changes to make sure
q->request_fn() is not called directly from request completion path.
- blk_flush_complete_seq_end_io() now asks __blk_run_queue() to always
use kblockd instead of calling directly into q->request_fn().
- queue_next_fseq() uses ELEVATOR_INSERT_REQUEUE instead of
ELEVATOR_INSERT_FRONT so that elv_insert() doesn't try to unplug the
request queue directly.
Reported by Jan in the following threads.
http://thread.gmane.org/gmane.linux.ide/48778
http://thread.gmane.org/gmane.linux.ide/48786
stable: applicable to v2.6.37.
Signed-off-by: Tejun Heo <tj@kernel.org>
Reported-by: Jan Beulich <JBeulich@novell.com>
Cc: "David S. Miller" <davem@davemloft.net>
Cc: stable@kernel.org
Signed-off-by: Jens Axboe <jaxboe@fusionio.com>
Diffstat (limited to 'block/blk-flush.c')
-rw-r--r-- | block/blk-flush.c | 8 |
1 files changed, 5 insertions, 3 deletions
diff --git a/block/blk-flush.c b/block/blk-flush.c index 56adaa8d55c..b27d0208611 100644 --- a/block/blk-flush.c +++ b/block/blk-flush.c | |||
@@ -66,10 +66,12 @@ static void blk_flush_complete_seq_end_io(struct request_queue *q, | |||
66 | 66 | ||
67 | /* | 67 | /* |
68 | * Moving a request silently to empty queue_head may stall the | 68 | * Moving a request silently to empty queue_head may stall the |
69 | * queue. Kick the queue in those cases. | 69 | * queue. Kick the queue in those cases. This function is called |
70 | * from request completion path and calling directly into | ||
71 | * request_fn may confuse the driver. Always use kblockd. | ||
70 | */ | 72 | */ |
71 | if (was_empty && next_rq) | 73 | if (was_empty && next_rq) |
72 | __blk_run_queue(q, false); | 74 | __blk_run_queue(q, true); |
73 | } | 75 | } |
74 | 76 | ||
75 | static void pre_flush_end_io(struct request *rq, int error) | 77 | static void pre_flush_end_io(struct request *rq, int error) |
@@ -130,7 +132,7 @@ static struct request *queue_next_fseq(struct request_queue *q) | |||
130 | BUG(); | 132 | BUG(); |
131 | } | 133 | } |
132 | 134 | ||
133 | elv_insert(q, rq, ELEVATOR_INSERT_FRONT); | 135 | elv_insert(q, rq, ELEVATOR_INSERT_REQUEUE); |
134 | return rq; | 136 | return rq; |
135 | } | 137 | } |
136 | 138 | ||