diff options
author | Tejun Heo | 2012-03-05 15:15:19 -0600 |
---|---|---|
committer | Jens Axboe | 2012-03-06 14:27:23 -0600 |
commit | 03aa264ac15637b6f98374270bcdf31400965505 (patch) | |
tree | 6fa9ca54d3f775fba19123790f6655158034a1d8 /block/cfq-iosched.c | |
parent | 4eef3049986e8397d5003916aed8cad6567a5e02 (diff) | |
download | kernel-common-03aa264ac15637b6f98374270bcdf31400965505.tar.gz kernel-common-03aa264ac15637b6f98374270bcdf31400965505.tar.xz kernel-common-03aa264ac15637b6f98374270bcdf31400965505.zip |
blkcg: let blkcg core manage per-queue blkg list and counter
With the previous patch to move blkg list heads and counters to
request_queue and blkg, logic to manage them in both policies are
almost identical and can be moved to blkcg core.
This patch moves blkg link logic into blkg_lookup_create(), implements
common blkg unlink code in blkg_destroy(), and updates
blkg_destory_all() so that it's policy specific and can skip root
group. The updated blkg_destroy_all() is now used to both clear queue
for bypassing and elv switching, and release all blkgs on q exit.
This patch introduces a race window where policy [de]registration may
race against queue blkg clearing. This can only be a problem on cfq
unload and shouldn't be a real problem in practice (and we have many
other places where this race already exists). Future patches will
remove these unlikely races.
Signed-off-by: Tejun Heo <tj@kernel.org>
Cc: Vivek Goyal <vgoyal@redhat.com>
Signed-off-by: Jens Axboe <axboe@kernel.dk>
Diffstat (limited to 'block/cfq-iosched.c')
-rw-r--r-- | block/cfq-iosched.c | 100 |
1 files changed, 6 insertions, 94 deletions
diff --git a/block/cfq-iosched.c b/block/cfq-iosched.c index e846803280a..dc73690dec4 100644 --- a/block/cfq-iosched.c +++ b/block/cfq-iosched.c | |||
@@ -1045,14 +1045,6 @@ static void cfq_update_blkio_group_weight(struct request_queue *q, | |||
1045 | cfqg->needs_update = true; | 1045 | cfqg->needs_update = true; |
1046 | } | 1046 | } |
1047 | 1047 | ||
1048 | static void cfq_link_blkio_group(struct request_queue *q, | ||
1049 | struct blkio_group *blkg) | ||
1050 | { | ||
1051 | list_add(&blkg->q_node[BLKIO_POLICY_PROP], | ||
1052 | &q->blkg_list[BLKIO_POLICY_PROP]); | ||
1053 | q->nr_blkgs[BLKIO_POLICY_PROP]++; | ||
1054 | } | ||
1055 | |||
1056 | static void cfq_init_blkio_group(struct blkio_group *blkg) | 1048 | static void cfq_init_blkio_group(struct blkio_group *blkg) |
1057 | { | 1049 | { |
1058 | struct cfq_group *cfqg = blkg_to_cfqg(blkg); | 1050 | struct cfq_group *cfqg = blkg_to_cfqg(blkg); |
@@ -1096,84 +1088,6 @@ static void cfq_link_cfqq_cfqg(struct cfq_queue *cfqq, struct cfq_group *cfqg) | |||
1096 | blkg_get(cfqg_to_blkg(cfqg)); | 1088 | blkg_get(cfqg_to_blkg(cfqg)); |
1097 | } | 1089 | } |
1098 | 1090 | ||
1099 | static void cfq_destroy_cfqg(struct cfq_data *cfqd, struct cfq_group *cfqg) | ||
1100 | { | ||
1101 | struct blkio_group *blkg = cfqg_to_blkg(cfqg); | ||
1102 | |||
1103 | /* Something wrong if we are trying to remove same group twice */ | ||
1104 | BUG_ON(list_empty(&blkg->q_node[BLKIO_POLICY_PROP])); | ||
1105 | |||
1106 | list_del_init(&blkg->q_node[BLKIO_POLICY_PROP]); | ||
1107 | |||
1108 | BUG_ON(cfqd->queue->nr_blkgs[BLKIO_POLICY_PROP] <= 0); | ||
1109 | cfqd->queue->nr_blkgs[BLKIO_POLICY_PROP]--; | ||
1110 | |||
1111 | /* | ||
1112 | * Put the reference taken at the time of creation so that when all | ||
1113 | * queues are gone, group can be destroyed. | ||
1114 | */ | ||
1115 | blkg_put(cfqg_to_blkg(cfqg)); | ||
1116 | } | ||
1117 | |||
1118 | static bool cfq_release_cfq_groups(struct cfq_data *cfqd) | ||
1119 | { | ||
1120 | struct request_queue *q = cfqd->queue; | ||
1121 | struct blkio_group *blkg, *n; | ||
1122 | bool empty = true; | ||
1123 | |||
1124 | list_for_each_entry_safe(blkg, n, &q->blkg_list[BLKIO_POLICY_PROP], | ||
1125 | q_node[BLKIO_POLICY_PROP]) { | ||
1126 | /* | ||
1127 | * If cgroup removal path got to blk_group first and removed | ||
1128 | * it from cgroup list, then it will take care of destroying | ||
1129 | * cfqg also. | ||
1130 | */ | ||
1131 | if (!cfq_blkiocg_del_blkio_group(blkg)) | ||
1132 | cfq_destroy_cfqg(cfqd, blkg_to_cfqg(blkg)); | ||
1133 | else | ||
1134 | empty = false; | ||
1135 | } | ||
1136 | return empty; | ||
1137 | } | ||
1138 | |||
1139 | /* | ||
1140 | * Blk cgroup controller notification saying that blkio_group object is being | ||
1141 | * delinked as associated cgroup object is going away. That also means that | ||
1142 | * no new IO will come in this group. So get rid of this group as soon as | ||
1143 | * any pending IO in the group is finished. | ||
1144 | * | ||
1145 | * This function is called under rcu_read_lock(). key is the rcu protected | ||
1146 | * pointer. That means @q is a valid request_queue pointer as long as we | ||
1147 | * are rcu read lock. | ||
1148 | * | ||
1149 | * @q was fetched from blkio_group under blkio_cgroup->lock. That means | ||
1150 | * it should not be NULL as even if elevator was exiting, cgroup deltion | ||
1151 | * path got to it first. | ||
1152 | */ | ||
1153 | static void cfq_unlink_blkio_group(struct request_queue *q, | ||
1154 | struct blkio_group *blkg) | ||
1155 | { | ||
1156 | struct cfq_data *cfqd = q->elevator->elevator_data; | ||
1157 | unsigned long flags; | ||
1158 | |||
1159 | spin_lock_irqsave(q->queue_lock, flags); | ||
1160 | cfq_destroy_cfqg(cfqd, blkg_to_cfqg(blkg)); | ||
1161 | spin_unlock_irqrestore(q->queue_lock, flags); | ||
1162 | } | ||
1163 | |||
1164 | static struct elevator_type iosched_cfq; | ||
1165 | |||
1166 | static bool cfq_clear_queue(struct request_queue *q) | ||
1167 | { | ||
1168 | lockdep_assert_held(q->queue_lock); | ||
1169 | |||
1170 | /* shoot down blkgs iff the current elevator is cfq */ | ||
1171 | if (!q->elevator || q->elevator->type != &iosched_cfq) | ||
1172 | return true; | ||
1173 | |||
1174 | return cfq_release_cfq_groups(q->elevator->elevator_data); | ||
1175 | } | ||
1176 | |||
1177 | #else /* GROUP_IOSCHED */ | 1091 | #else /* GROUP_IOSCHED */ |
1178 | static struct cfq_group *cfq_lookup_create_cfqg(struct cfq_data *cfqd, | 1092 | static struct cfq_group *cfq_lookup_create_cfqg(struct cfq_data *cfqd, |
1179 | struct blkio_cgroup *blkcg) | 1093 | struct blkio_cgroup *blkcg) |
@@ -1186,8 +1100,6 @@ cfq_link_cfqq_cfqg(struct cfq_queue *cfqq, struct cfq_group *cfqg) { | |||
1186 | cfqq->cfqg = cfqg; | 1100 | cfqq->cfqg = cfqg; |
1187 | } | 1101 | } |
1188 | 1102 | ||
1189 | static void cfq_release_cfq_groups(struct cfq_data *cfqd) {} | ||
1190 | |||
1191 | #endif /* GROUP_IOSCHED */ | 1103 | #endif /* GROUP_IOSCHED */ |
1192 | 1104 | ||
1193 | /* | 1105 | /* |
@@ -3547,17 +3459,20 @@ static void cfq_exit_queue(struct elevator_queue *e) | |||
3547 | __cfq_slice_expired(cfqd, cfqd->active_queue, 0); | 3459 | __cfq_slice_expired(cfqd, cfqd->active_queue, 0); |
3548 | 3460 | ||
3549 | cfq_put_async_queues(cfqd); | 3461 | cfq_put_async_queues(cfqd); |
3550 | cfq_release_cfq_groups(cfqd); | 3462 | |
3463 | spin_unlock_irq(q->queue_lock); | ||
3464 | |||
3465 | blkg_destroy_all(q, BLKIO_POLICY_PROP, true); | ||
3551 | 3466 | ||
3552 | #ifdef CONFIG_BLK_CGROUP | 3467 | #ifdef CONFIG_BLK_CGROUP |
3553 | /* | 3468 | /* |
3554 | * If there are groups which we could not unlink from blkcg list, | 3469 | * If there are groups which we could not unlink from blkcg list, |
3555 | * wait for a rcu period for them to be freed. | 3470 | * wait for a rcu period for them to be freed. |
3556 | */ | 3471 | */ |
3472 | spin_lock_irq(q->queue_lock); | ||
3557 | wait = q->nr_blkgs[BLKIO_POLICY_PROP]; | 3473 | wait = q->nr_blkgs[BLKIO_POLICY_PROP]; |
3558 | #endif | ||
3559 | spin_unlock_irq(q->queue_lock); | 3474 | spin_unlock_irq(q->queue_lock); |
3560 | 3475 | #endif | |
3561 | cfq_shutdown_timer_wq(cfqd); | 3476 | cfq_shutdown_timer_wq(cfqd); |
3562 | 3477 | ||
3563 | /* | 3478 | /* |
@@ -3794,9 +3709,6 @@ static struct elevator_type iosched_cfq = { | |||
3794 | static struct blkio_policy_type blkio_policy_cfq = { | 3709 | static struct blkio_policy_type blkio_policy_cfq = { |
3795 | .ops = { | 3710 | .ops = { |
3796 | .blkio_init_group_fn = cfq_init_blkio_group, | 3711 | .blkio_init_group_fn = cfq_init_blkio_group, |
3797 | .blkio_link_group_fn = cfq_link_blkio_group, | ||
3798 | .blkio_unlink_group_fn = cfq_unlink_blkio_group, | ||
3799 | .blkio_clear_queue_fn = cfq_clear_queue, | ||
3800 | .blkio_update_group_weight_fn = cfq_update_blkio_group_weight, | 3712 | .blkio_update_group_weight_fn = cfq_update_blkio_group_weight, |
3801 | }, | 3713 | }, |
3802 | .plid = BLKIO_POLICY_PROP, | 3714 | .plid = BLKIO_POLICY_PROP, |