diff options
author | Shaohua Li | 2011-01-07 01:46:59 -0600 |
---|---|---|
committer | Jens Axboe | 2011-01-07 01:46:59 -0600 |
commit | 30d7b9448f03f2c82d0fd44738674cc156a8ce0a (patch) | |
tree | f925a59dfe6a7b2da5240e9d43d873de7b1de273 /block/cfq-iosched.c | |
parent | b7908c1035af7652cd613991b54dbff9c8b6bd3a (diff) | |
download | kernel-common-30d7b9448f03f2c82d0fd44738674cc156a8ce0a.tar.gz kernel-common-30d7b9448f03f2c82d0fd44738674cc156a8ce0a.tar.xz kernel-common-30d7b9448f03f2c82d0fd44738674cc156a8ce0a.zip |
block cfq: don't use atomic_t for cfq_queue
cfq_queue->ref is used with queue_lock hold, so ref doesn't need to be an atomic
and atomic operation is slower.
Signed-off-by: Shaohua Li <shaohua.li@intel.com>
Reviewed-by: Jeff Moyer <jmoyer@redhat.com>
Acked-by: Vivek Goyal <vgoyal@redhat.com>
Signed-off-by: Jens Axboe <jaxboe@fusionio.com>
Diffstat (limited to 'block/cfq-iosched.c')
-rw-r--r-- | block/cfq-iosched.c | 27 |
1 files changed, 16 insertions, 11 deletions
diff --git a/block/cfq-iosched.c b/block/cfq-iosched.c index c19d015ac5a..4cb4cf73ac0 100644 --- a/block/cfq-iosched.c +++ b/block/cfq-iosched.c | |||
@@ -96,7 +96,7 @@ struct cfq_rb_root { | |||
96 | */ | 96 | */ |
97 | struct cfq_queue { | 97 | struct cfq_queue { |
98 | /* reference count */ | 98 | /* reference count */ |
99 | atomic_t ref; | 99 | int ref; |
100 | /* various state flags, see below */ | 100 | /* various state flags, see below */ |
101 | unsigned int flags; | 101 | unsigned int flags; |
102 | /* parent cfq_data */ | 102 | /* parent cfq_data */ |
@@ -2025,7 +2025,7 @@ static int cfqq_process_refs(struct cfq_queue *cfqq) | |||
2025 | int process_refs, io_refs; | 2025 | int process_refs, io_refs; |
2026 | 2026 | ||
2027 | io_refs = cfqq->allocated[READ] + cfqq->allocated[WRITE]; | 2027 | io_refs = cfqq->allocated[READ] + cfqq->allocated[WRITE]; |
2028 | process_refs = atomic_read(&cfqq->ref) - io_refs; | 2028 | process_refs = cfqq->ref - io_refs; |
2029 | BUG_ON(process_refs < 0); | 2029 | BUG_ON(process_refs < 0); |
2030 | return process_refs; | 2030 | return process_refs; |
2031 | } | 2031 | } |
@@ -2065,10 +2065,10 @@ static void cfq_setup_merge(struct cfq_queue *cfqq, struct cfq_queue *new_cfqq) | |||
2065 | */ | 2065 | */ |
2066 | if (new_process_refs >= process_refs) { | 2066 | if (new_process_refs >= process_refs) { |
2067 | cfqq->new_cfqq = new_cfqq; | 2067 | cfqq->new_cfqq = new_cfqq; |
2068 | atomic_add(process_refs, &new_cfqq->ref); | 2068 | new_cfqq->ref += process_refs; |
2069 | } else { | 2069 | } else { |
2070 | new_cfqq->new_cfqq = cfqq; | 2070 | new_cfqq->new_cfqq = cfqq; |
2071 | atomic_add(new_process_refs, &cfqq->ref); | 2071 | cfqq->ref += new_process_refs; |
2072 | } | 2072 | } |
2073 | } | 2073 | } |
2074 | 2074 | ||
@@ -2532,9 +2532,10 @@ static void cfq_put_queue(struct cfq_queue *cfqq) | |||
2532 | struct cfq_data *cfqd = cfqq->cfqd; | 2532 | struct cfq_data *cfqd = cfqq->cfqd; |
2533 | struct cfq_group *cfqg, *orig_cfqg; | 2533 | struct cfq_group *cfqg, *orig_cfqg; |
2534 | 2534 | ||
2535 | BUG_ON(atomic_read(&cfqq->ref) <= 0); | 2535 | BUG_ON(cfqq->ref <= 0); |
2536 | 2536 | ||
2537 | if (!atomic_dec_and_test(&cfqq->ref)) | 2537 | cfqq->ref--; |
2538 | if (cfqq->ref) | ||
2538 | return; | 2539 | return; |
2539 | 2540 | ||
2540 | cfq_log_cfqq(cfqd, cfqq, "put_queue"); | 2541 | cfq_log_cfqq(cfqd, cfqq, "put_queue"); |
@@ -2837,7 +2838,7 @@ static void cfq_init_cfqq(struct cfq_data *cfqd, struct cfq_queue *cfqq, | |||
2837 | RB_CLEAR_NODE(&cfqq->p_node); | 2838 | RB_CLEAR_NODE(&cfqq->p_node); |
2838 | INIT_LIST_HEAD(&cfqq->fifo); | 2839 | INIT_LIST_HEAD(&cfqq->fifo); |
2839 | 2840 | ||
2840 | atomic_set(&cfqq->ref, 0); | 2841 | cfqq->ref = 0; |
2841 | cfqq->cfqd = cfqd; | 2842 | cfqq->cfqd = cfqd; |
2842 | 2843 | ||
2843 | cfq_mark_cfqq_prio_changed(cfqq); | 2844 | cfq_mark_cfqq_prio_changed(cfqq); |
@@ -2973,11 +2974,11 @@ cfq_get_queue(struct cfq_data *cfqd, bool is_sync, struct io_context *ioc, | |||
2973 | * pin the queue now that it's allocated, scheduler exit will prune it | 2974 | * pin the queue now that it's allocated, scheduler exit will prune it |
2974 | */ | 2975 | */ |
2975 | if (!is_sync && !(*async_cfqq)) { | 2976 | if (!is_sync && !(*async_cfqq)) { |
2976 | atomic_inc(&cfqq->ref); | 2977 | cfqq->ref++; |
2977 | *async_cfqq = cfqq; | 2978 | *async_cfqq = cfqq; |
2978 | } | 2979 | } |
2979 | 2980 | ||
2980 | atomic_inc(&cfqq->ref); | 2981 | cfqq->ref++; |
2981 | return cfqq; | 2982 | return cfqq; |
2982 | } | 2983 | } |
2983 | 2984 | ||
@@ -3679,7 +3680,7 @@ new_queue: | |||
3679 | } | 3680 | } |
3680 | 3681 | ||
3681 | cfqq->allocated[rw]++; | 3682 | cfqq->allocated[rw]++; |
3682 | atomic_inc(&cfqq->ref); | 3683 | cfqq->ref++; |
3683 | 3684 | ||
3684 | spin_unlock_irqrestore(q->queue_lock, flags); | 3685 | spin_unlock_irqrestore(q->queue_lock, flags); |
3685 | 3686 | ||
@@ -3860,6 +3861,10 @@ static void *cfq_init_queue(struct request_queue *q) | |||
3860 | if (!cfqd) | 3861 | if (!cfqd) |
3861 | return NULL; | 3862 | return NULL; |
3862 | 3863 | ||
3864 | /* | ||
3865 | * Don't need take queue_lock in the routine, since we are | ||
3866 | * initializing the ioscheduler, and nobody is using cfqd | ||
3867 | */ | ||
3863 | cfqd->cic_index = i; | 3868 | cfqd->cic_index = i; |
3864 | 3869 | ||
3865 | /* Init root service tree */ | 3870 | /* Init root service tree */ |
@@ -3899,7 +3904,7 @@ static void *cfq_init_queue(struct request_queue *q) | |||
3899 | * will not attempt to free it. | 3904 | * will not attempt to free it. |
3900 | */ | 3905 | */ |
3901 | cfq_init_cfqq(cfqd, &cfqd->oom_cfqq, 1, 0); | 3906 | cfq_init_cfqq(cfqd, &cfqd->oom_cfqq, 1, 0); |
3902 | atomic_inc(&cfqd->oom_cfqq.ref); | 3907 | cfqd->oom_cfqq.ref++; |
3903 | cfq_link_cfqq_cfqg(&cfqd->oom_cfqq, &cfqd->root_group); | 3908 | cfq_link_cfqq_cfqg(&cfqd->oom_cfqq, &cfqd->root_group); |
3904 | 3909 | ||
3905 | INIT_LIST_HEAD(&cfqd->cic_list); | 3910 | INIT_LIST_HEAD(&cfqd->cic_list); |