diff options
author | Linus Torvalds | 2012-01-15 14:24:45 -0600 |
---|---|---|
committer | Linus Torvalds | 2012-01-15 14:24:45 -0600 |
commit | b3c9dd182ed3bdcdaf0e42625a35924b0497afdc (patch) | |
tree | ad48ad4d923fee147c736318d0fad35b3755f4f5 /block/genhd.c | |
parent | 83c2f912b43c3a7babbb6cb7ae2a5276c1ed2a3e (diff) | |
parent | 5d381efb3d1f1ef10535a31ca0dd9b22fe1e1922 (diff) | |
download | kernel-common-b3c9dd182ed3bdcdaf0e42625a35924b0497afdc.tar.gz kernel-common-b3c9dd182ed3bdcdaf0e42625a35924b0497afdc.tar.xz kernel-common-b3c9dd182ed3bdcdaf0e42625a35924b0497afdc.zip |
Merge branch 'for-3.3/core' of git://git.kernel.dk/linux-block
* 'for-3.3/core' of git://git.kernel.dk/linux-block: (37 commits)
Revert "block: recursive merge requests"
block: Stop using macro stubs for the bio data integrity calls
blockdev: convert some macros to static inlines
fs: remove unneeded plug in mpage_readpages()
block: Add BLKROTATIONAL ioctl
block: Introduce blk_set_stacking_limits function
block: remove WARN_ON_ONCE() in exit_io_context()
block: an exiting task should be allowed to create io_context
block: ioc_cgroup_changed() needs to be exported
block: recursive merge requests
block, cfq: fix empty queue crash caused by request merge
block, cfq: move icq creation and rq->elv.icq association to block core
block, cfq: restructure io_cq creation path for io_context interface cleanup
block, cfq: move io_cq exit/release to blk-ioc.c
block, cfq: move icq cache management to block core
block, cfq: move io_cq lookup to blk-ioc.c
block, cfq: move cfqd->icq_list to request_queue and add request->elv.icq
block, cfq: reorganize cfq_io_context into generic and cfq specific parts
block: remove elevator_queue->ops
block: reorder elevator switch sequence
...
Fix up conflicts in:
- block/blk-cgroup.c
Switch from can_attach_task to can_attach
- block/cfq-iosched.c
conflict with now removed cic index changes (we now use q->id instead)
Diffstat (limited to 'block/genhd.c')
-rw-r--r-- | block/genhd.c | 2 |
1 files changed, 1 insertions, 1 deletions
diff --git a/block/genhd.c b/block/genhd.c index 83e7c04015e..23b4f706332 100644 --- a/block/genhd.c +++ b/block/genhd.c | |||
@@ -614,7 +614,7 @@ void add_disk(struct gendisk *disk) | |||
614 | * Take an extra ref on queue which will be put on disk_release() | 614 | * Take an extra ref on queue which will be put on disk_release() |
615 | * so that it sticks around as long as @disk is there. | 615 | * so that it sticks around as long as @disk is there. |
616 | */ | 616 | */ |
617 | WARN_ON_ONCE(blk_get_queue(disk->queue)); | 617 | WARN_ON_ONCE(!blk_get_queue(disk->queue)); |
618 | 618 | ||
619 | retval = sysfs_create_link(&disk_to_dev(disk)->kobj, &bdi->dev->kobj, | 619 | retval = sysfs_create_link(&disk_to_dev(disk)->kobj, &bdi->dev->kobj, |
620 | "bdi"); | 620 | "bdi"); |