diff options
author | Alan Stern | 2007-02-20 10:01:57 -0600 |
---|---|---|
committer | James Bottomley | 2007-04-17 17:09:56 -0500 |
commit | 44ec95425c1d9dce6e4638c29e4362cfb44814e7 (patch) | |
tree | 6af593dc23a2f7cdb9a0d3ecc46d37aae640c0d8 /block/ll_rw_blk.c | |
parent | 1079a2d251f24a7d9e7576217f5f738bc4218337 (diff) | |
download | kernel-common-44ec95425c1d9dce6e4638c29e4362cfb44814e7.tar.gz kernel-common-44ec95425c1d9dce6e4638c29e4362cfb44814e7.tar.xz kernel-common-44ec95425c1d9dce6e4638c29e4362cfb44814e7.zip |
[SCSI] sg: cap reserved_size values at max_sectors
This patch (as857) modifies the SG_GET_RESERVED_SIZE and
SG_SET_RESERVED_SIZE ioctls in the sg driver, capping the values at
the device's request_queue's max_sectors value. This will permit
cdrecord to obtain a legal value for the maximum transfer length,
fixing Bugzilla #7026.
The patch also caps the initial reserved_size value. There's no
reason to have a reserved buffer larger than max_sectors, since it
would be impossible to use the extra space.
The corresponding ioctls in the block layer are modified similarly,
and the initial value for the reserved_size is set as large as
possible. This will effectively make it default to max_sectors.
Note that the actual value is meaningless anyway, since block devices
don't have a reserved buffer.
Finally, the BLKSECTGET ioctl is added to sg, so that there will be a
uniform way for users to determine the actual max_sectors value for
any raw SCSI transport.
Signed-off-by: Alan Stern <stern@rowland.harvard.edu>
Acked-by: Jens Axboe <jens.axboe@oracle.com>
Acked-by: Douglas Gilbert <dougg@torque.net>
Signed-off-by: James Bottomley <James.Bottomley@SteelEye.com>
Diffstat (limited to 'block/ll_rw_blk.c')
-rw-r--r-- | block/ll_rw_blk.c | 2 |
1 files changed, 2 insertions, 0 deletions
diff --git a/block/ll_rw_blk.c b/block/ll_rw_blk.c index 38c293b987b..cf8752abd61 100644 --- a/block/ll_rw_blk.c +++ b/block/ll_rw_blk.c | |||
@@ -1925,6 +1925,8 @@ blk_init_queue_node(request_fn_proc *rfn, spinlock_t *lock, int node_id) | |||
1925 | blk_queue_max_hw_segments(q, MAX_HW_SEGMENTS); | 1925 | blk_queue_max_hw_segments(q, MAX_HW_SEGMENTS); |
1926 | blk_queue_max_phys_segments(q, MAX_PHYS_SEGMENTS); | 1926 | blk_queue_max_phys_segments(q, MAX_PHYS_SEGMENTS); |
1927 | 1927 | ||
1928 | q->sg_reserved_size = INT_MAX; | ||
1929 | |||
1928 | /* | 1930 | /* |
1929 | * all done | 1931 | * all done |
1930 | */ | 1932 | */ |