diff options
author | Diego Calleja | 2012-12-03 09:04:21 -0600 |
---|---|---|
committer | Jens Axboe | 2012-12-06 07:34:58 -0600 |
commit | 5f6f38dbb0fc8518b19542b0ad0739a8a95f05a1 (patch) | |
tree | 37b516afe21594499f3c0a8e9e9fee8141883983 /block | |
parent | 80729beb3326fd682543f4f4ea534df47ab48967 (diff) | |
download | kernel-common-5f6f38dbb0fc8518b19542b0ad0739a8a95f05a1.tar.gz kernel-common-5f6f38dbb0fc8518b19542b0ad0739a8a95f05a1.tar.xz kernel-common-5f6f38dbb0fc8518b19542b0ad0739a8a95f05a1.zip |
partitions: enable EFI/GPT support by default
The Kconfig currently enables MSDOS partitions by default because they
are assumed to be essential, but it's necessary to enable "advanced
partition selection" in order to get GPT support. IMO GPT partitions
are becoming common enought to deserve the same treatment MSDOS
partitions get.
(Side note: I got bit by a disk that had MSDOS and GPT partition
tables, but for some reason the MSDOS table was different from the
GPT one. I was stupid enought to disable "advanced partition
selection" in my .config, which disabled GPT partitioning and made
my btrfs pool unbootable because it couldn't find the partitions)
Signed-off-by: Diego Calleja <diegocg@gmail.com>
Signed-off-by: Jens Axboe <axboe@kernel.dk>
Diffstat (limited to 'block')
-rw-r--r-- | block/partitions/Kconfig | 4 |
1 files changed, 2 insertions, 2 deletions
diff --git a/block/partitions/Kconfig b/block/partitions/Kconfig index cb5f0a3f1b0..75a54e1adbb 100644 --- a/block/partitions/Kconfig +++ b/block/partitions/Kconfig | |||
@@ -234,8 +234,8 @@ config KARMA_PARTITION | |||
234 | uses a proprietary partition table. | 234 | uses a proprietary partition table. |
235 | 235 | ||
236 | config EFI_PARTITION | 236 | config EFI_PARTITION |
237 | bool "EFI GUID Partition support" | 237 | bool "EFI GUID Partition support" if PARTITION_ADVANCED |
238 | depends on PARTITION_ADVANCED | 238 | default y |
239 | select CRC32 | 239 | select CRC32 |
240 | help | 240 | help |
241 | Say Y here if you would like to use hard disks under Linux which | 241 | Say Y here if you would like to use hard disks under Linux which |