diff options
author | Hannes Reinecke | 2011-09-28 09:07:01 -0500 |
---|---|---|
committer | Jens Axboe | 2011-09-28 09:07:01 -0500 |
commit | 777eb1bf15b8532c396821774bf6451e563438f5 (patch) | |
tree | 8363e63bae76eb049f4c8d0460ef8e1f74f0ca91 /block | |
parent | a102a9ece5489e1718cd7543aa079082450ac3a2 (diff) | |
download | kernel-common-777eb1bf15b8532c396821774bf6451e563438f5.tar.gz kernel-common-777eb1bf15b8532c396821774bf6451e563438f5.tar.xz kernel-common-777eb1bf15b8532c396821774bf6451e563438f5.zip |
block: Free queue resources at blk_release_queue()
A kernel crash is observed when a mounted ext3/ext4 filesystem is
physically removed. The problem is that blk_cleanup_queue() frees up
some resources eg by calling elevator_exit(), which are not checked for
in normal operation. So we should rather move these calls to the
destructor function blk_release_queue() as at that point all remaining
references are gone. However, in doing so we have to ensure that any
externally supplied queue_lock is disconnected as the driver might free
up the lock after the call of blk_cleanup_queue(),
Signed-off-by: Hannes Reinecke <hare@suse.de>
Signed-off-by: Jens Axboe <axboe@kernel.dk>
Diffstat (limited to 'block')
-rw-r--r-- | block/blk-core.c | 13 | ||||
-rw-r--r-- | block/blk-sysfs.c | 5 |
2 files changed, 11 insertions, 7 deletions
diff --git a/block/blk-core.c b/block/blk-core.c index b2ed78afd9f..d34433ae791 100644 --- a/block/blk-core.c +++ b/block/blk-core.c | |||
@@ -348,9 +348,10 @@ void blk_put_queue(struct request_queue *q) | |||
348 | EXPORT_SYMBOL(blk_put_queue); | 348 | EXPORT_SYMBOL(blk_put_queue); |
349 | 349 | ||
350 | /* | 350 | /* |
351 | * Note: If a driver supplied the queue lock, it should not zap that lock | 351 | * Note: If a driver supplied the queue lock, it is disconnected |
352 | * unexpectedly as some queue cleanup components like elevator_exit() and | 352 | * by this function. The actual state of the lock doesn't matter |
353 | * blk_throtl_exit() need queue lock. | 353 | * here as the request_queue isn't accessible after this point |
354 | * (QUEUE_FLAG_DEAD is set) and no other requests will be queued. | ||
354 | */ | 355 | */ |
355 | void blk_cleanup_queue(struct request_queue *q) | 356 | void blk_cleanup_queue(struct request_queue *q) |
356 | { | 357 | { |
@@ -367,10 +368,8 @@ void blk_cleanup_queue(struct request_queue *q) | |||
367 | queue_flag_set_unlocked(QUEUE_FLAG_DEAD, q); | 368 | queue_flag_set_unlocked(QUEUE_FLAG_DEAD, q); |
368 | mutex_unlock(&q->sysfs_lock); | 369 | mutex_unlock(&q->sysfs_lock); |
369 | 370 | ||
370 | if (q->elevator) | 371 | if (q->queue_lock != &q->__queue_lock) |
371 | elevator_exit(q->elevator); | 372 | q->queue_lock = &q->__queue_lock; |
372 | |||
373 | blk_throtl_exit(q); | ||
374 | 373 | ||
375 | blk_put_queue(q); | 374 | blk_put_queue(q); |
376 | } | 375 | } |
diff --git a/block/blk-sysfs.c b/block/blk-sysfs.c index e681805cdb4..60fda88c57f 100644 --- a/block/blk-sysfs.c +++ b/block/blk-sysfs.c | |||
@@ -479,6 +479,11 @@ static void blk_release_queue(struct kobject *kobj) | |||
479 | 479 | ||
480 | blk_sync_queue(q); | 480 | blk_sync_queue(q); |
481 | 481 | ||
482 | if (q->elevator) | ||
483 | elevator_exit(q->elevator); | ||
484 | |||
485 | blk_throtl_exit(q); | ||
486 | |||
482 | if (rl->rq_pool) | 487 | if (rl->rq_pool) |
483 | mempool_destroy(rl->rq_pool); | 488 | mempool_destroy(rl->rq_pool); |
484 | 489 | ||