diff options
author | Linus Torvalds | 2012-10-02 13:11:09 -0500 |
---|---|---|
committer | Linus Torvalds | 2012-10-02 13:11:09 -0500 |
commit | 437589a74b6a590d175f86cf9f7b2efcee7765e7 (patch) | |
tree | 37bf8635b1356d80ef002b00e84f3faf3d555a63 /ipc | |
parent | 68d47a137c3bef754923bccf73fb639c9b0bbd5e (diff) | |
parent | 72235465864d84cedb2d9f26f8e1de824ee20339 (diff) | |
download | kernel-common-437589a74b6a590d175f86cf9f7b2efcee7765e7.tar.gz kernel-common-437589a74b6a590d175f86cf9f7b2efcee7765e7.tar.xz kernel-common-437589a74b6a590d175f86cf9f7b2efcee7765e7.zip |
Merge branch 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ebiederm/user-namespace
Pull user namespace changes from Eric Biederman:
"This is a mostly modest set of changes to enable basic user namespace
support. This allows the code to code to compile with user namespaces
enabled and removes the assumption there is only the initial user
namespace. Everything is converted except for the most complex of the
filesystems: autofs4, 9p, afs, ceph, cifs, coda, fuse, gfs2, ncpfs,
nfs, ocfs2 and xfs as those patches need a bit more review.
The strategy is to push kuid_t and kgid_t values are far down into
subsystems and filesystems as reasonable. Leaving the make_kuid and
from_kuid operations to happen at the edge of userspace, as the values
come off the disk, and as the values come in from the network.
Letting compile type incompatible compile errors (present when user
namespaces are enabled) guide me to find the issues.
The most tricky areas have been the places where we had an implicit
union of uid and gid values and were storing them in an unsigned int.
Those places were converted into explicit unions. I made certain to
handle those places with simple trivial patches.
Out of that work I discovered we have generic interfaces for storing
quota by projid. I had never heard of the project identifiers before.
Adding full user namespace support for project identifiers accounts
for most of the code size growth in my git tree.
Ultimately there will be work to relax privlige checks from
"capable(FOO)" to "ns_capable(user_ns, FOO)" where it is safe allowing
root in a user names to do those things that today we only forbid to
non-root users because it will confuse suid root applications.
While I was pushing kuid_t and kgid_t changes deep into the audit code
I made a few other cleanups. I capitalized on the fact we process
netlink messages in the context of the message sender. I removed
usage of NETLINK_CRED, and started directly using current->tty.
Some of these patches have also made it into maintainer trees, with no
problems from identical code from different trees showing up in
linux-next.
After reading through all of this code I feel like I might be able to
win a game of kernel trivial pursuit."
Fix up some fairly trivial conflicts in netfilter uid/git logging code.
* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/ebiederm/user-namespace: (107 commits)
userns: Convert the ufs filesystem to use kuid/kgid where appropriate
userns: Convert the udf filesystem to use kuid/kgid where appropriate
userns: Convert ubifs to use kuid/kgid
userns: Convert squashfs to use kuid/kgid where appropriate
userns: Convert reiserfs to use kuid and kgid where appropriate
userns: Convert jfs to use kuid/kgid where appropriate
userns: Convert jffs2 to use kuid and kgid where appropriate
userns: Convert hpfs to use kuid and kgid where appropriate
userns: Convert btrfs to use kuid/kgid where appropriate
userns: Convert bfs to use kuid/kgid where appropriate
userns: Convert affs to use kuid/kgid wherwe appropriate
userns: On alpha modify linux_to_osf_stat to use convert from kuids and kgids
userns: On ia64 deal with current_uid and current_gid being kuid and kgid
userns: On ppc convert current_uid from a kuid before printing.
userns: Convert s390 getting uid and gid system calls to use kuid and kgid
userns: Convert s390 hypfs to use kuid and kgid where appropriate
userns: Convert binder ipc to use kuids
userns: Teach security_path_chown to take kuids and kgids
userns: Add user namespace support to IMA
userns: Convert EVM to deal with kuids and kgids in it's hmac computation
...
Diffstat (limited to 'ipc')
-rw-r--r-- | ipc/msg.c | 14 | ||||
-rw-r--r-- | ipc/sem.c | 13 | ||||
-rw-r--r-- | ipc/shm.c | 19 | ||||
-rw-r--r-- | ipc/util.c | 35 | ||||
-rw-r--r-- | ipc/util.h | 2 |
5 files changed, 50 insertions, 33 deletions
@@ -443,9 +443,12 @@ static int msgctl_down(struct ipc_namespace *ns, int msqid, int cmd, | |||
443 | goto out_unlock; | 443 | goto out_unlock; |
444 | } | 444 | } |
445 | 445 | ||
446 | err = ipc_update_perm(&msqid64.msg_perm, ipcp); | ||
447 | if (err) | ||
448 | goto out_unlock; | ||
449 | |||
446 | msq->q_qbytes = msqid64.msg_qbytes; | 450 | msq->q_qbytes = msqid64.msg_qbytes; |
447 | 451 | ||
448 | ipc_update_perm(&msqid64.msg_perm, ipcp); | ||
449 | msq->q_ctime = get_seconds(); | 452 | msq->q_ctime = get_seconds(); |
450 | /* sleeping receivers might be excluded by | 453 | /* sleeping receivers might be excluded by |
451 | * stricter permissions. | 454 | * stricter permissions. |
@@ -922,6 +925,7 @@ out: | |||
922 | #ifdef CONFIG_PROC_FS | 925 | #ifdef CONFIG_PROC_FS |
923 | static int sysvipc_msg_proc_show(struct seq_file *s, void *it) | 926 | static int sysvipc_msg_proc_show(struct seq_file *s, void *it) |
924 | { | 927 | { |
928 | struct user_namespace *user_ns = seq_user_ns(s); | ||
925 | struct msg_queue *msq = it; | 929 | struct msg_queue *msq = it; |
926 | 930 | ||
927 | return seq_printf(s, | 931 | return seq_printf(s, |
@@ -933,10 +937,10 @@ static int sysvipc_msg_proc_show(struct seq_file *s, void *it) | |||
933 | msq->q_qnum, | 937 | msq->q_qnum, |
934 | msq->q_lspid, | 938 | msq->q_lspid, |
935 | msq->q_lrpid, | 939 | msq->q_lrpid, |
936 | msq->q_perm.uid, | 940 | from_kuid_munged(user_ns, msq->q_perm.uid), |
937 | msq->q_perm.gid, | 941 | from_kgid_munged(user_ns, msq->q_perm.gid), |
938 | msq->q_perm.cuid, | 942 | from_kuid_munged(user_ns, msq->q_perm.cuid), |
939 | msq->q_perm.cgid, | 943 | from_kgid_munged(user_ns, msq->q_perm.cgid), |
940 | msq->q_stime, | 944 | msq->q_stime, |
941 | msq->q_rtime, | 945 | msq->q_rtime, |
942 | msq->q_ctime); | 946 | msq->q_ctime); |
@@ -1104,7 +1104,9 @@ static int semctl_down(struct ipc_namespace *ns, int semid, | |||
1104 | freeary(ns, ipcp); | 1104 | freeary(ns, ipcp); |
1105 | goto out_up; | 1105 | goto out_up; |
1106 | case IPC_SET: | 1106 | case IPC_SET: |
1107 | ipc_update_perm(&semid64.sem_perm, ipcp); | 1107 | err = ipc_update_perm(&semid64.sem_perm, ipcp); |
1108 | if (err) | ||
1109 | goto out_unlock; | ||
1108 | sma->sem_ctime = get_seconds(); | 1110 | sma->sem_ctime = get_seconds(); |
1109 | break; | 1111 | break; |
1110 | default: | 1112 | default: |
@@ -1677,6 +1679,7 @@ void exit_sem(struct task_struct *tsk) | |||
1677 | #ifdef CONFIG_PROC_FS | 1679 | #ifdef CONFIG_PROC_FS |
1678 | static int sysvipc_sem_proc_show(struct seq_file *s, void *it) | 1680 | static int sysvipc_sem_proc_show(struct seq_file *s, void *it) |
1679 | { | 1681 | { |
1682 | struct user_namespace *user_ns = seq_user_ns(s); | ||
1680 | struct sem_array *sma = it; | 1683 | struct sem_array *sma = it; |
1681 | 1684 | ||
1682 | return seq_printf(s, | 1685 | return seq_printf(s, |
@@ -1685,10 +1688,10 @@ static int sysvipc_sem_proc_show(struct seq_file *s, void *it) | |||
1685 | sma->sem_perm.id, | 1688 | sma->sem_perm.id, |
1686 | sma->sem_perm.mode, | 1689 | sma->sem_perm.mode, |
1687 | sma->sem_nsems, | 1690 | sma->sem_nsems, |
1688 | sma->sem_perm.uid, | 1691 | from_kuid_munged(user_ns, sma->sem_perm.uid), |
1689 | sma->sem_perm.gid, | 1692 | from_kgid_munged(user_ns, sma->sem_perm.gid), |
1690 | sma->sem_perm.cuid, | 1693 | from_kuid_munged(user_ns, sma->sem_perm.cuid), |
1691 | sma->sem_perm.cgid, | 1694 | from_kgid_munged(user_ns, sma->sem_perm.cgid), |
1692 | sma->sem_otime, | 1695 | sma->sem_otime, |
1693 | sma->sem_ctime); | 1696 | sma->sem_ctime); |
1694 | } | 1697 | } |
@@ -758,7 +758,9 @@ static int shmctl_down(struct ipc_namespace *ns, int shmid, int cmd, | |||
758 | do_shm_rmid(ns, ipcp); | 758 | do_shm_rmid(ns, ipcp); |
759 | goto out_up; | 759 | goto out_up; |
760 | case IPC_SET: | 760 | case IPC_SET: |
761 | ipc_update_perm(&shmid64.shm_perm, ipcp); | 761 | err = ipc_update_perm(&shmid64.shm_perm, ipcp); |
762 | if (err) | ||
763 | goto out_unlock; | ||
762 | shp->shm_ctim = get_seconds(); | 764 | shp->shm_ctim = get_seconds(); |
763 | break; | 765 | break; |
764 | default: | 766 | default: |
@@ -893,10 +895,10 @@ SYSCALL_DEFINE3(shmctl, int, shmid, int, cmd, struct shmid_ds __user *, buf) | |||
893 | audit_ipc_obj(&(shp->shm_perm)); | 895 | audit_ipc_obj(&(shp->shm_perm)); |
894 | 896 | ||
895 | if (!ns_capable(ns->user_ns, CAP_IPC_LOCK)) { | 897 | if (!ns_capable(ns->user_ns, CAP_IPC_LOCK)) { |
896 | uid_t euid = current_euid(); | 898 | kuid_t euid = current_euid(); |
897 | err = -EPERM; | 899 | err = -EPERM; |
898 | if (euid != shp->shm_perm.uid && | 900 | if (!uid_eq(euid, shp->shm_perm.uid) && |
899 | euid != shp->shm_perm.cuid) | 901 | !uid_eq(euid, shp->shm_perm.cuid)) |
900 | goto out_unlock; | 902 | goto out_unlock; |
901 | if (cmd == SHM_LOCK && !rlimit(RLIMIT_MEMLOCK)) | 903 | if (cmd == SHM_LOCK && !rlimit(RLIMIT_MEMLOCK)) |
902 | goto out_unlock; | 904 | goto out_unlock; |
@@ -1220,6 +1222,7 @@ SYSCALL_DEFINE1(shmdt, char __user *, shmaddr) | |||
1220 | #ifdef CONFIG_PROC_FS | 1222 | #ifdef CONFIG_PROC_FS |
1221 | static int sysvipc_shm_proc_show(struct seq_file *s, void *it) | 1223 | static int sysvipc_shm_proc_show(struct seq_file *s, void *it) |
1222 | { | 1224 | { |
1225 | struct user_namespace *user_ns = seq_user_ns(s); | ||
1223 | struct shmid_kernel *shp = it; | 1226 | struct shmid_kernel *shp = it; |
1224 | unsigned long rss = 0, swp = 0; | 1227 | unsigned long rss = 0, swp = 0; |
1225 | 1228 | ||
@@ -1242,10 +1245,10 @@ static int sysvipc_shm_proc_show(struct seq_file *s, void *it) | |||
1242 | shp->shm_cprid, | 1245 | shp->shm_cprid, |
1243 | shp->shm_lprid, | 1246 | shp->shm_lprid, |
1244 | shp->shm_nattch, | 1247 | shp->shm_nattch, |
1245 | shp->shm_perm.uid, | 1248 | from_kuid_munged(user_ns, shp->shm_perm.uid), |
1246 | shp->shm_perm.gid, | 1249 | from_kgid_munged(user_ns, shp->shm_perm.gid), |
1247 | shp->shm_perm.cuid, | 1250 | from_kuid_munged(user_ns, shp->shm_perm.cuid), |
1248 | shp->shm_perm.cgid, | 1251 | from_kgid_munged(user_ns, shp->shm_perm.cgid), |
1249 | shp->shm_atim, | 1252 | shp->shm_atim, |
1250 | shp->shm_dtim, | 1253 | shp->shm_dtim, |
1251 | shp->shm_ctim, | 1254 | shp->shm_ctim, |
diff --git a/ipc/util.c b/ipc/util.c index eb07fd356f2..72fd0785ac9 100644 --- a/ipc/util.c +++ b/ipc/util.c | |||
@@ -249,8 +249,8 @@ int ipc_get_maxid(struct ipc_ids *ids) | |||
249 | 249 | ||
250 | int ipc_addid(struct ipc_ids* ids, struct kern_ipc_perm* new, int size) | 250 | int ipc_addid(struct ipc_ids* ids, struct kern_ipc_perm* new, int size) |
251 | { | 251 | { |
252 | uid_t euid; | 252 | kuid_t euid; |
253 | gid_t egid; | 253 | kgid_t egid; |
254 | int id, err; | 254 | int id, err; |
255 | 255 | ||
256 | if (size > IPCMNI) | 256 | if (size > IPCMNI) |
@@ -606,14 +606,14 @@ void ipc_rcu_putref(void *ptr) | |||
606 | 606 | ||
607 | int ipcperms(struct ipc_namespace *ns, struct kern_ipc_perm *ipcp, short flag) | 607 | int ipcperms(struct ipc_namespace *ns, struct kern_ipc_perm *ipcp, short flag) |
608 | { | 608 | { |
609 | uid_t euid = current_euid(); | 609 | kuid_t euid = current_euid(); |
610 | int requested_mode, granted_mode; | 610 | int requested_mode, granted_mode; |
611 | 611 | ||
612 | audit_ipc_obj(ipcp); | 612 | audit_ipc_obj(ipcp); |
613 | requested_mode = (flag >> 6) | (flag >> 3) | flag; | 613 | requested_mode = (flag >> 6) | (flag >> 3) | flag; |
614 | granted_mode = ipcp->mode; | 614 | granted_mode = ipcp->mode; |
615 | if (euid == ipcp->cuid || | 615 | if (uid_eq(euid, ipcp->cuid) || |
616 | euid == ipcp->uid) | 616 | uid_eq(euid, ipcp->uid)) |
617 | granted_mode >>= 6; | 617 | granted_mode >>= 6; |
618 | else if (in_group_p(ipcp->cgid) || in_group_p(ipcp->gid)) | 618 | else if (in_group_p(ipcp->cgid) || in_group_p(ipcp->gid)) |
619 | granted_mode >>= 3; | 619 | granted_mode >>= 3; |
@@ -643,10 +643,10 @@ int ipcperms(struct ipc_namespace *ns, struct kern_ipc_perm *ipcp, short flag) | |||
643 | void kernel_to_ipc64_perm (struct kern_ipc_perm *in, struct ipc64_perm *out) | 643 | void kernel_to_ipc64_perm (struct kern_ipc_perm *in, struct ipc64_perm *out) |
644 | { | 644 | { |
645 | out->key = in->key; | 645 | out->key = in->key; |
646 | out->uid = in->uid; | 646 | out->uid = from_kuid_munged(current_user_ns(), in->uid); |
647 | out->gid = in->gid; | 647 | out->gid = from_kgid_munged(current_user_ns(), in->gid); |
648 | out->cuid = in->cuid; | 648 | out->cuid = from_kuid_munged(current_user_ns(), in->cuid); |
649 | out->cgid = in->cgid; | 649 | out->cgid = from_kgid_munged(current_user_ns(), in->cgid); |
650 | out->mode = in->mode; | 650 | out->mode = in->mode; |
651 | out->seq = in->seq; | 651 | out->seq = in->seq; |
652 | } | 652 | } |
@@ -747,12 +747,19 @@ int ipcget(struct ipc_namespace *ns, struct ipc_ids *ids, | |||
747 | * @in: the permission given as input. | 747 | * @in: the permission given as input. |
748 | * @out: the permission of the ipc to set. | 748 | * @out: the permission of the ipc to set. |
749 | */ | 749 | */ |
750 | void ipc_update_perm(struct ipc64_perm *in, struct kern_ipc_perm *out) | 750 | int ipc_update_perm(struct ipc64_perm *in, struct kern_ipc_perm *out) |
751 | { | 751 | { |
752 | out->uid = in->uid; | 752 | kuid_t uid = make_kuid(current_user_ns(), in->uid); |
753 | out->gid = in->gid; | 753 | kgid_t gid = make_kgid(current_user_ns(), in->gid); |
754 | if (!uid_valid(uid) || !gid_valid(gid)) | ||
755 | return -EINVAL; | ||
756 | |||
757 | out->uid = uid; | ||
758 | out->gid = gid; | ||
754 | out->mode = (out->mode & ~S_IRWXUGO) | 759 | out->mode = (out->mode & ~S_IRWXUGO) |
755 | | (in->mode & S_IRWXUGO); | 760 | | (in->mode & S_IRWXUGO); |
761 | |||
762 | return 0; | ||
756 | } | 763 | } |
757 | 764 | ||
758 | /** | 765 | /** |
@@ -777,7 +784,7 @@ struct kern_ipc_perm *ipcctl_pre_down(struct ipc_namespace *ns, | |||
777 | struct ipc64_perm *perm, int extra_perm) | 784 | struct ipc64_perm *perm, int extra_perm) |
778 | { | 785 | { |
779 | struct kern_ipc_perm *ipcp; | 786 | struct kern_ipc_perm *ipcp; |
780 | uid_t euid; | 787 | kuid_t euid; |
781 | int err; | 788 | int err; |
782 | 789 | ||
783 | down_write(&ids->rw_mutex); | 790 | down_write(&ids->rw_mutex); |
@@ -793,7 +800,7 @@ struct kern_ipc_perm *ipcctl_pre_down(struct ipc_namespace *ns, | |||
793 | perm->gid, perm->mode); | 800 | perm->gid, perm->mode); |
794 | 801 | ||
795 | euid = current_euid(); | 802 | euid = current_euid(); |
796 | if (euid == ipcp->cuid || euid == ipcp->uid || | 803 | if (uid_eq(euid, ipcp->cuid) || uid_eq(euid, ipcp->uid) || |
797 | ns_capable(ns->user_ns, CAP_SYS_ADMIN)) | 804 | ns_capable(ns->user_ns, CAP_SYS_ADMIN)) |
798 | return ipcp; | 805 | return ipcp; |
799 | 806 | ||
diff --git a/ipc/util.h b/ipc/util.h index 850ef3e962c..c8fe2f7631e 100644 --- a/ipc/util.h +++ b/ipc/util.h | |||
@@ -125,7 +125,7 @@ struct kern_ipc_perm *ipc_lock(struct ipc_ids *, int); | |||
125 | 125 | ||
126 | void kernel_to_ipc64_perm(struct kern_ipc_perm *in, struct ipc64_perm *out); | 126 | void kernel_to_ipc64_perm(struct kern_ipc_perm *in, struct ipc64_perm *out); |
127 | void ipc64_perm_to_ipc_perm(struct ipc64_perm *in, struct ipc_perm *out); | 127 | void ipc64_perm_to_ipc_perm(struct ipc64_perm *in, struct ipc_perm *out); |
128 | void ipc_update_perm(struct ipc64_perm *in, struct kern_ipc_perm *out); | 128 | int ipc_update_perm(struct ipc64_perm *in, struct kern_ipc_perm *out); |
129 | struct kern_ipc_perm *ipcctl_pre_down(struct ipc_namespace *ns, | 129 | struct kern_ipc_perm *ipcctl_pre_down(struct ipc_namespace *ns, |
130 | struct ipc_ids *ids, int id, int cmd, | 130 | struct ipc_ids *ids, int id, int cmd, |
131 | struct ipc64_perm *perm, int extra_perm); | 131 | struct ipc64_perm *perm, int extra_perm); |