aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorTejun Heo2010-02-05 02:57:02 -0600
committerGreg Kroah-Hartman2010-03-07 19:04:46 -0600
commit77d3d7c1d561f49f755d7390f0764dff90765974 (patch)
tree4a510d5dedd5681fb76353bbaae6d622452fd749 /samples/kobject
parent25cf84cf377c0aae5dbcf937ea89bc7893db5176 (diff)
downloadkernel-common-77d3d7c1d561f49f755d7390f0764dff90765974.tar.gz
kernel-common-77d3d7c1d561f49f755d7390f0764dff90765974.tar.xz
kernel-common-77d3d7c1d561f49f755d7390f0764dff90765974.zip
driver-core: fix race condition in get_device_parent()
sysfs is creating several devices in cuse class concurrently and with CONFIG_SYSFS_DEPRECATED turned off, it triggers the following oops. BUG: unable to handle kernel NULL pointer dereference at 0000000000000038 IP: [<ffffffff81158b0a>] sysfs_addrm_start+0x4a/0xf0 PGD 75bb067 PUD 75be067 PMD 0 Oops: 0000 [#1] PREEMPT SMP last sysfs file: /sys/devices/system/cpu/cpu7/topology/core_siblings CPU 1 Modules linked in: cuse fuse Pid: 4737, comm: osspd Not tainted 2.6.31-work #77 RIP: 0010:[<ffffffff81158b0a>] [<ffffffff81158b0a>] sysfs_addrm_start+0x4a/0xf0 RSP: 0018:ffff88000042f8f8 EFLAGS: 00010296 RAX: ffff88000042ffd8 RBX: 0000000000000000 RCX: 0000000000000000 RDX: 0000000000000000 RSI: ffff880007eef660 RDI: 0000000000000001 RBP: ffff88000042f918 R08: 0000000000000000 R09: 0000000000000000 R10: 0000000000000001 R11: ffffffff81158b0a R12: ffff88000042f928 R13: 00000000fffffff4 R14: 0000000000000000 R15: ffff88000042f9a0 FS: 00007fe93905a950(0000) GS:ffff880008600000(0000) knlGS:0000000000000000 CS: 0010 DS: 0000 ES: 0000 CR0: 000000008005003b CR2: 0000000000000038 CR3: 00000000077c9000 CR4: 00000000000006e0 DR0: 0000000000000000 DR1: 0000000000000000 DR2: 0000000000000000 DR3: 0000000000000000 DR6: 00000000ffff0ff0 DR7: 0000000000000400 Process osspd (pid: 4737, threadinfo ffff88000042e000, task ffff880007eef040) Stack: ffff880005da10e8 0000000011cc8d6e ffff88000042f928 ffff880003d28a28 <0> ffff88000042f988 ffffffff811592d7 0000000000000000 0000000000000000 <0> 0000000000000000 0000000000000000 ffff88000042f958 0000000011cc8d6e Call Trace: [<ffffffff811592d7>] create_dir+0x67/0xe0 [<ffffffff811593a8>] sysfs_create_dir+0x58/0xb0 [<ffffffff8128ca7c>] ? kobject_add_internal+0xcc/0x220 [<ffffffff812942e1>] ? vsnprintf+0x3c1/0xb90 [<ffffffff8128cab7>] kobject_add_internal+0x107/0x220 [<ffffffff8128cd37>] kobject_add_varg+0x47/0x80 [<ffffffff8128ce53>] kobject_add+0x53/0x90 [<ffffffff81357d84>] device_add+0xd4/0x690 [<ffffffff81356c2b>] ? dev_set_name+0x4b/0x70 [<ffffffffa001a884>] cuse_process_init_reply+0x2b4/0x420 [cuse] ... The problem is that kobject_add_internal() first adds a kobject to the kset and then try to create sysfs directory for it. If the creation fails, it remove the kobject from the kset. get_device_parent() accesses class_dirs kset while only holding class_dirs.list_lock to see whether the cuse class dir exists. But when it exists, it may not have finished initialization yet or may fail and get removed soon. In the above case, the former happened so the second one ends up trying to create subdirectory under NULL sysfs_dirent. Fix it by grabbing a mutex in get_device_parent(). Signed-off-by: Tejun Heo <tj@kernel.org> Reported-by: Colin Guthrie <cguthrie@mandriva.org> Cc: stable <stable@kernel.org> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
Diffstat (limited to 'samples/kobject')
0 files changed, 0 insertions, 0 deletions