aboutsummaryrefslogtreecommitdiffstats
diff options
context:
space:
mode:
authorLinus Torvalds2012-10-19 14:43:19 -0500
committerLinus Torvalds2012-10-19 14:43:19 -0500
commitb05e585d4964cf0a70573d29113a1236ced98abf (patch)
tree30a74a1d0475a2d651cb67b324c4b494d65038bd /scripts
parent16757372ffa5ee0ef7e82f73a6adbb054a434a13 (diff)
downloadkernel-common-b05e585d4964cf0a70573d29113a1236ced98abf.tar.gz
kernel-common-b05e585d4964cf0a70573d29113a1236ced98abf.tar.xz
kernel-common-b05e585d4964cf0a70573d29113a1236ced98abf.zip
kbuild: Fix module signature generation
Rusty had clearly not actually tested his module signing changes that I (trustingly) applied as commit e2a666d52b48 ("kbuild: sign the modules at install time"). That commit had multiple bugs: - using "${#VARIABLE}" to get the number of characters in a shell variable may look clever, but it's locale-dependent: it returns the number of *characters*, not bytes. And we do need bytes. So don't use "${#..}" expansion, do the stupid "wc -c" thing instead (where "c" stands for "bytes", not "characters", despite the letter. - Rusty had confused "siglen" and "signerlen", and his conversion didn't set "signerlen" at all, and incorrectly set "siglen" to the size of the signer, not the size of the signature. End result: the modified sign-file script did create something that superficially *looked* like a signature, but didn't actually work at all, and would fail the signature check. Oops. Tssk, tssk, Rusty. But Rusty was definitely right that this whole thing should be rewritten in perl by somebody who has the perl-fu to do so. That is not me, though - I'm just doing an emergency fix for the shell script. Cc: Rusty Russell <rusty@rustcorp.com.au> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'scripts')
-rw-r--r--scripts/sign-file5
1 files changed, 3 insertions, 2 deletions
diff --git a/scripts/sign-file b/scripts/sign-file
index 095a953bdb8..d014abd11f1 100644
--- a/scripts/sign-file
+++ b/scripts/sign-file
@@ -81,11 +81,12 @@ openssl dgst $dgst -binary $mod || exit $?
81# the signature with no metadata attached. 81# the signature with no metadata attached.
82# 82#
83openssl rsautl -sign -inkey $key -keyform PEM -in $mod.dig -out $mod.sig || exit $? 83openssl rsautl -sign -inkey $key -keyform PEM -in $mod.dig -out $mod.sig || exit $?
84siglen=`stat -c %s $mod.sig`
84 85
85SIGNER="`perl $keyid_script $x509 signer-name`" 86SIGNER="`perl $keyid_script $x509 signer-name`"
86KEYID="`perl $keyid_script $x509 keyid`" 87KEYID="`perl $keyid_script $x509 keyid`"
87keyidlen=${#KEYID} 88keyidlen=$(echo -n "$KEYID" | wc -c)
88siglen=${#SIGNER} 89signerlen=$(echo -n "$SIGNER" | wc -c)
89 90
90# 91#
91# Build the signed binary 92# Build the signed binary