diff options
author | James Morris | 2007-10-17 01:31:32 -0500 |
---|---|---|
committer | Linus Torvalds | 2007-10-17 10:43:07 -0500 |
commit | 20510f2f4e2dabb0ff6c13901807627ec9452f98 (patch) | |
tree | d64b9eeb90d577f7f9688a215c4c6c3c2405188a /security/Kconfig | |
parent | 5c3b447457789374cdb7b03afe2540d48c649a36 (diff) | |
download | kernel-common-20510f2f4e2dabb0ff6c13901807627ec9452f98.tar.gz kernel-common-20510f2f4e2dabb0ff6c13901807627ec9452f98.tar.xz kernel-common-20510f2f4e2dabb0ff6c13901807627ec9452f98.zip |
security: Convert LSM into a static interface
Convert LSM into a static interface, as the ability to unload a security
module is not required by in-tree users and potentially complicates the
overall security architecture.
Needlessly exported LSM symbols have been unexported, to help reduce API
abuse.
Parameters for the capability and root_plug modules are now specified
at boot.
The SECURITY_FRAMEWORK_VERSION macro has also been removed.
In a nutshell, there is no safe way to unload an LSM. The modular interface
is thus unecessary and broken infrastructure. It is used only by out-of-tree
modules, which are often binary-only, illegal, abusive of the API and
dangerous, e.g. silently re-vectoring SELinux.
[akpm@linux-foundation.org: cleanups]
[akpm@linux-foundation.org: USB Kconfig fix]
[randy.dunlap@oracle.com: fix LSM kernel-doc]
Signed-off-by: James Morris <jmorris@namei.org>
Acked-by: Chris Wright <chrisw@sous-sol.org>
Cc: Stephen Smalley <sds@tycho.nsa.gov>
Cc: "Serge E. Hallyn" <serue@us.ibm.com>
Acked-by: Arjan van de Ven <arjan@infradead.org>
Signed-off-by: Randy Dunlap <randy.dunlap@oracle.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Diffstat (limited to 'security/Kconfig')
-rw-r--r-- | security/Kconfig | 6 |
1 files changed, 3 insertions, 3 deletions
diff --git a/security/Kconfig b/security/Kconfig index 460e5c9cf49..a94ee94cf49 100644 --- a/security/Kconfig +++ b/security/Kconfig | |||
@@ -74,15 +74,15 @@ config SECURITY_NETWORK_XFRM | |||
74 | If you are unsure how to answer this question, answer N. | 74 | If you are unsure how to answer this question, answer N. |
75 | 75 | ||
76 | config SECURITY_CAPABILITIES | 76 | config SECURITY_CAPABILITIES |
77 | tristate "Default Linux Capabilities" | 77 | bool "Default Linux Capabilities" |
78 | depends on SECURITY | 78 | depends on SECURITY |
79 | help | 79 | help |
80 | This enables the "default" Linux capabilities functionality. | 80 | This enables the "default" Linux capabilities functionality. |
81 | If you are unsure how to answer this question, answer Y. | 81 | If you are unsure how to answer this question, answer Y. |
82 | 82 | ||
83 | config SECURITY_ROOTPLUG | 83 | config SECURITY_ROOTPLUG |
84 | tristate "Root Plug Support" | 84 | bool "Root Plug Support" |
85 | depends on USB && SECURITY | 85 | depends on USB=y && SECURITY |
86 | help | 86 | help |
87 | This is a sample LSM module that should only be used as such. | 87 | This is a sample LSM module that should only be used as such. |
88 | It prevents any programs running with egid == 0 if a specific | 88 | It prevents any programs running with egid == 0 if a specific |