diff options
author | David Howells | 2008-11-13 17:39:23 -0600 |
---|---|---|
committer | James Morris | 2008-11-13 17:39:23 -0600 |
commit | d84f4f992cbd76e8f39c488cf0c5d123843923b1 (patch) | |
tree | fc4a0349c42995715b93d0f7a3c78e9ea9b3f36e /security/commoncap.c | |
parent | 745ca2475a6ac596e3d8d37c2759c0fbe2586227 (diff) | |
download | kernel-common-d84f4f992cbd76e8f39c488cf0c5d123843923b1.tar.gz kernel-common-d84f4f992cbd76e8f39c488cf0c5d123843923b1.tar.xz kernel-common-d84f4f992cbd76e8f39c488cf0c5d123843923b1.zip |
CRED: Inaugurate COW credentials
Inaugurate copy-on-write credentials management. This uses RCU to manage the
credentials pointer in the task_struct with respect to accesses by other tasks.
A process may only modify its own credentials, and so does not need locking to
access or modify its own credentials.
A mutex (cred_replace_mutex) is added to the task_struct to control the effect
of PTRACE_ATTACHED on credential calculations, particularly with respect to
execve().
With this patch, the contents of an active credentials struct may not be
changed directly; rather a new set of credentials must be prepared, modified
and committed using something like the following sequence of events:
struct cred *new = prepare_creds();
int ret = blah(new);
if (ret < 0) {
abort_creds(new);
return ret;
}
return commit_creds(new);
There are some exceptions to this rule: the keyrings pointed to by the active
credentials may be instantiated - keyrings violate the COW rule as managing
COW keyrings is tricky, given that it is possible for a task to directly alter
the keys in a keyring in use by another task.
To help enforce this, various pointers to sets of credentials, such as those in
the task_struct, are declared const. The purpose of this is compile-time
discouragement of altering credentials through those pointers. Once a set of
credentials has been made public through one of these pointers, it may not be
modified, except under special circumstances:
(1) Its reference count may incremented and decremented.
(2) The keyrings to which it points may be modified, but not replaced.
The only safe way to modify anything else is to create a replacement and commit
using the functions described in Documentation/credentials.txt (which will be
added by a later patch).
This patch and the preceding patches have been tested with the LTP SELinux
testsuite.
This patch makes several logical sets of alteration:
(1) execve().
This now prepares and commits credentials in various places in the
security code rather than altering the current creds directly.
(2) Temporary credential overrides.
do_coredump() and sys_faccessat() now prepare their own credentials and
temporarily override the ones currently on the acting thread, whilst
preventing interference from other threads by holding cred_replace_mutex
on the thread being dumped.
This will be replaced in a future patch by something that hands down the
credentials directly to the functions being called, rather than altering
the task's objective credentials.
(3) LSM interface.
A number of functions have been changed, added or removed:
(*) security_capset_check(), ->capset_check()
(*) security_capset_set(), ->capset_set()
Removed in favour of security_capset().
(*) security_capset(), ->capset()
New. This is passed a pointer to the new creds, a pointer to the old
creds and the proposed capability sets. It should fill in the new
creds or return an error. All pointers, barring the pointer to the
new creds, are now const.
(*) security_bprm_apply_creds(), ->bprm_apply_creds()
Changed; now returns a value, which will cause the process to be
killed if it's an error.
(*) security_task_alloc(), ->task_alloc_security()
Removed in favour of security_prepare_creds().
(*) security_cred_free(), ->cred_free()
New. Free security data attached to cred->security.
(*) security_prepare_creds(), ->cred_prepare()
New. Duplicate any security data attached to cred->security.
(*) security_commit_creds(), ->cred_commit()
New. Apply any security effects for the upcoming installation of new
security by commit_creds().
(*) security_task_post_setuid(), ->task_post_setuid()
Removed in favour of security_task_fix_setuid().
(*) security_task_fix_setuid(), ->task_fix_setuid()
Fix up the proposed new credentials for setuid(). This is used by
cap_set_fix_setuid() to implicitly adjust capabilities in line with
setuid() changes. Changes are made to the new credentials, rather
than the task itself as in security_task_post_setuid().
(*) security_task_reparent_to_init(), ->task_reparent_to_init()
Removed. Instead the task being reparented to init is referred
directly to init's credentials.
NOTE! This results in the loss of some state: SELinux's osid no
longer records the sid of the thread that forked it.
(*) security_key_alloc(), ->key_alloc()
(*) security_key_permission(), ->key_permission()
Changed. These now take cred pointers rather than task pointers to
refer to the security context.
(4) sys_capset().
This has been simplified and uses less locking. The LSM functions it
calls have been merged.
(5) reparent_to_kthreadd().
This gives the current thread the same credentials as init by simply using
commit_thread() to point that way.
(6) __sigqueue_alloc() and switch_uid()
__sigqueue_alloc() can't stop the target task from changing its creds
beneath it, so this function gets a reference to the currently applicable
user_struct which it then passes into the sigqueue struct it returns if
successful.
switch_uid() is now called from commit_creds(), and possibly should be
folded into that. commit_creds() should take care of protecting
__sigqueue_alloc().
(7) [sg]et[ug]id() and co and [sg]et_current_groups.
The set functions now all use prepare_creds(), commit_creds() and
abort_creds() to build and check a new set of credentials before applying
it.
security_task_set[ug]id() is called inside the prepared section. This
guarantees that nothing else will affect the creds until we've finished.
The calling of set_dumpable() has been moved into commit_creds().
Much of the functionality of set_user() has been moved into
commit_creds().
The get functions all simply access the data directly.
(8) security_task_prctl() and cap_task_prctl().
security_task_prctl() has been modified to return -ENOSYS if it doesn't
want to handle a function, or otherwise return the return value directly
rather than through an argument.
Additionally, cap_task_prctl() now prepares a new set of credentials, even
if it doesn't end up using it.
(9) Keyrings.
A number of changes have been made to the keyrings code:
(a) switch_uid_keyring(), copy_keys(), exit_keys() and suid_keys() have
all been dropped and built in to the credentials functions directly.
They may want separating out again later.
(b) key_alloc() and search_process_keyrings() now take a cred pointer
rather than a task pointer to specify the security context.
(c) copy_creds() gives a new thread within the same thread group a new
thread keyring if its parent had one, otherwise it discards the thread
keyring.
(d) The authorisation key now points directly to the credentials to extend
the search into rather pointing to the task that carries them.
(e) Installing thread, process or session keyrings causes a new set of
credentials to be created, even though it's not strictly necessary for
process or session keyrings (they're shared).
(10) Usermode helper.
The usermode helper code now carries a cred struct pointer in its
subprocess_info struct instead of a new session keyring pointer. This set
of credentials is derived from init_cred and installed on the new process
after it has been cloned.
call_usermodehelper_setup() allocates the new credentials and
call_usermodehelper_freeinfo() discards them if they haven't been used. A
special cred function (prepare_usermodeinfo_creds()) is provided
specifically for call_usermodehelper_setup() to call.
call_usermodehelper_setkeys() adjusts the credentials to sport the
supplied keyring as the new session keyring.
(11) SELinux.
SELinux has a number of changes, in addition to those to support the LSM
interface changes mentioned above:
(a) selinux_setprocattr() no longer does its check for whether the
current ptracer can access processes with the new SID inside the lock
that covers getting the ptracer's SID. Whilst this lock ensures that
the check is done with the ptracer pinned, the result is only valid
until the lock is released, so there's no point doing it inside the
lock.
(12) is_single_threaded().
This function has been extracted from selinux_setprocattr() and put into
a file of its own in the lib/ directory as join_session_keyring() now
wants to use it too.
The code in SELinux just checked to see whether a task shared mm_structs
with other tasks (CLONE_VM), but that isn't good enough. We really want
to know if they're part of the same thread group (CLONE_THREAD).
(13) nfsd.
The NFS server daemon now has to use the COW credentials to set the
credentials it is going to use. It really needs to pass the credentials
down to the functions it calls, but it can't do that until other patches
in this series have been applied.
Signed-off-by: David Howells <dhowells@redhat.com>
Acked-by: James Morris <jmorris@namei.org>
Signed-off-by: James Morris <jmorris@namei.org>
Diffstat (limited to 'security/commoncap.c')
-rw-r--r-- | security/commoncap.c | 265 |
1 files changed, 125 insertions, 140 deletions
diff --git a/security/commoncap.c b/security/commoncap.c index 0384bf95db6..b5419273f92 100644 --- a/security/commoncap.c +++ b/security/commoncap.c | |||
@@ -72,8 +72,8 @@ int cap_ptrace_may_access(struct task_struct *child, unsigned int mode) | |||
72 | int ret = 0; | 72 | int ret = 0; |
73 | 73 | ||
74 | rcu_read_lock(); | 74 | rcu_read_lock(); |
75 | if (!cap_issubset(child->cred->cap_permitted, | 75 | if (!cap_issubset(__task_cred(child)->cap_permitted, |
76 | current->cred->cap_permitted) && | 76 | current_cred()->cap_permitted) && |
77 | !capable(CAP_SYS_PTRACE)) | 77 | !capable(CAP_SYS_PTRACE)) |
78 | ret = -EPERM; | 78 | ret = -EPERM; |
79 | rcu_read_unlock(); | 79 | rcu_read_unlock(); |
@@ -85,8 +85,8 @@ int cap_ptrace_traceme(struct task_struct *parent) | |||
85 | int ret = 0; | 85 | int ret = 0; |
86 | 86 | ||
87 | rcu_read_lock(); | 87 | rcu_read_lock(); |
88 | if (!cap_issubset(current->cred->cap_permitted, | 88 | if (!cap_issubset(current_cred()->cap_permitted, |
89 | parent->cred->cap_permitted) && | 89 | __task_cred(parent)->cap_permitted) && |
90 | !has_capability(parent, CAP_SYS_PTRACE)) | 90 | !has_capability(parent, CAP_SYS_PTRACE)) |
91 | ret = -EPERM; | 91 | ret = -EPERM; |
92 | rcu_read_unlock(); | 92 | rcu_read_unlock(); |
@@ -117,7 +117,7 @@ static inline int cap_inh_is_capped(void) | |||
117 | * to the old permitted set. That is, if the current task | 117 | * to the old permitted set. That is, if the current task |
118 | * does *not* possess the CAP_SETPCAP capability. | 118 | * does *not* possess the CAP_SETPCAP capability. |
119 | */ | 119 | */ |
120 | return (cap_capable(current, CAP_SETPCAP, SECURITY_CAP_AUDIT) != 0); | 120 | return cap_capable(current, CAP_SETPCAP, SECURITY_CAP_AUDIT) != 0; |
121 | } | 121 | } |
122 | 122 | ||
123 | static inline int cap_limit_ptraced_target(void) { return 1; } | 123 | static inline int cap_limit_ptraced_target(void) { return 1; } |
@@ -132,52 +132,39 @@ static inline int cap_limit_ptraced_target(void) | |||
132 | 132 | ||
133 | #endif /* def CONFIG_SECURITY_FILE_CAPABILITIES */ | 133 | #endif /* def CONFIG_SECURITY_FILE_CAPABILITIES */ |
134 | 134 | ||
135 | int cap_capset_check(const kernel_cap_t *effective, | 135 | int cap_capset(struct cred *new, |
136 | const kernel_cap_t *inheritable, | 136 | const struct cred *old, |
137 | const kernel_cap_t *permitted) | 137 | const kernel_cap_t *effective, |
138 | const kernel_cap_t *inheritable, | ||
139 | const kernel_cap_t *permitted) | ||
138 | { | 140 | { |
139 | const struct cred *cred = current->cred; | 141 | if (cap_inh_is_capped() && |
140 | 142 | !cap_issubset(*inheritable, | |
141 | if (cap_inh_is_capped() | 143 | cap_combine(old->cap_inheritable, |
142 | && !cap_issubset(*inheritable, | 144 | old->cap_permitted))) |
143 | cap_combine(cred->cap_inheritable, | ||
144 | cred->cap_permitted))) { | ||
145 | /* incapable of using this inheritable set */ | 145 | /* incapable of using this inheritable set */ |
146 | return -EPERM; | 146 | return -EPERM; |
147 | } | 147 | |
148 | if (!cap_issubset(*inheritable, | 148 | if (!cap_issubset(*inheritable, |
149 | cap_combine(cred->cap_inheritable, | 149 | cap_combine(old->cap_inheritable, |
150 | cred->cap_bset))) { | 150 | old->cap_bset))) |
151 | /* no new pI capabilities outside bounding set */ | 151 | /* no new pI capabilities outside bounding set */ |
152 | return -EPERM; | 152 | return -EPERM; |
153 | } | ||
154 | 153 | ||
155 | /* verify restrictions on target's new Permitted set */ | 154 | /* verify restrictions on target's new Permitted set */ |
156 | if (!cap_issubset (*permitted, | 155 | if (!cap_issubset(*permitted, old->cap_permitted)) |
157 | cap_combine (cred->cap_permitted, | ||
158 | cred->cap_permitted))) { | ||
159 | return -EPERM; | 156 | return -EPERM; |
160 | } | ||
161 | 157 | ||
162 | /* verify the _new_Effective_ is a subset of the _new_Permitted_ */ | 158 | /* verify the _new_Effective_ is a subset of the _new_Permitted_ */ |
163 | if (!cap_issubset (*effective, *permitted)) { | 159 | if (!cap_issubset(*effective, *permitted)) |
164 | return -EPERM; | 160 | return -EPERM; |
165 | } | ||
166 | 161 | ||
162 | new->cap_effective = *effective; | ||
163 | new->cap_inheritable = *inheritable; | ||
164 | new->cap_permitted = *permitted; | ||
167 | return 0; | 165 | return 0; |
168 | } | 166 | } |
169 | 167 | ||
170 | void cap_capset_set(const kernel_cap_t *effective, | ||
171 | const kernel_cap_t *inheritable, | ||
172 | const kernel_cap_t *permitted) | ||
173 | { | ||
174 | struct cred *cred = current->cred; | ||
175 | |||
176 | cred->cap_effective = *effective; | ||
177 | cred->cap_inheritable = *inheritable; | ||
178 | cred->cap_permitted = *permitted; | ||
179 | } | ||
180 | |||
181 | static inline void bprm_clear_caps(struct linux_binprm *bprm) | 168 | static inline void bprm_clear_caps(struct linux_binprm *bprm) |
182 | { | 169 | { |
183 | cap_clear(bprm->cap_post_exec_permitted); | 170 | cap_clear(bprm->cap_post_exec_permitted); |
@@ -382,41 +369,46 @@ int cap_bprm_set_security (struct linux_binprm *bprm) | |||
382 | return ret; | 369 | return ret; |
383 | } | 370 | } |
384 | 371 | ||
385 | void cap_bprm_apply_creds (struct linux_binprm *bprm, int unsafe) | 372 | int cap_bprm_apply_creds (struct linux_binprm *bprm, int unsafe) |
386 | { | 373 | { |
387 | struct cred *cred = current->cred; | 374 | const struct cred *old = current_cred(); |
375 | struct cred *new; | ||
376 | |||
377 | new = prepare_creds(); | ||
378 | if (!new) | ||
379 | return -ENOMEM; | ||
388 | 380 | ||
389 | if (bprm->e_uid != cred->uid || bprm->e_gid != cred->gid || | 381 | if (bprm->e_uid != old->uid || bprm->e_gid != old->gid || |
390 | !cap_issubset(bprm->cap_post_exec_permitted, | 382 | !cap_issubset(bprm->cap_post_exec_permitted, |
391 | cred->cap_permitted)) { | 383 | old->cap_permitted)) { |
392 | set_dumpable(current->mm, suid_dumpable); | 384 | set_dumpable(current->mm, suid_dumpable); |
393 | current->pdeath_signal = 0; | 385 | current->pdeath_signal = 0; |
394 | 386 | ||
395 | if (unsafe & ~LSM_UNSAFE_PTRACE_CAP) { | 387 | if (unsafe & ~LSM_UNSAFE_PTRACE_CAP) { |
396 | if (!capable(CAP_SETUID)) { | 388 | if (!capable(CAP_SETUID)) { |
397 | bprm->e_uid = cred->uid; | 389 | bprm->e_uid = old->uid; |
398 | bprm->e_gid = cred->gid; | 390 | bprm->e_gid = old->gid; |
399 | } | 391 | } |
400 | if (cap_limit_ptraced_target()) { | 392 | if (cap_limit_ptraced_target()) { |
401 | bprm->cap_post_exec_permitted = cap_intersect( | 393 | bprm->cap_post_exec_permitted = cap_intersect( |
402 | bprm->cap_post_exec_permitted, | 394 | bprm->cap_post_exec_permitted, |
403 | cred->cap_permitted); | 395 | new->cap_permitted); |
404 | } | 396 | } |
405 | } | 397 | } |
406 | } | 398 | } |
407 | 399 | ||
408 | cred->suid = cred->euid = cred->fsuid = bprm->e_uid; | 400 | new->suid = new->euid = new->fsuid = bprm->e_uid; |
409 | cred->sgid = cred->egid = cred->fsgid = bprm->e_gid; | 401 | new->sgid = new->egid = new->fsgid = bprm->e_gid; |
410 | 402 | ||
411 | /* For init, we want to retain the capabilities set | 403 | /* For init, we want to retain the capabilities set |
412 | * in the init_task struct. Thus we skip the usual | 404 | * in the init_task struct. Thus we skip the usual |
413 | * capability rules */ | 405 | * capability rules */ |
414 | if (!is_global_init(current)) { | 406 | if (!is_global_init(current)) { |
415 | cred->cap_permitted = bprm->cap_post_exec_permitted; | 407 | new->cap_permitted = bprm->cap_post_exec_permitted; |
416 | if (bprm->cap_effective) | 408 | if (bprm->cap_effective) |
417 | cred->cap_effective = bprm->cap_post_exec_permitted; | 409 | new->cap_effective = bprm->cap_post_exec_permitted; |
418 | else | 410 | else |
419 | cap_clear(cred->cap_effective); | 411 | cap_clear(new->cap_effective); |
420 | } | 412 | } |
421 | 413 | ||
422 | /* | 414 | /* |
@@ -431,15 +423,15 @@ void cap_bprm_apply_creds (struct linux_binprm *bprm, int unsafe) | |||
431 | * Number 1 above might fail if you don't have a full bset, but I think | 423 | * Number 1 above might fail if you don't have a full bset, but I think |
432 | * that is interesting information to audit. | 424 | * that is interesting information to audit. |
433 | */ | 425 | */ |
434 | if (!cap_isclear(cred->cap_effective)) { | 426 | if (!cap_isclear(new->cap_effective)) { |
435 | if (!cap_issubset(CAP_FULL_SET, cred->cap_effective) || | 427 | if (!cap_issubset(CAP_FULL_SET, new->cap_effective) || |
436 | (bprm->e_uid != 0) || (cred->uid != 0) || | 428 | bprm->e_uid != 0 || new->uid != 0 || |
437 | issecure(SECURE_NOROOT)) | 429 | issecure(SECURE_NOROOT)) |
438 | audit_log_bprm_fcaps(bprm, &cred->cap_permitted, | 430 | audit_log_bprm_fcaps(bprm, new, old); |
439 | &cred->cap_effective); | ||
440 | } | 431 | } |
441 | 432 | ||
442 | cred->securebits &= ~issecure_mask(SECURE_KEEP_CAPS); | 433 | new->securebits &= ~issecure_mask(SECURE_KEEP_CAPS); |
434 | return commit_creds(new); | ||
443 | } | 435 | } |
444 | 436 | ||
445 | int cap_bprm_secureexec (struct linux_binprm *bprm) | 437 | int cap_bprm_secureexec (struct linux_binprm *bprm) |
@@ -514,65 +506,49 @@ int cap_inode_removexattr(struct dentry *dentry, const char *name) | |||
514 | * files.. | 506 | * files.. |
515 | * Thanks to Olaf Kirch and Peter Benie for spotting this. | 507 | * Thanks to Olaf Kirch and Peter Benie for spotting this. |
516 | */ | 508 | */ |
517 | static inline void cap_emulate_setxuid (int old_ruid, int old_euid, | 509 | static inline void cap_emulate_setxuid(struct cred *new, const struct cred *old) |
518 | int old_suid) | ||
519 | { | 510 | { |
520 | struct cred *cred = current->cred; | 511 | if ((old->uid == 0 || old->euid == 0 || old->suid == 0) && |
521 | 512 | (new->uid != 0 && new->euid != 0 && new->suid != 0) && | |
522 | if ((old_ruid == 0 || old_euid == 0 || old_suid == 0) && | ||
523 | (cred->uid != 0 && cred->euid != 0 && cred->suid != 0) && | ||
524 | !issecure(SECURE_KEEP_CAPS)) { | 513 | !issecure(SECURE_KEEP_CAPS)) { |
525 | cap_clear(cred->cap_permitted); | 514 | cap_clear(new->cap_permitted); |
526 | cap_clear(cred->cap_effective); | 515 | cap_clear(new->cap_effective); |
527 | } | ||
528 | if (old_euid == 0 && cred->euid != 0) { | ||
529 | cap_clear(cred->cap_effective); | ||
530 | } | ||
531 | if (old_euid != 0 && cred->euid == 0) { | ||
532 | cred->cap_effective = cred->cap_permitted; | ||
533 | } | 516 | } |
517 | if (old->euid == 0 && new->euid != 0) | ||
518 | cap_clear(new->cap_effective); | ||
519 | if (old->euid != 0 && new->euid == 0) | ||
520 | new->cap_effective = new->cap_permitted; | ||
534 | } | 521 | } |
535 | 522 | ||
536 | int cap_task_post_setuid (uid_t old_ruid, uid_t old_euid, uid_t old_suid, | 523 | int cap_task_fix_setuid(struct cred *new, const struct cred *old, int flags) |
537 | int flags) | ||
538 | { | 524 | { |
539 | struct cred *cred = current->cred; | ||
540 | |||
541 | switch (flags) { | 525 | switch (flags) { |
542 | case LSM_SETID_RE: | 526 | case LSM_SETID_RE: |
543 | case LSM_SETID_ID: | 527 | case LSM_SETID_ID: |
544 | case LSM_SETID_RES: | 528 | case LSM_SETID_RES: |
545 | /* Copied from kernel/sys.c:setreuid/setuid/setresuid. */ | 529 | /* Copied from kernel/sys.c:setreuid/setuid/setresuid. */ |
546 | if (!issecure (SECURE_NO_SETUID_FIXUP)) { | 530 | if (!issecure(SECURE_NO_SETUID_FIXUP)) |
547 | cap_emulate_setxuid (old_ruid, old_euid, old_suid); | 531 | cap_emulate_setxuid(new, old); |
548 | } | ||
549 | break; | 532 | break; |
550 | case LSM_SETID_FS: | 533 | case LSM_SETID_FS: |
551 | { | 534 | /* Copied from kernel/sys.c:setfsuid. */ |
552 | uid_t old_fsuid = old_ruid; | ||
553 | |||
554 | /* Copied from kernel/sys.c:setfsuid. */ | ||
555 | 535 | ||
556 | /* | 536 | /* |
557 | * FIXME - is fsuser used for all CAP_FS_MASK capabilities? | 537 | * FIXME - is fsuser used for all CAP_FS_MASK capabilities? |
558 | * if not, we might be a bit too harsh here. | 538 | * if not, we might be a bit too harsh here. |
559 | */ | 539 | */ |
560 | 540 | if (!issecure(SECURE_NO_SETUID_FIXUP)) { | |
561 | if (!issecure (SECURE_NO_SETUID_FIXUP)) { | 541 | if (old->fsuid == 0 && new->fsuid != 0) { |
562 | if (old_fsuid == 0 && cred->fsuid != 0) { | 542 | new->cap_effective = |
563 | cred->cap_effective = | 543 | cap_drop_fs_set(new->cap_effective); |
564 | cap_drop_fs_set( | 544 | } |
565 | cred->cap_effective); | 545 | if (old->fsuid != 0 && new->fsuid == 0) { |
566 | } | 546 | new->cap_effective = |
567 | if (old_fsuid != 0 && cred->fsuid == 0) { | 547 | cap_raise_fs_set(new->cap_effective, |
568 | cred->cap_effective = | 548 | new->cap_permitted); |
569 | cap_raise_fs_set( | ||
570 | cred->cap_effective, | ||
571 | cred->cap_permitted); | ||
572 | } | ||
573 | } | 549 | } |
574 | break; | ||
575 | } | 550 | } |
551 | break; | ||
576 | default: | 552 | default: |
577 | return -EINVAL; | 553 | return -EINVAL; |
578 | } | 554 | } |
@@ -628,13 +604,14 @@ int cap_task_setnice (struct task_struct *p, int nice) | |||
628 | * this task could get inconsistent info. There can be no | 604 | * this task could get inconsistent info. There can be no |
629 | * racing writer bc a task can only change its own caps. | 605 | * racing writer bc a task can only change its own caps. |
630 | */ | 606 | */ |
631 | static long cap_prctl_drop(unsigned long cap) | 607 | static long cap_prctl_drop(struct cred *new, unsigned long cap) |
632 | { | 608 | { |
633 | if (!capable(CAP_SETPCAP)) | 609 | if (!capable(CAP_SETPCAP)) |
634 | return -EPERM; | 610 | return -EPERM; |
635 | if (!cap_valid(cap)) | 611 | if (!cap_valid(cap)) |
636 | return -EINVAL; | 612 | return -EINVAL; |
637 | cap_lower(current->cred->cap_bset, cap); | 613 | |
614 | cap_lower(new->cap_bset, cap); | ||
638 | return 0; | 615 | return 0; |
639 | } | 616 | } |
640 | 617 | ||
@@ -655,22 +632,29 @@ int cap_task_setnice (struct task_struct *p, int nice) | |||
655 | #endif | 632 | #endif |
656 | 633 | ||
657 | int cap_task_prctl(int option, unsigned long arg2, unsigned long arg3, | 634 | int cap_task_prctl(int option, unsigned long arg2, unsigned long arg3, |
658 | unsigned long arg4, unsigned long arg5, long *rc_p) | 635 | unsigned long arg4, unsigned long arg5) |
659 | { | 636 | { |
660 | struct cred *cred = current_cred(); | 637 | struct cred *new; |
661 | long error = 0; | 638 | long error = 0; |
662 | 639 | ||
640 | new = prepare_creds(); | ||
641 | if (!new) | ||
642 | return -ENOMEM; | ||
643 | |||
663 | switch (option) { | 644 | switch (option) { |
664 | case PR_CAPBSET_READ: | 645 | case PR_CAPBSET_READ: |
646 | error = -EINVAL; | ||
665 | if (!cap_valid(arg2)) | 647 | if (!cap_valid(arg2)) |
666 | error = -EINVAL; | 648 | goto error; |
667 | else | 649 | error = !!cap_raised(new->cap_bset, arg2); |
668 | error = !!cap_raised(cred->cap_bset, arg2); | 650 | goto no_change; |
669 | break; | 651 | |
670 | #ifdef CONFIG_SECURITY_FILE_CAPABILITIES | 652 | #ifdef CONFIG_SECURITY_FILE_CAPABILITIES |
671 | case PR_CAPBSET_DROP: | 653 | case PR_CAPBSET_DROP: |
672 | error = cap_prctl_drop(arg2); | 654 | error = cap_prctl_drop(new, arg2); |
673 | break; | 655 | if (error < 0) |
656 | goto error; | ||
657 | goto changed; | ||
674 | 658 | ||
675 | /* | 659 | /* |
676 | * The next four prctl's remain to assist with transitioning a | 660 | * The next four prctl's remain to assist with transitioning a |
@@ -692,12 +676,12 @@ int cap_task_prctl(int option, unsigned long arg2, unsigned long arg3, | |||
692 | * capability-based-privilege environment. | 676 | * capability-based-privilege environment. |
693 | */ | 677 | */ |
694 | case PR_SET_SECUREBITS: | 678 | case PR_SET_SECUREBITS: |
695 | if ((((cred->securebits & SECURE_ALL_LOCKS) >> 1) | 679 | error = -EPERM; |
696 | & (cred->securebits ^ arg2)) /*[1]*/ | 680 | if ((((new->securebits & SECURE_ALL_LOCKS) >> 1) |
697 | || ((cred->securebits & SECURE_ALL_LOCKS | 681 | & (new->securebits ^ arg2)) /*[1]*/ |
698 | & ~arg2)) /*[2]*/ | 682 | || ((new->securebits & SECURE_ALL_LOCKS & ~arg2)) /*[2]*/ |
699 | || (arg2 & ~(SECURE_ALL_LOCKS | SECURE_ALL_BITS)) /*[3]*/ | 683 | || (arg2 & ~(SECURE_ALL_LOCKS | SECURE_ALL_BITS)) /*[3]*/ |
700 | || (cap_capable(current, CAP_SETPCAP, SECURITY_CAP_AUDIT) != 0)) { /*[4]*/ | 684 | || (cap_capable(current, CAP_SETPCAP, SECURITY_CAP_AUDIT) != 0) /*[4]*/ |
701 | /* | 685 | /* |
702 | * [1] no changing of bits that are locked | 686 | * [1] no changing of bits that are locked |
703 | * [2] no unlocking of locks | 687 | * [2] no unlocking of locks |
@@ -705,50 +689,51 @@ int cap_task_prctl(int option, unsigned long arg2, unsigned long arg3, | |||
705 | * [4] doing anything requires privilege (go read about | 689 | * [4] doing anything requires privilege (go read about |
706 | * the "sendmail capabilities bug") | 690 | * the "sendmail capabilities bug") |
707 | */ | 691 | */ |
708 | error = -EPERM; /* cannot change a locked bit */ | 692 | ) |
709 | } else { | 693 | /* cannot change a locked bit */ |
710 | cred->securebits = arg2; | 694 | goto error; |
711 | } | 695 | new->securebits = arg2; |
712 | break; | 696 | goto changed; |
697 | |||
713 | case PR_GET_SECUREBITS: | 698 | case PR_GET_SECUREBITS: |
714 | error = cred->securebits; | 699 | error = new->securebits; |
715 | break; | 700 | goto no_change; |
716 | 701 | ||
717 | #endif /* def CONFIG_SECURITY_FILE_CAPABILITIES */ | 702 | #endif /* def CONFIG_SECURITY_FILE_CAPABILITIES */ |
718 | 703 | ||
719 | case PR_GET_KEEPCAPS: | 704 | case PR_GET_KEEPCAPS: |
720 | if (issecure(SECURE_KEEP_CAPS)) | 705 | if (issecure(SECURE_KEEP_CAPS)) |
721 | error = 1; | 706 | error = 1; |
722 | break; | 707 | goto no_change; |
708 | |||
723 | case PR_SET_KEEPCAPS: | 709 | case PR_SET_KEEPCAPS: |
710 | error = -EINVAL; | ||
724 | if (arg2 > 1) /* Note, we rely on arg2 being unsigned here */ | 711 | if (arg2 > 1) /* Note, we rely on arg2 being unsigned here */ |
725 | error = -EINVAL; | 712 | goto error; |
726 | else if (issecure(SECURE_KEEP_CAPS_LOCKED)) | 713 | error = -EPERM; |
727 | error = -EPERM; | 714 | if (issecure(SECURE_KEEP_CAPS_LOCKED)) |
728 | else if (arg2) | 715 | goto error; |
729 | cred->securebits |= issecure_mask(SECURE_KEEP_CAPS); | 716 | if (arg2) |
717 | new->securebits |= issecure_mask(SECURE_KEEP_CAPS); | ||
730 | else | 718 | else |
731 | cred->securebits &= ~issecure_mask(SECURE_KEEP_CAPS); | 719 | new->securebits &= ~issecure_mask(SECURE_KEEP_CAPS); |
732 | break; | 720 | goto changed; |
733 | 721 | ||
734 | default: | 722 | default: |
735 | /* No functionality available - continue with default */ | 723 | /* No functionality available - continue with default */ |
736 | return 0; | 724 | error = -ENOSYS; |
725 | goto error; | ||
737 | } | 726 | } |
738 | 727 | ||
739 | /* Functionality provided */ | 728 | /* Functionality provided */ |
740 | *rc_p = error; | 729 | changed: |
741 | return 1; | 730 | return commit_creds(new); |
742 | } | 731 | |
743 | 732 | no_change: | |
744 | void cap_task_reparent_to_init (struct task_struct *p) | 733 | error = 0; |
745 | { | 734 | error: |
746 | struct cred *cred = p->cred; | 735 | abort_creds(new); |
747 | 736 | return error; | |
748 | cap_set_init_eff(cred->cap_effective); | ||
749 | cap_clear(cred->cap_inheritable); | ||
750 | cap_set_full(cred->cap_permitted); | ||
751 | p->cred->securebits = SECUREBITS_DEFAULT; | ||
752 | } | 737 | } |
753 | 738 | ||
754 | int cap_syslog (int type) | 739 | int cap_syslog (int type) |