diff options
author | David Howells | 2012-09-13 07:06:29 -0500 |
---|---|---|
committer | Rusty Russell | 2012-10-07 22:19:48 -0500 |
commit | cf7f601c067994f371ba77721d1e45fce61a4569 (patch) | |
tree | 4ff5a12ae84cf47a9815c3e3979341a66360cb31 /security/keys | |
parent | 9bb9c3be56834653878f766f471fa1c20e562f4c (diff) | |
download | kernel-common-cf7f601c067994f371ba77721d1e45fce61a4569.tar.gz kernel-common-cf7f601c067994f371ba77721d1e45fce61a4569.tar.xz kernel-common-cf7f601c067994f371ba77721d1e45fce61a4569.zip |
KEYS: Add payload preparsing opportunity prior to key instantiate or update
Give the key type the opportunity to preparse the payload prior to the
instantiation and update routines being called. This is done with the
provision of two new key type operations:
int (*preparse)(struct key_preparsed_payload *prep);
void (*free_preparse)(struct key_preparsed_payload *prep);
If the first operation is present, then it is called before key creation (in
the add/update case) or before the key semaphore is taken (in the update and
instantiate cases). The second operation is called to clean up if the first
was called.
preparse() is given the opportunity to fill in the following structure:
struct key_preparsed_payload {
char *description;
void *type_data[2];
void *payload;
const void *data;
size_t datalen;
size_t quotalen;
};
Before the preparser is called, the first three fields will have been cleared,
the payload pointer and size will be stored in data and datalen and the default
quota size from the key_type struct will be stored into quotalen.
The preparser may parse the payload in any way it likes and may store data in
the type_data[] and payload fields for use by the instantiate() and update()
ops.
The preparser may also propose a description for the key by attaching it as a
string to the description field. This can be used by passing a NULL or ""
description to the add_key() system call or the key_create_or_update()
function. This cannot work with request_key() as that required the description
to tell the upcall about the key to be created.
This, for example permits keys that store PGP public keys to generate their own
name from the user ID and public key fingerprint in the key.
The instantiate() and update() operations are then modified to look like this:
int (*instantiate)(struct key *key, struct key_preparsed_payload *prep);
int (*update)(struct key *key, struct key_preparsed_payload *prep);
and the new payload data is passed in *prep, whether or not it was preparsed.
Signed-off-by: David Howells <dhowells@redhat.com>
Signed-off-by: Rusty Russell <rusty@rustcorp.com.au>
Diffstat (limited to 'security/keys')
-rw-r--r-- | security/keys/encrypted-keys/encrypted.c | 16 | ||||
-rw-r--r-- | security/keys/key.c | 114 | ||||
-rw-r--r-- | security/keys/keyctl.c | 18 | ||||
-rw-r--r-- | security/keys/keyring.c | 6 | ||||
-rw-r--r-- | security/keys/request_key_auth.c | 8 | ||||
-rw-r--r-- | security/keys/trusted.c | 16 | ||||
-rw-r--r-- | security/keys/user_defined.c | 14 |
7 files changed, 129 insertions, 63 deletions
diff --git a/security/keys/encrypted-keys/encrypted.c b/security/keys/encrypted-keys/encrypted.c index 2d1bb8af769..9e1e005c759 100644 --- a/security/keys/encrypted-keys/encrypted.c +++ b/security/keys/encrypted-keys/encrypted.c | |||
@@ -773,8 +773,8 @@ static int encrypted_init(struct encrypted_key_payload *epayload, | |||
773 | * | 773 | * |
774 | * On success, return 0. Otherwise return errno. | 774 | * On success, return 0. Otherwise return errno. |
775 | */ | 775 | */ |
776 | static int encrypted_instantiate(struct key *key, const void *data, | 776 | static int encrypted_instantiate(struct key *key, |
777 | size_t datalen) | 777 | struct key_preparsed_payload *prep) |
778 | { | 778 | { |
779 | struct encrypted_key_payload *epayload = NULL; | 779 | struct encrypted_key_payload *epayload = NULL; |
780 | char *datablob = NULL; | 780 | char *datablob = NULL; |
@@ -782,16 +782,17 @@ static int encrypted_instantiate(struct key *key, const void *data, | |||
782 | char *master_desc = NULL; | 782 | char *master_desc = NULL; |
783 | char *decrypted_datalen = NULL; | 783 | char *decrypted_datalen = NULL; |
784 | char *hex_encoded_iv = NULL; | 784 | char *hex_encoded_iv = NULL; |
785 | size_t datalen = prep->datalen; | ||
785 | int ret; | 786 | int ret; |
786 | 787 | ||
787 | if (datalen <= 0 || datalen > 32767 || !data) | 788 | if (datalen <= 0 || datalen > 32767 || !prep->data) |
788 | return -EINVAL; | 789 | return -EINVAL; |
789 | 790 | ||
790 | datablob = kmalloc(datalen + 1, GFP_KERNEL); | 791 | datablob = kmalloc(datalen + 1, GFP_KERNEL); |
791 | if (!datablob) | 792 | if (!datablob) |
792 | return -ENOMEM; | 793 | return -ENOMEM; |
793 | datablob[datalen] = 0; | 794 | datablob[datalen] = 0; |
794 | memcpy(datablob, data, datalen); | 795 | memcpy(datablob, prep->data, datalen); |
795 | ret = datablob_parse(datablob, &format, &master_desc, | 796 | ret = datablob_parse(datablob, &format, &master_desc, |
796 | &decrypted_datalen, &hex_encoded_iv); | 797 | &decrypted_datalen, &hex_encoded_iv); |
797 | if (ret < 0) | 798 | if (ret < 0) |
@@ -834,16 +835,17 @@ static void encrypted_rcu_free(struct rcu_head *rcu) | |||
834 | * | 835 | * |
835 | * On success, return 0. Otherwise return errno. | 836 | * On success, return 0. Otherwise return errno. |
836 | */ | 837 | */ |
837 | static int encrypted_update(struct key *key, const void *data, size_t datalen) | 838 | static int encrypted_update(struct key *key, struct key_preparsed_payload *prep) |
838 | { | 839 | { |
839 | struct encrypted_key_payload *epayload = key->payload.data; | 840 | struct encrypted_key_payload *epayload = key->payload.data; |
840 | struct encrypted_key_payload *new_epayload; | 841 | struct encrypted_key_payload *new_epayload; |
841 | char *buf; | 842 | char *buf; |
842 | char *new_master_desc = NULL; | 843 | char *new_master_desc = NULL; |
843 | const char *format = NULL; | 844 | const char *format = NULL; |
845 | size_t datalen = prep->datalen; | ||
844 | int ret = 0; | 846 | int ret = 0; |
845 | 847 | ||
846 | if (datalen <= 0 || datalen > 32767 || !data) | 848 | if (datalen <= 0 || datalen > 32767 || !prep->data) |
847 | return -EINVAL; | 849 | return -EINVAL; |
848 | 850 | ||
849 | buf = kmalloc(datalen + 1, GFP_KERNEL); | 851 | buf = kmalloc(datalen + 1, GFP_KERNEL); |
@@ -851,7 +853,7 @@ static int encrypted_update(struct key *key, const void *data, size_t datalen) | |||
851 | return -ENOMEM; | 853 | return -ENOMEM; |
852 | 854 | ||
853 | buf[datalen] = 0; | 855 | buf[datalen] = 0; |
854 | memcpy(buf, data, datalen); | 856 | memcpy(buf, prep->data, datalen); |
855 | ret = datablob_parse(buf, &format, &new_master_desc, NULL, NULL); | 857 | ret = datablob_parse(buf, &format, &new_master_desc, NULL, NULL); |
856 | if (ret < 0) | 858 | if (ret < 0) |
857 | goto out; | 859 | goto out; |
diff --git a/security/keys/key.c b/security/keys/key.c index 50d96d4e06f..1d039af99f5 100644 --- a/security/keys/key.c +++ b/security/keys/key.c | |||
@@ -412,8 +412,7 @@ EXPORT_SYMBOL(key_payload_reserve); | |||
412 | * key_construction_mutex. | 412 | * key_construction_mutex. |
413 | */ | 413 | */ |
414 | static int __key_instantiate_and_link(struct key *key, | 414 | static int __key_instantiate_and_link(struct key *key, |
415 | const void *data, | 415 | struct key_preparsed_payload *prep, |
416 | size_t datalen, | ||
417 | struct key *keyring, | 416 | struct key *keyring, |
418 | struct key *authkey, | 417 | struct key *authkey, |
419 | unsigned long *_prealloc) | 418 | unsigned long *_prealloc) |
@@ -431,7 +430,7 @@ static int __key_instantiate_and_link(struct key *key, | |||
431 | /* can't instantiate twice */ | 430 | /* can't instantiate twice */ |
432 | if (!test_bit(KEY_FLAG_INSTANTIATED, &key->flags)) { | 431 | if (!test_bit(KEY_FLAG_INSTANTIATED, &key->flags)) { |
433 | /* instantiate the key */ | 432 | /* instantiate the key */ |
434 | ret = key->type->instantiate(key, data, datalen); | 433 | ret = key->type->instantiate(key, prep); |
435 | 434 | ||
436 | if (ret == 0) { | 435 | if (ret == 0) { |
437 | /* mark the key as being instantiated */ | 436 | /* mark the key as being instantiated */ |
@@ -482,22 +481,37 @@ int key_instantiate_and_link(struct key *key, | |||
482 | struct key *keyring, | 481 | struct key *keyring, |
483 | struct key *authkey) | 482 | struct key *authkey) |
484 | { | 483 | { |
484 | struct key_preparsed_payload prep; | ||
485 | unsigned long prealloc; | 485 | unsigned long prealloc; |
486 | int ret; | 486 | int ret; |
487 | 487 | ||
488 | memset(&prep, 0, sizeof(prep)); | ||
489 | prep.data = data; | ||
490 | prep.datalen = datalen; | ||
491 | prep.quotalen = key->type->def_datalen; | ||
492 | if (key->type->preparse) { | ||
493 | ret = key->type->preparse(&prep); | ||
494 | if (ret < 0) | ||
495 | goto error; | ||
496 | } | ||
497 | |||
488 | if (keyring) { | 498 | if (keyring) { |
489 | ret = __key_link_begin(keyring, key->type, key->description, | 499 | ret = __key_link_begin(keyring, key->type, key->description, |
490 | &prealloc); | 500 | &prealloc); |
491 | if (ret < 0) | 501 | if (ret < 0) |
492 | return ret; | 502 | goto error_free_preparse; |
493 | } | 503 | } |
494 | 504 | ||
495 | ret = __key_instantiate_and_link(key, data, datalen, keyring, authkey, | 505 | ret = __key_instantiate_and_link(key, &prep, keyring, authkey, |
496 | &prealloc); | 506 | &prealloc); |
497 | 507 | ||
498 | if (keyring) | 508 | if (keyring) |
499 | __key_link_end(keyring, key->type, prealloc); | 509 | __key_link_end(keyring, key->type, prealloc); |
500 | 510 | ||
511 | error_free_preparse: | ||
512 | if (key->type->preparse) | ||
513 | key->type->free_preparse(&prep); | ||
514 | error: | ||
501 | return ret; | 515 | return ret; |
502 | } | 516 | } |
503 | 517 | ||
@@ -706,7 +720,7 @@ void key_type_put(struct key_type *ktype) | |||
706 | * if we get an error. | 720 | * if we get an error. |
707 | */ | 721 | */ |
708 | static inline key_ref_t __key_update(key_ref_t key_ref, | 722 | static inline key_ref_t __key_update(key_ref_t key_ref, |
709 | const void *payload, size_t plen) | 723 | struct key_preparsed_payload *prep) |
710 | { | 724 | { |
711 | struct key *key = key_ref_to_ptr(key_ref); | 725 | struct key *key = key_ref_to_ptr(key_ref); |
712 | int ret; | 726 | int ret; |
@@ -722,7 +736,7 @@ static inline key_ref_t __key_update(key_ref_t key_ref, | |||
722 | 736 | ||
723 | down_write(&key->sem); | 737 | down_write(&key->sem); |
724 | 738 | ||
725 | ret = key->type->update(key, payload, plen); | 739 | ret = key->type->update(key, prep); |
726 | if (ret == 0) | 740 | if (ret == 0) |
727 | /* updating a negative key instantiates it */ | 741 | /* updating a negative key instantiates it */ |
728 | clear_bit(KEY_FLAG_NEGATIVE, &key->flags); | 742 | clear_bit(KEY_FLAG_NEGATIVE, &key->flags); |
@@ -774,6 +788,7 @@ key_ref_t key_create_or_update(key_ref_t keyring_ref, | |||
774 | unsigned long flags) | 788 | unsigned long flags) |
775 | { | 789 | { |
776 | unsigned long prealloc; | 790 | unsigned long prealloc; |
791 | struct key_preparsed_payload prep; | ||
777 | const struct cred *cred = current_cred(); | 792 | const struct cred *cred = current_cred(); |
778 | struct key_type *ktype; | 793 | struct key_type *ktype; |
779 | struct key *keyring, *key = NULL; | 794 | struct key *keyring, *key = NULL; |
@@ -789,8 +804,9 @@ key_ref_t key_create_or_update(key_ref_t keyring_ref, | |||
789 | } | 804 | } |
790 | 805 | ||
791 | key_ref = ERR_PTR(-EINVAL); | 806 | key_ref = ERR_PTR(-EINVAL); |
792 | if (!ktype->match || !ktype->instantiate) | 807 | if (!ktype->match || !ktype->instantiate || |
793 | goto error_2; | 808 | (!description && !ktype->preparse)) |
809 | goto error_put_type; | ||
794 | 810 | ||
795 | keyring = key_ref_to_ptr(keyring_ref); | 811 | keyring = key_ref_to_ptr(keyring_ref); |
796 | 812 | ||
@@ -798,18 +814,37 @@ key_ref_t key_create_or_update(key_ref_t keyring_ref, | |||
798 | 814 | ||
799 | key_ref = ERR_PTR(-ENOTDIR); | 815 | key_ref = ERR_PTR(-ENOTDIR); |
800 | if (keyring->type != &key_type_keyring) | 816 | if (keyring->type != &key_type_keyring) |
801 | goto error_2; | 817 | goto error_put_type; |
818 | |||
819 | memset(&prep, 0, sizeof(prep)); | ||
820 | prep.data = payload; | ||
821 | prep.datalen = plen; | ||
822 | prep.quotalen = ktype->def_datalen; | ||
823 | if (ktype->preparse) { | ||
824 | ret = ktype->preparse(&prep); | ||
825 | if (ret < 0) { | ||
826 | key_ref = ERR_PTR(ret); | ||
827 | goto error_put_type; | ||
828 | } | ||
829 | if (!description) | ||
830 | description = prep.description; | ||
831 | key_ref = ERR_PTR(-EINVAL); | ||
832 | if (!description) | ||
833 | goto error_free_prep; | ||
834 | } | ||
802 | 835 | ||
803 | ret = __key_link_begin(keyring, ktype, description, &prealloc); | 836 | ret = __key_link_begin(keyring, ktype, description, &prealloc); |
804 | if (ret < 0) | 837 | if (ret < 0) { |
805 | goto error_2; | 838 | key_ref = ERR_PTR(ret); |
839 | goto error_free_prep; | ||
840 | } | ||
806 | 841 | ||
807 | /* if we're going to allocate a new key, we're going to have | 842 | /* if we're going to allocate a new key, we're going to have |
808 | * to modify the keyring */ | 843 | * to modify the keyring */ |
809 | ret = key_permission(keyring_ref, KEY_WRITE); | 844 | ret = key_permission(keyring_ref, KEY_WRITE); |
810 | if (ret < 0) { | 845 | if (ret < 0) { |
811 | key_ref = ERR_PTR(ret); | 846 | key_ref = ERR_PTR(ret); |
812 | goto error_3; | 847 | goto error_link_end; |
813 | } | 848 | } |
814 | 849 | ||
815 | /* if it's possible to update this type of key, search for an existing | 850 | /* if it's possible to update this type of key, search for an existing |
@@ -840,25 +875,27 @@ key_ref_t key_create_or_update(key_ref_t keyring_ref, | |||
840 | perm, flags); | 875 | perm, flags); |
841 | if (IS_ERR(key)) { | 876 | if (IS_ERR(key)) { |
842 | key_ref = ERR_CAST(key); | 877 | key_ref = ERR_CAST(key); |
843 | goto error_3; | 878 | goto error_link_end; |
844 | } | 879 | } |
845 | 880 | ||
846 | /* instantiate it and link it into the target keyring */ | 881 | /* instantiate it and link it into the target keyring */ |
847 | ret = __key_instantiate_and_link(key, payload, plen, keyring, NULL, | 882 | ret = __key_instantiate_and_link(key, &prep, keyring, NULL, &prealloc); |
848 | &prealloc); | ||
849 | if (ret < 0) { | 883 | if (ret < 0) { |
850 | key_put(key); | 884 | key_put(key); |
851 | key_ref = ERR_PTR(ret); | 885 | key_ref = ERR_PTR(ret); |
852 | goto error_3; | 886 | goto error_link_end; |
853 | } | 887 | } |
854 | 888 | ||
855 | key_ref = make_key_ref(key, is_key_possessed(keyring_ref)); | 889 | key_ref = make_key_ref(key, is_key_possessed(keyring_ref)); |
856 | 890 | ||
857 | error_3: | 891 | error_link_end: |
858 | __key_link_end(keyring, ktype, prealloc); | 892 | __key_link_end(keyring, ktype, prealloc); |
859 | error_2: | 893 | error_free_prep: |
894 | if (ktype->preparse) | ||
895 | ktype->free_preparse(&prep); | ||
896 | error_put_type: | ||
860 | key_type_put(ktype); | 897 | key_type_put(ktype); |
861 | error: | 898 | error: |
862 | return key_ref; | 899 | return key_ref; |
863 | 900 | ||
864 | found_matching_key: | 901 | found_matching_key: |
@@ -866,10 +903,9 @@ key_ref_t key_create_or_update(key_ref_t keyring_ref, | |||
866 | * - we can drop the locks first as we have the key pinned | 903 | * - we can drop the locks first as we have the key pinned |
867 | */ | 904 | */ |
868 | __key_link_end(keyring, ktype, prealloc); | 905 | __key_link_end(keyring, ktype, prealloc); |
869 | key_type_put(ktype); | ||
870 | 906 | ||
871 | key_ref = __key_update(key_ref, payload, plen); | 907 | key_ref = __key_update(key_ref, &prep); |
872 | goto error; | 908 | goto error_free_prep; |
873 | } | 909 | } |
874 | EXPORT_SYMBOL(key_create_or_update); | 910 | EXPORT_SYMBOL(key_create_or_update); |
875 | 911 | ||
@@ -888,6 +924,7 @@ EXPORT_SYMBOL(key_create_or_update); | |||
888 | */ | 924 | */ |
889 | int key_update(key_ref_t key_ref, const void *payload, size_t plen) | 925 | int key_update(key_ref_t key_ref, const void *payload, size_t plen) |
890 | { | 926 | { |
927 | struct key_preparsed_payload prep; | ||
891 | struct key *key = key_ref_to_ptr(key_ref); | 928 | struct key *key = key_ref_to_ptr(key_ref); |
892 | int ret; | 929 | int ret; |
893 | 930 | ||
@@ -900,18 +937,31 @@ int key_update(key_ref_t key_ref, const void *payload, size_t plen) | |||
900 | 937 | ||
901 | /* attempt to update it if supported */ | 938 | /* attempt to update it if supported */ |
902 | ret = -EOPNOTSUPP; | 939 | ret = -EOPNOTSUPP; |
903 | if (key->type->update) { | 940 | if (!key->type->update) |
904 | down_write(&key->sem); | 941 | goto error; |
905 | |||
906 | ret = key->type->update(key, payload, plen); | ||
907 | if (ret == 0) | ||
908 | /* updating a negative key instantiates it */ | ||
909 | clear_bit(KEY_FLAG_NEGATIVE, &key->flags); | ||
910 | 942 | ||
911 | up_write(&key->sem); | 943 | memset(&prep, 0, sizeof(prep)); |
944 | prep.data = payload; | ||
945 | prep.datalen = plen; | ||
946 | prep.quotalen = key->type->def_datalen; | ||
947 | if (key->type->preparse) { | ||
948 | ret = key->type->preparse(&prep); | ||
949 | if (ret < 0) | ||
950 | goto error; | ||
912 | } | 951 | } |
913 | 952 | ||
914 | error: | 953 | down_write(&key->sem); |
954 | |||
955 | ret = key->type->update(key, &prep); | ||
956 | if (ret == 0) | ||
957 | /* updating a negative key instantiates it */ | ||
958 | clear_bit(KEY_FLAG_NEGATIVE, &key->flags); | ||
959 | |||
960 | up_write(&key->sem); | ||
961 | |||
962 | if (key->type->preparse) | ||
963 | key->type->free_preparse(&prep); | ||
964 | error: | ||
915 | return ret; | 965 | return ret; |
916 | } | 966 | } |
917 | EXPORT_SYMBOL(key_update); | 967 | EXPORT_SYMBOL(key_update); |
diff --git a/security/keys/keyctl.c b/security/keys/keyctl.c index 3364fbf4680..505d40be196 100644 --- a/security/keys/keyctl.c +++ b/security/keys/keyctl.c | |||
@@ -46,6 +46,9 @@ static int key_get_type_from_user(char *type, | |||
46 | * Extract the description of a new key from userspace and either add it as a | 46 | * Extract the description of a new key from userspace and either add it as a |
47 | * new key to the specified keyring or update a matching key in that keyring. | 47 | * new key to the specified keyring or update a matching key in that keyring. |
48 | * | 48 | * |
49 | * If the description is NULL or an empty string, the key type is asked to | ||
50 | * generate one from the payload. | ||
51 | * | ||
49 | * The keyring must be writable so that we can attach the key to it. | 52 | * The keyring must be writable so that we can attach the key to it. |
50 | * | 53 | * |
51 | * If successful, the new key's serial number is returned, otherwise an error | 54 | * If successful, the new key's serial number is returned, otherwise an error |
@@ -72,10 +75,17 @@ SYSCALL_DEFINE5(add_key, const char __user *, _type, | |||
72 | if (ret < 0) | 75 | if (ret < 0) |
73 | goto error; | 76 | goto error; |
74 | 77 | ||
75 | description = strndup_user(_description, PAGE_SIZE); | 78 | description = NULL; |
76 | if (IS_ERR(description)) { | 79 | if (_description) { |
77 | ret = PTR_ERR(description); | 80 | description = strndup_user(_description, PAGE_SIZE); |
78 | goto error; | 81 | if (IS_ERR(description)) { |
82 | ret = PTR_ERR(description); | ||
83 | goto error; | ||
84 | } | ||
85 | if (!*description) { | ||
86 | kfree(description); | ||
87 | description = NULL; | ||
88 | } | ||
79 | } | 89 | } |
80 | 90 | ||
81 | /* pull the payload in if one was supplied */ | 91 | /* pull the payload in if one was supplied */ |
diff --git a/security/keys/keyring.c b/security/keys/keyring.c index 81e7852d281..f04d8cf81f3 100644 --- a/security/keys/keyring.c +++ b/security/keys/keyring.c | |||
@@ -66,7 +66,7 @@ static inline unsigned keyring_hash(const char *desc) | |||
66 | * operations. | 66 | * operations. |
67 | */ | 67 | */ |
68 | static int keyring_instantiate(struct key *keyring, | 68 | static int keyring_instantiate(struct key *keyring, |
69 | const void *data, size_t datalen); | 69 | struct key_preparsed_payload *prep); |
70 | static int keyring_match(const struct key *keyring, const void *criterion); | 70 | static int keyring_match(const struct key *keyring, const void *criterion); |
71 | static void keyring_revoke(struct key *keyring); | 71 | static void keyring_revoke(struct key *keyring); |
72 | static void keyring_destroy(struct key *keyring); | 72 | static void keyring_destroy(struct key *keyring); |
@@ -121,12 +121,12 @@ static void keyring_publish_name(struct key *keyring) | |||
121 | * Returns 0 on success, -EINVAL if given any data. | 121 | * Returns 0 on success, -EINVAL if given any data. |
122 | */ | 122 | */ |
123 | static int keyring_instantiate(struct key *keyring, | 123 | static int keyring_instantiate(struct key *keyring, |
124 | const void *data, size_t datalen) | 124 | struct key_preparsed_payload *prep) |
125 | { | 125 | { |
126 | int ret; | 126 | int ret; |
127 | 127 | ||
128 | ret = -EINVAL; | 128 | ret = -EINVAL; |
129 | if (datalen == 0) { | 129 | if (prep->datalen == 0) { |
130 | /* make the keyring available by name if it has one */ | 130 | /* make the keyring available by name if it has one */ |
131 | keyring_publish_name(keyring); | 131 | keyring_publish_name(keyring); |
132 | ret = 0; | 132 | ret = 0; |
diff --git a/security/keys/request_key_auth.c b/security/keys/request_key_auth.c index 60d4e3f5e4b..85730d5a5a5 100644 --- a/security/keys/request_key_auth.c +++ b/security/keys/request_key_auth.c | |||
@@ -19,7 +19,8 @@ | |||
19 | #include <asm/uaccess.h> | 19 | #include <asm/uaccess.h> |
20 | #include "internal.h" | 20 | #include "internal.h" |
21 | 21 | ||
22 | static int request_key_auth_instantiate(struct key *, const void *, size_t); | 22 | static int request_key_auth_instantiate(struct key *, |
23 | struct key_preparsed_payload *); | ||
23 | static void request_key_auth_describe(const struct key *, struct seq_file *); | 24 | static void request_key_auth_describe(const struct key *, struct seq_file *); |
24 | static void request_key_auth_revoke(struct key *); | 25 | static void request_key_auth_revoke(struct key *); |
25 | static void request_key_auth_destroy(struct key *); | 26 | static void request_key_auth_destroy(struct key *); |
@@ -42,10 +43,9 @@ struct key_type key_type_request_key_auth = { | |||
42 | * Instantiate a request-key authorisation key. | 43 | * Instantiate a request-key authorisation key. |
43 | */ | 44 | */ |
44 | static int request_key_auth_instantiate(struct key *key, | 45 | static int request_key_auth_instantiate(struct key *key, |
45 | const void *data, | 46 | struct key_preparsed_payload *prep) |
46 | size_t datalen) | ||
47 | { | 47 | { |
48 | key->payload.data = (struct request_key_auth *) data; | 48 | key->payload.data = (struct request_key_auth *)prep->data; |
49 | return 0; | 49 | return 0; |
50 | } | 50 | } |
51 | 51 | ||
diff --git a/security/keys/trusted.c b/security/keys/trusted.c index 2d5d041f204..42036c7a085 100644 --- a/security/keys/trusted.c +++ b/security/keys/trusted.c | |||
@@ -927,22 +927,23 @@ static struct trusted_key_payload *trusted_payload_alloc(struct key *key) | |||
927 | * | 927 | * |
928 | * On success, return 0. Otherwise return errno. | 928 | * On success, return 0. Otherwise return errno. |
929 | */ | 929 | */ |
930 | static int trusted_instantiate(struct key *key, const void *data, | 930 | static int trusted_instantiate(struct key *key, |
931 | size_t datalen) | 931 | struct key_preparsed_payload *prep) |
932 | { | 932 | { |
933 | struct trusted_key_payload *payload = NULL; | 933 | struct trusted_key_payload *payload = NULL; |
934 | struct trusted_key_options *options = NULL; | 934 | struct trusted_key_options *options = NULL; |
935 | size_t datalen = prep->datalen; | ||
935 | char *datablob; | 936 | char *datablob; |
936 | int ret = 0; | 937 | int ret = 0; |
937 | int key_cmd; | 938 | int key_cmd; |
938 | 939 | ||
939 | if (datalen <= 0 || datalen > 32767 || !data) | 940 | if (datalen <= 0 || datalen > 32767 || !prep->data) |
940 | return -EINVAL; | 941 | return -EINVAL; |
941 | 942 | ||
942 | datablob = kmalloc(datalen + 1, GFP_KERNEL); | 943 | datablob = kmalloc(datalen + 1, GFP_KERNEL); |
943 | if (!datablob) | 944 | if (!datablob) |
944 | return -ENOMEM; | 945 | return -ENOMEM; |
945 | memcpy(datablob, data, datalen); | 946 | memcpy(datablob, prep->data, datalen); |
946 | datablob[datalen] = '\0'; | 947 | datablob[datalen] = '\0'; |
947 | 948 | ||
948 | options = trusted_options_alloc(); | 949 | options = trusted_options_alloc(); |
@@ -1011,17 +1012,18 @@ static void trusted_rcu_free(struct rcu_head *rcu) | |||
1011 | /* | 1012 | /* |
1012 | * trusted_update - reseal an existing key with new PCR values | 1013 | * trusted_update - reseal an existing key with new PCR values |
1013 | */ | 1014 | */ |
1014 | static int trusted_update(struct key *key, const void *data, size_t datalen) | 1015 | static int trusted_update(struct key *key, struct key_preparsed_payload *prep) |
1015 | { | 1016 | { |
1016 | struct trusted_key_payload *p = key->payload.data; | 1017 | struct trusted_key_payload *p = key->payload.data; |
1017 | struct trusted_key_payload *new_p; | 1018 | struct trusted_key_payload *new_p; |
1018 | struct trusted_key_options *new_o; | 1019 | struct trusted_key_options *new_o; |
1020 | size_t datalen = prep->datalen; | ||
1019 | char *datablob; | 1021 | char *datablob; |
1020 | int ret = 0; | 1022 | int ret = 0; |
1021 | 1023 | ||
1022 | if (!p->migratable) | 1024 | if (!p->migratable) |
1023 | return -EPERM; | 1025 | return -EPERM; |
1024 | if (datalen <= 0 || datalen > 32767 || !data) | 1026 | if (datalen <= 0 || datalen > 32767 || !prep->data) |
1025 | return -EINVAL; | 1027 | return -EINVAL; |
1026 | 1028 | ||
1027 | datablob = kmalloc(datalen + 1, GFP_KERNEL); | 1029 | datablob = kmalloc(datalen + 1, GFP_KERNEL); |
@@ -1038,7 +1040,7 @@ static int trusted_update(struct key *key, const void *data, size_t datalen) | |||
1038 | goto out; | 1040 | goto out; |
1039 | } | 1041 | } |
1040 | 1042 | ||
1041 | memcpy(datablob, data, datalen); | 1043 | memcpy(datablob, prep->data, datalen); |
1042 | datablob[datalen] = '\0'; | 1044 | datablob[datalen] = '\0'; |
1043 | ret = datablob_parse(datablob, new_p, new_o); | 1045 | ret = datablob_parse(datablob, new_p, new_o); |
1044 | if (ret != Opt_update) { | 1046 | if (ret != Opt_update) { |
diff --git a/security/keys/user_defined.c b/security/keys/user_defined.c index c7660a25a3e..55dc8893918 100644 --- a/security/keys/user_defined.c +++ b/security/keys/user_defined.c | |||
@@ -58,13 +58,14 @@ EXPORT_SYMBOL_GPL(key_type_logon); | |||
58 | /* | 58 | /* |
59 | * instantiate a user defined key | 59 | * instantiate a user defined key |
60 | */ | 60 | */ |
61 | int user_instantiate(struct key *key, const void *data, size_t datalen) | 61 | int user_instantiate(struct key *key, struct key_preparsed_payload *prep) |
62 | { | 62 | { |
63 | struct user_key_payload *upayload; | 63 | struct user_key_payload *upayload; |
64 | size_t datalen = prep->datalen; | ||
64 | int ret; | 65 | int ret; |
65 | 66 | ||
66 | ret = -EINVAL; | 67 | ret = -EINVAL; |
67 | if (datalen <= 0 || datalen > 32767 || !data) | 68 | if (datalen <= 0 || datalen > 32767 || !prep->data) |
68 | goto error; | 69 | goto error; |
69 | 70 | ||
70 | ret = key_payload_reserve(key, datalen); | 71 | ret = key_payload_reserve(key, datalen); |
@@ -78,7 +79,7 @@ int user_instantiate(struct key *key, const void *data, size_t datalen) | |||
78 | 79 | ||
79 | /* attach the data */ | 80 | /* attach the data */ |
80 | upayload->datalen = datalen; | 81 | upayload->datalen = datalen; |
81 | memcpy(upayload->data, data, datalen); | 82 | memcpy(upayload->data, prep->data, datalen); |
82 | rcu_assign_keypointer(key, upayload); | 83 | rcu_assign_keypointer(key, upayload); |
83 | ret = 0; | 84 | ret = 0; |
84 | 85 | ||
@@ -92,13 +93,14 @@ EXPORT_SYMBOL_GPL(user_instantiate); | |||
92 | * update a user defined key | 93 | * update a user defined key |
93 | * - the key's semaphore is write-locked | 94 | * - the key's semaphore is write-locked |
94 | */ | 95 | */ |
95 | int user_update(struct key *key, const void *data, size_t datalen) | 96 | int user_update(struct key *key, struct key_preparsed_payload *prep) |
96 | { | 97 | { |
97 | struct user_key_payload *upayload, *zap; | 98 | struct user_key_payload *upayload, *zap; |
99 | size_t datalen = prep->datalen; | ||
98 | int ret; | 100 | int ret; |
99 | 101 | ||
100 | ret = -EINVAL; | 102 | ret = -EINVAL; |
101 | if (datalen <= 0 || datalen > 32767 || !data) | 103 | if (datalen <= 0 || datalen > 32767 || !prep->data) |
102 | goto error; | 104 | goto error; |
103 | 105 | ||
104 | /* construct a replacement payload */ | 106 | /* construct a replacement payload */ |
@@ -108,7 +110,7 @@ int user_update(struct key *key, const void *data, size_t datalen) | |||
108 | goto error; | 110 | goto error; |
109 | 111 | ||
110 | upayload->datalen = datalen; | 112 | upayload->datalen = datalen; |
111 | memcpy(upayload->data, data, datalen); | 113 | memcpy(upayload->data, prep->data, datalen); |
112 | 114 | ||
113 | /* check the quota and attach the new data */ | 115 | /* check the quota and attach the new data */ |
114 | zap = upayload; | 116 | zap = upayload; |