diff options
-rw-r--r-- | block/Kconfig | 23 | ||||
-rw-r--r-- | fs/ext4/super.c | 8 | ||||
-rw-r--r-- | include/linux/types.h | 11 |
3 files changed, 12 insertions, 30 deletions
diff --git a/block/Kconfig b/block/Kconfig index 290b219fad9..ac0956f7778 100644 --- a/block/Kconfig +++ b/block/Kconfig | |||
@@ -24,21 +24,17 @@ menuconfig BLOCK | |||
24 | if BLOCK | 24 | if BLOCK |
25 | 25 | ||
26 | config LBD | 26 | config LBD |
27 | bool "Support for Large Block Devices" | 27 | bool "Support for large block devices and files" |
28 | depends on !64BIT | 28 | depends on !64BIT |
29 | help | 29 | help |
30 | Enable block devices of size 2TB and larger. | 30 | Enable block devices or files of size 2TB and larger. |
31 | 31 | ||
32 | This option is required to support the full capacity of large | 32 | This option is required to support the full capacity of large |
33 | (2TB+) block devices, including RAID, disk, Network Block Device, | 33 | (2TB+) block devices, including RAID, disk, Network Block Device, |
34 | Logical Volume Manager (LVM) and loopback. | 34 | Logical Volume Manager (LVM) and loopback. |
35 | 35 | ||
36 | For example, RAID devices are frequently bigger than the capacity | 36 | This option also enables support for single files larger than |
37 | of the largest individual hard drive. | 37 | 2TB. |
38 | |||
39 | This option is not required if you have individual disk drives | ||
40 | which total 2TB+ and you are not aggregating the capacity into | ||
41 | a large block device (e.g. using RAID or LVM). | ||
42 | 38 | ||
43 | If unsure, say N. | 39 | If unsure, say N. |
44 | 40 | ||
@@ -58,15 +54,6 @@ config BLK_DEV_IO_TRACE | |||
58 | 54 | ||
59 | If unsure, say N. | 55 | If unsure, say N. |
60 | 56 | ||
61 | config LSF | ||
62 | bool "Support for Large Single Files" | ||
63 | depends on !64BIT | ||
64 | help | ||
65 | Say Y here if you want to be able to handle very large files (2TB | ||
66 | and larger), otherwise say N. | ||
67 | |||
68 | If unsure, say Y. | ||
69 | |||
70 | config BLK_DEV_BSG | 57 | config BLK_DEV_BSG |
71 | bool "Block layer SG support v4 (EXPERIMENTAL)" | 58 | bool "Block layer SG support v4 (EXPERIMENTAL)" |
72 | depends on EXPERIMENTAL | 59 | depends on EXPERIMENTAL |
diff --git a/fs/ext4/super.c b/fs/ext4/super.c index e4a241c65db..04158ad74db 100644 --- a/fs/ext4/super.c +++ b/fs/ext4/super.c | |||
@@ -1721,7 +1721,7 @@ static loff_t ext4_max_size(int blkbits, int has_huge_files) | |||
1721 | /* small i_blocks in vfs inode? */ | 1721 | /* small i_blocks in vfs inode? */ |
1722 | if (!has_huge_files || sizeof(blkcnt_t) < sizeof(u64)) { | 1722 | if (!has_huge_files || sizeof(blkcnt_t) < sizeof(u64)) { |
1723 | /* | 1723 | /* |
1724 | * CONFIG_LSF is not enabled implies the inode | 1724 | * CONFIG_LBD is not enabled implies the inode |
1725 | * i_block represent total blocks in 512 bytes | 1725 | * i_block represent total blocks in 512 bytes |
1726 | * 32 == size of vfs inode i_blocks * 8 | 1726 | * 32 == size of vfs inode i_blocks * 8 |
1727 | */ | 1727 | */ |
@@ -1764,7 +1764,7 @@ static loff_t ext4_max_bitmap_size(int bits, int has_huge_files) | |||
1764 | 1764 | ||
1765 | if (!has_huge_files || sizeof(blkcnt_t) < sizeof(u64)) { | 1765 | if (!has_huge_files || sizeof(blkcnt_t) < sizeof(u64)) { |
1766 | /* | 1766 | /* |
1767 | * !has_huge_files or CONFIG_LSF is not enabled | 1767 | * !has_huge_files or CONFIG_LBD is not enabled |
1768 | * implies the inode i_block represent total blocks in | 1768 | * implies the inode i_block represent total blocks in |
1769 | * 512 bytes 32 == size of vfs inode i_blocks * 8 | 1769 | * 512 bytes 32 == size of vfs inode i_blocks * 8 |
1770 | */ | 1770 | */ |
@@ -2021,13 +2021,13 @@ static int ext4_fill_super(struct super_block *sb, void *data, int silent) | |||
2021 | if (has_huge_files) { | 2021 | if (has_huge_files) { |
2022 | /* | 2022 | /* |
2023 | * Large file size enabled file system can only be | 2023 | * Large file size enabled file system can only be |
2024 | * mount if kernel is build with CONFIG_LSF | 2024 | * mount if kernel is build with CONFIG_LBD |
2025 | */ | 2025 | */ |
2026 | if (sizeof(root->i_blocks) < sizeof(u64) && | 2026 | if (sizeof(root->i_blocks) < sizeof(u64) && |
2027 | !(sb->s_flags & MS_RDONLY)) { | 2027 | !(sb->s_flags & MS_RDONLY)) { |
2028 | printk(KERN_ERR "EXT4-fs: %s: Filesystem with huge " | 2028 | printk(KERN_ERR "EXT4-fs: %s: Filesystem with huge " |
2029 | "files cannot be mounted read-write " | 2029 | "files cannot be mounted read-write " |
2030 | "without CONFIG_LSF.\n", sb->s_id); | 2030 | "without CONFIG_LBD.\n", sb->s_id); |
2031 | goto failed_mount; | 2031 | goto failed_mount; |
2032 | } | 2032 | } |
2033 | } | 2033 | } |
diff --git a/include/linux/types.h b/include/linux/types.h index 1d98330b1f2..121f349cb7e 100644 --- a/include/linux/types.h +++ b/include/linux/types.h | |||
@@ -135,19 +135,14 @@ typedef __s64 int64_t; | |||
135 | * | 135 | * |
136 | * Linux always considers sectors to be 512 bytes long independently | 136 | * Linux always considers sectors to be 512 bytes long independently |
137 | * of the devices real block size. | 137 | * of the devices real block size. |
138 | * | ||
139 | * blkcnt_t is the type of the inode's block count. | ||
138 | */ | 140 | */ |
139 | #ifdef CONFIG_LBD | 141 | #ifdef CONFIG_LBD |
140 | typedef u64 sector_t; | 142 | typedef u64 sector_t; |
141 | #else | ||
142 | typedef unsigned long sector_t; | ||
143 | #endif | ||
144 | |||
145 | /* | ||
146 | * The type of the inode's block count. | ||
147 | */ | ||
148 | #ifdef CONFIG_LSF | ||
149 | typedef u64 blkcnt_t; | 143 | typedef u64 blkcnt_t; |
150 | #else | 144 | #else |
145 | typedef unsigned long sector_t; | ||
151 | typedef unsigned long blkcnt_t; | 146 | typedef unsigned long blkcnt_t; |
152 | #endif | 147 | #endif |
153 | 148 | ||