diff options
Diffstat (limited to 'drivers/net/wireless/bcm4329/bcmsdh_sdmmc.c')
-rw-r--r-- | drivers/net/wireless/bcm4329/bcmsdh_sdmmc.c | 1304 |
1 files changed, 1304 insertions, 0 deletions
diff --git a/drivers/net/wireless/bcm4329/bcmsdh_sdmmc.c b/drivers/net/wireless/bcm4329/bcmsdh_sdmmc.c new file mode 100644 index 00000000000..031367b8f18 --- /dev/null +++ b/drivers/net/wireless/bcm4329/bcmsdh_sdmmc.c | |||
@@ -0,0 +1,1304 @@ | |||
1 | /* | ||
2 | * BCMSDH Function Driver for the native SDIO/MMC driver in the Linux Kernel | ||
3 | * | ||
4 | * Copyright (C) 1999-2010, Broadcom Corporation | ||
5 | * | ||
6 | * Unless you and Broadcom execute a separate written software license | ||
7 | * agreement governing use of this software, this software is licensed to you | ||
8 | * under the terms of the GNU General Public License version 2 (the "GPL"), | ||
9 | * available at http://www.broadcom.com/licenses/GPLv2.php, with the | ||
10 | * following added to such license: | ||
11 | * | ||
12 | * As a special exception, the copyright holders of this software give you | ||
13 | * permission to link this software with independent modules, and to copy and | ||
14 | * distribute the resulting executable under terms of your choice, provided that | ||
15 | * you also meet, for each linked independent module, the terms and conditions of | ||
16 | * the license of that module. An independent module is a module which is not | ||
17 | * derived from this software. The special exception does not apply to any | ||
18 | * modifications of the software. | ||
19 | * | ||
20 | * Notwithstanding the above, under no circumstances may you combine this | ||
21 | * software in any way with any other Broadcom software provided under a license | ||
22 | * other than the GPL, without Broadcom's express prior written consent. | ||
23 | * | ||
24 | * $Id: bcmsdh_sdmmc.c,v 1.1.2.5.6.30.4.1 2010/09/02 23:12:21 Exp $ | ||
25 | */ | ||
26 | #include <typedefs.h> | ||
27 | |||
28 | #include <bcmdevs.h> | ||
29 | #include <bcmendian.h> | ||
30 | #include <bcmutils.h> | ||
31 | #include <osl.h> | ||
32 | #include <sdio.h> /* SDIO Device and Protocol Specs */ | ||
33 | #include <sdioh.h> /* SDIO Host Controller Specification */ | ||
34 | #include <bcmsdbus.h> /* bcmsdh to/from specific controller APIs */ | ||
35 | #include <sdiovar.h> /* ioctl/iovars */ | ||
36 | |||
37 | #include <linux/mmc/core.h> | ||
38 | #include <linux/mmc/sdio_func.h> | ||
39 | #include <linux/mmc/sdio_ids.h> | ||
40 | |||
41 | #include <dngl_stats.h> | ||
42 | #include <dhd.h> | ||
43 | |||
44 | #if (LINUX_VERSION_CODE >= KERNEL_VERSION(2, 6, 27)) && defined(CONFIG_PM_SLEEP) | ||
45 | #include <linux/suspend.h> | ||
46 | extern volatile bool dhd_mmc_suspend; | ||
47 | #endif | ||
48 | #include "bcmsdh_sdmmc.h" | ||
49 | |||
50 | #ifndef BCMSDH_MODULE | ||
51 | extern int sdio_function_init(void); | ||
52 | extern void sdio_function_cleanup(void); | ||
53 | #endif /* BCMSDH_MODULE */ | ||
54 | |||
55 | #if !defined(OOB_INTR_ONLY) | ||
56 | static void IRQHandler(struct sdio_func *func); | ||
57 | static void IRQHandlerF2(struct sdio_func *func); | ||
58 | #endif /* !defined(OOB_INTR_ONLY) */ | ||
59 | static int sdioh_sdmmc_get_cisaddr(sdioh_info_t *sd, uint32 regaddr); | ||
60 | extern int sdio_reset_comm(struct mmc_card *card); | ||
61 | |||
62 | extern PBCMSDH_SDMMC_INSTANCE gInstance; | ||
63 | |||
64 | uint sd_sdmode = SDIOH_MODE_SD4; /* Use SD4 mode by default */ | ||
65 | uint sd_f2_blocksize = 512; /* Default blocksize */ | ||
66 | |||
67 | uint sd_divisor = 2; /* Default 48MHz/2 = 24MHz */ | ||
68 | |||
69 | uint sd_power = 1; /* Default to SD Slot powered ON */ | ||
70 | uint sd_clock = 1; /* Default to SD Clock turned ON */ | ||
71 | uint sd_hiok = FALSE; /* Don't use hi-speed mode by default */ | ||
72 | uint sd_msglevel = 0x01; | ||
73 | uint sd_use_dma = TRUE; | ||
74 | DHD_PM_RESUME_WAIT_INIT(sdioh_request_byte_wait); | ||
75 | DHD_PM_RESUME_WAIT_INIT(sdioh_request_word_wait); | ||
76 | DHD_PM_RESUME_WAIT_INIT(sdioh_request_packet_wait); | ||
77 | DHD_PM_RESUME_WAIT_INIT(sdioh_request_buffer_wait); | ||
78 | |||
79 | #define DMA_ALIGN_MASK 0x03 | ||
80 | |||
81 | int sdioh_sdmmc_card_regread(sdioh_info_t *sd, int func, uint32 regaddr, int regsize, uint32 *data); | ||
82 | |||
83 | static int | ||
84 | sdioh_sdmmc_card_enablefuncs(sdioh_info_t *sd) | ||
85 | { | ||
86 | int err_ret; | ||
87 | uint32 fbraddr; | ||
88 | uint8 func; | ||
89 | |||
90 | sd_trace(("%s\n", __FUNCTION__)); | ||
91 | |||
92 | /* Get the Card's common CIS address */ | ||
93 | sd->com_cis_ptr = sdioh_sdmmc_get_cisaddr(sd, SDIOD_CCCR_CISPTR_0); | ||
94 | sd->func_cis_ptr[0] = sd->com_cis_ptr; | ||
95 | sd_info(("%s: Card's Common CIS Ptr = 0x%x\n", __FUNCTION__, sd->com_cis_ptr)); | ||
96 | |||
97 | /* Get the Card's function CIS (for each function) */ | ||
98 | for (fbraddr = SDIOD_FBR_STARTADDR, func = 1; | ||
99 | func <= sd->num_funcs; func++, fbraddr += SDIOD_FBR_SIZE) { | ||
100 | sd->func_cis_ptr[func] = sdioh_sdmmc_get_cisaddr(sd, SDIOD_FBR_CISPTR_0 + fbraddr); | ||
101 | sd_info(("%s: Function %d CIS Ptr = 0x%x\n", | ||
102 | __FUNCTION__, func, sd->func_cis_ptr[func])); | ||
103 | } | ||
104 | |||
105 | sd->func_cis_ptr[0] = sd->com_cis_ptr; | ||
106 | sd_info(("%s: Card's Common CIS Ptr = 0x%x\n", __FUNCTION__, sd->com_cis_ptr)); | ||
107 | |||
108 | /* Enable Function 1 */ | ||
109 | sdio_claim_host(gInstance->func[1]); | ||
110 | err_ret = sdio_enable_func(gInstance->func[1]); | ||
111 | sdio_release_host(gInstance->func[1]); | ||
112 | if (err_ret) { | ||
113 | sd_err(("bcmsdh_sdmmc: Failed to enable F1 Err: 0x%08x", err_ret)); | ||
114 | } | ||
115 | |||
116 | return FALSE; | ||
117 | } | ||
118 | |||
119 | /* | ||
120 | * Public entry points & extern's | ||
121 | */ | ||
122 | extern sdioh_info_t * | ||
123 | sdioh_attach(osl_t *osh, void *bar0, uint irq) | ||
124 | { | ||
125 | sdioh_info_t *sd; | ||
126 | int err_ret; | ||
127 | |||
128 | sd_trace(("%s\n", __FUNCTION__)); | ||
129 | |||
130 | if (gInstance == NULL) { | ||
131 | sd_err(("%s: SDIO Device not present\n", __FUNCTION__)); | ||
132 | return NULL; | ||
133 | } | ||
134 | |||
135 | if ((sd = (sdioh_info_t *)MALLOC(osh, sizeof(sdioh_info_t))) == NULL) { | ||
136 | sd_err(("sdioh_attach: out of memory, malloced %d bytes\n", MALLOCED(osh))); | ||
137 | return NULL; | ||
138 | } | ||
139 | bzero((char *)sd, sizeof(sdioh_info_t)); | ||
140 | sd->osh = osh; | ||
141 | if (sdioh_sdmmc_osinit(sd) != 0) { | ||
142 | sd_err(("%s:sdioh_sdmmc_osinit() failed\n", __FUNCTION__)); | ||
143 | MFREE(sd->osh, sd, sizeof(sdioh_info_t)); | ||
144 | return NULL; | ||
145 | } | ||
146 | |||
147 | sd->num_funcs = 2; | ||
148 | sd->sd_blockmode = TRUE; | ||
149 | sd->use_client_ints = TRUE; | ||
150 | sd->client_block_size[0] = 64; | ||
151 | |||
152 | gInstance->sd = sd; | ||
153 | |||
154 | /* Claim host controller */ | ||
155 | sdio_claim_host(gInstance->func[1]); | ||
156 | |||
157 | sd->client_block_size[1] = 64; | ||
158 | err_ret = sdio_set_block_size(gInstance->func[1], 64); | ||
159 | if (err_ret) { | ||
160 | sd_err(("bcmsdh_sdmmc: Failed to set F1 blocksize\n")); | ||
161 | } | ||
162 | |||
163 | /* Release host controller F1 */ | ||
164 | sdio_release_host(gInstance->func[1]); | ||
165 | |||
166 | if (gInstance->func[2]) { | ||
167 | /* Claim host controller F2 */ | ||
168 | sdio_claim_host(gInstance->func[2]); | ||
169 | |||
170 | sd->client_block_size[2] = sd_f2_blocksize; | ||
171 | err_ret = sdio_set_block_size(gInstance->func[2], sd_f2_blocksize); | ||
172 | if (err_ret) { | ||
173 | sd_err(("bcmsdh_sdmmc: Failed to set F2 blocksize to %d\n", | ||
174 | sd_f2_blocksize)); | ||
175 | } | ||
176 | |||
177 | /* Release host controller F2 */ | ||
178 | sdio_release_host(gInstance->func[2]); | ||
179 | } | ||
180 | |||
181 | sdioh_sdmmc_card_enablefuncs(sd); | ||
182 | |||
183 | sd_trace(("%s: Done\n", __FUNCTION__)); | ||
184 | return sd; | ||
185 | } | ||
186 | |||
187 | |||
188 | extern SDIOH_API_RC | ||
189 | sdioh_detach(osl_t *osh, sdioh_info_t *sd) | ||
190 | { | ||
191 | sd_trace(("%s\n", __FUNCTION__)); | ||
192 | |||
193 | if (sd) { | ||
194 | |||
195 | /* Disable Function 2 */ | ||
196 | sdio_claim_host(gInstance->func[2]); | ||
197 | sdio_disable_func(gInstance->func[2]); | ||
198 | sdio_release_host(gInstance->func[2]); | ||
199 | |||
200 | /* Disable Function 1 */ | ||
201 | sdio_claim_host(gInstance->func[1]); | ||
202 | sdio_disable_func(gInstance->func[1]); | ||
203 | sdio_release_host(gInstance->func[1]); | ||
204 | |||
205 | /* deregister irq */ | ||
206 | sdioh_sdmmc_osfree(sd); | ||
207 | |||
208 | MFREE(sd->osh, sd, sizeof(sdioh_info_t)); | ||
209 | } | ||
210 | return SDIOH_API_RC_SUCCESS; | ||
211 | } | ||
212 | |||
213 | #if defined(OOB_INTR_ONLY) && defined(HW_OOB) | ||
214 | |||
215 | extern SDIOH_API_RC | ||
216 | sdioh_enable_func_intr(void) | ||
217 | { | ||
218 | uint8 reg; | ||
219 | int err; | ||
220 | |||
221 | if (gInstance->func[0]) { | ||
222 | sdio_claim_host(gInstance->func[0]); | ||
223 | |||
224 | reg = sdio_readb(gInstance->func[0], SDIOD_CCCR_INTEN, &err); | ||
225 | if (err) { | ||
226 | sd_err(("%s: error for read SDIO_CCCR_IENx : 0x%x\n", __FUNCTION__, err)); | ||
227 | sdio_release_host(gInstance->func[0]); | ||
228 | return SDIOH_API_RC_FAIL; | ||
229 | } | ||
230 | |||
231 | /* Enable F1 and F2 interrupts, set master enable */ | ||
232 | reg |= (INTR_CTL_FUNC1_EN | INTR_CTL_FUNC2_EN | INTR_CTL_MASTER_EN); | ||
233 | |||
234 | sdio_writeb(gInstance->func[0], reg, SDIOD_CCCR_INTEN, &err); | ||
235 | sdio_release_host(gInstance->func[0]); | ||
236 | |||
237 | if (err) { | ||
238 | sd_err(("%s: error for write SDIO_CCCR_IENx : 0x%x\n", __FUNCTION__, err)); | ||
239 | return SDIOH_API_RC_FAIL; | ||
240 | } | ||
241 | } | ||
242 | |||
243 | return SDIOH_API_RC_SUCCESS; | ||
244 | } | ||
245 | |||
246 | extern SDIOH_API_RC | ||
247 | sdioh_disable_func_intr(void) | ||
248 | { | ||
249 | uint8 reg; | ||
250 | int err; | ||
251 | |||
252 | if (gInstance->func[0]) { | ||
253 | sdio_claim_host(gInstance->func[0]); | ||
254 | reg = sdio_readb(gInstance->func[0], SDIOD_CCCR_INTEN, &err); | ||
255 | if (err) { | ||
256 | sd_err(("%s: error for read SDIO_CCCR_IENx : 0x%x\n", __FUNCTION__, err)); | ||
257 | sdio_release_host(gInstance->func[0]); | ||
258 | return SDIOH_API_RC_FAIL; | ||
259 | } | ||
260 | |||
261 | reg &= ~(INTR_CTL_FUNC1_EN | INTR_CTL_FUNC2_EN); | ||
262 | /* Disable master interrupt with the last function interrupt */ | ||
263 | if (!(reg & 0xFE)) | ||
264 | reg = 0; | ||
265 | sdio_writeb(gInstance->func[0], reg, SDIOD_CCCR_INTEN, &err); | ||
266 | |||
267 | sdio_release_host(gInstance->func[0]); | ||
268 | if (err) { | ||
269 | sd_err(("%s: error for write SDIO_CCCR_IENx : 0x%x\n", __FUNCTION__, err)); | ||
270 | return SDIOH_API_RC_FAIL; | ||
271 | } | ||
272 | } | ||
273 | return SDIOH_API_RC_SUCCESS; | ||
274 | } | ||
275 | #endif /* defined(OOB_INTR_ONLY) && defined(HW_OOB) */ | ||
276 | |||
277 | /* Configure callback to client when we recieve client interrupt */ | ||
278 | extern SDIOH_API_RC | ||
279 | sdioh_interrupt_register(sdioh_info_t *sd, sdioh_cb_fn_t fn, void *argh) | ||
280 | { | ||
281 | sd_trace(("%s: Entering\n", __FUNCTION__)); | ||
282 | if (fn == NULL) { | ||
283 | sd_err(("%s: interrupt handler is NULL, not registering\n", __FUNCTION__)); | ||
284 | return SDIOH_API_RC_FAIL; | ||
285 | } | ||
286 | #if !defined(OOB_INTR_ONLY) | ||
287 | sd->intr_handler = fn; | ||
288 | sd->intr_handler_arg = argh; | ||
289 | sd->intr_handler_valid = TRUE; | ||
290 | |||
291 | /* register and unmask irq */ | ||
292 | if (gInstance->func[2]) { | ||
293 | sdio_claim_host(gInstance->func[2]); | ||
294 | sdio_claim_irq(gInstance->func[2], IRQHandlerF2); | ||
295 | sdio_release_host(gInstance->func[2]); | ||
296 | } | ||
297 | |||
298 | if (gInstance->func[1]) { | ||
299 | sdio_claim_host(gInstance->func[1]); | ||
300 | sdio_claim_irq(gInstance->func[1], IRQHandler); | ||
301 | sdio_release_host(gInstance->func[1]); | ||
302 | } | ||
303 | #elif defined(HW_OOB) | ||
304 | sdioh_enable_func_intr(); | ||
305 | #endif /* defined(OOB_INTR_ONLY) */ | ||
306 | return SDIOH_API_RC_SUCCESS; | ||
307 | } | ||
308 | |||
309 | extern SDIOH_API_RC | ||
310 | sdioh_interrupt_deregister(sdioh_info_t *sd) | ||
311 | { | ||
312 | sd_trace(("%s: Entering\n", __FUNCTION__)); | ||
313 | |||
314 | #if !defined(OOB_INTR_ONLY) | ||
315 | if (gInstance->func[1]) { | ||
316 | /* register and unmask irq */ | ||
317 | sdio_claim_host(gInstance->func[1]); | ||
318 | sdio_release_irq(gInstance->func[1]); | ||
319 | sdio_release_host(gInstance->func[1]); | ||
320 | } | ||
321 | |||
322 | if (gInstance->func[2]) { | ||
323 | /* Claim host controller F2 */ | ||
324 | sdio_claim_host(gInstance->func[2]); | ||
325 | sdio_release_irq(gInstance->func[2]); | ||
326 | /* Release host controller F2 */ | ||
327 | sdio_release_host(gInstance->func[2]); | ||
328 | } | ||
329 | |||
330 | sd->intr_handler_valid = FALSE; | ||
331 | sd->intr_handler = NULL; | ||
332 | sd->intr_handler_arg = NULL; | ||
333 | #elif defined(HW_OOB) | ||
334 | sdioh_disable_func_intr(); | ||
335 | #endif /* !defined(OOB_INTR_ONLY) */ | ||
336 | return SDIOH_API_RC_SUCCESS; | ||
337 | } | ||
338 | |||
339 | extern SDIOH_API_RC | ||
340 | sdioh_interrupt_query(sdioh_info_t *sd, bool *onoff) | ||
341 | { | ||
342 | sd_trace(("%s: Entering\n", __FUNCTION__)); | ||
343 | *onoff = sd->client_intr_enabled; | ||
344 | return SDIOH_API_RC_SUCCESS; | ||
345 | } | ||
346 | |||
347 | #if defined(DHD_DEBUG) | ||
348 | extern bool | ||
349 | sdioh_interrupt_pending(sdioh_info_t *sd) | ||
350 | { | ||
351 | return (0); | ||
352 | } | ||
353 | #endif | ||
354 | |||
355 | uint | ||
356 | sdioh_query_iofnum(sdioh_info_t *sd) | ||
357 | { | ||
358 | return sd->num_funcs; | ||
359 | } | ||
360 | |||
361 | /* IOVar table */ | ||
362 | enum { | ||
363 | IOV_MSGLEVEL = 1, | ||
364 | IOV_BLOCKMODE, | ||
365 | IOV_BLOCKSIZE, | ||
366 | IOV_DMA, | ||
367 | IOV_USEINTS, | ||
368 | IOV_NUMINTS, | ||
369 | IOV_NUMLOCALINTS, | ||
370 | IOV_HOSTREG, | ||
371 | IOV_DEVREG, | ||
372 | IOV_DIVISOR, | ||
373 | IOV_SDMODE, | ||
374 | IOV_HISPEED, | ||
375 | IOV_HCIREGS, | ||
376 | IOV_POWER, | ||
377 | IOV_CLOCK, | ||
378 | IOV_RXCHAIN | ||
379 | }; | ||
380 | |||
381 | const bcm_iovar_t sdioh_iovars[] = { | ||
382 | {"sd_msglevel", IOV_MSGLEVEL, 0, IOVT_UINT32, 0 }, | ||
383 | {"sd_blockmode", IOV_BLOCKMODE, 0, IOVT_BOOL, 0 }, | ||
384 | {"sd_blocksize", IOV_BLOCKSIZE, 0, IOVT_UINT32, 0 }, /* ((fn << 16) | size) */ | ||
385 | {"sd_dma", IOV_DMA, 0, IOVT_BOOL, 0 }, | ||
386 | {"sd_ints", IOV_USEINTS, 0, IOVT_BOOL, 0 }, | ||
387 | {"sd_numints", IOV_NUMINTS, 0, IOVT_UINT32, 0 }, | ||
388 | {"sd_numlocalints", IOV_NUMLOCALINTS, 0, IOVT_UINT32, 0 }, | ||
389 | {"sd_hostreg", IOV_HOSTREG, 0, IOVT_BUFFER, sizeof(sdreg_t) }, | ||
390 | {"sd_devreg", IOV_DEVREG, 0, IOVT_BUFFER, sizeof(sdreg_t) }, | ||
391 | {"sd_divisor", IOV_DIVISOR, 0, IOVT_UINT32, 0 }, | ||
392 | {"sd_power", IOV_POWER, 0, IOVT_UINT32, 0 }, | ||
393 | {"sd_clock", IOV_CLOCK, 0, IOVT_UINT32, 0 }, | ||
394 | {"sd_mode", IOV_SDMODE, 0, IOVT_UINT32, 100}, | ||
395 | {"sd_highspeed", IOV_HISPEED, 0, IOVT_UINT32, 0 }, | ||
396 | {"sd_rxchain", IOV_RXCHAIN, 0, IOVT_BOOL, 0 }, | ||
397 | {NULL, 0, 0, 0, 0 } | ||
398 | }; | ||
399 | |||
400 | int | ||
401 | sdioh_iovar_op(sdioh_info_t *si, const char *name, | ||
402 | void *params, int plen, void *arg, int len, bool set) | ||
403 | { | ||
404 | const bcm_iovar_t *vi = NULL; | ||
405 | int bcmerror = 0; | ||
406 | int val_size; | ||
407 | int32 int_val = 0; | ||
408 | bool bool_val; | ||
409 | uint32 actionid; | ||
410 | |||
411 | ASSERT(name); | ||
412 | ASSERT(len >= 0); | ||
413 | |||
414 | /* Get must have return space; Set does not take qualifiers */ | ||
415 | ASSERT(set || (arg && len)); | ||
416 | ASSERT(!set || (!params && !plen)); | ||
417 | |||
418 | sd_trace(("%s: Enter (%s %s)\n", __FUNCTION__, (set ? "set" : "get"), name)); | ||
419 | |||
420 | if ((vi = bcm_iovar_lookup(sdioh_iovars, name)) == NULL) { | ||
421 | bcmerror = BCME_UNSUPPORTED; | ||
422 | goto exit; | ||
423 | } | ||
424 | |||
425 | if ((bcmerror = bcm_iovar_lencheck(vi, arg, len, set)) != 0) | ||
426 | goto exit; | ||
427 | |||
428 | /* Set up params so get and set can share the convenience variables */ | ||
429 | if (params == NULL) { | ||
430 | params = arg; | ||
431 | plen = len; | ||
432 | } | ||
433 | |||
434 | if (vi->type == IOVT_VOID) | ||
435 | val_size = 0; | ||
436 | else if (vi->type == IOVT_BUFFER) | ||
437 | val_size = len; | ||
438 | else | ||
439 | val_size = sizeof(int); | ||
440 | |||
441 | if (plen >= (int)sizeof(int_val)) | ||
442 | bcopy(params, &int_val, sizeof(int_val)); | ||
443 | |||
444 | bool_val = (int_val != 0) ? TRUE : FALSE; | ||
445 | |||
446 | actionid = set ? IOV_SVAL(vi->varid) : IOV_GVAL(vi->varid); | ||
447 | switch (actionid) { | ||
448 | case IOV_GVAL(IOV_MSGLEVEL): | ||
449 | int_val = (int32)sd_msglevel; | ||
450 | bcopy(&int_val, arg, val_size); | ||
451 | break; | ||
452 | |||
453 | case IOV_SVAL(IOV_MSGLEVEL): | ||
454 | sd_msglevel = int_val; | ||
455 | break; | ||
456 | |||
457 | case IOV_GVAL(IOV_BLOCKMODE): | ||
458 | int_val = (int32)si->sd_blockmode; | ||
459 | bcopy(&int_val, arg, val_size); | ||
460 | break; | ||
461 | |||
462 | case IOV_SVAL(IOV_BLOCKMODE): | ||
463 | si->sd_blockmode = (bool)int_val; | ||
464 | /* Haven't figured out how to make non-block mode with DMA */ | ||
465 | break; | ||
466 | |||
467 | case IOV_GVAL(IOV_BLOCKSIZE): | ||
468 | if ((uint32)int_val > si->num_funcs) { | ||
469 | bcmerror = BCME_BADARG; | ||
470 | break; | ||
471 | } | ||
472 | int_val = (int32)si->client_block_size[int_val]; | ||
473 | bcopy(&int_val, arg, val_size); | ||
474 | break; | ||
475 | |||
476 | case IOV_SVAL(IOV_BLOCKSIZE): | ||
477 | { | ||
478 | uint func = ((uint32)int_val >> 16); | ||
479 | uint blksize = (uint16)int_val; | ||
480 | uint maxsize; | ||
481 | |||
482 | if (func > si->num_funcs) { | ||
483 | bcmerror = BCME_BADARG; | ||
484 | break; | ||
485 | } | ||
486 | |||
487 | switch (func) { | ||
488 | case 0: maxsize = 32; break; | ||
489 | case 1: maxsize = BLOCK_SIZE_4318; break; | ||
490 | case 2: maxsize = BLOCK_SIZE_4328; break; | ||
491 | default: maxsize = 0; | ||
492 | } | ||
493 | if (blksize > maxsize) { | ||
494 | bcmerror = BCME_BADARG; | ||
495 | break; | ||
496 | } | ||
497 | if (!blksize) { | ||
498 | blksize = maxsize; | ||
499 | } | ||
500 | |||
501 | /* Now set it */ | ||
502 | si->client_block_size[func] = blksize; | ||
503 | |||
504 | break; | ||
505 | } | ||
506 | |||
507 | case IOV_GVAL(IOV_RXCHAIN): | ||
508 | int_val = FALSE; | ||
509 | bcopy(&int_val, arg, val_size); | ||
510 | break; | ||
511 | |||
512 | case IOV_GVAL(IOV_DMA): | ||
513 | int_val = (int32)si->sd_use_dma; | ||
514 | bcopy(&int_val, arg, val_size); | ||
515 | break; | ||
516 | |||
517 | case IOV_SVAL(IOV_DMA): | ||
518 | si->sd_use_dma = (bool)int_val; | ||
519 | break; | ||
520 | |||
521 | case IOV_GVAL(IOV_USEINTS): | ||
522 | int_val = (int32)si->use_client_ints; | ||
523 | bcopy(&int_val, arg, val_size); | ||
524 | break; | ||
525 | |||
526 | case IOV_SVAL(IOV_USEINTS): | ||
527 | si->use_client_ints = (bool)int_val; | ||
528 | if (si->use_client_ints) | ||
529 | si->intmask |= CLIENT_INTR; | ||
530 | else | ||
531 | si->intmask &= ~CLIENT_INTR; | ||
532 | |||
533 | break; | ||
534 | |||
535 | case IOV_GVAL(IOV_DIVISOR): | ||
536 | int_val = (uint32)sd_divisor; | ||
537 | bcopy(&int_val, arg, val_size); | ||
538 | break; | ||
539 | |||
540 | case IOV_SVAL(IOV_DIVISOR): | ||
541 | sd_divisor = int_val; | ||
542 | break; | ||
543 | |||
544 | case IOV_GVAL(IOV_POWER): | ||
545 | int_val = (uint32)sd_power; | ||
546 | bcopy(&int_val, arg, val_size); | ||
547 | break; | ||
548 | |||
549 | case IOV_SVAL(IOV_POWER): | ||
550 | sd_power = int_val; | ||
551 | break; | ||
552 | |||
553 | case IOV_GVAL(IOV_CLOCK): | ||
554 | int_val = (uint32)sd_clock; | ||
555 | bcopy(&int_val, arg, val_size); | ||
556 | break; | ||
557 | |||
558 | case IOV_SVAL(IOV_CLOCK): | ||
559 | sd_clock = int_val; | ||
560 | break; | ||
561 | |||
562 | case IOV_GVAL(IOV_SDMODE): | ||
563 | int_val = (uint32)sd_sdmode; | ||
564 | bcopy(&int_val, arg, val_size); | ||
565 | break; | ||
566 | |||
567 | case IOV_SVAL(IOV_SDMODE): | ||
568 | sd_sdmode = int_val; | ||
569 | break; | ||
570 | |||
571 | case IOV_GVAL(IOV_HISPEED): | ||
572 | int_val = (uint32)sd_hiok; | ||
573 | bcopy(&int_val, arg, val_size); | ||
574 | break; | ||
575 | |||
576 | case IOV_SVAL(IOV_HISPEED): | ||
577 | sd_hiok = int_val; | ||
578 | break; | ||
579 | |||
580 | case IOV_GVAL(IOV_NUMINTS): | ||
581 | int_val = (int32)si->intrcount; | ||
582 | bcopy(&int_val, arg, val_size); | ||
583 | break; | ||
584 | |||
585 | case IOV_GVAL(IOV_NUMLOCALINTS): | ||
586 | int_val = (int32)0; | ||
587 | bcopy(&int_val, arg, val_size); | ||
588 | break; | ||
589 | |||
590 | case IOV_GVAL(IOV_HOSTREG): | ||
591 | { | ||
592 | sdreg_t *sd_ptr = (sdreg_t *)params; | ||
593 | |||
594 | if (sd_ptr->offset < SD_SysAddr || sd_ptr->offset > SD_MaxCurCap) { | ||
595 | sd_err(("%s: bad offset 0x%x\n", __FUNCTION__, sd_ptr->offset)); | ||
596 | bcmerror = BCME_BADARG; | ||
597 | break; | ||
598 | } | ||
599 | |||
600 | sd_trace(("%s: rreg%d at offset %d\n", __FUNCTION__, | ||
601 | (sd_ptr->offset & 1) ? 8 : ((sd_ptr->offset & 2) ? 16 : 32), | ||
602 | sd_ptr->offset)); | ||
603 | if (sd_ptr->offset & 1) | ||
604 | int_val = 8; /* sdioh_sdmmc_rreg8(si, sd_ptr->offset); */ | ||
605 | else if (sd_ptr->offset & 2) | ||
606 | int_val = 16; /* sdioh_sdmmc_rreg16(si, sd_ptr->offset); */ | ||
607 | else | ||
608 | int_val = 32; /* sdioh_sdmmc_rreg(si, sd_ptr->offset); */ | ||
609 | |||
610 | bcopy(&int_val, arg, sizeof(int_val)); | ||
611 | break; | ||
612 | } | ||
613 | |||
614 | case IOV_SVAL(IOV_HOSTREG): | ||
615 | { | ||
616 | sdreg_t *sd_ptr = (sdreg_t *)params; | ||
617 | |||
618 | if (sd_ptr->offset < SD_SysAddr || sd_ptr->offset > SD_MaxCurCap) { | ||
619 | sd_err(("%s: bad offset 0x%x\n", __FUNCTION__, sd_ptr->offset)); | ||
620 | bcmerror = BCME_BADARG; | ||
621 | break; | ||
622 | } | ||
623 | |||
624 | sd_trace(("%s: wreg%d value 0x%08x at offset %d\n", __FUNCTION__, sd_ptr->value, | ||
625 | (sd_ptr->offset & 1) ? 8 : ((sd_ptr->offset & 2) ? 16 : 32), | ||
626 | sd_ptr->offset)); | ||
627 | break; | ||
628 | } | ||
629 | |||
630 | case IOV_GVAL(IOV_DEVREG): | ||
631 | { | ||
632 | sdreg_t *sd_ptr = (sdreg_t *)params; | ||
633 | uint8 data = 0; | ||
634 | |||
635 | if (sdioh_cfg_read(si, sd_ptr->func, sd_ptr->offset, &data)) { | ||
636 | bcmerror = BCME_SDIO_ERROR; | ||
637 | break; | ||
638 | } | ||
639 | |||
640 | int_val = (int)data; | ||
641 | bcopy(&int_val, arg, sizeof(int_val)); | ||
642 | break; | ||
643 | } | ||
644 | |||
645 | case IOV_SVAL(IOV_DEVREG): | ||
646 | { | ||
647 | sdreg_t *sd_ptr = (sdreg_t *)params; | ||
648 | uint8 data = (uint8)sd_ptr->value; | ||
649 | |||
650 | if (sdioh_cfg_write(si, sd_ptr->func, sd_ptr->offset, &data)) { | ||
651 | bcmerror = BCME_SDIO_ERROR; | ||
652 | break; | ||
653 | } | ||
654 | break; | ||
655 | } | ||
656 | |||
657 | default: | ||
658 | bcmerror = BCME_UNSUPPORTED; | ||
659 | break; | ||
660 | } | ||
661 | exit: | ||
662 | |||
663 | return bcmerror; | ||
664 | } | ||
665 | |||
666 | #if defined(OOB_INTR_ONLY) && defined(HW_OOB) | ||
667 | |||
668 | SDIOH_API_RC | ||
669 | sdioh_enable_hw_oob_intr(sdioh_info_t *sd, bool enable) | ||
670 | { | ||
671 | SDIOH_API_RC status; | ||
672 | uint8 data; | ||
673 | |||
674 | if (enable) | ||
675 | data = 3; /* enable hw oob interrupt */ | ||
676 | else | ||
677 | data = 4; /* disable hw oob interrupt */ | ||
678 | data |= 4; /* Active HIGH */ | ||
679 | |||
680 | status = sdioh_request_byte(sd, SDIOH_WRITE, 0, 0xf2, &data); | ||
681 | return status; | ||
682 | } | ||
683 | #endif /* defined(OOB_INTR_ONLY) && defined(HW_OOB) */ | ||
684 | |||
685 | extern SDIOH_API_RC | ||
686 | sdioh_cfg_read(sdioh_info_t *sd, uint fnc_num, uint32 addr, uint8 *data) | ||
687 | { | ||
688 | SDIOH_API_RC status; | ||
689 | /* No lock needed since sdioh_request_byte does locking */ | ||
690 | status = sdioh_request_byte(sd, SDIOH_READ, fnc_num, addr, data); | ||
691 | return status; | ||
692 | } | ||
693 | |||
694 | extern SDIOH_API_RC | ||
695 | sdioh_cfg_write(sdioh_info_t *sd, uint fnc_num, uint32 addr, uint8 *data) | ||
696 | { | ||
697 | /* No lock needed since sdioh_request_byte does locking */ | ||
698 | SDIOH_API_RC status; | ||
699 | status = sdioh_request_byte(sd, SDIOH_WRITE, fnc_num, addr, data); | ||
700 | return status; | ||
701 | } | ||
702 | |||
703 | static int | ||
704 | sdioh_sdmmc_get_cisaddr(sdioh_info_t *sd, uint32 regaddr) | ||
705 | { | ||
706 | /* read 24 bits and return valid 17 bit addr */ | ||
707 | int i; | ||
708 | uint32 scratch, regdata; | ||
709 | uint8 *ptr = (uint8 *)&scratch; | ||
710 | for (i = 0; i < 3; i++) { | ||
711 | if ((sdioh_sdmmc_card_regread (sd, 0, regaddr, 1, ®data)) != SUCCESS) | ||
712 | sd_err(("%s: Can't read!\n", __FUNCTION__)); | ||
713 | |||
714 | *ptr++ = (uint8) regdata; | ||
715 | regaddr++; | ||
716 | } | ||
717 | |||
718 | /* Only the lower 17-bits are valid */ | ||
719 | scratch = ltoh32(scratch); | ||
720 | scratch &= 0x0001FFFF; | ||
721 | return (scratch); | ||
722 | } | ||
723 | |||
724 | extern SDIOH_API_RC | ||
725 | sdioh_cis_read(sdioh_info_t *sd, uint func, uint8 *cisd, uint32 length) | ||
726 | { | ||
727 | uint32 count; | ||
728 | int offset; | ||
729 | uint32 foo; | ||
730 | uint8 *cis = cisd; | ||
731 | |||
732 | sd_trace(("%s: Func = %d\n", __FUNCTION__, func)); | ||
733 | |||
734 | if (!sd->func_cis_ptr[func]) { | ||
735 | bzero(cis, length); | ||
736 | sd_err(("%s: no func_cis_ptr[%d]\n", __FUNCTION__, func)); | ||
737 | return SDIOH_API_RC_FAIL; | ||
738 | } | ||
739 | |||
740 | sd_err(("%s: func_cis_ptr[%d]=0x%04x\n", __FUNCTION__, func, sd->func_cis_ptr[func])); | ||
741 | |||
742 | for (count = 0; count < length; count++) { | ||
743 | offset = sd->func_cis_ptr[func] + count; | ||
744 | if (sdioh_sdmmc_card_regread (sd, 0, offset, 1, &foo) < 0) { | ||
745 | sd_err(("%s: regread failed: Can't read CIS\n", __FUNCTION__)); | ||
746 | return SDIOH_API_RC_FAIL; | ||
747 | } | ||
748 | |||
749 | *cis = (uint8)(foo & 0xff); | ||
750 | cis++; | ||
751 | } | ||
752 | |||
753 | return SDIOH_API_RC_SUCCESS; | ||
754 | } | ||
755 | |||
756 | extern SDIOH_API_RC | ||
757 | sdioh_request_byte(sdioh_info_t *sd, uint rw, uint func, uint regaddr, uint8 *byte) | ||
758 | { | ||
759 | int err_ret; | ||
760 | |||
761 | sd_info(("%s: rw=%d, func=%d, addr=0x%05x\n", __FUNCTION__, rw, func, regaddr)); | ||
762 | |||
763 | DHD_PM_RESUME_WAIT(sdioh_request_byte_wait); | ||
764 | DHD_PM_RESUME_RETURN_ERROR(SDIOH_API_RC_FAIL); | ||
765 | if(rw) { /* CMD52 Write */ | ||
766 | if (func == 0) { | ||
767 | /* Can only directly write to some F0 registers. Handle F2 enable | ||
768 | * as a special case. | ||
769 | */ | ||
770 | if (regaddr == SDIOD_CCCR_IOEN) { | ||
771 | if (gInstance->func[2]) { | ||
772 | sdio_claim_host(gInstance->func[2]); | ||
773 | if (*byte & SDIO_FUNC_ENABLE_2) { | ||
774 | /* Enable Function 2 */ | ||
775 | err_ret = sdio_enable_func(gInstance->func[2]); | ||
776 | if (err_ret) { | ||
777 | sd_err(("bcmsdh_sdmmc: enable F2 failed:%d", | ||
778 | err_ret)); | ||
779 | } | ||
780 | } else { | ||
781 | /* Disable Function 2 */ | ||
782 | err_ret = sdio_disable_func(gInstance->func[2]); | ||
783 | if (err_ret) { | ||
784 | sd_err(("bcmsdh_sdmmc: Disab F2 failed:%d", | ||
785 | err_ret)); | ||
786 | } | ||
787 | } | ||
788 | sdio_release_host(gInstance->func[2]); | ||
789 | } | ||
790 | } | ||
791 | #if defined(MMC_SDIO_ABORT) | ||
792 | /* to allow abort command through F1 */ | ||
793 | else if (regaddr == SDIOD_CCCR_IOABORT) { | ||
794 | sdio_claim_host(gInstance->func[func]); | ||
795 | /* | ||
796 | * this sdio_f0_writeb() can be replaced with another api | ||
797 | * depending upon MMC driver change. | ||
798 | * As of this time, this is temporaray one | ||
799 | */ | ||
800 | sdio_writeb(gInstance->func[func], *byte, regaddr, &err_ret); | ||
801 | sdio_release_host(gInstance->func[func]); | ||
802 | } | ||
803 | #endif /* MMC_SDIO_ABORT */ | ||
804 | else if (regaddr < 0xF0) { | ||
805 | sd_err(("bcmsdh_sdmmc: F0 Wr:0x%02x: write disallowed\n", regaddr)); | ||
806 | } else { | ||
807 | /* Claim host controller, perform F0 write, and release */ | ||
808 | sdio_claim_host(gInstance->func[func]); | ||
809 | sdio_f0_writeb(gInstance->func[func], *byte, regaddr, &err_ret); | ||
810 | sdio_release_host(gInstance->func[func]); | ||
811 | } | ||
812 | } else { | ||
813 | /* Claim host controller, perform Fn write, and release */ | ||
814 | sdio_claim_host(gInstance->func[func]); | ||
815 | sdio_writeb(gInstance->func[func], *byte, regaddr, &err_ret); | ||
816 | sdio_release_host(gInstance->func[func]); | ||
817 | } | ||
818 | } else { /* CMD52 Read */ | ||
819 | /* Claim host controller, perform Fn read, and release */ | ||
820 | sdio_claim_host(gInstance->func[func]); | ||
821 | |||
822 | if (func == 0) { | ||
823 | *byte = sdio_f0_readb(gInstance->func[func], regaddr, &err_ret); | ||
824 | } else { | ||
825 | *byte = sdio_readb(gInstance->func[func], regaddr, &err_ret); | ||
826 | } | ||
827 | |||
828 | sdio_release_host(gInstance->func[func]); | ||
829 | } | ||
830 | |||
831 | if (err_ret) { | ||
832 | sd_err(("bcmsdh_sdmmc: Failed to %s byte F%d:@0x%05x=%02x, Err: %d\n", | ||
833 | rw ? "Write" : "Read", func, regaddr, *byte, err_ret)); | ||
834 | } | ||
835 | |||
836 | return ((err_ret == 0) ? SDIOH_API_RC_SUCCESS : SDIOH_API_RC_FAIL); | ||
837 | } | ||
838 | |||
839 | extern SDIOH_API_RC | ||
840 | sdioh_request_word(sdioh_info_t *sd, uint cmd_type, uint rw, uint func, uint addr, | ||
841 | uint32 *word, uint nbytes) | ||
842 | { | ||
843 | int err_ret = SDIOH_API_RC_FAIL; | ||
844 | |||
845 | if (func == 0) { | ||
846 | sd_err(("%s: Only CMD52 allowed to F0.\n", __FUNCTION__)); | ||
847 | return SDIOH_API_RC_FAIL; | ||
848 | } | ||
849 | |||
850 | sd_info(("%s: cmd_type=%d, rw=%d, func=%d, addr=0x%05x, nbytes=%d\n", | ||
851 | __FUNCTION__, cmd_type, rw, func, addr, nbytes)); | ||
852 | |||
853 | DHD_PM_RESUME_WAIT(sdioh_request_word_wait); | ||
854 | DHD_PM_RESUME_RETURN_ERROR(SDIOH_API_RC_FAIL); | ||
855 | /* Claim host controller */ | ||
856 | sdio_claim_host(gInstance->func[func]); | ||
857 | |||
858 | if(rw) { /* CMD52 Write */ | ||
859 | if (nbytes == 4) { | ||
860 | sdio_writel(gInstance->func[func], *word, addr, &err_ret); | ||
861 | } else if (nbytes == 2) { | ||
862 | sdio_writew(gInstance->func[func], (*word & 0xFFFF), addr, &err_ret); | ||
863 | } else { | ||
864 | sd_err(("%s: Invalid nbytes: %d\n", __FUNCTION__, nbytes)); | ||
865 | } | ||
866 | } else { /* CMD52 Read */ | ||
867 | if (nbytes == 4) { | ||
868 | *word = sdio_readl(gInstance->func[func], addr, &err_ret); | ||
869 | } else if (nbytes == 2) { | ||
870 | *word = sdio_readw(gInstance->func[func], addr, &err_ret) & 0xFFFF; | ||
871 | } else { | ||
872 | sd_err(("%s: Invalid nbytes: %d\n", __FUNCTION__, nbytes)); | ||
873 | } | ||
874 | } | ||
875 | |||
876 | /* Release host controller */ | ||
877 | sdio_release_host(gInstance->func[func]); | ||
878 | |||
879 | if (err_ret) { | ||
880 | sd_err(("bcmsdh_sdmmc: Failed to %s word, Err: 0x%08x", | ||
881 | rw ? "Write" : "Read", err_ret)); | ||
882 | } | ||
883 | |||
884 | return ((err_ret == 0) ? SDIOH_API_RC_SUCCESS : SDIOH_API_RC_FAIL); | ||
885 | } | ||
886 | |||
887 | static SDIOH_API_RC | ||
888 | sdioh_request_packet(sdioh_info_t *sd, uint fix_inc, uint write, uint func, | ||
889 | uint addr, void *pkt) | ||
890 | { | ||
891 | bool fifo = (fix_inc == SDIOH_DATA_FIX); | ||
892 | uint32 SGCount = 0; | ||
893 | int err_ret = 0; | ||
894 | |||
895 | void *pnext; | ||
896 | |||
897 | sd_trace(("%s: Enter\n", __FUNCTION__)); | ||
898 | |||
899 | ASSERT(pkt); | ||
900 | DHD_PM_RESUME_WAIT(sdioh_request_packet_wait); | ||
901 | DHD_PM_RESUME_RETURN_ERROR(SDIOH_API_RC_FAIL); | ||
902 | |||
903 | /* Claim host controller */ | ||
904 | sdio_claim_host(gInstance->func[func]); | ||
905 | for (pnext = pkt; pnext; pnext = PKTNEXT(sd->osh, pnext)) { | ||
906 | uint pkt_len = PKTLEN(sd->osh, pnext); | ||
907 | pkt_len += 3; | ||
908 | pkt_len &= 0xFFFFFFFC; | ||
909 | |||
910 | #ifdef CONFIG_MMC_MSM7X00A | ||
911 | if ((pkt_len % 64) == 32) { | ||
912 | sd_trace(("%s: Rounding up TX packet +=32\n", __FUNCTION__)); | ||
913 | pkt_len += 32; | ||
914 | } | ||
915 | #endif /* CONFIG_MMC_MSM7X00A */ | ||
916 | /* Make sure the packet is aligned properly. If it isn't, then this | ||
917 | * is the fault of sdioh_request_buffer() which is supposed to give | ||
918 | * us something we can work with. | ||
919 | */ | ||
920 | ASSERT(((uint32)(PKTDATA(sd->osh, pkt)) & DMA_ALIGN_MASK) == 0); | ||
921 | |||
922 | if ((write) && (!fifo)) { | ||
923 | err_ret = sdio_memcpy_toio(gInstance->func[func], addr, | ||
924 | ((uint8*)PKTDATA(sd->osh, pnext)), | ||
925 | pkt_len); | ||
926 | } else if (write) { | ||
927 | err_ret = sdio_memcpy_toio(gInstance->func[func], addr, | ||
928 | ((uint8*)PKTDATA(sd->osh, pnext)), | ||
929 | pkt_len); | ||
930 | } else if (fifo) { | ||
931 | err_ret = sdio_readsb(gInstance->func[func], | ||
932 | ((uint8*)PKTDATA(sd->osh, pnext)), | ||
933 | addr, | ||
934 | pkt_len); | ||
935 | } else { | ||
936 | err_ret = sdio_memcpy_fromio(gInstance->func[func], | ||
937 | ((uint8*)PKTDATA(sd->osh, pnext)), | ||
938 | addr, | ||
939 | pkt_len); | ||
940 | } | ||
941 | |||
942 | if (err_ret) { | ||
943 | sd_err(("%s: %s FAILED %p[%d], addr=0x%05x, pkt_len=%d, ERR=0x%08x\n", | ||
944 | __FUNCTION__, | ||
945 | (write) ? "TX" : "RX", | ||
946 | pnext, SGCount, addr, pkt_len, err_ret)); | ||
947 | } else { | ||
948 | sd_trace(("%s: %s xfr'd %p[%d], addr=0x%05x, len=%d\n", | ||
949 | __FUNCTION__, | ||
950 | (write) ? "TX" : "RX", | ||
951 | pnext, SGCount, addr, pkt_len)); | ||
952 | } | ||
953 | |||
954 | if (!fifo) { | ||
955 | addr += pkt_len; | ||
956 | } | ||
957 | SGCount ++; | ||
958 | |||
959 | } | ||
960 | |||
961 | /* Release host controller */ | ||
962 | sdio_release_host(gInstance->func[func]); | ||
963 | |||
964 | sd_trace(("%s: Exit\n", __FUNCTION__)); | ||
965 | return ((err_ret == 0) ? SDIOH_API_RC_SUCCESS : SDIOH_API_RC_FAIL); | ||
966 | } | ||
967 | |||
968 | |||
969 | /* | ||
970 | * This function takes a buffer or packet, and fixes everything up so that in the | ||
971 | * end, a DMA-able packet is created. | ||
972 | * | ||
973 | * A buffer does not have an associated packet pointer, and may or may not be aligned. | ||
974 | * A packet may consist of a single packet, or a packet chain. If it is a packet chain, | ||
975 | * then all the packets in the chain must be properly aligned. If the packet data is not | ||
976 | * aligned, then there may only be one packet, and in this case, it is copied to a new | ||
977 | * aligned packet. | ||
978 | * | ||
979 | */ | ||
980 | extern SDIOH_API_RC | ||
981 | sdioh_request_buffer(sdioh_info_t *sd, uint pio_dma, uint fix_inc, uint write, uint func, | ||
982 | uint addr, uint reg_width, uint buflen_u, uint8 *buffer, void *pkt) | ||
983 | { | ||
984 | SDIOH_API_RC Status; | ||
985 | void *mypkt = NULL; | ||
986 | |||
987 | sd_trace(("%s: Enter\n", __FUNCTION__)); | ||
988 | |||
989 | DHD_PM_RESUME_WAIT(sdioh_request_buffer_wait); | ||
990 | DHD_PM_RESUME_RETURN_ERROR(SDIOH_API_RC_FAIL); | ||
991 | /* Case 1: we don't have a packet. */ | ||
992 | if (pkt == NULL) { | ||
993 | sd_data(("%s: Creating new %s Packet, len=%d\n", | ||
994 | __FUNCTION__, write ? "TX" : "RX", buflen_u)); | ||
995 | #ifdef DHD_USE_STATIC_BUF | ||
996 | if (!(mypkt = PKTGET_STATIC(sd->osh, buflen_u, write ? TRUE : FALSE))) { | ||
997 | #else | ||
998 | if (!(mypkt = PKTGET(sd->osh, buflen_u, write ? TRUE : FALSE))) { | ||
999 | #endif /* DHD_USE_STATIC_BUF */ | ||
1000 | sd_err(("%s: PKTGET failed: len %d\n", | ||
1001 | __FUNCTION__, buflen_u)); | ||
1002 | return SDIOH_API_RC_FAIL; | ||
1003 | } | ||
1004 | |||
1005 | /* For a write, copy the buffer data into the packet. */ | ||
1006 | if (write) { | ||
1007 | bcopy(buffer, PKTDATA(sd->osh, mypkt), buflen_u); | ||
1008 | } | ||
1009 | |||
1010 | Status = sdioh_request_packet(sd, fix_inc, write, func, addr, mypkt); | ||
1011 | |||
1012 | /* For a read, copy the packet data back to the buffer. */ | ||
1013 | if (!write) { | ||
1014 | bcopy(PKTDATA(sd->osh, mypkt), buffer, buflen_u); | ||
1015 | } | ||
1016 | #ifdef DHD_USE_STATIC_BUF | ||
1017 | PKTFREE_STATIC(sd->osh, mypkt, write ? TRUE : FALSE); | ||
1018 | #else | ||
1019 | PKTFREE(sd->osh, mypkt, write ? TRUE : FALSE); | ||
1020 | #endif /* DHD_USE_STATIC_BUF */ | ||
1021 | } else if (((uint32)(PKTDATA(sd->osh, pkt)) & DMA_ALIGN_MASK) != 0) { | ||
1022 | /* Case 2: We have a packet, but it is unaligned. */ | ||
1023 | |||
1024 | /* In this case, we cannot have a chain. */ | ||
1025 | ASSERT(PKTNEXT(sd->osh, pkt) == NULL); | ||
1026 | |||
1027 | sd_data(("%s: Creating aligned %s Packet, len=%d\n", | ||
1028 | __FUNCTION__, write ? "TX" : "RX", PKTLEN(sd->osh, pkt))); | ||
1029 | #ifdef DHD_USE_STATIC_BUF | ||
1030 | if (!(mypkt = PKTGET_STATIC(sd->osh, PKTLEN(sd->osh, pkt), write ? TRUE : FALSE))) { | ||
1031 | #else | ||
1032 | if (!(mypkt = PKTGET(sd->osh, PKTLEN(sd->osh, pkt), write ? TRUE : FALSE))) { | ||
1033 | #endif /* DHD_USE_STATIC_BUF */ | ||
1034 | sd_err(("%s: PKTGET failed: len %d\n", | ||
1035 | __FUNCTION__, PKTLEN(sd->osh, pkt))); | ||
1036 | return SDIOH_API_RC_FAIL; | ||
1037 | } | ||
1038 | |||
1039 | /* For a write, copy the buffer data into the packet. */ | ||
1040 | if (write) { | ||
1041 | bcopy(PKTDATA(sd->osh, pkt), | ||
1042 | PKTDATA(sd->osh, mypkt), | ||
1043 | PKTLEN(sd->osh, pkt)); | ||
1044 | } | ||
1045 | |||
1046 | Status = sdioh_request_packet(sd, fix_inc, write, func, addr, mypkt); | ||
1047 | |||
1048 | /* For a read, copy the packet data back to the buffer. */ | ||
1049 | if (!write) { | ||
1050 | bcopy(PKTDATA(sd->osh, mypkt), | ||
1051 | PKTDATA(sd->osh, pkt), | ||
1052 | PKTLEN(sd->osh, mypkt)); | ||
1053 | } | ||
1054 | #ifdef DHD_USE_STATIC_BUF | ||
1055 | PKTFREE_STATIC(sd->osh, mypkt, write ? TRUE : FALSE); | ||
1056 | #else | ||
1057 | PKTFREE(sd->osh, mypkt, write ? TRUE : FALSE); | ||
1058 | #endif /* DHD_USE_STATIC_BUF */ | ||
1059 | } else { /* case 3: We have a packet and it is aligned. */ | ||
1060 | sd_data(("%s: Aligned %s Packet, direct DMA\n", | ||
1061 | __FUNCTION__, write ? "Tx" : "Rx")); | ||
1062 | Status = sdioh_request_packet(sd, fix_inc, write, func, addr, pkt); | ||
1063 | } | ||
1064 | |||
1065 | return (Status); | ||
1066 | } | ||
1067 | |||
1068 | /* this function performs "abort" for both of host & device */ | ||
1069 | extern int | ||
1070 | sdioh_abort(sdioh_info_t *sd, uint func) | ||
1071 | { | ||
1072 | #if defined(MMC_SDIO_ABORT) | ||
1073 | char t_func = (char) func; | ||
1074 | #endif /* defined(MMC_SDIO_ABORT) */ | ||
1075 | sd_trace(("%s: Enter\n", __FUNCTION__)); | ||
1076 | |||
1077 | #if defined(MMC_SDIO_ABORT) | ||
1078 | /* issue abort cmd52 command through F1 */ | ||
1079 | sdioh_request_byte(sd, SD_IO_OP_WRITE, SDIO_FUNC_0, SDIOD_CCCR_IOABORT, &t_func); | ||
1080 | #endif /* defined(MMC_SDIO_ABORT) */ | ||
1081 | |||
1082 | sd_trace(("%s: Exit\n", __FUNCTION__)); | ||
1083 | return SDIOH_API_RC_SUCCESS; | ||
1084 | } | ||
1085 | |||
1086 | /* Reset and re-initialize the device */ | ||
1087 | int sdioh_sdio_reset(sdioh_info_t *si) | ||
1088 | { | ||
1089 | sd_trace(("%s: Enter\n", __FUNCTION__)); | ||
1090 | sd_trace(("%s: Exit\n", __FUNCTION__)); | ||
1091 | return SDIOH_API_RC_SUCCESS; | ||
1092 | } | ||
1093 | |||
1094 | /* Disable device interrupt */ | ||
1095 | void | ||
1096 | sdioh_sdmmc_devintr_off(sdioh_info_t *sd) | ||
1097 | { | ||
1098 | sd_trace(("%s: %d\n", __FUNCTION__, sd->use_client_ints)); | ||
1099 | sd->intmask &= ~CLIENT_INTR; | ||
1100 | } | ||
1101 | |||
1102 | /* Enable device interrupt */ | ||
1103 | void | ||
1104 | sdioh_sdmmc_devintr_on(sdioh_info_t *sd) | ||
1105 | { | ||
1106 | sd_trace(("%s: %d\n", __FUNCTION__, sd->use_client_ints)); | ||
1107 | sd->intmask |= CLIENT_INTR; | ||
1108 | } | ||
1109 | |||
1110 | /* Read client card reg */ | ||
1111 | int | ||
1112 | sdioh_sdmmc_card_regread(sdioh_info_t *sd, int func, uint32 regaddr, int regsize, uint32 *data) | ||
1113 | { | ||
1114 | |||
1115 | if ((func == 0) || (regsize == 1)) { | ||
1116 | uint8 temp = 0; | ||
1117 | |||
1118 | sdioh_request_byte(sd, SDIOH_READ, func, regaddr, &temp); | ||
1119 | *data = temp; | ||
1120 | *data &= 0xff; | ||
1121 | sd_data(("%s: byte read data=0x%02x\n", | ||
1122 | __FUNCTION__, *data)); | ||
1123 | } else { | ||
1124 | sdioh_request_word(sd, 0, SDIOH_READ, func, regaddr, data, regsize); | ||
1125 | if (regsize == 2) | ||
1126 | *data &= 0xffff; | ||
1127 | |||
1128 | sd_data(("%s: word read data=0x%08x\n", | ||
1129 | __FUNCTION__, *data)); | ||
1130 | } | ||
1131 | |||
1132 | return SUCCESS; | ||
1133 | } | ||
1134 | |||
1135 | #if !defined(OOB_INTR_ONLY) | ||
1136 | /* bcmsdh_sdmmc interrupt handler */ | ||
1137 | static void IRQHandler(struct sdio_func *func) | ||
1138 | { | ||
1139 | sdioh_info_t *sd; | ||
1140 | |||
1141 | sd_trace(("bcmsdh_sdmmc: ***IRQHandler\n")); | ||
1142 | sd = gInstance->sd; | ||
1143 | |||
1144 | ASSERT(sd != NULL); | ||
1145 | sdio_release_host(gInstance->func[0]); | ||
1146 | |||
1147 | if (sd->use_client_ints) { | ||
1148 | sd->intrcount++; | ||
1149 | ASSERT(sd->intr_handler); | ||
1150 | ASSERT(sd->intr_handler_arg); | ||
1151 | (sd->intr_handler)(sd->intr_handler_arg); | ||
1152 | } else { | ||
1153 | sd_err(("bcmsdh_sdmmc: ***IRQHandler\n")); | ||
1154 | |||
1155 | sd_err(("%s: Not ready for intr: enabled %d, handler %p\n", | ||
1156 | __FUNCTION__, sd->client_intr_enabled, sd->intr_handler)); | ||
1157 | } | ||
1158 | |||
1159 | sdio_claim_host(gInstance->func[0]); | ||
1160 | } | ||
1161 | |||
1162 | /* bcmsdh_sdmmc interrupt handler for F2 (dummy handler) */ | ||
1163 | static void IRQHandlerF2(struct sdio_func *func) | ||
1164 | { | ||
1165 | sdioh_info_t *sd; | ||
1166 | |||
1167 | sd_trace(("bcmsdh_sdmmc: ***IRQHandlerF2\n")); | ||
1168 | |||
1169 | sd = gInstance->sd; | ||
1170 | |||
1171 | ASSERT(sd != NULL); | ||
1172 | } | ||
1173 | #endif /* !defined(OOB_INTR_ONLY) */ | ||
1174 | |||
1175 | #ifdef NOTUSED | ||
1176 | /* Write client card reg */ | ||
1177 | static int | ||
1178 | sdioh_sdmmc_card_regwrite(sdioh_info_t *sd, int func, uint32 regaddr, int regsize, uint32 data) | ||
1179 | { | ||
1180 | |||
1181 | if ((func == 0) || (regsize == 1)) { | ||
1182 | uint8 temp; | ||
1183 | |||
1184 | temp = data & 0xff; | ||
1185 | sdioh_request_byte(sd, SDIOH_READ, func, regaddr, &temp); | ||
1186 | sd_data(("%s: byte write data=0x%02x\n", | ||
1187 | __FUNCTION__, data)); | ||
1188 | } else { | ||
1189 | if (regsize == 2) | ||
1190 | data &= 0xffff; | ||
1191 | |||
1192 | sdioh_request_word(sd, 0, SDIOH_READ, func, regaddr, &data, regsize); | ||
1193 | |||
1194 | sd_data(("%s: word write data=0x%08x\n", | ||
1195 | __FUNCTION__, data)); | ||
1196 | } | ||
1197 | |||
1198 | return SUCCESS; | ||
1199 | } | ||
1200 | #endif /* NOTUSED */ | ||
1201 | |||
1202 | int | ||
1203 | sdioh_start(sdioh_info_t *si, int stage) | ||
1204 | { | ||
1205 | int ret; | ||
1206 | sdioh_info_t *sd = gInstance->sd; | ||
1207 | |||
1208 | /* Need to do this stages as we can't enable the interrupt till | ||
1209 | downloading of the firmware is complete, other wise polling | ||
1210 | sdio access will come in way | ||
1211 | */ | ||
1212 | if (gInstance->func[0]) { | ||
1213 | if (stage == 0) { | ||
1214 | /* Since the power to the chip is killed, we will have | ||
1215 | re enumerate the device again. Set the block size | ||
1216 | and enable the fucntion 1 for in preparation for | ||
1217 | downloading the code | ||
1218 | */ | ||
1219 | /* sdio_reset_comm() - has been fixed in latest kernel/msm.git for Linux | ||
1220 | 2.6.27. The implementation prior to that is buggy, and needs broadcom's | ||
1221 | patch for it | ||
1222 | */ | ||
1223 | if ((ret = sdio_reset_comm(gInstance->func[0]->card))) | ||
1224 | sd_err(("%s Failed, error = %d\n", __FUNCTION__, ret)); | ||
1225 | else { | ||
1226 | sd->num_funcs = 2; | ||
1227 | sd->sd_blockmode = TRUE; | ||
1228 | sd->use_client_ints = TRUE; | ||
1229 | sd->client_block_size[0] = 64; | ||
1230 | |||
1231 | /* Claim host controller */ | ||
1232 | sdio_claim_host(gInstance->func[1]); | ||
1233 | |||
1234 | sd->client_block_size[1] = 64; | ||
1235 | if (sdio_set_block_size(gInstance->func[1], 64)) { | ||
1236 | sd_err(("bcmsdh_sdmmc: Failed to set F1 blocksize\n")); | ||
1237 | } | ||
1238 | |||
1239 | /* Release host controller F1 */ | ||
1240 | sdio_release_host(gInstance->func[1]); | ||
1241 | |||
1242 | if (gInstance->func[2]) { | ||
1243 | /* Claim host controller F2 */ | ||
1244 | sdio_claim_host(gInstance->func[2]); | ||
1245 | |||
1246 | sd->client_block_size[2] = sd_f2_blocksize; | ||
1247 | if (sdio_set_block_size(gInstance->func[2], | ||
1248 | sd_f2_blocksize)) { | ||
1249 | sd_err(("bcmsdh_sdmmc: Failed to set F2 " | ||
1250 | "blocksize to %d\n", sd_f2_blocksize)); | ||
1251 | } | ||
1252 | |||
1253 | /* Release host controller F2 */ | ||
1254 | sdio_release_host(gInstance->func[2]); | ||
1255 | } | ||
1256 | |||
1257 | sdioh_sdmmc_card_enablefuncs(sd); | ||
1258 | } | ||
1259 | } else { | ||
1260 | #if !defined(OOB_INTR_ONLY) | ||
1261 | sdio_claim_host(gInstance->func[0]); | ||
1262 | sdio_claim_irq(gInstance->func[2], IRQHandlerF2); | ||
1263 | sdio_claim_irq(gInstance->func[1], IRQHandler); | ||
1264 | sdio_release_host(gInstance->func[0]); | ||
1265 | #else /* defined(OOB_INTR_ONLY) */ | ||
1266 | #if defined(HW_OOB) | ||
1267 | sdioh_enable_func_intr(); | ||
1268 | #endif | ||
1269 | bcmsdh_oob_intr_set(TRUE); | ||
1270 | #endif /* !defined(OOB_INTR_ONLY) */ | ||
1271 | } | ||
1272 | } | ||
1273 | else | ||
1274 | sd_err(("%s Failed\n", __FUNCTION__)); | ||
1275 | |||
1276 | return (0); | ||
1277 | } | ||
1278 | |||
1279 | int | ||
1280 | sdioh_stop(sdioh_info_t *si) | ||
1281 | { | ||
1282 | /* MSM7201A Android sdio stack has bug with interrupt | ||
1283 | So internaly within SDIO stack they are polling | ||
1284 | which cause issue when device is turned off. So | ||
1285 | unregister interrupt with SDIO stack to stop the | ||
1286 | polling | ||
1287 | */ | ||
1288 | if (gInstance->func[0]) { | ||
1289 | #if !defined(OOB_INTR_ONLY) | ||
1290 | sdio_claim_host(gInstance->func[0]); | ||
1291 | sdio_release_irq(gInstance->func[1]); | ||
1292 | sdio_release_irq(gInstance->func[2]); | ||
1293 | sdio_release_host(gInstance->func[0]); | ||
1294 | #else /* defined(OOB_INTR_ONLY) */ | ||
1295 | #if defined(HW_OOB) | ||
1296 | sdioh_disable_func_intr(); | ||
1297 | #endif | ||
1298 | bcmsdh_oob_intr_set(FALSE); | ||
1299 | #endif /* !defined(OOB_INTR_ONLY) */ | ||
1300 | } | ||
1301 | else | ||
1302 | sd_err(("%s Failed\n", __FUNCTION__)); | ||
1303 | return (0); | ||
1304 | } | ||