diff options
Diffstat (limited to 'drivers/net/wireless/bcm4329/include/typedefs.h')
-rw-r--r-- | drivers/net/wireless/bcm4329/include/typedefs.h | 303 |
1 files changed, 303 insertions, 0 deletions
diff --git a/drivers/net/wireless/bcm4329/include/typedefs.h b/drivers/net/wireless/bcm4329/include/typedefs.h new file mode 100644 index 00000000000..4d9dd761ed6 --- /dev/null +++ b/drivers/net/wireless/bcm4329/include/typedefs.h | |||
@@ -0,0 +1,303 @@ | |||
1 | /* | ||
2 | * Copyright (C) 1999-2010, Broadcom Corporation | ||
3 | * | ||
4 | * Unless you and Broadcom execute a separate written software license | ||
5 | * agreement governing use of this software, this software is licensed to you | ||
6 | * under the terms of the GNU General Public License version 2 (the "GPL"), | ||
7 | * available at http://www.broadcom.com/licenses/GPLv2.php, with the | ||
8 | * following added to such license: | ||
9 | * | ||
10 | * As a special exception, the copyright holders of this software give you | ||
11 | * permission to link this software with independent modules, and to copy and | ||
12 | * distribute the resulting executable under terms of your choice, provided that | ||
13 | * you also meet, for each linked independent module, the terms and conditions of | ||
14 | * the license of that module. An independent module is a module which is not | ||
15 | * derived from this software. The special exception does not apply to any | ||
16 | * modifications of the software. | ||
17 | * | ||
18 | * Notwithstanding the above, under no circumstances may you combine this | ||
19 | * software in any way with any other Broadcom software provided under a license | ||
20 | * other than the GPL, without Broadcom's express prior written consent. | ||
21 | * $Id: typedefs.h,v 1.85.34.1.2.5 2009/01/27 04:09:40 Exp $ | ||
22 | */ | ||
23 | |||
24 | |||
25 | #ifndef _TYPEDEFS_H_ | ||
26 | #define _TYPEDEFS_H_ | ||
27 | |||
28 | #ifdef SITE_TYPEDEFS | ||
29 | |||
30 | |||
31 | |||
32 | #include "site_typedefs.h" | ||
33 | |||
34 | #else | ||
35 | |||
36 | |||
37 | |||
38 | #ifdef __cplusplus | ||
39 | |||
40 | #define TYPEDEF_BOOL | ||
41 | #ifndef FALSE | ||
42 | #define FALSE false | ||
43 | #endif | ||
44 | #ifndef TRUE | ||
45 | #define TRUE true | ||
46 | #endif | ||
47 | |||
48 | #else | ||
49 | |||
50 | |||
51 | #endif | ||
52 | |||
53 | #if defined(__x86_64__) | ||
54 | #define TYPEDEF_UINTPTR | ||
55 | typedef unsigned long long int uintptr; | ||
56 | #endif | ||
57 | |||
58 | |||
59 | |||
60 | |||
61 | #if defined(TARGETOS_nucleus) | ||
62 | |||
63 | #include <stddef.h> | ||
64 | |||
65 | |||
66 | #define TYPEDEF_FLOAT_T | ||
67 | #endif | ||
68 | |||
69 | #if defined(_NEED_SIZE_T_) | ||
70 | typedef long unsigned int size_t; | ||
71 | #endif | ||
72 | |||
73 | #ifdef __DJGPP__ | ||
74 | typedef long unsigned int size_t; | ||
75 | #endif | ||
76 | |||
77 | |||
78 | |||
79 | |||
80 | |||
81 | #define TYPEDEF_UINT | ||
82 | #ifndef TARGETENV_android | ||
83 | #define TYPEDEF_USHORT | ||
84 | #define TYPEDEF_ULONG | ||
85 | #endif | ||
86 | #ifdef __KERNEL__ | ||
87 | #include <linux/version.h> | ||
88 | #if (LINUX_VERSION_CODE >= KERNEL_VERSION(2, 6, 19)) | ||
89 | #define TYPEDEF_BOOL | ||
90 | #endif | ||
91 | #endif | ||
92 | |||
93 | |||
94 | |||
95 | |||
96 | |||
97 | #if defined(__GNUC__) && defined(__STRICT_ANSI__) | ||
98 | #define TYPEDEF_INT64 | ||
99 | #define TYPEDEF_UINT64 | ||
100 | #endif | ||
101 | |||
102 | |||
103 | #if defined(__ICL) | ||
104 | |||
105 | #define TYPEDEF_INT64 | ||
106 | |||
107 | #if defined(__STDC__) | ||
108 | #define TYPEDEF_UINT64 | ||
109 | #endif | ||
110 | |||
111 | #endif | ||
112 | |||
113 | #if !defined(__DJGPP__) && !defined(TARGETOS_nucleus) | ||
114 | |||
115 | |||
116 | #if defined(__KERNEL__) | ||
117 | |||
118 | #include <linux/types.h> | ||
119 | |||
120 | #else | ||
121 | |||
122 | |||
123 | #include <sys/types.h> | ||
124 | |||
125 | #endif | ||
126 | |||
127 | #endif | ||
128 | |||
129 | |||
130 | |||
131 | |||
132 | #define USE_TYPEDEF_DEFAULTS | ||
133 | |||
134 | #endif | ||
135 | |||
136 | |||
137 | |||
138 | |||
139 | #ifdef USE_TYPEDEF_DEFAULTS | ||
140 | #undef USE_TYPEDEF_DEFAULTS | ||
141 | |||
142 | #ifndef TYPEDEF_BOOL | ||
143 | typedef unsigned char bool; | ||
144 | #endif | ||
145 | |||
146 | |||
147 | |||
148 | #ifndef TYPEDEF_UCHAR | ||
149 | typedef unsigned char uchar; | ||
150 | #endif | ||
151 | |||
152 | #ifndef TYPEDEF_USHORT | ||
153 | typedef unsigned short ushort; | ||
154 | #endif | ||
155 | |||
156 | #ifndef TYPEDEF_UINT | ||
157 | typedef unsigned int uint; | ||
158 | #endif | ||
159 | |||
160 | #ifndef TYPEDEF_ULONG | ||
161 | typedef unsigned long ulong; | ||
162 | #endif | ||
163 | |||
164 | |||
165 | |||
166 | #ifndef TYPEDEF_UINT8 | ||
167 | typedef unsigned char uint8; | ||
168 | #endif | ||
169 | |||
170 | #ifndef TYPEDEF_UINT16 | ||
171 | typedef unsigned short uint16; | ||
172 | #endif | ||
173 | |||
174 | #ifndef TYPEDEF_UINT32 | ||
175 | typedef unsigned int uint32; | ||
176 | #endif | ||
177 | |||
178 | #ifndef TYPEDEF_UINT64 | ||
179 | typedef unsigned long long uint64; | ||
180 | #endif | ||
181 | |||
182 | #ifndef TYPEDEF_UINTPTR | ||
183 | typedef unsigned int uintptr; | ||
184 | #endif | ||
185 | |||
186 | #ifndef TYPEDEF_INT8 | ||
187 | typedef signed char int8; | ||
188 | #endif | ||
189 | |||
190 | #ifndef TYPEDEF_INT16 | ||
191 | typedef signed short int16; | ||
192 | #endif | ||
193 | |||
194 | #ifndef TYPEDEF_INT32 | ||
195 | typedef signed int int32; | ||
196 | #endif | ||
197 | |||
198 | #ifndef TYPEDEF_INT64 | ||
199 | typedef signed long long int64; | ||
200 | #endif | ||
201 | |||
202 | |||
203 | |||
204 | #ifndef TYPEDEF_FLOAT32 | ||
205 | typedef float float32; | ||
206 | #endif | ||
207 | |||
208 | #ifndef TYPEDEF_FLOAT64 | ||
209 | typedef double float64; | ||
210 | #endif | ||
211 | |||
212 | |||
213 | |||
214 | #ifndef TYPEDEF_FLOAT_T | ||
215 | |||
216 | #if defined(FLOAT32) | ||
217 | typedef float32 float_t; | ||
218 | #else | ||
219 | typedef float64 float_t; | ||
220 | #endif | ||
221 | |||
222 | #endif | ||
223 | |||
224 | |||
225 | |||
226 | #ifndef FALSE | ||
227 | #define FALSE 0 | ||
228 | #endif | ||
229 | |||
230 | #ifndef TRUE | ||
231 | #define TRUE 1 | ||
232 | #endif | ||
233 | |||
234 | #ifndef NULL | ||
235 | #define NULL 0 | ||
236 | #endif | ||
237 | |||
238 | #ifndef OFF | ||
239 | #define OFF 0 | ||
240 | #endif | ||
241 | |||
242 | #ifndef ON | ||
243 | #define ON 1 | ||
244 | #endif | ||
245 | |||
246 | #define AUTO (-1) | ||
247 | |||
248 | |||
249 | |||
250 | #ifndef PTRSZ | ||
251 | #define PTRSZ sizeof(char*) | ||
252 | #endif | ||
253 | |||
254 | |||
255 | |||
256 | #if defined(__GNUC__) | ||
257 | #define BWL_COMPILER_GNU | ||
258 | #elif defined(__CC_ARM) | ||
259 | #define BWL_COMPILER_ARMCC | ||
260 | #else | ||
261 | #error "Unknown compiler!" | ||
262 | #endif | ||
263 | |||
264 | |||
265 | #ifndef INLINE | ||
266 | #if defined(BWL_COMPILER_MICROSOFT) | ||
267 | #define INLINE __inline | ||
268 | #elif defined(BWL_COMPILER_GNU) | ||
269 | #define INLINE __inline__ | ||
270 | #elif defined(BWL_COMPILER_ARMCC) | ||
271 | #define INLINE __inline | ||
272 | #else | ||
273 | #define INLINE | ||
274 | #endif | ||
275 | #endif | ||
276 | |||
277 | #undef TYPEDEF_BOOL | ||
278 | #undef TYPEDEF_UCHAR | ||
279 | #undef TYPEDEF_USHORT | ||
280 | #undef TYPEDEF_UINT | ||
281 | #undef TYPEDEF_ULONG | ||
282 | #undef TYPEDEF_UINT8 | ||
283 | #undef TYPEDEF_UINT16 | ||
284 | #undef TYPEDEF_UINT32 | ||
285 | #undef TYPEDEF_UINT64 | ||
286 | #undef TYPEDEF_UINTPTR | ||
287 | #undef TYPEDEF_INT8 | ||
288 | #undef TYPEDEF_INT16 | ||
289 | #undef TYPEDEF_INT32 | ||
290 | #undef TYPEDEF_INT64 | ||
291 | #undef TYPEDEF_FLOAT32 | ||
292 | #undef TYPEDEF_FLOAT64 | ||
293 | #undef TYPEDEF_FLOAT_T | ||
294 | |||
295 | #endif | ||
296 | |||
297 | |||
298 | #define UNUSED_PARAMETER(x) (void)(x) | ||
299 | |||
300 | |||
301 | #include <bcmdefs.h> | ||
302 | |||
303 | #endif | ||