aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* scsi: Silence unnecessary warnings about ioctl to partitionJan Kara2012-06-151-1/+4
| | | | | | | | | | | | | | | | | | | | Sometimes, warnings about ioctls to partition happen often enough that they form majority of the warnings in the kernel log and users complain. In some cases warnings are about ioctls such as SG_IO so it's not good to get rid of the warnings completely as they can ease debugging of userspace problems when ioctl is refused. Since I have seen warnings from lots of commands, including some proprietary userspace applications, I don't think disallowing the ioctls for processes with CAP_SYS_RAWIO will happen in the near future if ever. So lets just stop warning for processes with CAP_SYS_RAWIO for which ioctl is allowed. CC: Paolo Bonzini <pbonzini@redhat.com> CC: James Bottomley <JBottomley@parallels.com> CC: linux-scsi@vger.kernel.org Acked-by: Paolo Bonzini <pbonzini@redhat.com> Signed-off-by: Jan Kara <jack@suse.cz> Signed-off-by: Jens Axboe <axboe@kernel.dk>
* block: fail SCSI passthrough ioctls on partition devicesPaolo Bonzini2012-01-141-0/+45
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Linux allows executing the SG_IO ioctl on a partition or LVM volume, and will pass the command to the underlying block device. This is well-known, but it is also a large security problem when (via Unix permissions, ACLs, SELinux or a combination thereof) a program or user needs to be granted access only to part of the disk. This patch lets partitions forward a small set of harmless ioctls; others are logged with printk so that we can see which ioctls are actually sent. In my tests only CDROM_GET_CAPABILITY actually occurred. Of course it was being sent to a (partition on a) hard disk, so it would have failed with ENOTTY and the patch isn't changing anything in practice. Still, I'm treating it specially to avoid spamming the logs. In principle, this restriction should include programs running with CAP_SYS_RAWIO. If for example I let a program access /dev/sda2 and /dev/sdb, it still should not be able to read/write outside the boundaries of /dev/sda2 independent of the capabilities. However, for now programs with CAP_SYS_RAWIO will still be allowed to send the ioctls. Their actions will still be logged. This patch does not affect the non-libata IDE driver. That driver however already tests for bd != bd->bd_contains before issuing some ioctl; it could be restricted further to forbid these ioctls even for programs running with CAP_SYS_ADMIN/CAP_SYS_RAWIO. Cc: linux-scsi@vger.kernel.org Cc: Jens Axboe <axboe@kernel.dk> Cc: James Bottomley <JBottomley@parallels.com> Signed-off-by: Paolo Bonzini <pbonzini@redhat.com> [ Make it also print the command name when warning - Linus ] Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* block: add and use scsi_blk_cmd_ioctlPaolo Bonzini2012-01-141-0/+7
| | | | | | | | | | | | | Introduce a wrapper around scsi_cmd_ioctl that takes a block device. The function will then be enhanced to detect partition block devices and, in that case, subject the ioctls to whitelisting. Cc: linux-scsi@vger.kernel.org Cc: Jens Axboe <axboe@kernel.dk> Cc: James Bottomley <JBottomley@parallels.com> Signed-off-by: Paolo Bonzini <pbonzini@redhat.com> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* block: drop unnecessary blk_get/put_queue() in scsi_cmd_ioctl() and blk_get_tg()Tejun Heo2011-10-191-2/+1
| | | | | | | | | | | | | | | | | | | | | | blk_get/put_queue() in scsi_cmd_ioctl() and throtl_get_tg() are completely bogus. The caller must have a reference to the queue on entry and taking an extra reference doesn't change anything. For scsi_cmd_ioctl(), the only effect is that it ends up checking QUEUE_FLAG_DEAD on entry; however, this is bogus as queue can die right after blk_get_queue(). Dead queue should be and is handled in request issue path (it's somewhat broken now but that's a separate problem and doesn't affect this one much). throtl_get_tg() incorrectly assumes that q is rcu freed. Also, it doesn't check return value of blk_get_queue(). If the queue is already dead, it ends up doing an extra put. Drop them. Signed-off-by: Tejun Heo <tj@kernel.org> Cc: Vivek Goyal <vgoyal@redhat.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
* block: take care not to overflow when calculating total iov lengthJens Axboe2010-11-101-10/+24
| | | | | | Reported-by: Dan Rosenberg <drosenberg@vsecurity.com> Cc: stable@kernel.org Signed-off-by: Jens Axboe <jaxboe@fusionio.com>
* block/scsi_ioctl.c: quiet sparse noiseH Hartley Sweeten2009-11-041-2/+4
| | | | | | | | | | | | | Quiet sparse noise about symbol's not being declared. Symbol blk_default_cmd_filter is only used locally and should be static. The function blk_scsi_ioctl_init() is a fs_initcall and should also be static. Signed-off-by: H Hartley Sweeten <hsweeten@visionengravers.com> Cc: James Bottomley <James.Bottomley@HansenPartnership.com> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: call blk_scsi_ioctl_init()FUJITA Tomonori2009-07-101-0/+1
| | | | | | | | | | | | | Currently, blk_scsi_ioctl_init() is not called since it lacks an initcall marking. This causes the command table to be unitialized, hence somce commands are block when they should not have been. This fixes a regression introduced by commit 018e0446890661504783f92388ecce7138c1566d Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: get rid of queue-private command filterJens Axboe2009-07-011-5/+38
| | | | | | | | | | The initial patches to support this through sysfs export were broken and have been if 0'ed out in any release. So lets just kill the code and reclaim some space in struct request_queue, if anyone would later like to fixup the sysfs bits, the git history can easily restore the removed bits. Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: Use accessor functions for queue limitsMartin K. Petersen2009-05-221-4/+4
| | | | | | | | Convert all external users of queue limits to using wrapper functions instead of poking the request queue variables directly. Signed-off-by: Martin K. Petersen <martin.petersen@oracle.com> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: add rq->resid_lenTejun Heo2009-05-111-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | rq->data_len served two purposes - the length of data buffer on issue and the residual count on completion. This duality creates some headaches. First of all, block layer and low level drivers can't really determine what rq->data_len contains while a request is executing. It could be the total request length or it coulde be anything else one of the lower layers is using to keep track of residual count. This complicates things because blk_rq_bytes() and thus [__]blk_end_request_all() relies on rq->data_len for PC commands. Drivers which want to report residual count should first cache the total request length, update rq->data_len and then complete the request with the cached data length. Secondly, it makes requests default to reporting full residual count, ie. reporting that no data transfer occurred. The residual count is an exception not the norm; however, the driver should clear rq->data_len to zero to signify the normal cases while leaving it alone means no data transfer occurred at all. This reverse default behavior complicates code unnecessarily and renders block PC on some drivers (ide-tape/floppy) unuseable. This patch adds rq->resid_len which is used only for residual count. While at it, remove now unnecessasry blk_rq_bytes() caching in ide_pc_intr() as rq->data_len is not changed anymore. Boaz : spotted missing conversion in osd Sergei : spotted too early conversion to blk_rq_bytes() in ide-tape [ Impact: cleanup residual count handling, report 0 resid by default ] Signed-off-by: Tejun Heo <tj@kernel.org> Cc: James Bottomley <James.Bottomley@HansenPartnership.com> Cc: Bartlomiej Zolnierkiewicz <bzolnier@gmail.com> Cc: Borislav Petkov <petkovbb@googlemail.com> Cc: Sergei Shtylyov <sshtylyov@ru.mvista.com> Cc: Mike Miller <mike.miller@hp.com> Cc: Eric Moore <Eric.Moore@lsi.com> Cc: Alan Stern <stern@rowland.harvard.edu> Cc: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Cc: Doug Gilbert <dgilbert@interlog.com> Cc: Mike Miller <mike.miller@hp.com> Cc: Eric Moore <Eric.Moore@lsi.com> Cc: Darrick J. Wong <djwong@us.ibm.com> Cc: Pete Zaitcev <zaitcev@redhat.com> Cc: Boaz Harrosh <bharrosh@panasas.com> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: don't init rq fields unnecessarilyTejun Heo2009-04-281-2/+0
| | | | | | | | | | blk_get_request() always returns properly zeroed requests. Don't set fields to zero/NULL unnecessarily. [ Impact: cleanup ] Signed-off-by: Tejun Heo <tj@kernel.org> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: kill rq->dataTejun Heo2009-04-281-1/+0
| | | | | | | | | | | | Now that all block request data transfer is done via bio, rq->data isn't used. Kill it. While at it, make the roles of rq->special and buffer clear. [ Impact: drop now unncessary field from struct request ] Signed-off-by: Tejun Heo <tj@kernel.org> Cc: Boaz Harrosh <bharrosh@panasas.com>
* block: fix SG_IO vector request data length handlingTejun Heo2009-04-221-1/+12
| | | | | | | | | | | | | | | Impact: fix SG_IO behavior such that it matches the documentation SG_IO howto says that if ->dxfer_len and sum of iovec disagress, the shorter one wins. However, the current implementation returns -EINVAL for such cases. Trim iovc if it's longer than ->dxfer_len. This patch uses iov_*() helpers which take struct iovec * by casting struct sg_iovec * to it. sg_iovec is always identical to iovec and this will be further cleaned up with later patches. Signed-off-by: Tejun Heo <tj@kernel.org> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: fix SG_IO to return a proper error valueFUJITA Tomonori2009-04-151-2/+4
| | | | | | | | | blk_rq_unmap_user() returns -EFAULT if a program passes an invalid address to kernel. SG_IO path needs to pass the returned value to user space instead of ignoring it. Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: WARN in __blk_put_request() for potential bio leakBoaz Harrosh2009-03-261-17/+4
| | | | | | | | | | | | | Put a WARN_ON in __blk_put_request if it is about to leak bio(s). This is a serious bug that can happen in error handling code paths. For this to work I have fixed a couple of places in block/ where request->bio != NULL ownership was not honored. And a small cleanup at sg_io() while at it. Signed-off-by: Boaz Harrosh <bharrosh@panasas.com> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* scsi-ioctl: use clock_t <> jiffiesMilton Miller2008-12-291-2/+2
| | | | | | | | Convert the timeout ioctl scalling to use the clock_t functions which are much more accurate with some USER_HZ vs HZ combinations. Signed-off-by: Milton Miller <miltonm@bga.com> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* Enforce a minimum SG_IO timeoutLinus Torvalds2008-12-051-0/+2
| | | | | | | | | | | | | | | | | | There's no point in having too short SG_IO timeouts, since if the command does end up timing out, we'll end up through the reset sequence that is several seconds long in order to abort the command that timed out. As a result, shorter timeouts than a few seconds simply do not make sense, as the recovery would be longer than the timeout itself. Add a BLK_MIN_SG_TIMEOUT to match the existign BLK_DEFAULT_SG_TIMEOUT. Suggested-by: Alan Cox <alan@lxorguk.ukuu.org.uk> Acked-by: Tejun Heo <tj@kernel.org> Acked-by: Jens Axboe <jens.axboe@oracle.com> Cc: Jeff Garzik <jeff@garzik.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* [PATCH] switch scsi_cmd_ioctl() to passing fmode_tAl Viro2008-10-211-5/+5
| | | | Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
* [PATCH] switch sg_scsi_ioctl() to passing fmode_tAl Viro2008-10-211-9/+4
| | | | Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
* [PATCH] pass mode instead of file to sg_io()Al Viro2008-10-211-8/+7
| | | | Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
* [PATCH] introduce fmode_t, do annotationsAl Viro2008-10-211-2/+3
| | | | Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
* block: introduce struct rq_map_data to use reserved pagesFUJITA Tomonori2008-10-091-2/+2
| | | | | | | | | | | | | | | | | | | | This patch introduces struct rq_map_data to enable bio_copy_use_iov() use reserved pages. Currently, bio_copy_user_iov allocates bounce pages but drivers/scsi/sg.c wants to allocate pages by itself and use them. struct rq_map_data can be used to pass allocated pages to bio_copy_user_iov. The current users of bio_copy_user_iov simply passes NULL (they don't want to use pre-allocated pages). Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Cc: Jens Axboe <jens.axboe@oracle.com> Cc: Douglas Gilbert <dougg@torque.net> Cc: Mike Christie <michaelc@cs.wisc.edu> Cc: James Bottomley <James.Bottomley@HansenPartnership.com> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: add gfp_mask argument to blk_rq_map_user and blk_rq_map_user_iovFUJITA Tomonori2008-10-091-2/+3
| | | | | | | | | | | | | | Currently, blk_rq_map_user and blk_rq_map_user_iov always do GFP_KERNEL allocation. This adds gfp_mask argument to blk_rq_map_user and blk_rq_map_user_iov so sg can use it (sg always does GFP_ATOMIC allocation). Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: Douglas Gilbert <dougg@torque.net> Cc: Mike Christie <michaelc@cs.wisc.edu> Cc: James Bottomley <James.Bottomley@HansenPartnership.com> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* SG_IO block filter whitelist missing MMC SET READ AHEAD commandxiphmont@xiph.org2008-10-091-0/+1
| | | | | | | | | | | | | | | | | | | | | I have another request for the block filter SG_IO command whitelist, specifically the MMC streaming command set SET READ AHEAD command. The command applies only to MMC CDROM/DVDROM drives with the streaming optional feature set. The command is useful to cdparanoia in that it allows explicit cache control side effects that are, on many drives, cdparanoia's most efficient way to flush/disable the media cache on cdrom drives. I am aware of no reason why it should not be accessible from usespace. Also note that the command is already fully accessible through the SCSI-native version of the SG_IO ioctl as well as the traditional SG interface. The command is only being refused on block devices. That means that on a typical stock distro, the command is available through /dev/sg* but not /dev/scd* although both are typically available and accessible. Filtering the command is not providing any protection, only a confusing inconsistency. Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: rename blk_scsi_cmd_filter to blk_cmd_filterFUJITA Tomonori2008-08-271-1/+1
| | | | | | | | | Technically, the cmd_filter would be applied to other protocols though it's unlikely to happen. Putting SCSI stuff to request_queue is kinda layer violation. So let's rename it. Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: move cmdfilter from gendisk to request_queueFUJITA Tomonori2008-08-271-3/+91
| | | | | | | | | | | | | | | | | | | | | | | | | | cmd_filter works only for the block layer SG_IO with SCSI block devices. It breaks scsi/sg.c, bsg, and the block layer SG_IO with SCSI character devices (such as st). We hit a kernel crash with them. The problem is that cmd_filter code accesses to gendisk (having struct blk_scsi_cmd_filter) via inode->i_bdev->bd_disk. It works for only SCSI block device files. With character device files, inode->i_bdev leads you to struct cdev. inode->i_bdev->bd_disk->blk_scsi_cmd_filter isn't safe. SCSI ULDs don't expose gendisk; they keep it private. bsg needs to be independent on any protocols. We shouldn't change ULDs to expose their gendisk. This patch moves struct blk_scsi_cmd_filter from gendisk to request_queue, a common object, which eveyone can access to. The user interface doesn't change; users can change the filters via /sys/block/. gendisk has a pointer to request_queue so the cmd_filter code accesses to struct blk_scsi_cmd_filter. Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* [SCSI] block: Fix miscalculation of sg_io timeout in CDROM_SEND_PACKET handler.Tim Wright2008-07-301-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | It seems cdrwtool in the udftools has been unusable on "modern" kernels for some time. A Google search reveals many people with the same issue but no solution (cdrwtool fails to format the disk). After spending some time tracking down the issue, it comes down to the following: The udftools still use the older CDROM_SEND_PACKET interface to send things like FORMAT_UNIT through to the drive. They should really be updated, but that's another story. Since most distros are using libata now, the cd or dvd burner appears as a SCSI device, and we wind up in block/scsi_ioctl.c. Here, the code tries to take the "struct cdrom_generic_command" and translate it and stuff it into a "struct sg_io_hdr" structure so it can pass it to the modern sg_io() routine instead. Unfortunately, there is one error, or rather an omission in the translation. The timeout that is passed in in the "struct cdrom_generic_command" is in HZ=100 units, and this is modified and correctly converted to jiffies by use of clock_t_to_jiffies(). However, a little further down, this cgc.timeout value in jiffies is simply copied into the sg_io_hdr timeout, which should be in milliseconds. Since most modern x86 kernels seems to be getting build with HZ=250, the timeout that is passed to sg_io and eventually converted to the timeout_per_command member of the scsi_cmnd structure is now four times too small. Since cdrwtool tries to set the timeout to one hour for the FORMAT_UNIT command, and it takes about 20 minutes to format a 4x CDRW, the SCSI error-handler kicks in after the FORMAT_UNIT completes because it took longer than the incorrectly-calculated timeout. [jejb: fix up whitespace] Signed-off-by: Tim Wright <timw@splhi.com> Cc: Stable Tree <stable@kernel.org> Signed-off-by: James Bottomley <James.Bottomley@HansenPartnership.com>
* allow userspace to modify scsi command filter on per device basisAdel Gadllah2008-07-031-116/+5
| | | | | | | | | | | | This patch exports the per-gendisk command filter to user space through sysfs, so it can be changed by the system administrator. All users of the old cmd filter have been converted to use the new one. Original patch from Peter Jones. Signed-off-by: Adel Gadllah <adel.gadllah@gmail.com> Signed-off-by: Peter Jones <pjones@redhat.com> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* Merge git://git.kernel.org/pub/scm/linux/kernel/git/jejb/scsi-misc-2.6Linus Torvalds2008-05-021-3/+2
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | * git://git.kernel.org/pub/scm/linux/kernel/git/jejb/scsi-misc-2.6: [SCSI] aic94xx: fix section mismatch [SCSI] u14-34f: Fix 32bit only problem [SCSI] dpt_i2o: sysfs code [SCSI] dpt_i2o: 64 bit support [SCSI] dpt_i2o: move from virt_to_bus/bus_to_virt to dma_alloc_coherent [SCSI] dpt_i2o: use standard __init / __exit code [SCSI] megaraid_sas: fix suspend/resume sections [SCSI] aacraid: Add Power Management support [SCSI] aacraid: Fix jbod operations scan issues [SCSI] aacraid: Fix warning about macro side-effects [SCSI] add support for variable length extended commands [SCSI] Let scsi_cmnd->cmnd use request->cmd buffer [SCSI] bsg: add large command support [SCSI] aacraid: Fix down_interruptible() to check the return value correctly [SCSI] megaraid_sas; Update the Version and Changelog [SCSI] ibmvscsi: Handle non SCSI error status [SCSI] bug fix for free list handling [SCSI] ipr: Rename ipr's state scsi host attribute to prevent collisions [SCSI] megaraid_mbox: fix Dell CERC firmware problem
| * [SCSI] add support for variable length extended commandsBoaz Harrosh2008-05-021-3/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Add support for variable-length, extended, and vendor specific CDBs to scsi-ml. It is now possible for initiators and ULD's to issue these types of commands. LLDs need not change much. All they need is to raise the .max_cmd_len to the longest command they support (see iscsi patch). - clean-up some code paths that did not expect commands to be larger than 16, and change cmd_len members' type to short as char is not enough. Signed-off-by: Boaz Harrosh <bharrosh@panasas.com> Signed-off-by: Benny Halevy <bhalevy@panasas.com> Signed-off-by: James Bottomley <James.Bottomley@HansenPartnership.com>
* | block: no need to initialize rq->cmd with blk_get_requestFUJITA Tomonori2008-04-291-3/+0
|/ | | | | | | | | | | | | | | | blk_get_request initializes rq->cmd (rq_init does) so the users don't need to do that. The purpose of this patch is to remove sizeof(rq->cmd) and &rq->cmd, as a preparation for large command support, which changes rq->cmd from the static array to a pointer. sizeof(rq->cmd) will not make sense and &rq->cmd won't work. Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Cc: James Bottomley <James.Bottomley@HansenPartnership.com> Cc: Alasdair G Kergon <agk@redhat.com> Cc: Jens Axboe <jens.axboe@oracle.com> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: restore the meaning of rq->data_len to the true data lengthFUJITA Tomonori2008-03-041-2/+2
| | | | | | | | | | | | | | | | | | The meaning of rq->data_len was changed to the length of an allocated buffer from the true data length. It breaks SG_IO friends and bsg. This patch restores the meaning of rq->data_len to the true data length and adds rq->extra_len to store an extended length (due to drain buffer and padding). This patch also removes the code to update bio in blk_rq_map_user introduced by the commit 40b01b9bbdf51ae543a04744283bf2d56c4a6afa. The commit adjusts bio according to memory alignment (queue_dma_alignment). However, memory alignment is NOT padding alignment. This adjustment also breaks SG_IO friends and bsg. Padding alignment needs to be fixed in a proper way (by a separate patch). Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: Jens Axboe <axboe@carl.home.kernel.dk>
* block: add request->raw_data_lenTejun Heo2008-02-191-1/+2
| | | | | | | | | | | | | | | | | | | | | | | With padding and draining moved into it, block layer now may extend requests as directed by queue parameters, so now a request has two sizes - the original request size and the extended size which matches the size of area pointed to by bios and later by sgs. The latter size is what lower layers are primarily interested in when allocating, filling up DMA tables and setting up the controller. Both padding and draining extend the data area to accomodate controller characteristics. As any controller which speaks SCSI can handle underflows, feeding larger data area is safe. So, this patch makes the primary data length field, request->data_len, indicate the size of full data area and add a separate length field, request->raw_data_len, for the unmodified request size. The latter is used to report to higher layer (userland) and where the original request size should be fed to the controller or device. Signed-off-by: Tejun Heo <htejun@gmail.com> Cc: James Bottomley <James.Bottomley@HansenPartnership.com> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: use jiffies conversion functions in scsi_ioctl.cTejun Heo2007-12-181-2/+2
| | | | | | | | | Use msecs_to_jiffies() and jiffies_to_msecs() in scsi_ioctl(). Sometimes callers use very large values for e.g. vendor specific media clear command and calculation can overflow. Signed-off-by: Tejun Heo <htejun@gmail.com> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* [BLOCK] Get rid of request_queue_t typedefJens Axboe2007-07-241-11/+13
| | | | | | | | | Some of the code has been gradually transitioned to using the proper struct request_queue, but there's lots left. So do a full sweet of the kernel and get rid of this typedef and replace its uses with the proper type. Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* Merge master.kernel.org:/pub/scm/linux/kernel/git/jejb/scsi-misc-2.6Linus Torvalds2007-07-221-8/+5
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | * master.kernel.org:/pub/scm/linux/kernel/git/jejb/scsi-misc-2.6: (60 commits) [SCSI] libsas: make ATA functions selectable by a config option [SCSI] bsg: unexport sg v3 helper functions [SCSI] bsg: fix bsg_unregister_queue [SCSI] bsg: make class backlinks [SCSI] 3w-9xxx: add support for 9690SA [SCSI] bsg: fix bsg_register_queue error path [SCSI] ESP: Increase ESP_BUS_TIMEOUT to 275. [SCSI] libsas: fix scr_read/write users and update the libata documentation [SCSI] mpt fusion: update Kconfig help [SCSI] scsi_transport_sas: add destructor for bsg [SCSI] iscsi_tcp: buggered kmalloc() [SCSI] qla2xxx: Update version number to 8.02.00-k2. [SCSI] qla2xxx: Add ISP25XX support. [SCSI] qla2xxx: Use pci_try_set_mwi(). [SCSI] qla2xxx: Use PCI-X/PCI-Express read control interfaces. [SCSI] qla2xxx: Re-factor isp_operations to static structures. [SCSI] qla2xxx: Validate mid-layer 'underflow' during check-condition handling. [SCSI] qla2xxx: Correct setting of 'current' and 'supported' speeds during FDMI registration. [SCSI] qla2xxx: Generalize iIDMA support. [SCSI] qla2xxx: Generalize FW-Interface-2 support. ...
| * [SCSI] bsg: unexport sg v3 helper functionsFUJITA Tomonori2007-07-221-8/+5
| | | | | | | | | | | | | | | | blk_fill_sghdr_rq, blk_unmap_sghdr_rq, and blk_complete_sghdr_rq were exported for bsg, however bsg was changed to support only sg v4. Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: James Bottomley <James.Bottomley@SteelEye.com>
* | some kmalloc/memset ->kzalloc (tree wide)Yoann Padioleau2007-07-191-2/+1
|/ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Transform some calls to kmalloc/memset to a single kzalloc (or kcalloc). Here is a short excerpt of the semantic patch performing this transformation: @@ type T2; expression x; identifier f,fld; expression E; expression E1,E2; expression e1,e2,e3,y; statement S; @@ x = - kmalloc + kzalloc (E1,E2) ... when != \(x->fld=E;\|y=f(...,x,...);\|f(...,x,...);\|x=E;\|while(...) S\|for(e1;e2;e3) S\) - memset((T2)x,0,E1); @@ expression E1,E2,E3; @@ - kzalloc(E1 * E2,E3) + kcalloc(E1,E2,E3) [akpm@linux-foundation.org: get kcalloc args the right way around] Signed-off-by: Yoann Padioleau <padator@wanadoo.fr> Cc: Richard Henderson <rth@twiddle.net> Cc: Ivan Kokshaysky <ink@jurassic.park.msu.ru> Acked-by: Russell King <rmk@arm.linux.org.uk> Cc: Bryan Wu <bryan.wu@analog.com> Acked-by: Jiri Slaby <jirislaby@gmail.com> Cc: Dave Airlie <airlied@linux.ie> Acked-by: Roland Dreier <rolandd@cisco.com> Cc: Jiri Kosina <jkosina@suse.cz> Acked-by: Dmitry Torokhov <dtor@mail.ru> Cc: Benjamin Herrenschmidt <benh@kernel.crashing.org> Acked-by: Mauro Carvalho Chehab <mchehab@infradead.org> Acked-by: Pierre Ossman <drzeus-list@drzeus.cx> Cc: Jeff Garzik <jeff@garzik.org> Cc: "David S. Miller" <davem@davemloft.net> Acked-by: Greg KH <greg@kroah.com> Cc: James Bottomley <James.Bottomley@steeleye.com> Cc: "Antonino A. Daplas" <adaplas@pol.net> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* bsg: add a request_queue argument to scsi_cmd_ioctl()FUJITA Tomonori2007-07-161-7/+3
| | | | | | | | | | | | bsg uses scsi_cmd_ioctl() for some SCSI/sg ioctl commands. scsi_cmd_ioctl() gets a request queue from a gendisk arguement. This prevents bsg being bound to SCSI devices that don't have a gendisk (like OSD). This adds a request_queue argument to scsi_cmd_ioctl(). The SCSI/sg ioctl commands doesn't use a gendisk so it's safe for any SCSI devices to use scsi_cmd_ioctl(). Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: export blk_verify_command for SG v4FUJITA Tomonori2007-07-161-3/+4
| | | | | | | | blk_fill_sghdr_rq doesn't work for SG v4 so verify_command needed to be exported. Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* block: changes for blk_rq_unmap_user new APIFUJITA Tomonori2007-07-161-12/+1
| | | | | | | | | This converts block/scsi_ioctl.c use blk_rq_unmap_user new API. blk_unmap_sghdr_rq is too simple and it might be better to remove it. Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* bsg: support for full generic block layer SG v3Jens Axboe2007-07-161-61/+102
| | | | Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* [SCSI] sg: cap reserved_size values at max_sectorsAlan Stern2007-04-171-1/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | This patch (as857) modifies the SG_GET_RESERVED_SIZE and SG_SET_RESERVED_SIZE ioctls in the sg driver, capping the values at the device's request_queue's max_sectors value. This will permit cdrecord to obtain a legal value for the maximum transfer length, fixing Bugzilla #7026. The patch also caps the initial reserved_size value. There's no reason to have a reserved buffer larger than max_sectors, since it would be impossible to use the extra space. The corresponding ioctls in the block layer are modified similarly, and the initial value for the reserved_size is set as large as possible. This will effectively make it default to max_sectors. Note that the actual value is meaningless anyway, since block devices don't have a reserved buffer. Finally, the BLKSECTGET ioctl is added to sg, so that there will be a uniform way for users to determine the actual max_sectors value for any raw SCSI transport. Signed-off-by: Alan Stern <stern@rowland.harvard.edu> Acked-by: Jens Axboe <jens.axboe@oracle.com> Acked-by: Douglas Gilbert <dougg@torque.net> Signed-off-by: James Bottomley <James.Bottomley@SteelEye.com>
* [PATCH] Fix SG_IO timeout jiffy conversionMike Christie2007-01-291-2/+3
| | | | | | | | | | | | | | Commit 85e04e371b5a321b5df2bc3f8e0099a64fb087d7 cleaned up the timeout conversion, but did it exactly the wrong way. We get msecs from user space, and should convert them into jiffies. Not the other way around. Here is a fix with the overflow check sg.c has added in. This fixes DVD burnign with Nero. Signed-off-by: Mike Christie <michaelc@cs.wisc.edu> [ "you'll be wanting a comma there" - Andrew ] Cc: Andrew Morton <akpm@osdl.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* [PATCH] Fixup blk_rq_unmap_user() APIJens Axboe2006-12-191-2/+1
| | | | | | | | | The blk_rq_unmap_user() API is not very nice. It expects the caller to know that rq->bio has to be reset to the original bio, and it will silently do nothing if that is not done. Instead make it explicit that we need to pass in the first bio, by expecting a bio argument. Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* [PATCH] remove unnecessary blk_queue_bounce in SG_IOFUJITA Tomonori2006-12-121-7/+0
| | | | | | | | | When I converted the original patch, I left unnecessary blk_queue_bounce in SG_IO. Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: Mike Christie <michaelc@cs.wisc.edu> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* [PATCH] fix SG_IO bio leakFUJITA Tomonori2006-12-121-0/+3
| | | | | | | | | | This patch fixes bio leaks in SG_IO. rq->bio can be changed after io completion, so we need to reset rq->bio before calling blk_rq_unmap_user() http://marc.theaimsgroup.com/?l=linux-kernel&m=116570666807983&w=2 Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp> Signed-off-by: Jens Axboe <jens.axboe@oracle.com>
* Merge master.kernel.org:/pub/scm/linux/kernel/git/jejb/scsi-misc-2.6Linus Torvalds2006-12-051-1/+1
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | * master.kernel.org:/pub/scm/linux/kernel/git/jejb/scsi-misc-2.6: (73 commits) [SCSI] aic79xx: Add ASC-29320LPE ids to driver [SCSI] stex: version update [SCSI] stex: change wait loop code [SCSI] stex: add new device type support [SCSI] stex: update device id info [SCSI] stex: adjust default queue length [SCSI] stex: add value check in hard reset routine [SCSI] stex: fix controller_info command handling [SCSI] stex: fix biosparam calculation [SCSI] megaraid: fix MMIO casts [SCSI] tgt: fix undefined flush_dcache_page() problem [SCSI] libsas: better error handling in sas_expander.c [SCSI] lpfc 8.1.11 : Change version number to 8.1.11 [SCSI] lpfc 8.1.11 : Misc Fixes [SCSI] lpfc 8.1.11 : Add soft_wwnn sysfs attribute, rename soft_wwn_enable [SCSI] lpfc 8.1.11 : Removed decoding of PCI Subsystem Id [SCSI] lpfc 8.1.11 : Add MSI (Message Signalled Interrupts) support [SCSI] lpfc 8.1.11 : Adjust LOG_FCP logging [SCSI] lpfc 8.1.11 : Fix Memory leaks [SCSI] lpfc 8.1.11 : Fix lpfc_multi_ring_support ...
| * Merge ../scsi-rc-fixes-2.6James Bottomley2006-11-221-3/+2
| |\
| * | [SCSI] block: convert jiffies to msecs in scsi_ioctl()Hannes Reinecke2006-11-151-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | Use the proper conversion function for convert jiffies to msecs in sg_io(). Signed-off-by: Hannes Reinecke <hare@suse.de> Signed-off-by: James Bottomley <James.Bottomley@SteelEye.com>