aboutsummaryrefslogtreecommitdiffstats
path: root/block
Commit message (Collapse)AuthorAgeFilesLines
* block: genhd: Add disk/partition specific uevent callbacks for partition infoSan Mehat2013-02-192-0/+28
| | | | | | | | | For disk devices, a new uevent parameter 'NPARTS' specifies the number of partitions detected by the kernel. Partition devices get 'PARTN' which specifies the partitions index in the table, and 'PARTNAME', which specifies PARTNAME specifices the partition name of a partition device Signed-off-by: Dima Zavin <dima@android.com>
* block: prevent race/cleanupDerek Basehore2012-12-191-15/+30
| | | | | | | | | | | | | | | | | | | | | | Remove a race condition which causes a warning in disk_clear_events. This is a race between disk_clear_events() and disk_flush_events(). ev->clearing will be altered by disk_flush_events() even though we are blocking event checking through disk_flush_events(). If this happens after ev->clearing was cleared for disk_clear_events(), this can cause the WARN_ON_ONCE() in that function to be triggered. This change also has disk_clear_events() not go through a workqueue. Since we have to wait for the work to complete, we should just call the function directly. Also, since this work cannot be put on a freezable workqueue, it will have to contend with increased demand, so calling the function directly avoids this. [akpm@linux-foundation.org: fix spello in comment] Signed-off-by: Derek Basehore <dbasehore@chromium.org> Cc: Mandeep Singh Baines <msb@chromium.org> Cc: Jens Axboe <axboe@kernel.dk> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
* block: remove deadlock in disk_clear_eventsDerek Basehore2012-12-191-1/+8
| | | | | | | | | | | | | | | | | | | | | | | | | | | In disk_clear_events, do not put work on system_nrt_freezable_wq. Instead, put it on system_nrt_wq. There is a race between probing a usb and suspending the device. Since probing a usb calls disk_clear_events, which puts work on a frozen workqueue, probing cannot finish after the workqueue is frozen. However, suspending cannot finish until the usb probe is finished, so we get a deadlock, causing the system to reboot. The way to reproduce this bug is to wake up from suspend with a usb storage device plugged in, or plugging in a usb storage device right before suspend. The window of time is on the order of time it takes to probe the usb device. As long as the workqueues are frozen before the call to add_disk within sd_probe_async finishes, there will be a deadlock (which calls blkdev_get, sd_open, check_disk_change, then disk_clear_events). This is not difficult to reproduce after figuring out the timings. [akpm@linux-foundation.org: fix up comment] Signed-off-by: Derek Basehore <dbasehore@chromium.org> Reviewed-by: Mandeep Singh Baines <msb@chromium.org> Cc: Jens Axboe <axboe@kernel.dk> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
* Merge branch 'akpm' (Andrew's patch-bomb)Linus Torvalds2012-12-171-0/+1
|\ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Merge misc patches from Andrew Morton: "Incoming: - lots of misc stuff - backlight tree updates - lib/ updates - Oleg's percpu-rwsem changes - checkpatch - rtc - aoe - more checkpoint/restart support I still have a pile of MM stuff pending - Pekka should be merging later today after which that is good to go. A number of other things are twiddling thumbs awaiting maintainer merges." * emailed patches from Andrew Morton <akpm@linux-foundation.org>: (180 commits) scatterlist: don't BUG when we can trivially return a proper error. docs: update documentation about /proc/<pid>/fdinfo/<fd> fanotify output fs, fanotify: add @mflags field to fanotify output docs: add documentation about /proc/<pid>/fdinfo/<fd> output fs, notify: add procfs fdinfo helper fs, exportfs: add exportfs_encode_inode_fh() helper fs, exportfs: escape nil dereference if no s_export_op present fs, epoll: add procfs fdinfo helper fs, eventfd: add procfs fdinfo helper procfs: add ability to plug in auxiliary fdinfo providers tools/testing/selftests/kcmp/kcmp_test.c: print reason for failure in kcmp_test breakpoint selftests: print failure status instead of cause make error kcmp selftests: print fail status instead of cause make error kcmp selftests: make run_tests fix mem-hotplug selftests: print failure status instead of cause make error cpu-hotplug selftests: print failure status instead of cause make error mqueue selftests: print failure status instead of cause make error vm selftests: print failure status instead of cause make error ubifs: use prandom_bytes mtd: nandsim: use prandom_bytes ...
| * percpu_rw_semaphore: introduce CONFIG_PERCPU_RWSEMOleg Nesterov2012-12-171-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Currently only block_dev and uprobes use percpu_rw_semaphore, add the config option selected by BLOCK || UPROBES. Signed-off-by: Oleg Nesterov <oleg@redhat.com> Cc: Anton Arapov <anton@redhat.com> Cc: Ingo Molnar <mingo@elte.hu> Cc: Linus Torvalds <torvalds@linux-foundation.org> Cc: Michal Marek <mmarek@suse.cz> Cc: Mikulas Patocka <mpatocka@redhat.com> Cc: "Paul E. McKenney" <paulmck@linux.vnet.ibm.com> Cc: Peter Zijlstra <peterz@infradead.org> Cc: Srikar Dronamraju <srikar@linux.vnet.ibm.com> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* | Merge branch 'for-3.8/drivers' of git://git.kernel.dk/linux-blockLinus Torvalds2012-12-173-15/+21
|\ \ | |/ |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull block driver update from Jens Axboe: "Now that the core bits are in, here are the driver bits for 3.8. The branch contains: - A huge pile of drbd bits that were dumped from the 3.7 merge window. Following that, it was both made perfectly clear that there is going to be no more over-the-wall pulls and how the situation on individual pulls can be improved. - A few cleanups from Akinobu Mita for drbd and cciss. - Queue improvement for loop from Lukas. This grew into adding a generic interface for waiting/checking an even with a specific lock, allowing this to be pulled out of md and now loop and drbd is also using it. - A few fixes for xen back/front block driver from Roger Pau Monne. - Partition improvements from Stephen Warren, allowing partiion UUID to be used as an identifier." * 'for-3.8/drivers' of git://git.kernel.dk/linux-block: (609 commits) drbd: update Kconfig to match current dependencies drbd: Fix drbdsetup wait-connect, wait-sync etc... commands drbd: close race between drbd_set_role and drbd_connect drbd: respect no-md-barriers setting also when changed online via disk-options drbd: Remove obsolete check drbd: fixup after wait_even_lock_irq() addition to generic code loop: Limit the number of requests in the bio list wait: add wait_event_lock_irq() interface xen-blkfront: free allocated page xen-blkback: move free persistent grants code block: partition: msdos: provide UUIDs for partitions init: reduce PARTUUID min length to 1 from 36 block: store partition_meta_info.uuid as a string cciss: use check_signature() cciss: cleanup bitops usage drbd: use copy_highpage drbd: if the replication link breaks during handshake, keep retrying drbd: check return of kmalloc in receive_uuids drbd: Broadcast sync progress no more often than once per second drbd: don't try to clear bits once the disk has failed ...
| * block: partition: msdos: provide UUIDs for partitionsStephen Warren2012-11-231-2/+19
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The MSDOS/MBR partition table includes a 32-bit unique ID, often referred to as the NT disk signature. When combined with a partition number within the table, this can form a unique ID similar in concept to EFI/GPT's partition UUID. Constructing and recording this value in struct partition_meta_info allows MSDOS partitions to be referred to on the kernel command-line using the following syntax: root=PARTUUID=0002dd75-01 Signed-off-by: Stephen Warren <swarren@nvidia.com> Cc: Tejun Heo <tj@kernel.org> Cc: Will Drewry <wad@chromium.org> Cc: Kay Sievers <kay.sievers@vrfy.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * block: store partition_meta_info.uuid as a stringStephen Warren2012-11-232-13/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This will allow other types of UUID to be stored here, aside from true UUIDs. This also simplifies code that uses this field, since it's usually constructed from a, used as a, or compared to other, strings. Note: A simplistic approach here would be to set uuid_str[36]=0 whenever a /PARTNROFF option was found to be present. However, this modifies the input string, and causes subsequent calls to devt_from_partuuid() not to see the /PARTNROFF option, which causes different results. In order to avoid misleading future maintainers, this parameter is marked const. Signed-off-by: Stephen Warren <swarren@nvidia.com> Cc: Tejun Heo <tj@kernel.org> Cc: Will Drewry <wad@chromium.org> Cc: Kay Sievers <kay.sievers@vrfy.org> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
* | Merge branch 'for-3.8/core' of git://git.kernel.dk/linux-blockLinus Torvalds2012-12-1714-93/+122
|\ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull block layer core updates from Jens Axboe: "Here are the core block IO bits for 3.8. The branch contains: - The final version of the surprise device removal fixups from Bart. - Don't hide EFI partitions under advanced partition types. It's fairly wide spread these days. This is especially dangerous for systems that have both msdos and efi partition tables, where you want to keep them in sync. - Cleanup of using -1 instead of the proper NUMA_NO_NODE - Export control of bdi flusher thread CPU mask and default to using the home node (if known) from Jeff. - Export unplug tracepoint for MD. - Core improvements from Shaohua. Reinstate the recursive merge, as the original bug has been fixed. Add plugging for discard and also fix a problem handling non pow-of-2 discard limits. There's a trivial merge in block/blk-exec.c due to a fix that went into 3.7-rc at a later point than -rc4 where this is based." * 'for-3.8/core' of git://git.kernel.dk/linux-block: block: export block_unplug tracepoint block: add plug for blkdev_issue_discard block: discard granularity might not be power of 2 deadline: Allow 0ms deadline latency, increase the read speed partitions: enable EFI/GPT support by default bsg: Remove unused function bsg_goose_queue() block: Make blk_cleanup_queue() wait until request_fn finished block: Avoid scheduling delayed work on a dead queue block: Avoid that request_fn is invoked on a dead queue block: Let blk_drain_queue() caller obtain the queue lock block: Rename queue dead flag bdi: add a user-tunable cpu_list for the bdi flusher threads block: use NUMA_NO_NODE instead of -1 block: recursive merge requests block CFQ: avoid moving request to different queue
| * | block: export block_unplug tracepointNeilBrown2012-12-141-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | This allows stacked devices (like md/raid5) to provide blktrace tracing, including unplug events. Reported-by: Fengguang Wu <fengguang.wu@intel.com> Signed-off-by: NeilBrown <neilb@suse.de> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: add plug for blkdev_issue_discardShaohua Li2012-12-141-0/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Last post of this patch appears lost, so I resend this. Now discard merge works, add plug for blkdev_issue_discard. This will help discard request merge especially for raid0 case. In raid0, a big discard request is split to small requests, and if correct plug is added, such small requests can be merged in low layer. Signed-off-by: Shaohua Li <shli@fusionio.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: discard granularity might not be power of 2Shaohua Li2012-12-142-13/+16
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | In MD raid case, discard granularity might not be power of 2, for example, a 4-disk raid5 has 3*chunk_size discard granularity. Correct the calculation for such cases. Reported-by: Neil Brown <neilb@suse.de> Signed-off-by: Shaohua Li <shli@fusionio.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | deadline: Allow 0ms deadline latency, increase the read speedxiaobing tu2012-12-091-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | Change a timer compare from after to after-equals, thus allowing 0 timeout and making deadline schedule FIFO. Signed-off-by: xiaobing tu <xiaobing.tu@intel.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | partitions: enable EFI/GPT support by defaultDiego Calleja2012-12-061-2/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The Kconfig currently enables MSDOS partitions by default because they are assumed to be essential, but it's necessary to enable "advanced partition selection" in order to get GPT support. IMO GPT partitions are becoming common enought to deserve the same treatment MSDOS partitions get. (Side note: I got bit by a disk that had MSDOS and GPT partition tables, but for some reason the MSDOS table was different from the GPT one. I was stupid enought to disable "advanced partition selection" in my .config, which disabled GPT partitioning and made my btrfs pool unbootable because it couldn't find the partitions) Signed-off-by: Diego Calleja <diegocg@gmail.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | bsg: Remove unused function bsg_goose_queue()Bart Van Assche2012-12-061-13/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | The function bsg_goose_queue() does not have any in-tree callers, so let's remove it. Signed-off-by: Bart Van Assche <bvanassche@acm.org> Acked-by: Tejun Heo <tj@kernel.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Make blk_cleanup_queue() wait until request_fn finishedBart Van Assche2012-12-061-0/+10
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Some request_fn implementations, e.g. scsi_request_fn(), unlock the queue lock internally. This may result in multiple threads executing request_fn for the same queue simultaneously. Keep track of the number of active request_fn calls and make sure that blk_cleanup_queue() waits until all active request_fn invocations have finished. A block driver may start cleaning up resources needed by its request_fn as soon as blk_cleanup_queue() finished, so blk_cleanup_queue() must wait for all outstanding request_fn invocations to finish. Signed-off-by: Bart Van Assche <bvanassche@acm.org> Reported-by: Chanho Min <chanho.min@lge.com> Cc: James Bottomley <JBottomley@Parallels.com> Cc: Mike Christie <michaelc@cs.wisc.edu> Acked-by: Tejun Heo <tj@kernel.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Avoid scheduling delayed work on a dead queueBart Van Assche2012-12-061-24/+9
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Running a queue must continue after it has been marked dying until it has been marked dead. So the function blk_run_queue_async() must not schedule delayed work after blk_cleanup_queue() has marked a queue dead. Hence add a test for that queue state in blk_run_queue_async() and make sure that queue_unplugged() invokes that function with the queue lock held. This avoids that the queue state can change after it has been tested and before mod_delayed_work() is invoked. Drop the queue dying test in queue_unplugged() since it is now superfluous: __blk_run_queue() already tests whether or not the queue is dead. Signed-off-by: Bart Van Assche <bvanassche@acm.org> Cc: Mike Christie <michaelc@cs.wisc.edu> Acked-by: Tejun Heo <tj@kernel.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Avoid that request_fn is invoked on a dead queueBart Van Assche2012-12-063-5/+30
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | A block driver may start cleaning up resources needed by its request_fn as soon as blk_cleanup_queue() finished, so request_fn must not be invoked after draining finished. This is important when blk_run_queue() is invoked without any requests in progress. As an example, if blk_drain_queue() and scsi_run_queue() run in parallel, blk_drain_queue() may have finished all requests after scsi_run_queue() has taken a SCSI device off the starved list but before that last function has had a chance to run the queue. Signed-off-by: Bart Van Assche <bvanassche@acm.org> Cc: James Bottomley <JBottomley@Parallels.com> Cc: Mike Christie <michaelc@cs.wisc.edu> Cc: Chanho Min <chanho.min@lge.com> Acked-by: Tejun Heo <tj@kernel.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Let blk_drain_queue() caller obtain the queue lockBart Van Assche2012-12-061-12/+18
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Let the caller of blk_drain_queue() obtain the queue lock to improve readability of the patch called "Avoid that request_fn is invoked on a dead queue". Signed-off-by: Bart Van Assche <bvanassche@acm.org> Acked-by: Tejun Heo <tj@kernel.org> Cc: James Bottomley <JBottomley@Parallels.com> Cc: Mike Christie <michaelc@cs.wisc.edu> Cc: Jens Axboe <axboe@kernel.dk> Cc: Chanho Min <chanho.min@lge.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Rename queue dead flagBart Van Assche2012-12-066-19/+19
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | QUEUE_FLAG_DEAD is used to indicate that queuing new requests must stop. After this flag has been set queue draining starts. However, during the queue draining phase it is still safe to invoke the queue's request_fn, so QUEUE_FLAG_DYING is a better name for this flag. This patch has been generated by running the following command over the kernel source tree: git grep -lEw 'blk_queue_dead|QUEUE_FLAG_DEAD' | xargs sed -i.tmp -e 's/blk_queue_dead/blk_queue_dying/g' \ -e 's/QUEUE_FLAG_DEAD/QUEUE_FLAG_DYING/g'; \ sed -i.tmp -e "s/QUEUE_FLAG_DYING$(printf \\t)*5/QUEUE_FLAG_DYING$(printf \\t)5/g" \ include/linux/blkdev.h; \ sed -i.tmp -e 's/ DEAD/ DYING/g' -e 's/dead queue/a dying queue/' \ -e 's/Dead queue/A dying queue/' block/blk-core.c Signed-off-by: Bart Van Assche <bvanassche@acm.org> Acked-by: Tejun Heo <tj@kernel.org> Cc: James Bottomley <JBottomley@Parallels.com> Cc: Mike Christie <michaelc@cs.wisc.edu> Cc: Jens Axboe <axboe@kernel.dk> Cc: Chanho Min <chanho.min@lge.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: use NUMA_NO_NODE instead of -1Ezequiel Garcia2012-11-102-3/+3
| | | | | | | | | | | | | | | | | | | | | | | | Signed-off-by: Ezequiel Garcia <elezegarcia@gmail.com> Modified by me to cover blk_init_queue() as well. Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: recursive merge requestsShaohua Li2012-11-091-4/+12
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | In a workload, thread 1 accesses a, a+2, ..., thread 2 accesses a+1, a+3,.... When the requests are flushed to queue, a and a+1 are merged to (a, a+1), a+2 and a+3 too to (a+2, a+3), but (a, a+1) and (a+2, a+3) aren't merged. If we do recursive merge for such interleave access, some workloads throughput get improvement. A recent worload I'm checking on is swap, below change boostes the throughput around 5% ~ 10%. Signed-off-by: Shaohua Li <shli@fusionio.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block CFQ: avoid moving request to different queueShaohua Li2012-11-061-1/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | request is queued in cfqq->fifo list. Looks it's possible we are moving a request from one cfqq to another in request merge case. In such case, adjusting the fifo list order doesn't make sense and is impossible if we don't iterate the whole fifo list. My test does hit one case the two cfqq are different, but didn't cause kernel crash, maybe it's because fifo list isn't used frequently. Anyway, from the code logic, this is buggy. I thought we can re-enable the recusive merge logic after this is fixed. Signed-off-by: Shaohua Li <shli@fusionio.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
* | | Merge branch 'for-3.8' of ↵Linus Torvalds2012-12-121-8/+7
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/tj/cgroup Pull cgroup changes from Tejun Heo: "A lot of activities on cgroup side. The big changes are focused on making cgroup hierarchy handling saner. - cgroup_rmdir() had peculiar semantics - it allowed cgroup destruction to be vetoed by individual controllers and tried to drain refcnt synchronously. The vetoing never worked properly and caused good deal of contortions in cgroup. memcg was the last reamining user. Michal Hocko removed the usage and cgroup_rmdir() path has been simplified significantly. This was done in a separate branch so that the memcg people can base further memcg changes on top. - The above allowed cleaning up cgroup lifecycle management and implementation of generic cgroup iterators which are used to improve hierarchy support. - cgroup_freezer updated to allow migration in and out of a frozen cgroup and handle hierarchy. If a cgroup is frozen, all descendant cgroups are frozen. - netcls_cgroup and netprio_cgroup updated to handle hierarchy properly. - Various fixes and cleanups. - Two merge commits. One to pull in memcg and rmdir cleanups (needed to build iterators). The other pulled in cgroup/for-3.7-fixes for device_cgroup fixes so that further device_cgroup patches can be stacked on top." Fixed up a trivial conflict in mm/memcontrol.c as per Tejun (due to commit bea8c150a7 ("memcg: fix hotplugged memory zone oops") in master touching code close to commit 2ef37d3fe4 ("memcg: Simplify mem_cgroup_force_empty_list error handling") in for-3.8) * 'for-3.8' of git://git.kernel.org/pub/scm/linux/kernel/git/tj/cgroup: (65 commits) cgroup: update Documentation/cgroups/00-INDEX cgroup_rm_file: don't delete the uncreated files cgroup: remove subsystem files when remounting cgroup cgroup: use cgroup_addrm_files() in cgroup_clear_directory() cgroup: warn about broken hierarchies only after css_online cgroup: list_del_init() on removed events cgroup: fix lockdep warning for event_control cgroup: move list add after list head initilization netprio_cgroup: allow nesting and inherit config on cgroup creation netprio_cgroup: implement netprio[_set]_prio() helpers netprio_cgroup: use cgroup->id instead of cgroup_netprio_state->prioidx netprio_cgroup: reimplement priomap expansion netprio_cgroup: shorten variable names in extend_netdev_table() netprio_cgroup: simplify write_priomap() netcls_cgroup: move config inheritance to ->css_online() and remove .broken_hierarchy marking cgroup: remove obsolete guarantee from cgroup_task_migrate. cgroup: add cgroup->id cgroup, cpuset: remove cgroup_subsys->post_clone() cgroup: s/CGRP_CLONE_CHILDREN/CGRP_CPUSET_CLONE_CHILDREN/ cgroup: rename ->create/post_create/pre_destroy/destroy() to ->css_alloc/online/offline/free() ...
| * | | cgroup: rename ->create/post_create/pre_destroy/destroy() to ↵Tejun Heo2012-11-191-7/+7
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | ->css_alloc/online/offline/free() Rename cgroup_subsys css lifetime related callbacks to better describe what their roles are. Also, update documentation. Signed-off-by: Tejun Heo <tj@kernel.org> Acked-by: Li Zefan <lizefan@huawei.com>
| * | | Merge branch 'cgroup/for-3.7-fixes' into cgroup/for-3.8Tejun Heo2012-11-063-2/+13
| |\| | | | | | | | | | | | | | | | | | | | | | | | | | This is to receive device_cgroup fixes so that further device_cgroup changes can be made in cgroup/for-3.8. Signed-off-by: Tejun Heo <tj@kernel.org>
| * | | Merge branch 'cgroup-rmdir-updates' into cgroup/for-3.8Tejun Heo2012-11-051-2/+1
| |\ \ \ | | |_|/ | |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull rmdir updates into for-3.8 so that further callback updates can be put on top. This pull created a trivial conflict between the following two commits. 8c7f6edbda ("cgroup: mark subsystems with broken hierarchy support and whine if cgroups are nested for them") ed95779340 ("cgroup: kill cgroup_subsys->__DEPRECATED_clear_css_refs") The former added a field to cgroup_subsys and the latter removed one from it. They happen to be colocated causing the conflict. Keeping what's added and removing what's removed resolves the conflict. Signed-off-by: Tejun Heo <tj@kernel.org>
| | * | cgroup: make ->pre_destroy() return voidTejun Heo2012-11-051-2/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | All ->pre_destory() implementations return 0 now, which is the only allowed return value. Make it return void. Signed-off-by: Tejun Heo <tj@kernel.org> Reviewed-by: Michal Hocko <mhocko@suse.cz> Acked-by: KAMEZAWA Hiroyuki <kamezawa.hiroyu@jp.fujitsu.com> Acked-by: Li Zefan <lizefan@huawei.com> Cc: Balbir Singh <bsingharora@gmail.com> Cc: Vivek Goyal <vgoyal@redhat.com>
* | | | block: Don't access request after it might be freedRoland Dreier2012-11-231-1/+7
| |_|/ |/| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | After we've done __elv_add_request() and __blk_run_queue() in blk_execute_rq_nowait(), the request might finish and be freed immediately. Therefore checking if the type is REQ_TYPE_PM_RESUME isn't safe afterwards, because if it isn't, rq might be gone. Instead, check beforehand and stash the result in a temporary. This fixes crashes in blk_execute_rq_nowait() I get occasionally when running with lots of memory debugging options enabled -- I think this race is usually harmless because the window for rq to be reallocated is so small. Signed-off-by: Roland Dreier <roland@purestorage.com> Cc: stable@kernel.org Signed-off-by: Jens Axboe <axboe@kernel.dk>
* | | block: Add blk_rq_pos(rq) to sort rq when plushingJianpeng Ma2012-10-251-1/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | My workload is a raid5 which had 16 disks. And used our filesystem to write using direct-io mode. I used the blktrace to find those message: 8,16 0 6647 2.453665504 2579 M W 7493152 + 8 [md0_raid5] 8,16 0 6648 2.453672411 2579 Q W 7493160 + 8 [md0_raid5] 8,16 0 6649 2.453672606 2579 M W 7493160 + 8 [md0_raid5] 8,16 0 6650 2.453679255 2579 Q W 7493168 + 8 [md0_raid5] 8,16 0 6651 2.453679441 2579 M W 7493168 + 8 [md0_raid5] 8,16 0 6652 2.453685948 2579 Q W 7493176 + 8 [md0_raid5] 8,16 0 6653 2.453686149 2579 M W 7493176 + 8 [md0_raid5] 8,16 0 6654 2.453693074 2579 Q W 7493184 + 8 [md0_raid5] 8,16 0 6655 2.453693254 2579 M W 7493184 + 8 [md0_raid5] 8,16 0 6656 2.453704290 2579 Q W 7493192 + 8 [md0_raid5] 8,16 0 6657 2.453704482 2579 M W 7493192 + 8 [md0_raid5] 8,16 0 6658 2.453715016 2579 Q W 7493200 + 8 [md0_raid5] 8,16 0 6659 2.453715247 2579 M W 7493200 + 8 [md0_raid5] 8,16 0 6660 2.453721730 2579 Q W 7493208 + 8 [md0_raid5] 8,16 0 6661 2.453721974 2579 M W 7493208 + 8 [md0_raid5] 8,16 0 6662 2.453728202 2579 Q W 7493216 + 8 [md0_raid5] 8,16 0 6663 2.453728436 2579 M W 7493216 + 8 [md0_raid5] 8,16 0 6664 2.453734782 2579 Q W 7493224 + 8 [md0_raid5] 8,16 0 6665 2.453735019 2579 M W 7493224 + 8 [md0_raid5] 8,16 0 6666 2.453741401 2579 Q W 7493232 + 8 [md0_raid5] 8,16 0 6667 2.453741632 2579 M W 7493232 + 8 [md0_raid5] 8,16 0 6668 2.453748148 2579 Q W 7493240 + 8 [md0_raid5] 8,16 0 6669 2.453748386 2579 M W 7493240 + 8 [md0_raid5] 8,16 0 6670 2.453851843 2579 I W 7493144 + 104 [md0_raid5] 8,16 0 0 2.453853661 0 m N cfq2579 insert_request 8,16 0 6671 2.453854064 2579 I W 7493120 + 24 [md0_raid5] 8,16 0 0 2.453854439 0 m N cfq2579 insert_request 8,16 0 6672 2.453854793 2579 U N [md0_raid5] 2 8,16 0 0 2.453855513 0 m N cfq2579 Not idling.st->count:1 8,16 0 0 2.453855927 0 m N cfq2579 dispatch_insert 8,16 0 0 2.453861771 0 m N cfq2579 dispatched a request 8,16 0 0 2.453862248 0 m N cfq2579 activate rq,drv=1 8,16 0 6673 2.453862332 2579 D W 7493120 + 24 [md0_raid5] 8,16 0 0 2.453865957 0 m N cfq2579 Not idling.st->count:1 8,16 0 0 2.453866269 0 m N cfq2579 dispatch_insert 8,16 0 0 2.453866707 0 m N cfq2579 dispatched a request 8,16 0 0 2.453867061 0 m N cfq2579 activate rq,drv=2 8,16 0 6674 2.453867145 2579 D W 7493144 + 104 [md0_raid5] 8,16 0 6675 2.454147608 0 C W 7493120 + 24 [0] 8,16 0 0 2.454149357 0 m N cfq2579 complete rqnoidle 0 8,16 0 6676 2.454791505 0 C W 7493144 + 104 [0] 8,16 0 0 2.454794803 0 m N cfq2579 complete rqnoidle 0 8,16 0 0 2.454795160 0 m N cfq schedule dispatch From above messages,we can find rq[W 7493144 + 104] and rq[W 7493120 + 24] do not merge. Because the bio order is: 8,16 0 6638 2.453619407 2579 Q W 7493144 + 8 [md0_raid5] 8,16 0 6639 2.453620460 2579 G W 7493144 + 8 [md0_raid5] 8,16 0 6640 2.453639311 2579 Q W 7493120 + 8 [md0_raid5] 8,16 0 6641 2.453639842 2579 G W 7493120 + 8 [md0_raid5] The bio(7493144) first and bio(7493120) later.So the subsequent bios will be divided into two parts. When flushing plug-list,because elv_attempt_insert_merge only support backmerge,not supporting frontmerge. So rq[7493120 + 24] can't merge with rq[7493144 + 104]. From my test,i found those situation can count 25% in our system. Using this patch, there is no this situation. Signed-off-by: Jianpeng Ma <majianpeng@gmail.com> CC:Shaohua Li <shli@kernel.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
* | | block: remove CONFIG_EXPERIMENTALKees Cook2012-10-231-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | This config item has not carried much meaning for a while now and is almost always enabled by default. As agreed during the Linux kernel summit, remove it. CC: Jens Axboe <axboe@kernel.dk> Signed-off-by: Kees Cook <keescook@chromium.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
* | | blkcg: stop iteration early if root_rl is the only request listJun'ichi Nomura2012-10-221-0/+3
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | __blk_queue_next_rl() finds next request list based on blkg_list while skipping root_blkg in the list. OTOH, root_rl is special as it may exist even without root_blkg. Though the later part of the function handles such a case correctly, exiting early is good for readability of the code. Signed-off-by: Jun'ichi Nomura <j-nomura@ce.jp.nec.com> Cc: Tejun Heo <tj@kernel.org> Acked-by: Vivek Goyal <vgoyal@redhat.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
* | | blkcg: Fix use-after-free of q->root_blkg and q->root_rl.blkgJun'ichi Nomura2012-10-221-0/+7
|/ / | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | blk_put_rl() does not call blkg_put() for q->root_rl because we don't take request list reference on q->root_blkg. However, if root_blkg is once attached then detached (freed), blk_put_rl() is confused by the bogus pointer in q->root_blkg. For example, with !CONFIG_BLK_DEV_THROTTLING && CONFIG_CFQ_GROUP_IOSCHED, switching IO scheduler from cfq to deadline will cause system stall after the following warning with 3.6: > WARNING: at /work/build/linux/block/blk-cgroup.h:250 > blk_put_rl+0x4d/0x95() > Modules linked in: bridge stp llc sunrpc acpi_cpufreq freq_table mperf > ipt_REJECT nf_conntrack_ipv4 nf_defrag_ipv4 > Pid: 0, comm: swapper/0 Not tainted 3.6.0 #1 > Call Trace: > <IRQ> [<ffffffff810453bd>] warn_slowpath_common+0x85/0x9d > [<ffffffff810453ef>] warn_slowpath_null+0x1a/0x1c > [<ffffffff811d5f8d>] blk_put_rl+0x4d/0x95 > [<ffffffff811d614a>] __blk_put_request+0xc3/0xcb > [<ffffffff811d71a3>] blk_finish_request+0x232/0x23f > [<ffffffff811d76c3>] ? blk_end_bidi_request+0x34/0x5d > [<ffffffff811d76d1>] blk_end_bidi_request+0x42/0x5d > [<ffffffff811d7728>] blk_end_request+0x10/0x12 > [<ffffffff812cdf16>] scsi_io_completion+0x207/0x4d5 > [<ffffffff812c6fcf>] scsi_finish_command+0xfa/0x103 > [<ffffffff812ce2f8>] scsi_softirq_done+0xff/0x108 > [<ffffffff811dcea5>] blk_done_softirq+0x8d/0xa1 > [<ffffffff810915d5>] ? > generic_smp_call_function_single_interrupt+0x9f/0xd7 > [<ffffffff8104cf5b>] __do_softirq+0x102/0x213 > [<ffffffff8108a5ec>] ? lock_release_holdtime+0xb6/0xbb > [<ffffffff8104d2b4>] ? raise_softirq_irqoff+0x9/0x3d > [<ffffffff81424dfc>] call_softirq+0x1c/0x30 > [<ffffffff81011beb>] do_softirq+0x4b/0xa3 > [<ffffffff8104cdb0>] irq_exit+0x53/0xd5 > [<ffffffff8102d865>] smp_call_function_single_interrupt+0x34/0x36 > [<ffffffff8142486f>] call_function_single_interrupt+0x6f/0x80 > <EOI> [<ffffffff8101800b>] ? mwait_idle+0x94/0xcd > [<ffffffff81018002>] ? mwait_idle+0x8b/0xcd > [<ffffffff81017811>] cpu_idle+0xbb/0x114 > [<ffffffff81401fbd>] rest_init+0xc1/0xc8 > [<ffffffff81401efc>] ? csum_partial_copy_generic+0x16c/0x16c > [<ffffffff81cdbd3d>] start_kernel+0x3d4/0x3e1 > [<ffffffff81cdb79e>] ? kernel_init+0x1f7/0x1f7 > [<ffffffff81cdb2dd>] x86_64_start_reservations+0xb8/0xbd > [<ffffffff81cdb3e3>] x86_64_start_kernel+0x101/0x110 This patch clears q->root_blkg and q->root_rl.blkg when root blkg is destroyed. Signed-off-by: Jun'ichi Nomura <j-nomura@ce.jp.nec.com> Acked-by: Vivek Goyal <vgoyal@redhat.com> Acked-by: Tejun Heo <tj@kernel.org> Cc: stable@kernel.org Signed-off-by: Jens Axboe <axboe@kernel.dk>
* | Merge branch 'for-3.7/core' of git://git.kernel.dk/linux-blockLinus Torvalds2012-10-109-76/+236
|\ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull block IO update from Jens Axboe: "Core block IO bits for 3.7. Not a huge round this time, it contains: - First series from Kent cleaning up and generalizing bio allocation and freeing. - WRITE_SAME support from Martin. - Mikulas patches to prevent O_DIRECT crashes when someone changes the block size of a device. - Make bio_split() work on data-less bio's (like trim/discards). - A few other minor fixups." Fixed up silent semantic mis-merge as per Mikulas Patocka and Andrew Morton. It is due to the VM no longer using a prio-tree (see commit 6b2dbba8b6ac: "mm: replace vma prio_tree with an interval tree"). So make set_blocksize() use mapping_mapped() instead of open-coding the internal VM knowledge that has changed. * 'for-3.7/core' of git://git.kernel.dk/linux-block: (26 commits) block: makes bio_split support bio without data scatterlist: refactor the sg_nents scatterlist: add sg_nents fs: fix include/percpu-rwsem.h export error percpu-rw-semaphore: fix documentation typos fs/block_dev.c:1644:5: sparse: symbol 'blkdev_mmap' was not declared blockdev: turn a rw semaphore into a percpu rw semaphore Fix a crash when block device is read and block size is changed at the same time block: fix request_queue->flags initialization block: lift the initial queue bypass mode on blk_register_queue() instead of blk_init_allocated_queue() block: ioctl to zero block ranges block: Make blkdev_issue_zeroout use WRITE SAME block: Implement support for WRITE SAME block: Consolidate command flag and queue limit checks for merges block: Clean up special command handling logic block/blk-tag.c: Remove useless kfree block: remove the duplicated setting for congestion_threshold block: reject invalid queue attribute values block: Add bio_clone_bioset(), bio_clone_kmalloc() block: Consolidate bio_alloc_bioset(), bio_kmalloc() ...
| * | block: fix request_queue->flags initializationTejun Heo2012-09-211-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | A queue newly allocated with blk_alloc_queue_node() has only QUEUE_FLAG_BYPASS set. For request-based drivers, blk_init_allocated_queue() is called and q->queue_flags is overwritten with QUEUE_FLAG_DEFAULT which doesn't include BYPASS even though the initial bypass is still in effect. In blk_init_allocated_queue(), or QUEUE_FLAG_DEFAULT to q->queue_flags instead of overwriting. Signed-off-by: Tejun Heo <tj@kernel.org> Cc: stable@vger.kernel.org Acked-by: Vivek Goyal <vgoyal@redhat.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: lift the initial queue bypass mode on blk_register_queue() instead of ↵Tejun Heo2012-09-212-5/+8
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | blk_init_allocated_queue() b82d4b197c ("blkcg: make request_queue bypassing on allocation") made request_queues bypassed on allocation to avoid switching on and off bypass mode on a queue being initialized. Some drivers allocate and then destroy a lot of queues without fully initializing them and incurring bypass latency overhead on each of them could add upto significant overhead. Unfortunately, blk_init_allocated_queue() is never used by queues of bio-based drivers, which means that all bio-based driver queues are in bypass mode even after initialization and registration complete successfully. Due to the limited way request_queues are used by bio drivers, this problem is hidden pretty well but it shows up when blk-throttle is used in combination with a bio-based driver. Trying to configure (echoing to cgroupfs file) blk-throttle for a bio-based driver hangs indefinitely in blkg_conf_prep() waiting for bypass mode to end. This patch moves the initial blk_queue_bypass_end() call from blk_init_allocated_queue() to blk_register_queue() which is called for any userland-visible queues regardless of its type. I believe this is correct because I don't think there is any block driver which needs or wants working elevator and blk-cgroup on a queue which isn't visible to userland. If there are such users, we need a different solution. Signed-off-by: Tejun Heo <tj@kernel.org> Reported-by: Joseph Glanville <joseph.glanville@orionvm.com.au> Cc: stable@vger.kernel.org Acked-by: Vivek Goyal <vgoyal@redhat.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: ioctl to zero block rangesMartin K. Petersen2012-09-201-0/+27
| | | | | | | | | | | | | | | | | | | | | | | | | | | Introduce a BLKZEROOUT ioctl which can be used to clear block ranges by way of blkdev_issue_zeroout(). Signed-off-by: Martin K. Petersen <martin.petersen@oracle.com> Acked-by: Mike Snitzer <snitzer@redhat.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Make blkdev_issue_zeroout use WRITE SAMEMartin K. Petersen2012-09-201-1/+29
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | If the device supports WRITE SAME, use that to optimize zeroing of blocks. If the device does not support WRITE SAME or if the operation fails, fall back to writing zeroes the old-fashioned way. Signed-off-by: Martin K. Petersen <martin.petersen@oracle.com> Acked-by: Mike Snitzer <snitzer@redhat.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Implement support for WRITE SAMEMartin K. Petersen2012-09-205-2/+124
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | The WRITE SAME command supported on some SCSI devices allows the same block to be efficiently replicated throughout a block range. Only a single logical block is transferred from the host and the storage device writes the same data to all blocks described by the I/O. This patch implements support for WRITE SAME in the block layer. The blkdev_issue_write_same() function can be used by filesystems and block drivers to replicate a buffer across a block range. This can be used to efficiently initialize software RAID devices, etc. Signed-off-by: Martin K. Petersen <martin.petersen@oracle.com> Acked-by: Mike Snitzer <snitzer@redhat.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Consolidate command flag and queue limit checks for mergesMartin K. Petersen2012-09-202-20/+13
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | - blk_check_merge_flags() verifies that cmd_flags / bi_rw are compatible. This function is called for both req-req and req-bio merging. - blk_rq_get_max_sectors() and blk_queue_get_max_sectors() can be used to query the maximum sector count for a given request or queue. The calls will return the right value from the queue limits given the type of command (RW, discard, write same, etc.) Signed-off-by: Martin K. Petersen <martin.petersen@oracle.com> Acked-by: Mike Snitzer <snitzer@redhat.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Clean up special command handling logicMartin K. Petersen2012-09-204-35/+11
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Remove special-casing of non-rw fs style requests (discard). The nomerge flags are consolidated in blk_types.h, and rq_mergeable() and bio_mergeable() have been modified to use them. bio_is_rw() is used in place of bio_has_data() a few places. This is done to to distinguish true reads and writes from other fs type requests that carry a payload (e.g. write same). Signed-off-by: Martin K. Petersen <martin.petersen@oracle.com> Acked-by: Mike Snitzer <snitzer@redhat.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block/blk-tag.c: Remove useless kfreePeter Senna Tschudin2012-09-121-4/+2
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Remove useless kfree() and clean up code related to the removal. The semantic patch that finds this problem is as follows: (http://coccinelle.lip6.fr/) // <smpl> @r exists@ position p1,p2; expression x; @@ if (x@p1 == NULL) { ... kfree@p2(x); ... return ...; } @unchanged exists@ position r.p1,r.p2; expression e <= r.x,x,e1; iterator I; statement S; @@ if (x@p1 == NULL) { ... when != I(x,...) S when != e = e1 when != e += e1 when != e -= e1 when != ++e when != --e when != e++ when != e-- when != &e kfree@p2(x); ... return ...; } @ok depends on unchanged exists@ position any r.p1; position r.p2; expression x; @@ ... when != true x@p1 == NULL kfree@p2(x); @depends on !ok && unchanged@ position r.p2; expression x; @@ *kfree@p2(x); // </smpl> Signed-off-by: Peter Senna Tschudin <peter.senna@gmail.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: remove the duplicated setting for congestion_thresholdJaehoon Chung2012-09-091-2/+0
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Before call the blk_queue_congestion_threshold(), the blk_queue_congestion_threshold() is already called at blk_queue_make_rquest(). Because this code is the duplicated, it has removed. Signed-off-by: Jaehoon Chung <jh80.chung@samsung.com> Signed-off-by: Kyungmin Park <kyungmin.park@samsung.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: reject invalid queue attribute valuesDave Reisner2012-09-091-2/+23
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Instead of using simple_strtoul which "converts" invalid numbers to 0, use strict_strtoul and perform error checking to ensure that userspace passes us a valid unsigned long. This addresses problems with functions such as writev, which might want to write a trailing newline -- the newline should rightfully be rejected, but the value preceeding it should be preserved. Fixes BZ#46981. Signed-off-by: Dave Reisner <dreisner@archlinux.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Add bio_clone_bioset(), bio_clone_kmalloc()Kent Overstreet2012-09-091-7/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Previously, there was bio_clone() but it only allocated from the fs bio set; as a result various users were open coding it and using __bio_clone(). This changes bio_clone() to become bio_clone_bioset(), and then we add bio_clone() and bio_clone_kmalloc() as wrappers around it, making use of the functionality the last patch adedd. This will also help in a later patch changing how bio cloning works. Signed-off-by: Kent Overstreet <koverstreet@google.com> CC: Jens Axboe <axboe@kernel.dk> CC: NeilBrown <neilb@suse.de> CC: Alasdair Kergon <agk@redhat.com> CC: Boaz Harrosh <bharrosh@panasas.com> CC: Jeff Garzik <jeff@garzik.org> Acked-by: Jeff Garzik <jgarzik@redhat.com> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Kill bi_destructorKent Overstreet2012-09-091-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Now that we've got generic code for freeing bios allocated from bio pools, this isn't needed anymore. This patch also makes bio_free() static, since without bi_destructor there should be no need for it to be called anywhere else. bio_free() is now only called from bio_put, so we can refactor those a bit - move some code from bio_put() to bio_free() and kill the redundant bio->bi_next = NULL. v5: Switch to BIO_KMALLOC_POOL ((void *)~0), per Boaz v6: BIO_KMALLOC_POOL now NULL, drop bio_free's EXPORT_SYMBOL v7: No #define BIO_KMALLOC_POOL anymore Signed-off-by: Kent Overstreet <koverstreet@google.com> CC: Jens Axboe <axboe@kernel.dk> Signed-off-by: Jens Axboe <axboe@kernel.dk>
| * | block: Ues bi_pool for bio_integrity_alloc()Kent Overstreet2012-09-091-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Now that bios keep track of where they were allocated from, bio_integrity_alloc_bioset() becomes redundant. Remove bio_integrity_alloc_bioset() and drop bio_set argument from the related functions and make them use bio->bi_pool. Signed-off-by: Kent Overstreet <koverstreet@google.com> CC: Jens Axboe <axboe@kernel.dk> CC: Martin K. Petersen <martin.petersen@oracle.com> Acked-by: Tejun Heo <tj@kernel.org> Signed-off-by: Jens Axboe <axboe@kernel.dk>
* | | Merge branch 'for-3.7-hierarchy' of ↵Linus Torvalds2012-10-021-0/+8
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | git://git.kernel.org/pub/scm/linux/kernel/git/tj/cgroup Pull cgroup hierarchy update from Tejun Heo: "Currently, different cgroup subsystems handle nested cgroups completely differently. There's no consistency among subsystems and the behaviors often are outright broken. People at least seem to agree that the broken hierarhcy behaviors need to be weeded out if any progress is gonna be made on this front and that the fallouts from deprecating the broken behaviors should be acceptable especially given that the current behaviors don't make much sense when nested. This patch makes cgroup emit warning messages if cgroups for subsystems with broken hierarchy behavior are nested to prepare for fixing them in the future. This was put in a separate branch because more related changes were expected (didn't make it this round) and the memory cgroup wanted to pull in this and make changes on top." * 'for-3.7-hierarchy' of git://git.kernel.org/pub/scm/linux/kernel/git/tj/cgroup: cgroup: mark subsystems with broken hierarchy support and whine if cgroups are nested for them
| * | | cgroup: mark subsystems with broken hierarchy support and whine if cgroups ↵Tejun Heo2012-09-141-0/+8
| |/ / | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | are nested for them Currently, cgroup hierarchy support is a mess. cpu related subsystems behave correctly - configuration, accounting and control on a parent properly cover its children. blkio and freezer completely ignore hierarchy and treat all cgroups as if they're directly under the root cgroup. Others show yet different behaviors. These differing interpretations of cgroup hierarchy make using cgroup confusing and it impossible to co-mount controllers into the same hierarchy and obtain sane behavior. Eventually, we want full hierarchy support from all subsystems and probably a unified hierarchy. Users using separate hierarchies expecting completely different behaviors depending on the mounted subsystem is deterimental to making any progress on this front. This patch adds cgroup_subsys.broken_hierarchy and sets it to %true for controllers which are lacking in hierarchy support. The goal of this patch is two-fold. * Move users away from using hierarchy on currently non-hierarchical subsystems, so that implementing proper hierarchy support on those doesn't surprise them. * Keep track of which controllers are broken how and nudge the subsystems to implement proper hierarchy support. For now, start with a single warning message. We can whine louder later on. v2: Fixed a typo spotted by Michal. Warning message updated. v3: Updated memcg part so that it doesn't generate warning in the cases where .use_hierarchy=false doesn't make the behavior different from root.use_hierarchy=true. Fixed a typo spotted by Glauber. v4: Check ->broken_hierarchy after cgroup creation is complete so that ->create() can affect the result per Michal. Dropped unnecessary memcg root handling per Michal. Signed-off-by: Tejun Heo <tj@kernel.org> Acked-by: Michal Hocko <mhocko@suse.cz> Acked-by: Li Zefan <lizefan@huawei.com> Acked-by: Serge E. Hallyn <serue@us.ibm.com> Cc: Glauber Costa <glommer@parallels.com> Cc: Peter Zijlstra <peterz@infradead.org> Cc: Paul Turner <pjt@google.com> Cc: Johannes Weiner <hannes@cmpxchg.org> Cc: Thomas Graf <tgraf@suug.ch> Cc: Vivek Goyal <vgoyal@redhat.com> Cc: Paul Mackerras <paulus@samba.org> Cc: Ingo Molnar <mingo@redhat.com> Cc: Arnaldo Carvalho de Melo <acme@ghostprotocols.net> Cc: Neil Horman <nhorman@tuxdriver.com> Cc: Aneesh Kumar K.V <aneesh.kumar@linux.vnet.ibm.com>
* | | Merge branch 'for-3.7' of git://git.kernel.org/pub/scm/linux/kernel/git/tj/wqLinus Torvalds2012-10-023-23/+13
|\ \ \ | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Pull workqueue changes from Tejun Heo: "This is workqueue updates for v3.7-rc1. A lot of activities this round including considerable API and behavior cleanups. * delayed_work combines a timer and a work item. The handling of the timer part has always been a bit clunky leading to confusing cancelation API with weird corner-case behaviors. delayed_work is updated to use new IRQ safe timer and cancelation now works as expected. * Another deficiency of delayed_work was lack of the counterpart of mod_timer() which led to cancel+queue combinations or open-coded timer+work usages. mod_delayed_work[_on]() are added. These two delayed_work changes make delayed_work provide interface and behave like timer which is executed with process context. * A work item could be executed concurrently on multiple CPUs, which is rather unintuitive and made flush_work() behavior confusing and half-broken under certain circumstances. This problem doesn't exist for non-reentrant workqueues. While non-reentrancy check isn't free, the overhead is incurred only when a work item bounces across different CPUs and even in simulated pathological scenario the overhead isn't too high. All workqueues are made non-reentrant. This removes the distinction between flush_[delayed_]work() and flush_[delayed_]_work_sync(). The former is now as strong as the latter and the specified work item is guaranteed to have finished execution of any previous queueing on return. * In addition to the various bug fixes, Lai redid and simplified CPU hotplug handling significantly. * Joonsoo introduced system_highpri_wq and used it during CPU hotplug. There are two merge commits - one to pull in IRQ safe timer from tip/timers/core and the other to pull in CPU hotplug fixes from wq/for-3.6-fixes as Lai's hotplug restructuring depended on them." Fixed a number of trivial conflicts, but the more interesting conflicts were silent ones where the deprecated interfaces had been used by new code in the merge window, and thus didn't cause any real data conflicts. Tejun pointed out a few of them, I fixed a couple more. * 'for-3.7' of git://git.kernel.org/pub/scm/linux/kernel/git/tj/wq: (46 commits) workqueue: remove spurious WARN_ON_ONCE(in_irq()) from try_to_grab_pending() workqueue: use cwq_set_max_active() helper for workqueue_set_max_active() workqueue: introduce cwq_set_max_active() helper for thaw_workqueues() workqueue: remove @delayed from cwq_dec_nr_in_flight() workqueue: fix possible stall on try_to_grab_pending() of a delayed work item workqueue: use hotcpu_notifier() for workqueue_cpu_down_callback() workqueue: use __cpuinit instead of __devinit for cpu callbacks workqueue: rename manager_mutex to assoc_mutex workqueue: WORKER_REBIND is no longer necessary for idle rebinding workqueue: WORKER_REBIND is no longer necessary for busy rebinding workqueue: reimplement idle worker rebinding workqueue: deprecate __cancel_delayed_work() workqueue: reimplement cancel_delayed_work() using try_to_grab_pending() workqueue: use mod_delayed_work() instead of __cancel + queue workqueue: use irqsafe timer for delayed_work workqueue: clean up delayed_work initializers and add missing one workqueue: make deferrable delayed_work initializer names consistent workqueue: cosmetic whitespace updates for macro definitions workqueue: deprecate system_nrt[_freezable]_wq workqueue: deprecate flush[_delayed]_work_sync() ...