| Commit message (Collapse) | Author | Age | Files | Lines |
|\
| |
| |
| |
| |
| |
| |
| |
| | |
This is the 3.0.68 stable release
Conflicts:
kernel/cgroup.c
Change-Id: I067982d25e18e3a12de93a5eb6429b8829d7ca11
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
commit 6cdae7416a1c45c2ce105a78187d9b7e8feb9e24 upstream.
The iteration logic of idr_get_next() is borrowed mostly verbatim from
idr_for_each(). It walks down the tree looking for the slot matching
the current ID. If the matching slot is not found, the ID is
incremented by the distance of single slot at the given level and
repeats.
The implementation assumes that during the whole iteration id is aligned
to the layer boundaries of the level closest to the leaf, which is true
for all iterations starting from zero or an existing element and thus is
fine for idr_for_each().
However, idr_get_next() may be given any point and if the starting id
hits in the middle of a non-existent layer, increment to the next layer
will end up skipping the same offset into it. For example, an IDR with
IDs filled between [64, 127] would look like the following.
[ 0 64 ... ]
/----/ |
| |
NULL [ 64 ... 127 ]
If idr_get_next() is called with 63 as the starting point, it will try
to follow down the pointer from 0. As it is NULL, it will then try to
proceed to the next slot in the same level by adding the slot distance
at that level which is 64 - making the next try 127. It goes around the
loop and finds and returns 127 skipping [64, 126].
Note that this bug also triggers in idr_for_each_entry() loop which
deletes during iteration as deletions can make layers go away leaving
the iteration with unaligned ID into missing layers.
Fix it by ensuring proceeding to the next slot doesn't carry over the
unaligned offset - ie. use round_up(id + 1, slot_distance) instead of
id += slot_distance.
Signed-off-by: Tejun Heo <tj@kernel.org>
Reported-by: David Teigland <teigland@redhat.com>
Cc: KAMEZAWA Hiroyuki <kamezawa.hiroyu@jp.fujitsu.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|\|
| |
| |
| |
| | |
Change-Id: I9685feb9277b450da10d78a455b3c0674d6cfe18
Signed-off-by: Todd Poynor <toddpoynor@google.com>
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
commit eedce141cd2dad8d0cefc5468ef41898949a7031 upstream.
The genalloc code uses the bitmap API from include/linux/bitmap.h and
lib/bitmap.c, which is based on long values. Both bitmap_set from
lib/bitmap.c and bitmap_set_ll, which is the lockless version from
genalloc.c, use BITMAP_LAST_WORD_MASK to set the first bits in a long in
the bitmap.
That one uses (1 << bits) - 1, 0b111, if you are setting the first three
bits. This means that the API counts from the least significant bits
(LSB from now on) to the MSB. The LSB in the first long is bit 0, then.
The same works for the lookup functions.
The genalloc code uses longs for the bitmap, as it should. In
include/linux/genalloc.h, struct gen_pool_chunk has unsigned long
bits[0] as its last member. When allocating the struct, genalloc should
reserve enough space for the bitmap. This should be a proper number of
longs that can fit the amount of bits in the bitmap.
However, genalloc allocates an integer number of bytes that fit the
amount of bits, but may not be an integer amount of longs. 9 bytes, for
example, could be allocated for 70 bits.
This is a problem in itself if the Least Significat Bit in a long is in
the byte with the largest address, which happens in Big Endian machines.
This means genalloc is not allocating the byte in which it will try to
set or check for a bit.
This may end up in memory corruption, where genalloc will try to set the
bits it has not allocated. In fact, genalloc may not set these bits
because it may find them already set, because they were not zeroed since
they were not allocated. And that's what causes a BUG when
gen_pool_destroy is called and check for any set bits.
What really happens is that genalloc uses kmalloc_node with __GFP_ZERO
on gen_pool_add_virt. With SLAB and SLUB, this means the whole slab
will be cleared, not only the requested bytes. Since struct
gen_pool_chunk has a size that is a multiple of 8, and slab sizes are
multiples of 8, we get lucky and allocate and clear the right amount of
bytes.
Hower, this is not the case with SLOB or with older code that did memset
after allocating instead of using __GFP_ZERO.
So, a simple module as this (running 3.6.0), will cause a crash when
rmmod'ed.
[root@phantom-lp2 foo]# cat foo.c
#include <linux/kernel.h>
#include <linux/module.h>
#include <linux/init.h>
#include <linux/genalloc.h>
MODULE_LICENSE("GPL");
MODULE_VERSION("0.1");
static struct gen_pool *foo_pool;
static __init int foo_init(void)
{
int ret;
foo_pool = gen_pool_create(10, -1);
if (!foo_pool)
return -ENOMEM;
ret = gen_pool_add(foo_pool, 0xa0000000, 32 << 10, -1);
if (ret) {
gen_pool_destroy(foo_pool);
return ret;
}
return 0;
}
static __exit void foo_exit(void)
{
gen_pool_destroy(foo_pool);
}
module_init(foo_init);
module_exit(foo_exit);
[root@phantom-lp2 foo]# zcat /proc/config.gz | grep SLOB
CONFIG_SLOB=y
[root@phantom-lp2 foo]# insmod ./foo.ko
[root@phantom-lp2 foo]# rmmod foo
------------[ cut here ]------------
kernel BUG at lib/genalloc.c:243!
cpu 0x4: Vector: 700 (Program Check) at [c0000000bb0e7960]
pc: c0000000003cb50c: .gen_pool_destroy+0xac/0x110
lr: c0000000003cb4fc: .gen_pool_destroy+0x9c/0x110
sp: c0000000bb0e7be0
msr: 8000000000029032
current = 0xc0000000bb0e0000
paca = 0xc000000006d30e00 softe: 0 irq_happened: 0x01
pid = 13044, comm = rmmod
kernel BUG at lib/genalloc.c:243!
[c0000000bb0e7ca0] d000000004b00020 .foo_exit+0x20/0x38 [foo]
[c0000000bb0e7d20] c0000000000dff98 .SyS_delete_module+0x1a8/0x290
[c0000000bb0e7e30] c0000000000097d4 syscall_exit+0x0/0x94
--- Exception: c00 (System Call) at 000000800753d1a0
SP (fffd0b0e640) is in userspace
Signed-off-by: Thadeu Lima de Souza Cascardo <cascardo@linux.vnet.ibm.com>
Cc: Paul Gortmaker <paul.gortmaker@windriver.com>
Cc: Benjamin Gaignard <benjamin.gaignard@stericsson.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
commit e96875677fb2b7cb739c5d7769824dff7260d31d upstream.
Account for all properties when a and/or b are 0:
gcd(0, 0) = 0
gcd(a, 0) = a
gcd(0, b) = b
Fixes no known problems in current kernels.
Signed-off-by: Davidlohr Bueso <dave@gnu.org>
Cc: Eric Dumazet <eric.dumazet@gmail.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
commit cbf8ae32f66a9ceb8907ad9e16663c2a29e48990 upstream.
The memory the parameter __key points to is used as an iterator in
btree_get_prev(), so if we save off a bkey() pointer in retry_key and
then assign that to __key, we'll end up corrupting the btree internals
when we do eg
longcpy(__key, bkey(geo, node, i), geo->keylen);
to return the key value. What we should do instead is use longcpy() to
copy the key value that retry_key points to __key.
This can cause a btree to get corrupted by seemingly read-only
operations such as btree_for_each_safe.
[akpm@linux-foundation.org: avoid the double longcpy()]
Signed-off-by: Roland Dreier <roland@purestorage.com>
Acked-by: Joern Engel <joern@logfs.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
|\|
| |
| |
| |
| | |
Change-Id: Iee820738e53627f5d0447a87ceff34443aa72786
Signed-off-by: Todd Poynor <toddpoynor@google.com>
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
commit 7b60a18da393ed70db043a777fd9e6d5363077c4 upstream.
The queue handling in the udev daemon assumes that the events are
ordered.
Before this patch uevent_seqnum is incremented under sequence_lock,
than an event is send uner uevent_sock_mutex. I want to say that code
contained a window between incrementing seqnum and sending an event.
This patch locks uevent_sock_mutex before incrementing uevent_seqnum.
v2: delete sequence_lock, uevent_seqnum is protected by uevent_sock_mutex
v3: unlock the mutex before the goto exit
Thanks for Kay for the comments.
Signed-off-by: Andrew Vagin <avagin@openvz.org>
Tested-By: Kay Sievers <kay.sievers@vrfy.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@linuxfoundation.org>
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
commit c30bc94758ae2a38a5eb31767c1985c0aae0950b upstream.
L2TP for example uses NLA_MSECS like this:
policy:
[L2TP_ATTR_RECV_TIMEOUT] = { .type = NLA_MSECS, },
code:
if (info->attrs[L2TP_ATTR_RECV_TIMEOUT])
cfg.reorder_timeout = nla_get_msecs(info->attrs[L2TP_ATTR_RECV_TIMEOUT]);
As nla_get_msecs() is essentially nla_get_u64() plus the
conversion to a HZ-based value, this will not properly
reject attributes from userspace that aren't long enough
and might overrun the message.
Add NLA_MSECS to the attribute minlen array to check the
size properly.
Cc: Thomas Graf <tgraf@suug.ch>
Signed-off-by: Johannes Berg <johannes.berg@intel.com>
Signed-off-by: David S. Miller <davem@davemloft.net>
Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
commit ebf4127cd677e9781b450e44dfaaa1cc595efcaa upstream.
kobject_uevent() uses a multicast socket and should ignore
if one of listeners cannot handle messages or nobody is
listening at all.
Easily reproducible when a process in system is cloned
with CLONE_NEWNET flag.
(See also http://article.gmane.org/gmane.linux.kernel.device-mapper.dm-crypt/5256)
Signed-off-by: Milan Broz <mbroz@redhat.com>
Acked-by: Kay Sievers <kay.sievers@vrfy.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
|
|\| |
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
commit 9c1f8594df4814ebfd6822ca3c9444fb3445888d upstream.
xz_dec_run() could incorrectly return XZ_BUF_ERROR if all of the
following was true:
- The caller knows how many bytes of output to expect and only provides
that much output space.
- When the last output bytes are decoded, the caller-provided input
buffer ends right before the LZMA2 end of payload marker. So LZMA2
won't provide more output anymore, but it won't know it yet and thus
won't return XZ_STREAM_END yet.
- A BCJ filter is in use and it hasn't left any unfiltered bytes in the
temp buffer. This can happen with any BCJ filter, but in practice
it's more likely with filters other than the x86 BCJ.
This fixes <https://bugzilla.redhat.com/show_bug.cgi?id=735408> where
Squashfs thinks that a valid file system is corrupt.
This also fixes a similar bug in single-call mode where the uncompressed
size of a block using BCJ + LZMA2 was 0 bytes and caller provided no
output space. Many empty .xz files don't contain any blocks and thus
don't trigger this bug.
This also tweaks a closely related detail: xz_dec_bcj_run() could call
xz_dec_lzma2_run() to decode into temp buffer when it was known to be
useless. This was harmless although it wasted a minuscule number of CPU
cycles.
Signed-off-by: Lasse Collin <lasse.collin@tukaani.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
|
| |
| |
| |
| |
| |
| |
| |
| | |
We are going to use this for TCP/IP sequence number and fragment ID
generation.
Signed-off-by: David S. Miller <davem@davemloft.net>
Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
|
|\| |
|
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| |
| | |
commit 81d67439855a7f928d90965d832aa4f2fb677342 upstream.
<linux/kernel.h> is needed for min_t. The old version
happened to work on x86 because <asm/unaligned.h>
indirectly includes <linux/kernel.h>, but it didn't
work on ARM.
<linux/kernel.h> includes <asm/byteorder.h> so it's
not necessary to include it explicitly anymore.
Signed-off-by: Lasse Collin <lasse.collin@tukaani.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
|
|\| |
|
| |\
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
'sched-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-2.6-tip
* 'core-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-2.6-tip:
debugobjects: Fix boot crash when kmemleak and debugobjects enabled
* 'perf-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-2.6-tip:
jump_label: Fix jump_label update for modules
oprofile, x86: Fix race in nmi handler while starting counters
* 'sched-urgent-for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/tip/linux-2.6-tip:
sched: Disable (revert) SCHED_LOAD_SCALE increase
sched, cgroups: Fix MIN_SHARES on 64-bit boxen
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
Order of initialization look like this:
...
debugobjects
kmemleak
...(lots of other subsystems)...
workqueues (through early initcall)
...
debugobjects use schedule_work for batch freeing of its data and kmemleak
heavily use debugobjects, so when it comes to freeing and workqueues were
not initialized yet, kernel crashes:
BUG: unable to handle kernel NULL pointer dereference at (null)
IP: [<ffffffff810854d1>] __queue_work+0x29/0x41a
[<ffffffff81085910>] queue_work_on+0x16/0x1d
[<ffffffff81085abc>] queue_work+0x29/0x55
[<ffffffff81085afb>] schedule_work+0x13/0x15
[<ffffffff81242de1>] free_object+0x90/0x95
[<ffffffff81242f6d>] debug_check_no_obj_freed+0x187/0x1d3
[<ffffffff814b6504>] ? _raw_spin_unlock_irqrestore+0x30/0x4d
[<ffffffff8110bd14>] ? free_object_rcu+0x68/0x6d
[<ffffffff8110890c>] kmem_cache_free+0x64/0x12c
[<ffffffff8110bd14>] free_object_rcu+0x68/0x6d
[<ffffffff810b58bc>] __rcu_process_callbacks+0x1b6/0x2d9
...
because system_wq is NULL.
Fix it by checking if workqueues susbystem was initialized before using.
Signed-off-by: Marcin Slusarz <marcin.slusarz@gmail.com>
Cc: Catalin Marinas <catalin.marinas@arm.com>
Cc: Tejun Heo <tj@kernel.org>
Cc: Dipankar Sarma <dipankar@in.ibm.com>
Cc: Paul E. McKenney <paulmck@linux.vnet.ibm.com>
Cc: stable@kernel.org
Link: http://lkml.kernel.org/r/20110528112342.GA3068@joi.lan
Signed-off-by: Thomas Gleixner <tglx@linutronix.de>
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
This was legacy code brought over from the RT tree and
is no longer necessary.
Signed-off-by: Dima Zavin <dima@android.com>
Acked-by: Thomas Gleixner <tglx@linutronix.de>
Cc: Daniel Walker <dwalker@codeaurora.org>
Cc: Steven Rostedt <rostedt@goodmis.org>
Cc: Peter Zijlstra <peterz@infradead.org>
Cc: Andi Kleen <andi@firstfloor.org>
Cc: Lai Jiangshan <laijs@cn.fujitsu.com>
Link: http://lkml.kernel.org/r/1310084879-10351-2-git-send-email-dima@android.com
Signed-off-by: Ingo Molnar <mingo@elte.hu>
|
|\| | |
|
| |\ \
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs-2.6
* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/viro/vfs-2.6:
AFS: Use i_generation not i_version for the vnode uniquifier
AFS: Set s_id in the superblock to the volume name
vfs: Fix data corruption after failed write in __block_write_begin()
afs: afs_fill_page reads too much, or wrong data
VFS: Fix vfsmount overput on simultaneous automount
fix wrong iput on d_inode introduced by e6bc45d65d
Delay struct net freeing while there's a sysfs instance refering to it
afs: fix sget() races, close leak on umount
ubifs: fix sget races
ubifs: split allocation of ubifs_info into a separate function
fix leak in proc_set_super()
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
* new refcount in struct net, controlling actual freeing of the memory
* new method in kobj_ns_type_operations (->drop_ns())
* ->current_ns() semantics change - it's supposed to be followed by
corresponding ->drop_ns(). For struct net in case of CONFIG_NET_NS it bumps
the new refcount; net_drop_ns() decrements it and calls net_free() if the
last reference has been dropped. Method renamed to ->grab_current_ns().
* old net_free() callers call net_drop_ns() instead.
* sysfs_exit_ns() is gone, along with a large part of callchain
leading to it; now that the references stored in ->ns[...] stay valid we
do not need to hunt them down and replace them with NULL. That fixes
problems in sysfs_lookup() and sysfs_readdir(), along with getting rid
of sb->s_instances abuse.
Note that struct net *shutdown* logics has not changed - net_cleanup()
is called exactly when it used to be called. The only thing postponed by
having a sysfs instance refering to that struct net is actual freeing of
memory occupied by struct net.
Signed-off-by: Al Viro <viro@zeniv.linux.org.uk>
|
| |/ /
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
Fix new kernel-doc warnings in lib/bitmap.c:
Warning(lib/bitmap.c:596): No description found for parameter 'buf'
Warning(lib/bitmap.c:596): Excess function parameter 'bp' description in '__bitmap_parselist'
Signed-off-by: Randy Dunlap <randy.dunlap@oracle.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
|/ /
| |
| |
| |
| |
| |
| |
| | |
This allows us to get a kernel stacktrace for a thread though /proc.
Also enable it by default.
Change-Id: If8c21cd02feaf9863f4841ace524fa30c7328d49
Signed-off-by: Arve Hjønnevåg <arve@android.com>
|
|\ \
| | |
| | |
| | |
| | |
| | |
| | | |
git://git.kernel.org/pub/scm/linux/kernel/git/konrad/swiotlb-2.6
* 'stable/xen-swiotlb.bugfix' of git://git.kernel.org/pub/scm/linux/kernel/git/konrad/swiotlb-2.6:
swiotlb: Export swioltb_nr_tbl and utilize it as appropiate.
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
By default the io_tlb_nslabs is set to zero, and gets set to
whatever value is passed in via swiotlb_init_with_tbl function.
The default value passed in is 64MB. However, if the user provides
the 'swiotlb=<nslabs>' the default value is ignored and
the value provided by the user is used... Except when the SWIOTLB
is used under Xen - there the default value of 64MB is used and
the Xen-SWIOTLB has no mechanism to get the 'io_tlb_nslabs' filled
out by setup_io_tlb_npages functions. This patch provides a function
for the Xen-SWIOTLB to call to see if the io_tlb_nslabs is set
and if so use that value.
Signed-off-by: FUJITA Tomonori <fujita.tomonori@lab.ntt.co.jp>
Signed-off-by: Konrad Rzeszutek Wilk <konrad.wilk@oracle.com>
|
| |/
|/|
| |
| |
| |
| |
| |
| |
| |
| |
| | |
RFC 5952 (http://tools.ietf.org/html/rfc5952) mandates that 2 or more
consecutive 0's are required before using :: compression.
Update ip6_compressed_string to match the RFC and update the http
reference as well.
Signed-off-by: Joe Perches <joe@perches.com>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
| |
| |
| |
| |
| |
| | |
Trivial config change to enable backtraces on panic.
Signed-off-by: Chris Metcalf <cmetcalf@tilera.com>
|
|\ \
| | |
| | |
| | | |
git://git.kernel.org/pub/scm/linux/kernel/git/paulmck/linux-2.6-rcu into core/urgent
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
HARDIRQ_ENTER() maps to irq_enter() which calls rcu_irq_enter().
But HARDIRQ_EXIT() maps to __irq_exit() which doesn't call
rcu_irq_exit().
So for every locking selftest that simulates hardirq disabled,
we create an imbalance in the rcu extended quiescent state
internal state.
As a result, after the first missing rcu_irq_exit(), subsequent
irqs won't exit dyntick-idle mode after leaving the interrupt
handler. This means that RCU won't see the affected CPU as being
in an extended quiescent state, resulting in long grace-period
delays (as in grace periods extending for hours).
To fix this, just use __irq_enter() to simulate the hardirq
context. This is sufficient for the locking selftests as we
don't need to exit any extended quiescent state or perform
any check that irqs normally do when they wake up from idle.
As a side effect, this patch makes it possible to restore
"rcu: Decrease memory-barrier usage based on semi-formal proof",
which eventually helped finding this bug.
Reported-and-tested-by: Yinghai Lu <yinghai@kernel.org>
Signed-off-by: Frederic Weisbecker <fweisbec@gmail.com>
Cc: Paul E. McKenney <paulmck@linux.vnet.ibm.com>
Cc: Ingo Molnar <mingo@elte.hu>
Cc: Peter Zijlstra <a.p.zijlstra@chello.nl>
Cc: Stable <stable@kernel.org>
Signed-off-by: Paul E. McKenney <paulmck@linux.vnet.ibm.com>
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
By the previous style change, CONFIG_GENERIC_FIND_NEXT_BIT,
CONFIG_GENERIC_FIND_BIT_LE, and CONFIG_GENERIC_FIND_LAST_BIT are not used
to test for existence of find bitops anymore.
Signed-off-by: Akinobu Mita <akinobu.mita@gmail.com>
Acked-by: Greg Ungerer <gerg@uclinux.org>
Cc: Arnd Bergmann <arnd@arndb.de>
Cc: Russell King <linux@arm.linux.org.uk>
Cc: Martin Schwidefsky <schwidefsky@de.ibm.com>
Cc: Heiko Carstens <heiko.carstens@de.ibm.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
The style that we normally use in asm-generic is to test the macro itself
for existence, so in asm-generic, do:
#ifndef find_next_zero_bit_le
extern unsigned long find_next_zero_bit_le(const void *addr,
unsigned long size, unsigned long offset);
#endif
and in the architectures, write
static inline unsigned long find_next_zero_bit_le(const void *addr,
unsigned long size, unsigned long offset)
#define find_next_zero_bit_le find_next_zero_bit_le
This adds the #ifndef for each of the find bitops in the generic header
and source files.
Suggested-by: Arnd Bergmann <arnd@arndb.de>
Signed-off-by: Akinobu Mita <akinobu.mita@gmail.com>
Acked-by: Russell King <rmk+kernel@arm.linux.org.uk>
Cc: Martin Schwidefsky <schwidefsky@de.ibm.com>
Cc: Heiko Carstens <heiko.carstens@de.ibm.com>
Cc: Greg Ungerer <gerg@uclinux.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | |
| | | |
On most architectures division is an expensive operation and accessing an
element currently requires four of them. This performance penalty
effectively precludes flex arrays from being used on any kind of fast
path. However, two of these divisions can be handled at creation time and
the others can be replaced by a reciprocal divide, completely avoiding
real divisions on access.
[eparis@redhat.com: rebase on top of changes to support 0 len elements]
[eparis@redhat.com: initialize part_nr when array fits entirely in base]
Signed-off-by: Jesse Gross <jesse@nicira.com>
Signed-off-by: Eric Paris <eparis@redhat.com>
Cc: Dave Hansen <dave@linux.vnet.ibm.com>
Cc: David Rientjes <rientjes@google.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
|\ \ \
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
* git://git.kernel.org/pub/scm/linux/kernel/git/cmetcalf/linux-tile: (26 commits)
arch/tile: prefer "tilepro" as the name of the 32-bit architecture
compat: include aio_abi.h for aio_context_t
arch/tile: cleanups for tilegx compat mode
arch/tile: allocate PCI IRQs later in boot
arch/tile: support signal "exception-trace" hook
arch/tile: use better definitions of xchg() and cmpxchg()
include/linux/compat.h: coding-style fixes
tile: add an RTC driver for the Tilera hypervisor
arch/tile: finish enabling support for TILE-Gx 64-bit chip
compat: fixes to allow working with tile arch
arch/tile: update defconfig file to something more useful
tile: do_hardwall_trap: do not play with task->sighand
tile: replace mm->cpu_vm_mask with mm_cpumask()
tile,mn10300: add device parameter to dma_cache_sync()
audit: support the "standard" <asm-generic/unistd.h>
arch/tile: clarify flush_buffer()/finv_buffer() function names
arch/tile: kernel-related cleanups from removing static page size
arch/tile: various header improvements for building drivers
arch/tile: disable GX prefetcher during cache flush
arch/tile: tolerate disabling CONFIG_BLK_DEV_INITRD
...
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Many of the syscalls mentioned in the audit code are not present
for architectures that implement only the "standard" set of
Linux syscalls (e.g. openat, but not open, etc.). This change
adds proper #ifdefs for all those syscalls.
Acked-by: Arnd Bergmann <arnd@arndb.de>
Signed-off-by: Chris Metcalf <cmetcalf@tilera.com>
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Most arches define CONFIG_DEBUG_STACK_USAGE exactly the same way. Move it
to lib/Kconfig.debug so each arch doesn't have to define it. This
obviously makes the option generic, but that's fine because the config is
already used in generic code.
It's not obvious to me that sysrq-P actually does anything caution by
keeping the most inclusive wording.
Signed-off-by: Stephen Boyd <sboyd@codeaurora.org>
Cc: Chris Metcalf <cmetcalf@tilera.com>
Acked-by: David S. Miller <davem@davemloft.net>
Acked-by: Richard Weinberger <richard@nod.at>
Acked-by: Mike Frysinger <vapier@gentoo.org>
Cc: Russell King <rmk@arm.linux.org.uk>
Cc: Hirokazu Takata <takata@linux-m32r.org>
Acked-by: Ralf Baechle <ralf@linux-mips.org>
Cc: Paul Mackerras <paulus@samba.org>
Acked-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
Cc: Chen Liqin <liqin.chen@sunplusct.com>
Cc: Lennox Wu <lennox.wu@gmail.com>
Cc: Ingo Molnar <mingo@elte.hu>
Cc: Thomas Gleixner <tglx@linutronix.de>
Cc: "H. Peter Anvin" <hpa@zytor.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
So we can specify the virtual address as the base of the pool chunk and
then get physical addresses for hardware IP.
For example on at91 we will use this on spi, uart or macb
Signed-off-by: Jean-Christophe PLAGNIOL-VILLARD <plagnioj@jcrosoft.com>
Cc: Nicolas Ferre <nicolas.ferre@atmel.com>
Cc: Patrice VILCHEZ <patrice.vilchez@atmel.com>
Cc: Jes Sorensen <jes@wildopensource.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
DEBUG_PER_CPU_MAPS is used in lib/cpumask.c as well as in
inlcude/linux/cpumask.h and thus it has outgrown its use within x86 and
powerpc alone. Any arch with SMP support may want to get some more
debugging, so make this option generic.
Signed-off-by: Stephen Boyd <sboyd@codeaurora.org>
Cc: <linux-arch@vger.kernel.org>
Cc: Ingo Molnar <mingo@elte.hu>
Cc: Thomas Gleixner <tglx@linutronix.de>
Cc: "H. Peter Anvin" <hpa@zytor.com>
Acked-by: Benjamin Herrenschmidt <benh@kernel.crashing.org>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
There is quite a lot of code which does copy_from_user() + strict_strto*()
or simple_strto*() combo in slightly different ways.
Before doing conversions all over tree, let's get final API correct.
Enter kstrtoull_from_user() and friends.
Typical code which uses them looks very simple:
TYPE val;
int rv;
rv = kstrtoTYPE_from_user(buf, count, 0, &val);
if (rv < 0)
return rv;
[use val]
return count;
There is a tiny semantic difference from the plain kstrto*() API -- the
latter allows any amount of leading zeroes, while the former copies data
into buffer on stack and thus allows leading zeroes as long as it fits
into buffer.
This shouldn't be a problem for typical usecase "echo 42 > /proc/x".
The point is to make reading one integer from userspace _very_ simple and
very bug free.
Signed-off-by: Alexey Dobriyan <adobriyan@gmail.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
This has no actual effect, since sizeof(struct hlist_head) ==
sizeof(struct hlist_head *), but it's still the wrong type to use.
The semantic match that finds this problem:
// <smpl>
@@
type T;
identifier x;
@@
T *x;
...
* x = kzalloc(... * sizeof(T*) * ..., ...);
// </smpl>
[akpm@linux-foundation.org: use kcalloc()]
Signed-off-by: Ilia Mirkin <imirkin@alum.mit.edu>
Acked-by: Lars Ellenberg <lars@linbit.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Otherwise, the warning at the top of vsnprintf() gets triggered by
kvasprintf()'s first invocation (with NULL buffer and zero size) of
vsnprintf().
Signed-off-by: Jan Beulich <jbeulich@novell.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Manually adjusting the smp_affinity for IRQ's becomes unwieldy when the
cpu count is large.
Setting smp affinity to cpus 256 to 263 would be:
echo 000000ff,00000000,00000000,00000000,00000000,00000000,00000000,00000000 > smp_affinity
instead of:
echo 256-263 > smp_affinity_list
Think about what it looks like for cpus around say, 4088 to 4095.
We already have many alternate "list" interfaces:
/sys/devices/system/cpu/cpuX/indexY/shared_cpu_list
/sys/devices/system/cpu/cpuX/topology/thread_siblings_list
/sys/devices/system/cpu/cpuX/topology/core_siblings_list
/sys/devices/system/node/nodeX/cpulist
/sys/devices/pci***/***/local_cpulist
Add a companion interface, smp_affinity_list to use cpu lists instead of
cpu maps. This conforms to other companion interfaces where both a map
and a list interface exists.
This required adding a bitmap_parselist_user() function in a manner
similar to the bitmap_parse_user() function.
[akpm@linux-foundation.org: make __bitmap_parselist() static]
Signed-off-by: Mike Travis <travis@sgi.com>
Cc: Thomas Gleixner <tglx@linutronix.de>
Cc: Jack Steiner <steiner@sgi.com>
Cc: Lee Schermerhorn <lee.schermerhorn@hp.com>
Cc: Andy Shevchenko <andy.shevchenko@gmail.com>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | |
| | | | |
Architectures that implement their own show_mem() function did not pass
the filter argument to show_free_areas() to appropriately avoid emitting
the state of nodes that are disallowed in the current context. This patch
now passes the filter argument to show_free_areas() so those nodes are now
avoided.
This patch also removes the show_free_areas() wrapper around
__show_free_areas() and converts existing callers to pass an empty filter.
ia64 emits additional information for each node, so skip_free_areas_zone()
must be made global to filter disallowed nodes and it is converted to use
a nid argument rather than a zone for this use case.
Signed-off-by: David Rientjes <rientjes@google.com>
Cc: Russell King <linux@arm.linux.org.uk>
Cc: Tony Luck <tony.luck@intel.com>
Cc: Fenghua Yu <fenghua.yu@intel.com>
Cc: Kyle McMartin <kyle@mcmartin.ca>
Cc: Helge Deller <deller@gmx.de>
Cc: James Bottomley <jejb@parisc-linux.org>
Cc: "David S. Miller" <davem@davemloft.net>
Cc: Guan Xuetao <gxt@mprc.pku.edu.cn>
Signed-off-by: Andrew Morton <akpm@linux-foundation.org>
Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
|
|\ \ \ \
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
for-linus
Conflicts:
lib/flex_array.c
security/selinux/avc.c
security/selinux/hooks.c
security/selinux/ss/policydb.c
security/smack/smack_lsm.c
Manually resolve conflicts.
Signed-off-by: James Morris <jmorris@namei.org>
|
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
flex_arrays are supposed to be a replacement for:
kmalloc(num_elements * sizeof(element))
If kmalloc is given 0 num_elements or a 0 size element it will happily return
ZERO_SIZE_PTR. Which looks like a valid allocation, but which will explode if
something actually try to use it. The current flex_array code will return an
equivalent result if num_elements is 0, but will fail to work if
sizeof(element) is 0. This patch allows allocation to work even for 0 size
elements. It will cause flex_arrays to explode though if they are used.
Imitating the kmalloc behavior.
Based-on-patch-by: Steffen Klassert <steffen.klassert@secunet.com>
Signed-off-by: Eric Paris <eparis@redhat.com>
Acked-by: Dave Hansen <dave@linux.vnet.ibm.com>
|
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
Just like kmalloc will allow one to allocate a 0 length segment of memory
flex arrays should do the same thing. It should bomb if you try to use
something, but it should at least allow the allocation.
This is needed because when SELinux switched to using flex_arrays in 2.6.38
the inability to allocate a 0 length array resulted in SELinux policy load
returning -ENOSPC when previously it worked.
Based-on-patch-by: Steffen Klassert <steffen.klassert@secunet.com>
Signed-off-by: Eric Paris <eparis@redhat.com>
Tested-by: Chris Richards <gizmo@giz-works.com>
Cc: stable@kernel.org [2.6.38+]
|
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | |
| | | | | |
Change flex_array_prealloc to take the number of elements for which space
should be allocated instead of the last (inclusive) element. Users
and documentation are updated accordingly. flex_arrays got introduced before
they had users. When folks started using it, they ended up needing a
different API than was coded up originally. This swaps over to the API that
folks apparently need.
Based-on-patch-by: Steffen Klassert <steffen.klassert@secunet.com>
Signed-off-by: Eric Paris <eparis@redhat.com>
Tested-by: Chris Richards <gizmo@giz-works.com>
Acked-by: Dave Hansen <dave@linux.vnet.ibm.com>
Cc: stable@kernel.org [2.6.38+]
|
|\ \ \ \ \
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | | |
git://git.kernel.org/pub/scm/linux/kernel/git/jikos/trivial
* 'for-linus' of git://git.kernel.org/pub/scm/linux/kernel/git/jikos/trivial: (39 commits)
b43: fix comment typo reqest -> request
Haavard Skinnemoen has left Atmel
cris: typo in mach-fs Makefile
Kconfig: fix copy/paste-ism for dell-wmi-aio driver
doc: timers-howto: fix a typo ("unsgined")
perf: Only include annotate.h once in tools/perf/util/ui/browsers/annotate.c
md, raid5: Fix spelling error in comment ('Ofcourse' --> 'Of course').
treewide: fix a few typos in comments
regulator: change debug statement be consistent with the style of the rest
Revert "arm: mach-u300/gpio: Fix mem_region resource size miscalculations"
audit: acquire creds selectively to reduce atomic op overhead
rtlwifi: don't touch with treewide double semicolon removal
treewide: cleanup continuations and remove logging message whitespace
ath9k_hw: don't touch with treewide double semicolon removal
include/linux/leds-regulator.h: fix syntax in example code
tty: fix typo in descripton of tty_termios_encode_baud_rate
xtensa: remove obsolete BKL kernel option from defconfig
m68k: fix comment typo 'occcured'
arch:Kconfig.locks Remove unused config option.
treewide: remove extra semicolons
...
|
| |\ \ \ \ \
| | | |/ / /
| | |/| | |
| | | | | |
| | | | | | |
Fast-forwarded to current state of Linus' tree as there are patches to be
applied for files that didn't exist on the old branch.
|
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | |
| | | | | | |
Cite Documentation/kernel-parameters.txt for an alternative to
building with PRINTK_TIME compiled in.
Signed-off-by: Jim Cromie <jim.cromie@gmail.com>
Signed-off-by: Jiri Kosina <jkosina@suse.cz>
|