aboutsummaryrefslogtreecommitdiffstats
Commit message (Collapse)AuthorAgeFilesLines
* include cleanup: Update gfp.h and slab.h includes to prepare for breaking ↵Tejun Heo2010-03-301-0/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | implicit slab.h inclusion from percpu.h percpu.h is included by sched.h and module.h and thus ends up being included when building most .c files. percpu.h includes slab.h which in turn includes gfp.h making everything defined by the two files universally available and complicating inclusion dependencies. percpu.h -> slab.h dependency is about to be removed. Prepare for this change by updating users of gfp and slab facilities include those headers directly instead of assuming availability. As this conversion needs to touch large number of source files, the following script is used as the basis of conversion. http://userweb.kernel.org/~tj/misc/slabh-sweep.py The script does the followings. * Scan files for gfp and slab usages and update includes such that only the necessary includes are there. ie. if only gfp is used, gfp.h, if slab is used, slab.h. * When the script inserts a new include, it looks at the include blocks and try to put the new include such that its order conforms to its surrounding. It's put in the include block which contains core kernel includes, in the same order that the rest are ordered - alphabetical, Christmas tree, rev-Xmas-tree or at the end if there doesn't seem to be any matching order. * If the script can't find a place to put a new include (mostly because the file doesn't have fitting include block), it prints out an error message indicating which .h file needs to be added to the file. The conversion was done in the following steps. 1. The initial automatic conversion of all .c files updated slightly over 4000 files, deleting around 700 includes and adding ~480 gfp.h and ~3000 slab.h inclusions. The script emitted errors for ~400 files. 2. Each error was manually checked. Some didn't need the inclusion, some needed manual addition while adding it to implementation .h or embedding .c file was more appropriate for others. This step added inclusions to around 150 files. 3. The script was run again and the output was compared to the edits from #2 to make sure no file was left behind. 4. Several build tests were done and a couple of problems were fixed. e.g. lib/decompress_*.c used malloc/free() wrappers around slab APIs requiring slab.h to be added manually. 5. The script was run on all .h files but without automatically editing them as sprinkling gfp.h and slab.h inclusions around .h files could easily lead to inclusion dependency hell. Most gfp.h inclusion directives were ignored as stuff from gfp.h was usually wildly available and often used in preprocessor macros. Each slab.h inclusion directive was examined and added manually as necessary. 6. percpu.h was updated not to include slab.h. 7. Build test were done on the following configurations and failures were fixed. CONFIG_GCOV_KERNEL was turned off for all tests (as my distributed build env didn't work with gcov compiles) and a few more options had to be turned off depending on archs to make things build (like ipr on powerpc/64 which failed due to missing writeq). * x86 and x86_64 UP and SMP allmodconfig and a custom test config. * powerpc and powerpc64 SMP allmodconfig * sparc and sparc64 SMP allmodconfig * ia64 SMP allmodconfig * s390 SMP allmodconfig * alpha SMP allmodconfig * um on x86_64 SMP allmodconfig 8. percpu.h modifications were reverted so that it could be applied as a separate patch and serve as bisection point. Given the fact that I had only a couple of failures from tests on step 6, I'm fairly confident about the coverage of this conversion patch. If there is a breakage, it's likely to be something in one of the arch headers which should be easily discoverable easily on most builds of the specific arch. Signed-off-by: Tejun Heo <tj@kernel.org> Guess-its-ok-by: Christoph Lameter <cl@linux-foundation.org> Cc: Ingo Molnar <mingo@redhat.com> Cc: Lee Schermerhorn <Lee.Schermerhorn@hp.com>
* Driver core: Constify struct sysfs_ops in struct kobj_typeEmese Revfy2010-03-071-1/+1
| | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | | Constify struct sysfs_ops. This is part of the ops structure constification effort started by Arjan van de Ven et al. Benefits of this constification: * prevents modification of data that is shared (referenced) by many other structure instances at runtime * detects/prevents accidental (but not intentional) modification attempts on archs that enforce read-only kernel data at runtime * potentially better optimized code as the compiler can assume that the const data cannot be changed * the compiler/linker move const data into .rodata and therefore exclude them from false sharing Signed-off-by: Emese Revfy <re.emese@gmail.com> Acked-by: David Teigland <teigland@redhat.com> Acked-by: Matt Domsch <Matt_Domsch@dell.com> Acked-by: Maciej Sosnowski <maciej.sosnowski@intel.com> Acked-by: Hans J. Koch <hjk@linutronix.de> Acked-by: Pekka Enberg <penberg@cs.helsinki.fi> Acked-by: Jens Axboe <jens.axboe@oracle.com> Acked-by: Stephen Hemminger <shemminger@vyatta.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* kset-example: Spelling fixes.Radu Voicilas2010-03-071-2/+2
| | | | | | | | No change in functionality. Signed-off-by: Radu Voicilas <rvoicilas@gmail.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* kobject-example: Spelling fixes.Radu Voicilas2010-03-071-2/+2
| | | | | | | | No change in functionality. Signed-off-by: Radu Voicilas <rvoicilas@gmail.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* samples: mark {static|__init|__exit} for {init|exit} functionsQinghuang Feng2009-01-062-4/+4
| | | | | | | | | | | | None of these (init|exit) functions is called from other functions which is outside the kernel module mechanism or kernel itself, so mark them as {static|__init|__exit}. Signed-off-by: Qinghuang Feng <qhfeng.kernel@gmail.com> Cc: Mathieu Desnoyers <mathieu.desnoyers@polymtl.ca> Acked-by: Greg Kroah-Hartman <gregkh@suse.de> Signed-off-by: Andrew Morton <akpm@linux-foundation.org> Signed-off-by: Linus Torvalds <torvalds@linux-foundation.org>
* kobject: should use kobject_put() in kset-exampleLi Zefan2008-07-211-1/+1
| | | | | | | | | We should call kobject_put() instead of kfree() if kobject_init_and_add() returns an error, shouldn't we? Don't set up a bad example ;) Signed-off-by: Li Zefan <lizf@cn.fujitsu.com> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* kobject: add sample code for how to use ksets/ktypes/kobjectsGreg Kroah-Hartman2008-01-242-1/+279
| | | | | | | | | This is a more complex example showing how to create a kset and a ktype and some default attributes for a group of kobjects. Cc: Kay Sievers <kay.sievers@vrfy.org> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>
* kobject: add sample code for how to use kobjects in a simple manner.Greg Kroah-Hartman2008-01-242-0/+138
This is a simple kobject module, showing how to use kobj_attributes in basic and more complex ways. Cc: Kay Sievers <kay.sievers@vrfy.org> Signed-off-by: Greg Kroah-Hartman <gregkh@suse.de>