From 28bb22379513ca3cac9d13766064a219c5fc21a9 Mon Sep 17 00:00:00 2001 From: Yinghai Lu Date: Mon, 30 Jun 2008 16:20:54 -0700 Subject: x86: move reserve_setup_data to setup.c Ying Huang would like setup_data to be reserved, but not included in the no save range. Here we try to modify the e820 table to reserve that range early. also add that in early_res in case bootloader messes up with the ramdisk. other solution would be 1. add early_res_to_highmem... 2. early_res_to_e820... but they could reserve another type memory wrongly, if early_res has some resource reserved early, and not needed later, but it is not removed from early_res in time. Like the RAMDISK (already handled). Signed-off-by: Yinghai Lu Cc: andi@firstfloor.org Tested-by: Huang, Ying Signed-off-by: Ingo Molnar --- arch/x86/kernel/head.c | 18 ------------------ 1 file changed, 18 deletions(-) (limited to 'arch/x86/kernel/head.c') diff --git a/arch/x86/kernel/head.c b/arch/x86/kernel/head.c index a6816be01cd..3e66bd364a9 100644 --- a/arch/x86/kernel/head.c +++ b/arch/x86/kernel/head.c @@ -53,21 +53,3 @@ void __init reserve_ebda_region(void) /* reserve all memory between lowmem and the 1MB mark */ reserve_early_overlap_ok(lowmem, 0x100000, "BIOS reserved"); } - -void __init reserve_setup_data(void) -{ - struct setup_data *data; - u64 pa_data; - char buf[32]; - - if (boot_params.hdr.version < 0x0209) - return; - pa_data = boot_params.hdr.setup_data; - while (pa_data) { - data = early_ioremap(pa_data, sizeof(*data)); - sprintf(buf, "setup data %x", data->type); - reserve_early(pa_data, pa_data+sizeof(*data)+data->len, buf); - pa_data = data->next; - early_iounmap(data, sizeof(*data)); - } -} -- cgit v1.2.3-54-g00ecf