#ifndef _ASM_X86_IPI_H #define _ASM_X86_IPI_H #ifdef CONFIG_X86_LOCAL_APIC /* * Copyright 2004 James Cleverdon, IBM. * Subject to the GNU Public License, v.2 * * Generic APIC InterProcessor Interrupt code. * * Moved to include file by James Cleverdon from * arch/x86-64/kernel/smp.c * * Copyrights from kernel/smp.c: * * (c) 1995 Alan Cox, Building #3 * (c) 1998-99, 2000 Ingo Molnar * (c) 2002,2003 Andi Kleen, SuSE Labs. * Subject to the GNU Public License, v.2 */ #include #include #include /* * the following functions deal with sending IPIs between CPUs. * * We use 'broadcast', CPU->CPU IPIs and self-IPIs too. */ static inline unsigned int __prepare_ICR(unsigned int shortcut, int vector, unsigned int dest) { unsigned int icr = shortcut | dest; switch (vector) { default: icr |= APIC_DM_FIXED | vector; break; case NMI_VECTOR: icr |= APIC_DM_NMI; break; } return icr; } static inline int __prepare_ICR2(unsigned int mask) { return SET_APIC_DEST_FIELD(mask); } static inline void __xapic_wait_icr_idle(void) { while (native_apic_mem_read(APIC_ICR) & APIC_ICR_BUSY) cpu_relax(); } static inline void __default_send_IPI_shortcut(unsigned int shortcut, int vector, unsigned int dest) { /* * Subtle. In the case of the 'never do double writes' workaround * we have to lock out interrupts to be safe. As we don't care * of the value read we use an atomic rmw access to avoid costly * cli/sti. Otherwise we use an even cheaper single atomic write * to the APIC. */ unsigned int cfg; /* * Wait for idle. */ __xapic_wait_icr_idle(); /* * No need to touch the target chip field */ cfg = __prepare_ICR(shortcut, vector, dest); /* * Send the IPI. The write to APIC_ICR fires this off. */ native_apic_mem_write(APIC_ICR, cfg); } /* * This is used to send an IPI with no shorthand notation (the destination is * specified in bits 56 to 63 of the ICR). */ static inline void __default_send_IPI_dest_field(unsigned int mask, int vector, unsigned int dest) { unsigned long cfg; /* * Wait for idle. */ if (unlikely(vector == NMI_VECTOR)) safe_apic_wait_icr_idle(); else __xapic_wait_icr_idle(); /* * prepare target chip field */ cfg = __prepare_ICR2(mask); native_apic_mem_write(APIC_ICR2, cfg); /* * program the ICR */ cfg = __prepare_ICR(0, vector, dest); /* * Send the IPI. The write to APIC_ICR fires this off. */ native_apic_mem_write(APIC_ICR, cfg); } extern void default_send_IPI_mask_sequence_phys(const struct cpumask *mask, int vector); extern void default_send_IPI_mask_allbutself_phys(const struct cpumask *mask, int vector); /* Avoid include hell */ #define NMI_VECTOR 0x02 extern int no_broadcast; static inline void __default_local_send_IPI_allbutself(int vector) { if (no_broadcast || vector == NMI_VECTOR) apic->send_IPI_mask_allbutself(cpu_online_mask, vector); else __default_send_IPI_shortcut(APIC_DEST_ALLBUT, vector, apic->dest_logical); } static inline void __default_local_send_IPI_all(int vector) { if (no_broadcast || vector == NMI_VECTOR) apic->send_IPI_mask(cpu_online_mask, vector); else __default_send_IPI_shortcut(APIC_DEST_ALLINC, vector, apic->dest_logical); } #ifdef CONFIG_X86_32 extern void default_send_IPI_mask_sequence_logical(const struct cpumask *mask, int vector); extern void default_send_IPI_mask_allbutself_logical(const struct cpumask *mask, int vector); extern void default_send_IPI_mask_logical(const struct cpumask *mask, int vector); extern void default_send_IPI_allbutself(int vector); extern void default_send_IPI_all(int vector); extern void default_send_IPI_self(int vector); #endif #endif #endif /* _ASM_X86_IPI_H */