/* * Functions related to tagged command queuing */ #include #include #include #include #include "blk.h" /** * blk_queue_find_tag - find a request by its tag and queue * @q: The request queue for the device * @tag: The tag of the request * * Notes: * Should be used when a device returns a tag and you want to match * it with a request. * * no locks need be held. **/ struct request *blk_queue_find_tag(struct request_queue *q, int tag) { return blk_map_queue_find_tag(q->queue_tags, tag); } EXPORT_SYMBOL(blk_queue_find_tag); /** * __blk_free_tags - release a given set of tag maintenance info * @bqt: the tag map to free * * Tries to free the specified @bqt. Returns true if it was * actually freed and false if there are still references using it */ static int __blk_free_tags(struct blk_queue_tag *bqt) { int retval; retval = atomic_dec_and_test(&bqt->refcnt); if (retval) { BUG_ON(find_first_bit(bqt->tag_map, bqt->max_depth) < bqt->max_depth); kfree(bqt->tag_index); bqt->tag_index = NULL; kfree(bqt->tag_map); bqt->tag_map = NULL; kfree(bqt); } return retval; } /** * __blk_queue_free_tags - release tag maintenance info * @q: the request queue for the device * * Notes: * blk_cleanup_queue() will take care of calling this function, if tagging * has been used. So there's no need to call this directly. **/ void __blk_queue_free_tags(struct request_queue *q) { struct blk_queue_tag *bqt = q->queue_tags; if (!bqt) return; __blk_free_tags(bqt); q->queue_tags = NULL; queue_flag_clear_unlocked(QUEUE_FLAG_QUEUED, q); } /** * blk_free_tags - release a given set of tag maintenance info * @bqt: the tag map to free * * For externally managed @bqt frees the map. Callers of this * function must guarantee to have released all the queues that * might have been using this tag map. */ void blk_free_tags(struct blk_queue_tag *bqt) { if (unlikely(!__blk_free_tags(bqt))) BUG(); } EXPORT_SYMBOL(blk_free_tags); /** * blk_queue_free_tags - release tag maintenance info * @q: the request queue for the device * * Notes: * This is used to disable tagged queuing to a device, yet leave * queue in function. **/ void blk_queue_free_tags(struct request_queue *q) { queue_flag_clear_unlocked(QUEUE_FLAG_QUEUED, q); } EXPORT_SYMBOL(blk_queue_free_tags); static int init_tag_map(struct request_queue *q, struct blk_queue_tag *tags, int depth) { struct request **tag_index; unsigned long *tag_map; int nr_ulongs; if (q && depth > q->nr_requests * 2) { depth = q->nr_requests * 2; printk(KERN_ERR "%s: adjusted depth to %d\n", __func__, depth); } tag_index = kzalloc(depth * sizeof(struct request *), GFP_ATOMIC); if (!tag_index) goto fail; nr_ulongs = ALIGN(depth, BITS_PER_LONG) / BITS_PER_LONG; tag_map = kzalloc(nr_ulongs * sizeof(unsigned long), GFP_ATOMIC); if (!tag_map) goto fail; tags->real_max_depth = depth; tags->max_depth = depth; tags->tag_index = tag_index; tags->tag_map = tag_map; return 0; fail: kfree(tag_index); return -ENOMEM; } static struct blk_queue_tag *__blk_queue_init_tags(struct request_queue *q, int depth) { struct blk_queue_tag *tags; tags = kmalloc(sizeof(struct blk_queue_tag), GFP_ATOMIC); if (!tags) goto fail; if (init_tag_map(q, tags, depth)) goto fail; atomic_set(&tags->refcnt, 1); return tags; fail: kfree(tags); return NULL; } /** * blk_init_tags - initialize the tag info for an external tag map * @depth: the maximum queue depth supported * @tags: the tag to use **/ struct blk_queue_tag *blk_init_tags(int depth) { return __blk_queue_init_tags(NULL, depth); } EXPORT_SYMBOL(blk_init_tags); /** * blk_queue_init_tags - initialize the queue tag info * @q: the request queue for the device * @depth: the maximum queue depth supported * @tags: the tag to use * * Queue lock must be held here if the function is called to resize an * existing map. **/ int blk_queue_init_tags(struct request_queue *q, int depth, struct blk_queue_tag *tags) { int rc; BUG_ON(tags && q->queue_tags && tags != q->queue_tags); if (!tags && !q->queue_tags) { tags = __blk_queue_init_tags(q, depth); if (!tags) goto fail; } else if (q->queue_tags) { rc = blk_queue_resize_tags(q, depth); if (rc) return rc; queue_flag_set(QUEUE_FLAG_QUEUED, q); return 0; } else atomic_inc(&tags->refcnt); /* * assign it, all done */ q->queue_tags = tags; queue_flag_set_unlocked(QUEUE_FLAG_QUEUED, q); INIT_LIST_HEAD(&q->tag_busy_list); return 0; fail: kfree(tags); return -ENOMEM; } EXPORT_SYMBOL(blk_queue_init_tags); /** * blk_queue_resize_tags - change the queueing depth * @q: the request queue for the device * @new_depth: the new max command queueing depth * * Notes: * Must be called with the queue lock held. **/ int blk_queue_resize_tags(struct request_queue *q, int new_depth) { struct blk_queue_tag *bqt = q->queue_tags; struct request **tag_index; unsigned long *tag_map; int max_depth, nr_ulongs; if (!bqt) return -ENXIO; /* * if we already have large enough real_max_depth. just * adjust max_depth. *NOTE* as requests with tag value * between new_depth and real_max_depth can be in-flight, tag * map can not be shrunk blindly here. */ if (new_depth <= bqt->real_max_depth) { bqt->max_depth = new_depth; return 0; } /* * Currently cannot replace a shared tag map with a new * one, so error out if this is the case */ if (atomic_read(&bqt->refcnt) != 1) return -EBUSY; /* * save the old state info, so we can copy it back */ tag_index = bqt->tag_index; tag_map = bqt->tag_map; max_depth = bqt->real_max_depth; if (init_tag_map(q, bqt, new_depth)) return -ENOMEM; memcpy(bqt->tag_index, tag_index, max_depth * sizeof(struct request *)); nr_ulongs = ALIGN(max_depth, BITS_PER_LONG) / BITS_PER_LONG; memcpy(bqt->tag_map, tag_map, nr_ulongs * sizeof(unsigned long)); kfree(tag_index); kfree(tag_map); return 0; } EXPORT_SYMBOL(blk_queue_resize_tags); /** * blk_queue_end_tag - end tag operations for a request * @q: the request queue for the device * @rq: the request that has completed * * Description: * Typically called when end_that_request_first() returns %0, meaning * all transfers have been done for a request. It's important to call * this function before end_that_request_last(), as that will put the * request back on the free list thus corrupting the internal tag list. * * Notes: * queue lock must be held. **/ void blk_queue_end_tag(struct request_queue *q, struct request *rq) { struct blk_queue_tag *bqt = q->queue_tags; int tag = rq->tag; BUG_ON(tag == -1); if (unlikely(tag >= bqt->real_max_depth)) /* * This can happen after tag depth has been reduced. * FIXME: how about a warning or info message here? */ return; list_del_init(&rq->queuelist); rq->cmd_flags &= ~REQ_QUEUED; rq->tag = -1; if (unlikely(bqt->tag_index[tag] == NULL)) printk(KERN_ERR "%s: tag %d is missing\n", __func__, tag); bqt->tag_index[tag] = NULL; if (unlikely(!test_bit(tag, bqt->tag_map))) { printk(KERN_ERR "%s: attempt to clear non-busy tag (%d)\n", __func__, tag); return; } /* * The tag_map bit acts as a lock for tag_index[bit], so we need * unlock memory barrier semantics. */ clear_bit_unlock(tag, bqt->tag_map); } EXPORT_SYMBOL(blk_queue_end_tag); /** * blk_queue_start_tag - find a free tag and assign it * @q: the request queue for the device * @rq: the block request that needs tagging * * Description: * This can either be used as a stand-alone helper, or possibly be * assigned as the queue &prep_rq_fn (in which case &struct request * automagically gets a tag assigned). Note that this function * assumes that any type of request can be queued! if this is not * true for your device, you must check the request type before * calling this function. The request will also be removed from * the request queue, so it's the drivers responsibility to readd * it if it should need to be restarted for some reason. * * Notes: * queue lock must be held. **/ int blk_queue_start_tag(struct request_queue *q, struct request *rq) { struct blk_queue_tag *bqt = q->queue_tags; unsigned max_depth, offset; int tag; if (unlikely((rq->cmd_flags & REQ_QUEUED))) { printk(KERN_ERR "%s: request %p for device [%s] already tagged %d", __func__, rq, rq->rq_disk ? rq->rq_disk->disk_name : "?", rq->tag); BUG(); } /* * Protect against shared tag maps, as we may not have exclusive * access to the tag map. * * We reserve a few tags just for sync IO, since we don't want * to starve sync IO on behalf of flooding async IO. */ max_depth = bqt->max_depth; if (rq_is_sync(rq)) offset = 0; else offset = max_depth >> 2; do { tag = find_next_zero_bit(bqt->tag_map, max_depth, offset); if (tag >= max_depth) return 1; } while (test_and_set_bit_lock(tag, bqt->tag_map)); /* * We need lock ordering semantics given by test_and_set_bit_lock. * See blk_queue_end_tag for details. */ rq->cmd_flags |= REQ_QUEUED; rq->tag = tag; bqt->tag_index[tag] = rq; blkdev_dequeue_request(rq); list_add(&rq->queuelist, &q->tag_busy_list); return 0; } EXPORT_SYMBOL(blk_queue_start_tag); /** * blk_queue_invalidate_tags - invalidate all pending tags * @q: the request queue for the device * * Description: * Hardware conditions may dictate a need to stop all pending requests. * In this case, we will safely clear the block side of the tag queue and * readd all requests to the request queue in the right order. * * Notes: * queue lock must be held. **/ void blk_queue_invalidate_tags(struct request_queue *q) { struct list_head *tmp, *n; list_for_each_safe(tmp, n, &q->tag_busy_list) blk_requeue_request(q, list_entry_rq(tmp)); } EXPORT_SYMBOL(blk_queue_invalidate_tags);